powered by CADENAS

Manual

Manual

8.6. Controlling PARTeditor externally - DDE commands

The table below lists the DDE commands with which PARTeditor can be activated externally. The server name and topic name must be PARTeditorfor all commands.

Poke translations :

Data can be transferred to PARTeditor with a Poke command. The Parameterof a Poke command for controlling PARTeditor is always a String .

COMMAND

ACTION

LoadTable

Opens a characteristic attribute file

This command loads a characteristic attribute file.

Parameter: file path

Example: c:/temp/test.tab

SaveTable

Saves a characteristic attribute file

This command allows the current characteristic attribute file to be saved.

Parameter: File path

Example: c:/temp/test.tab

Close

Closes the PARTeditor

ClearErrorMsg

Clear error message buffer

Error messages are not output in Hidden mode but are written to a buffer. The messages can be fetched from this buffer with the Request command GetErrorMsg.

StartEditTab

Starts editing table

This command must be invoked if the table is to be edited by DDE. The command must be invoked after LoadTable.

EndEditTab

Ends editing table

This command must be invoked when editing of the table is complete. The command must be invoked before SaveTable.

SetTabValue

Changes a value in the table

The command is used to change a value in the table.

Parameters: Column, Row, Value

Example: 0,5, "New value"

GetTabValue

Polls a value from the table

The command is used to poll a value of the table. The value can be fetched with the Request command in GetResult.

Parameters: Column, Row

Example: 0,5

AddTabCol

Adds a table variable

Parameters: Name, Designation, Data type

1st example: "IDNO","Ident number","A10"

--> Generates the text variable IDNO with a maximum text length of 10 characters.

2nd example: "L","Length","F5.3"

--> Generates numeric variable L with 5 places in front of the decimal point and 3 places after the decimal point.

GetTabColName

Determines variable name

Determines the name of the table variable. The name can be fetched with the Request command GetResult.

Parameter: Column number

Example: 0

FindTabCol

Determines column

Determines the column number for a variable name.

The result can be fetched with the Request command GetResult.

Parameter: Variable name

Example: IDNR

CountTabCols

Determines number of columns

The result can be fetched with the Request command GetResult.

CountTabRows

Determines number of rows

The result can be fetched with the Request command GetResult.

Request transactions

Request transactions allow values or status information to be polled from PARTeditor. All Request transactions return strings.

COMMAND

ACTION

GetResult

Fetches result of a Poke command

Certain Poke commands produce results. Command GetResult allows these results to be determined.

GetErrorMsg

Fetches error messages

If PARTeditor launched in Hidden mode (Invoked with parameter hidden), it does not issue error messages. These error messages can be polled instead with GetErrorMsg.