powered by CADENAS

Manual

Manual

7.6.4.11.  Construction sketch

[Note] Note

Construction sketches are not exported.

In order to mark a construction sketch as such, in the context menu, click on the option Construction sketch. In order to disable, click again.

In the 3D History, construction sketches are marked with a 'H' on the sketch symbol .

[Note] Note

Sketches already extruded or rotated, do not show the command.

Faulty sketches are automatically marked as construction sketch. Should the option Construction sketch become disabled the error symbol is displayed.

Faulty sketch which is marked as construction sketch

Faulty sketch which is marked as construction sketch