powered by CADENAS

Manual

Manual

3.2.19.  Release Notes

[Note] Note

Before publishing the setting of Release Notes is mandatory.

In order to set new release notes, proceed as described below. At the latest before publishing anew the Release Notes have to be set (see Section 6.10, “ Publish catalog ”).

  1. On the left, in the index tree, select the desired catalog folder.

    -> Now on the right, the tab Release Notes is displayed.

  2. Click on the tab.

    -> The respective dialog area is opened.

    If entries already exist, all these are displayed.

  3. Click on the button Add entry.

    -> A new dialog area is opened.

    1. The current Date is set. However, you can change it anytime.

    2. In the list field, select the adequate type:

      • Product Update: New, changed, deleted products (projects, project lines)

      • Translation: e.g. individual translations or a whole catalog language

      • System Update: Updates due to software changes (main versions, but also service packs)

      • Classification: Classification updates or classifications assigned to projects (classified according to eClass, for example)

      • Assistants:

      • Miscellaneous: Everything which does not fit one of the other categories, like data changes under Edit project - > tabbed page Documents.

    3. Enter the new text.

In order to edit or delete entries, put the cursor into the desired field.

Then click on to edit or on to delete.

More details can be found under Section 5.9.21, “Tabbed page Release Notes ”.