powered by CADENAS

Manual

Manual

5.8.2.1.9.  Move directory

Move directory "cuts" a directory/folder from its position in the tree. The directory or the folder can be "pasted" at a different position in the tree via Insert directory.

  1. Mark the directory or folder.

  2. Click on the command Move directory.

  3. Mark the destination directory and click on the Insert directory command.

    -> The dialog box Move directory is opened.

    You can see source and target directory. [22]

  4. Confirm with OK.



[22] If one assumes that through moving the directory, all other directories (assemblies, whose properties refer to this directory) are affected, set a checkmark at Adapt links in assemblies and enter the Assemblies path (Browse ...). See Section 5.8.2.1.7, “ Rename directory ”.