powered by CADENAS

Manual

Manual

9.9.1. Insert required parts for configuration

  1. Under training/subassembly/finished, beside the original configuration traeger_schelle_asmcfg.prj, create your own new one for testing.

    For this, under finished, click on the context menu command New project.

    Call: New project

    Call: New project

    -> The respective dialog box is opened.

    New project "traeger_schelle_test"

    New project "traeger_schelle_test"

  2. Click on Open with PARTdataManager.

    Open with PARTdataManager

    Open with PARTdataManager

    -> An empty configuration is opened.

  3. Click on Add Part.

    -> An Explorer window is opened.

  4. From the directory .../partsolutions/23d-libs/training/subassembly/finished_en (or wherever you created the dummy), insert the dummy starter part[109] and in the dialog box Part properties perform respective entries.

    [Note] Note

    Description and Equation name are displayed in the docking window Configurator under Parts.

    The Equation name is not changeable later!

  5. From the directory .../partsolutions/23d-libs/training/subassembly/profile, enter the file din_1025_s.prj (single part "T-beam") and in the dialog box Part properties perform respective entries.

  6. From the directory .../partsolutions/23d-libs/training/subassembly/din3015 insert the file din_3015_cfg.prj (assembly "pipe clip") and in the dialog page Part properties perform respective settings.

    -> Now in the Configurator, the parts t_beam_dummy (D), din_1025_s (TB) and din_3015_cfg (PC) are displayed (depending on naming in the dialog before).

  7. In the Configurator menu, click on Save configuration.

    -> The dialog box Assembly properties is opened.

  8. Insert a Description, activate the option Append free connection points automatically and confirm with OK.

    -> The Description will be shown as assembly name in the Configurator.

    Standard number and Standard title of the assembly need to be inserted in PARTproject under Edit project -> General -> General.

    "Edit project" -> tabbed page "General" -> item "General"

    "Edit project" -> tabbed page "General" -> item "General"



[109] The dummy starter part had been derived from the t-beam and in this example, it is already available.