powered by CADENAS

Manual

Manual

15.2.1. Fortran Syntax

Fortran syntax

.EQ.

eq ual (equal)

.GT.

g reater t han (greater than)

.GE.

g reater e qual (greater equal)

.LT.

l ower t han (lower than)

.LE.

l ower e qual (lower equal)

.AND.

(both conditions - right and left of .AND. - must be filled out)

.OR.

(one of the two conditions - right or left of .OR. - must be filled out)

.NE.

n ot e qual (unequal)

The following examples show key values:

  • (ERP_PDM_NUMBER.NE.'')

    The expression is true, if the respective field of the column ERP_PDM_NUMBER is not equal empty.

  • ((ERP_PDM_NUMBER.NE.'').AND.(ACTIVE_STATE.EQ.1))

    The expression is true, if the respective field of the column ERP_PDM_NUMBER is not equal empty AND the respective field of the column ACTIVE_STATE has the value 1 (=Released).

  • (PRICE.LT.0.4)

    The expression is true, if the respective field of the column PRICE has a value lower or equal than 0,4.

  • (REQUESTED_STATE.EQ.2) 

    The expression is true, if the respective field of the column REQUESTED_STATE has the value 2 (=Expired).

  • ((ACTIVE_STATE.EQ.1).AND.(LOCATION1.NE.''))

    The expression is true, if the respective field of the column ACTIVE_STATE has the value 1 (=Released) AND the respective field of the column LOCATION1 is not equal empty.

  • (CONTAINS(ERP_PDM_NUMBER,'AA').EQ..TRUE.)

    The expression is true, if the respective field of the column ERP_PDM_NUMBER contains the substring 'AA'.

  • (CONTAINS(ERP_PDM_NUMBER,'AA').EQ..FALSE.)

    The expression is true, if the respective field of the column ERP_PDM_NUMBER does NOT contain the substring 'AA'.