powered by CADENAS

Manual

Manual

5.10.2.1.  Mandatory parameters

[Note] Note

For editing the parameters, at first select the desired dimensioning.

Each dimensioning must contain the following parameters:

  • ID

    ID is only required, if a dimensioning serves as Base dimension for another dimensioning. Also see Section 5.10.2.2, “ Optional parameters ” -> Base dimension.

  • Description

    The description is automatically set and displayed in listing of dimensionings. You can adjust it as desired.

  • Type

    When creating a new dimensioning, initially HORIZONTAL is automatically set. Adjust the selection in the list field, if needed. You can change the type anytime.

    Under "Type" the following options are selectable:

    • HORIZONTAL

    • VERTICAL

    • PARALLEL

    • RADIAL

    • Angle

    • ANNOTATION

    • PART-ANNOTATION

    [Note] Note

    The parameter fields are not updated until you have clicked Save changes .

  • Views

    At the desired 2D views, where the dimensioning shall be displayed, activate the checkbox.

    Views which contain a dimensioning, can be recognized in the 3D toolbar, by a respective icon with dimensioning lines .

  • Start point and End point

    In order to select start and end point you have different options available:

    1. Select desired point via context menu in the 3D view

      1. In the list of dimensionings, select the desired one.

      2. In the 3D view click the secondary mouse key.

        -> The context menu is opened.

      3. Under Use as ... click on "Start point" or "End point".

        -> The exact point name is taken into the input field.

    2. Select desired point via list in the input field

      1. With the secondary mouse key, click into the field.

        -> A list with all available points of the object is opened.

      2. Select the desired point.

        -> The exact point name is taken into the field.

    3. Select desired point via Copy & Paste

      1. In the 3D view, click on the desired point.

        -> It is marked in red.

      2. Click into the input field of the point.

      3. Enter the point name via Ctrl+V from the clipboard into the input field.

        Example: Enter start point

        Example: Enter start point

  • Position

    You can refer to the Bounding Box or the element or use absolute values:

    • BBOX: Distance to bounding box.

      The red arrow shows the distance between dimensioning and bounding box.

      The red arrow shows the distance between dimensioning and bounding box.

    • ELEMENT Distance to the element itself to be dimensioned. Reference point is the connection point.

      The red arrow shows the distance between dimensioning and connection point.

      The red arrow shows the distance between dimensioning and connection point.

    • ABSOLUTE: Distance to the element itself to be dimensioned. Reference point is the element's origin. The specification happens via X and Y coordinate. In this way angular dimensionings can be set.

      Example for "Position" = "ABSOLUTE"

      Example for "Position" = "ABSOLUTE"

    Example:

    Offset: The value can be fixed, build by a variable or by PARTdesigner-Expressions (see Section 15.1, “PARTdesigner-Expressions ”).

    Example PARTdesigner-Expression:

    15*RZ500@D/20