powered by CADENAS

Manual

Manual

6.10.2.3. User interface: Reference of icons and functions in detail

User interface of the dialog box Edit ERP mapping

User interface at a glance

User interface at a glance

Icons in index tree

In the index tree you can see at a glance which projects have automatically been completely mapped (they do not show icons) and which projects have been automatically mapped, but still need to be verified (and possibly edited).

Bitmap

Meaning

no icon

There are changes (otherwise there would be no display at all), however, such ones do not need to be confirmed.

[Note] Note

Especially value ranges need greatest care. Here, sometimes no icon is displayed and nevertheless, the project needs a check and possibly, has to be verified. See Section 6.10.2.4.16, “Value range: Changed range”.

In following cases there is no need for verification:

Existing changes

... have to be manually confirmed and possibly edited.

Project/directory/catalog contains at least one line which could not be assigned.

The change has to be confirmed.

Possibly the correct line can be manually assigned via . See below.

Confirmed (regardless of whether assigned or removed)

Tooltips in the tree

When moving the mouse over icons tooltips are displayed.

Tooltip

Tooltip

Icons in the table

Bitmap

Meaning

no icon

There are changes (otherwise there would be no display at all), however, such ones do not need to be confirmed.

[Note] Note

Especially value ranges need greatest care. Here, sometimes no icon is displayed and nevertheless, the project needs a check and possibly, has to be verified. See Section 6.10.2.4.16, “Value range: Changed range”.

Furthermore if certain rows (characteristics) do not exist anymore (see Section 6.10.2.4.13, “Deleted/hidden table row” -> project din_28129.prj). Only when defining a fitting condition not fitting rows are correctly marked.

In following cases there is no need for verification:

There are changes (e.g. NB, value)

They have to be manually confirmed and possibly edited.

Line could not be assigned.

The change has to be confirmed.

This assignment has been confirmed by the modeler
This line is expired. This was confirmed by the editor

Tooltips in the table

When moving the mouse over the icons tooltips are displayed.

Tooltip

Tooltip

Functions

The functions are explained in the following sections.