powered by CADENAS

Manual

Manual

5.13.5.1.1.2.  Assign Attributes

[Note] Note

The browse button ... in the attributes field only becomes active if a classification has already been allocated.

By double clicking on the browse button ... you can open the dialog box Class variables.

Window: Class variables

Window: Class variables

A list of attributes pertaining to that class are shown.

Allocate the desired attributes now.

The following entry fields are available:

  • Variable

    Select the appropriate variable in the list field.

  • Value

    Enter a fixed value.

  • Reference

    Enter a reference to another directory.

[Note] Note

Only one of the options is possible at the same time!

Confirm with OK.