powered by CADENAS

Manual

Manual

7.9.3. Function buttons

7.9.3.1. Basics for use
7.9.3.2. Point
7.9.3.2.1. Connection points for assembly construction
7.9.3.2.1.1. Connection points in general
7.9.3.2.1.2. Name conventions for Connection points and Insertion lines
7.9.3.2.1.3. Direction of connection points
7.9.3.2.1.4. Connection points at miters
7.9.3.2.1.5. Connection points at connection elements
7.9.3.2.1.6. Create Connection line
7.9.3.2.2. Create pattern
7.9.3.2.2.1. Create pattern with linear alignment
7.9.3.2.2.2. Create rotated pattern
7.9.3.2.2.3. Irregular patterns
7.9.3.2.2.4. Using face attributes for patterns
7.9.3.2.3. Sweep
7.9.3.2.4. Connection points as Published elements for automatic placement in the CAD
7.9.3.3. Lines
7.9.3.3.1. Line through 2 points
7.9.3.3.2. Create parallel line
7.9.3.3.3. Perpendicular to line through point
7.9.3.3.4. Midpoint perpendicular to line
7.9.3.3.5. Angle bisector between two lines
7.9.3.3.6. Line at angle to line with length
7.9.3.3.7. Line at angle to horizontal, length
7.9.3.3.8. Horizontal line
7.9.3.3.9. Vertical line
7.9.3.3.10. Line tangent to 2 circles
7.9.3.3.11. Tangent from point to circle
7.9.3.4. N-edge
7.9.3.5. Circle
7.9.3.6. Arc
7.9.3.7. Delete
7.9.3.8. Transform
7.9.3.8.1. Move selection
7.9.3.8.2. Mirror selection
7.9.3.8.3. Rotate selection
7.9.3.8.4. Matrix copy
7.9.3.8.5. Variant copy
7.9.3.9. Attributes
7.9.3.10. Edit existing geometry
7.9.3.10.1. Insert Chamfer/Fillet... with Blend feature
7.9.3.10.1.1. What is the purpose of the Blend Feature
7.9.3.10.1.2. What is NOT the purpose of the Blend Feature
7.9.3.10.1.3. Basics - Create chamfer or fillet
7.9.3.10.1.4. General tips & notes
7.9.3.10.1.5. What should be considered
7.9.3.10.1.5.1. All blends, whose edges meet, have to be made as one blend
7.9.3.10.1.5.2. Blends in pattern
7.9.3.10.1.5.3. Tangent continuous
7.9.3.10.1.5.4. Preview presentation for Chamfer/Fillet
7.9.3.10.1.5.5. Face selection
7.9.3.10.1.5.6. Combination of Sweep and Blend
7.9.3.10.1.5.7. Depiction of Chamfer/Fillet in different CAD systems
7.9.3.10.1.6. Not supported installation situations
7.9.3.10.1.6.1. Function "Generate sketch on selected face" needs at least one edge without Blend
7.9.3.10.1.6.2. Several intersecting chamfers/fillets and Blend feature in addition
7.9.3.10.1.6.3. Edges resulting from Blends
7.9.3.10.1.6.4. Maximum radius of Chamfer/Fillet
7.9.3.10.1.6.5. Blends whose edges meet with different size each
7.9.3.10.1.6.6. Combination of a fillet and a chamfer
7.9.3.10.1.6.7. Radius of chamfer/fillet larger than distance to adjoining geometry
7.9.3.11. Threads
7.9.3.11.1. Cylindrical thread by length
7.9.3.11.1.1. Outer thread with example pin
7.9.3.11.1.1.1. Regular thread
7.9.3.11.1.1.2. Different pitches and derived automatic calculations for e.g. Row Label and Core diameter
7.9.3.11.1.2. Inner thread using the example of a cap nut
7.9.3.11.2. Conical thread by lengths
7.9.3.11.2.1. Regular thread
7.9.3.12. Text
7.9.3.13. File management
7.9.3.13.1. *.dbs-, *.skt bzw. *.hsk files - "Insert sketch" window
7.9.3.13.2. Window „DXF Import“