powered by CADENAS

Manual

Manual

5.9.17.4. Media Variables for tooltip information on PARTcommunity

On PARTcommunity, additional tooltip information is managed in Media Variables. The procedure of the creation of Media Variables is described in detail under Section 5.9.17.1, “Create Media Variables in PARTproject”.

When clicking on the info icon, a tooltip with additional information is opened.

When clicking on the info icon, a tooltip with additional information is opened.

In addition to the standard creation of texts please regard the following:

The created Media Variable's name must be according to following schema:

The Media Variable allocated to the table variable has the same name + "_HELP"

Tablevariable_HELP

Example:

If you want to create a HELP variable related to a table variable BNEB then the name of the Media Variable has to be BNEB_HELP.