powered by CADENAS

Manual

Manual

3.3.5. Use of PARTproject QA SVN

All catalogs that are planned to be published via official CADENAS end media later on must be managed with the eCATALOGsolutions Software module PARTproject QA SVN. It is the central tool for the creation of all catalog data. It provides a user- and role-management for the single parties / members of the Creation Team as well as a direct connection to the worldwide central catalog SVN server, to which the local copies of the database of all catalogs / suppliers are synchronised continuously. The use of the Server is always mandatory. The data transfers via a SSL Internet connection which makes it also very secure.

[Note] Note

On this please review Chapter 6, PARTproject QA.