powered by CADENAS

Manual

Manual

5.13.5.1.  Assignment of classifications and attributes

This chapter would like to assist you in classifying projects.

Classification can be done for different catalog types:

  1. Standard and supplier catalogs

  2. Parts inserted via CAD interface with Own parts library function

    PARTsolutions  
    Insert 3D
    Replace
    Verify if up-to-date
    Execute Geometric Search
    Standard and supplier parts library
    Own parts library Insert
    Connections library Import entire directory
    Embed library into CAD user interface  
    Extras
    Settings
    About CADENAS PARTsolutions

  3. Catalogs created by PLMsynchro

    Detailed information on PLMsynchro can be found under Section 1.2, “ PLM Synchro - Create your company parts catalog” in PARTwarehouse Manual.

  4. Quick&Simple catalogs

    See Section 5.14, “Create catalogs - Quick & Simple ”.

  • A number of functionalities simplify the procedure.

  • Classifications can be conducted at the project and directory levels.

  • After changes the search index has to be updated in PARTadmin -> Index administration, in order for the new assignments to be displayed in PARTdataManager. See Section 5.13.5.2, “ Index update ”.

    [Note] Note

    The update has to be performed both for concerned projects and for the classification!

  • Own parts can also be classified in PARTdataManager. See below.

  • Class and attribute information of the CNS classification is transferred to the interface (CAD) when exporting.