powered by CADENAS

Manual

Manual

6.5.4.1.6.  Download changed data of the project from the server

[Note] Note

If under Extras -> Settings... -> General the option Update index after downloading catalog is set, the index becomes updated with every download process. If only one single subdirectory is downloaded, only the index for this directory becomes updated.

(More expenditure of time)

Unlike check out of project / directory (for work), the downloaded file can be opened however no changes done.

Synchronization happens independent from editing right allocation!

[Note] Note

The lock symbol does not change during this process!