Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
7.6.3. Context menu base plane (Plane XY, ZX,
YZ)
7.6.3.5.
Insert new plane...
(Plane Feature)
|
|
---|---|
Prev | Next |
A parallel plane can be created on the currently selected plane. Its position is defined via Distance and Direction.
If you activate the option Other direction , the value in the Distance field is inverted and the reference plane is aligned in the "opposite" direction.
-> In the 3D History dialog area, the new plane shows up with the name that was assigned in the dialog under Name. Per default "Reference plane 1" has been entered. Further reference planes are numbered consecutively.
A plane with angle can be created on the current plane.
The following image shows the current plane ZX turned around the X axis by 45°.
With the help of the option Only create, if a Condition can be added to the reference plane.