powered by CADENAS

Manual

Manual

3.2.18.2. Benefits of classification according to CNSORDERNO and CNSTYPECODE

The benefits concern all product ranges and users of CADENAS products and applications accessing CADENAS.

For example, the classification can be used in the following scenarios:

  • Always good search results when searching for order numbers (article numbers) or type codes and so the base for correct orders both for parts without value range fields (yellow fields) and for parts which have built their order numbers or type codes from complex value ranges.

    -> Search in PARTdataManager for Order number or type code .

  • Cross link between portals are possible.

  • External assistants can directly request geometry by calling order number / type code instead of using a complex list of deeplinks

  • Article assignment with PARTdataCenter (New or existing customers with Parts Management)

    Initial Article assignment of ERP numbers to PARTsolutions projects with PARTdataCenter on the base of order number / type code is simplified, as numbers are absolutely unique.

    See Section 1.1.6, “ Article Number Search - Automated assignment by order number ” in PARTwarehouse Manual.

    Example: PARTdataCenter

    Example: PARTdataCenter

  • Enrichment of catalog data in eCATALOGsolutions

    • Data with additional value

    • Replacement parts

    • Accessories

    • Alternative products

    • Translations

    • Many other ...

  • Generic creation of vendor catalogs (merging tool)