powered by CADENAS

Manual

Manual

5.13.7.3.  Published elements - Select sketch

Via right-click, in the 3D view, call the context menu.

In order to create published elements on axes, points, etc., select Select sketch.

-> The dialog box Select sketch is opened.

For example, if you want to create an axis as "published element", select the respective sketch (here in this example "Axis: Sketch 1").

Confirm with OK.

-> The editing dialog is opened.

The process complies with the one described under Section 5.13.8, “ Classify standard parts for placement dialog ”.