powered by CADENAS

Manual

Manual

7.8.3. Change variable value

In order to make changes on single parameters, do the following:

  1. Select the desired variable in the table of Variable manager (or just as well the respective column in the characteristic attribute table).

    -> The single parameters are displayed.

  2. If needed, open the extended dialog area by clicking on More.

  3. Make the changes.

  4. Click on Accept changes.

    -> The changes are adopted.