powered by CADENAS

Manual

Manual

10.3.2.  Template configuration

The call up of the "Template configuration" dialog happens via:

  • Preferences menu -> Template configuration

    or

  • the respective icon in the toolbar.

  • Name: When clicking on the function Save as catalog template , this name is used. [112]

  • Visible name: Name, how it is displayed at the datasheet export in PARTdataManager as template name. If Visible name has not been determined, the entry under Name is used.

  • Background PDF: You can load a Background PDF - if needed.

    However, once a template is updated to the current format, the Background PDF should also be replaced by respective images.

    Also compare "Import".

  • Coordinates compatibility mode:

    When editing in PARTtemplateDesigner, values are in mm. Then the values are converted in PDF coordinates in the template.

    Up to < V11 SP10 values were read as integer, which led to differences in the range from 0.1 to 0.6 mm (what is not really striking when printing).

    As of V11 SP10 the calculation is made with floating-point number (meaning higher accuracy).

    In order for old datasheets not to be affected by this change, there is a new option Coordinates compatibility mode now.

    • Compatibility mode on: When opening (or exporting) an old template, the compatibility mode is on, so that integer values are used further on. Thus old datasheets are not affected, unless the compatibility mode is switched off intentionally.

    • Compatibility mode off: When creating a new template, the compatibility mode is switched off by default and so the calculation is made with floating-point numbers.

  • Test project:

    Changing the test project makes possibly sense, in order to check the depiction at different projects (different number of table lines or technical views).

  • Open in PARTproject:

    Certain functions are only available in PARTproject and not in the Media editor:

  • Edit media variables (and create):

    By clicking on the button, the dialog box Media editor opens.

    The Media editor includes functionality for the creation and editing of Media Variables. In PARTproject there is the same possibility. Advantage in the Media editor: Manageable user interface and you can work faster. However, the settings made here only refer to the test project and have to be transmitted to the catalog root element in PARTproject finally (see Section 5.9.17.3, “Transmit variable properties - Derivation hierarchy ”).

    Translations of Media Variables can both be done in the Media editor and in PARTproject (see ???).

    A detailed description on the Media editor is found under Section 10.6, “Edit Media Variables in the Media editor ”.



[112] The catalog template is saved with the file types .template and .ptdef under "_templates"; in the case of the above exemplary figure this would be training1.template and training1.ptdef.