powered by CADENAS

Manual

Manual

9.5.1.5.1. Manual assignment

For the first part (normally this is the dummy part), assignments have to be made manually. For other parts, normally the function Automatic saves considerable time (see Section 9.5.1.5.2, “Automatic assignment”).

  1. Select the desired variable where you want to make the assignment.

  2. In the input field Assignment call the Variable browser via context menu command Choose variable....

    -> The Variable browser is opened.

    Variable browser

    Variable browser

  3. Select part and variable of the part.

  4. Confirm with OK.

    -> The selection is shown in the input field under Assignment.

  5. Click Set.

    -> The assignment is entered in the respective column.

  6. In this way perform all required assignments and finally click OK.

    -> The assignments are displayed in the docking window Configurator under menu item Value range assignments.