powered by CADENAS

Manual

Manual

5.9.2.7.  Menu item PARTserver/PARTcommunity

[Note] Note

The menu item PARTserver/PARTcommunity is displayed at directory and project level.

  • Additional files:

    Visible at directory level.

    Enter those files here that should be copied after PARTserver/PARTcommuntiy. Per default the add-on ",0" is added.

    Should an entire subdirectory need to be copied (for ex., needed for assistants) however, then specify the subdirectory and change the parameter to "1".

  • Visible on PARTcommunity: Yes/No