powered by CADENAS

Manual

Manual

5.9.  Edit project

5.9.1. Overview on tabbed pages
5.9.2. Tabbed page General
5.9.2.1. Menu item General
5.9.2.2. Menu item Assistant
5.9.2.3. Menu item Variables
5.9.2.3.1. Create variable groups (on catalog level)
5.9.2.3.2. Order/Groups of Variables - Hide columns (variables)
5.9.2.3.3. Columns to sort natural
5.9.2.3.4. Variables containing external references
5.9.2.4. Menu item Settings for the catalog (display on catalog level)
5.9.2.5. Menu item Classification
5.9.2.6. Menu item Table filters
5.9.2.7. Menu item PARTserver/PARTcommunity
5.9.2.8. Menu item Color and texture
5.9.2.8.1. Color
5.9.2.8.2. Texture
5.9.2.9. Menu item Render attributes
5.9.2.9.1. Render material - Functionality
5.9.2.9.1.1. Render Materials for Face attributes
5.9.2.9.2. Render material - Settings
5.9.2.9.3. Rendering matrices
5.9.2.9.3.1. Matrix for attributes "Color" and "Color texture" ("Normalmap")
5.9.2.9.3.2. Matrix for attributes "Percentage Metallic" and "Roughness"
5.9.2.9.3.3. Matrix for Transparency
5.9.2.9.3.4. Legend
5.9.2.9.4. Examples
5.9.2.9.5. Maxwell Render rotation
5.9.2.10. Menu item Alternative 2D size
5.9.2.11. Menu item Dimensioning
5.9.2.12. Menu item Link (display at link projects)
5.9.2.13. Menu item Expiration date (End of Life)
5.9.3. Tabbed page 3D project
5.9.3.1. Dimensioning views
5.9.3.2. 3D models
5.9.3.3. Variants
5.9.3.3.1. General concept when using variants
5.9.3.3.2. Basic notes
5.9.3.3.3. Example: Variants of Dimensioning views
5.9.3.3.4. Example: Variants of 3D models
5.9.3.3.5. Example: Specifics for project creation especially in Architecture / BIM catalogs
5.9.4. Tabbed page 2D derivation
5.9.5. Tabbed page 2D project
5.9.6. Tabbed page Bitmaps
5.9.7. Tabbed page Roller bearing
5.9.8. Tabbed page Assembly
5.9.9. Tabbed page Variable assignment (project type „Assembly Table“)
5.9.10. Tabbed page Links
5.9.10.1. Simple example without use of dialog areas Variants and Filter
5.9.10.2. Dialog area Variants (optionally)
5.9.10.3. Dialog area Filter (optionally)
5.9.10.4. Dialog area ID (optional)
5.9.11. Tabbed page Translation
5.9.12. Tabbed page Image
5.9.13. Tabbed page Database
5.9.14. Tabbed page Picture file
5.9.15. Tabbed page Table file
5.9.15.1. Set standard table row
5.9.15.2. Mark lines as expired...
5.9.16. Tabbed page Document
5.9.17. Tabbed page Documents
5.9.17.1. Create Media Variables in PARTproject
5.9.17.2. Translate Media Variables
5.9.17.3. Transmit variable properties - Derivation hierarchy
5.9.17.3.1. Example 1 - Transmit datasheet PDF template
5.9.17.3.2. Example 2 - Transmit textual content
5.9.17.3.3. Dialog area "Derivation hierarchy"
5.9.17.4. Media Variables for tooltip information on PARTcommunity
5.9.18. Tabbed page History
5.9.19. Tabbed page QA check
5.9.20. Tabbed page Catalog separation
5.9.21. Tabbed page Release Notes

In the Project selection dialog area, you have applied directory files, project files and their sub-files (*.pra, *.3db, etc.).

These can be better specified within Edit project.

In the following sections the tabbed pages and the fields are described:

Project selection

Project selection

[Note] Note

The tabbed pages in the Edit project dialog area are composed differently depending on directory level (directory, folder, project, subfile) and Project type.

The following section "Overview" is to be used as orientation.