Elektron is the registered trademark of a wide range of magnesium alloys manufactured by a British company, Magnesium Elektron Limited.
There are about 100 different alloys in the Elektron range, containing from 0% to 9.5% of some of the following elements in varying proportions: aluminium (< 9.5%), yttrium (5.25%), neodymium (2.7%), silver (2.5%), gadolinium (1.3%), zinc (0.9%), zirconium (0.6%), manganese (0.5%) and other rare earth metals.
Varying amounts of alloying elements (up to 9.5%) added to the magnesium result in changes to mechanical properties such as increased tensile strength, creep resistance, thermal stability or corrosion resistance. Elektron is unusually light and has a specific gravity of about 1.8 compared with the 2.8 of aluminium alloy. Magnesium's relatively low density makes its alloy variants suitable for use in auto racing and aerospace engineering applications.