A bicycle parking rack, usually shortened to bike rack and also called a bicycle stand, is a device to which bicycles can be securely attached for parking purposes. A bike rack may be free standing or it may be securely attached to the ground or some stationary object such as a building. Indoor bike racks are commonly used for private bicycle parking, while outdoor bike racks are often used in commercial areas. General styles of racks include the Inverted U, Serpentine, Bollard, Grid, and Decorative. The most effective and secure bike racks are those that can secure both wheels and the frame of the bicycle, using a bicycle lock.
Bike racks can be constructed from a number of different materials. Durability, weather resistance, appearance, and functionality are extremely important variables of the material of the bike rack. Construction materials include stainless steel, steel, recycled plastic, or thermoplastic. Each material has advantages and disadvantages, and each is unique in appearance from the others.The visibility of the bike rack, adequate spacing from automobile parking and pedestrian traffic, weather coverage, and proximity to destinations are all important factors determining usefulness of a bicycle rack. These factors will help increase usage of the bike rack, and assure cyclists their bike is securely parked.