powered by CADENAS

Social Share

Gear (52161 views - Mechanical Engineering)

A gear or cogwheel is a rotating machine part having cut teeth, or cogs, which mesh with another toothed part to transmit torque. Geared devices can change the speed, torque, and direction of a power source. Gears almost always produce a change in torque, creating a mechanical advantage, through their gear ratio, and thus may be considered a simple machine. The teeth on the two meshing gears all have the same shape. Two or more meshing gears, working in a sequence, are called a gear train or a transmission. A gear can mesh with a linear toothed part, called a rack, thereby producing translation instead of rotation. The gears in a transmission are analogous to the wheels in a crossed, belt pulley system. An advantage of gears is that the teeth of a gear prevent slippage. When two gears mesh, if one gear is bigger than the other, a mechanical advantage is produced, with the rotational speeds, and the torques, of the two gears differing in proportion to their diameters. In transmissions with multiple gear ratios—such as bicycles, motorcycles, and cars—the term "gear" as in "first gear" refers to a gear ratio rather than an actual physical gear. The term describes similar devices, even when the gear ratio is continuous rather than discrete, or when the device does not actually contain gears, as in a continuously variable transmission.
Go to Article

Explanation by Hotspot Model

Gear

Gear

Gear

A gear or cogwheel is a rotating machine part having cut teeth, or cogs, which mesh with another toothed part to transmit torque. Geared devices can change the speed, torque, and direction of a power source. Gears almost always produce a change in torque, creating a mechanical advantage, through their gear ratio, and thus may be considered a simple machine. The teeth on the two meshing gears all have the same shape.[1] Two or more meshing gears, working in a sequence, are called a gear train or a transmission. A gear can mesh with a linear toothed part, called a rack, thereby producing translation instead of rotation.

The gears in a transmission are analogous to the wheels in a crossed, belt pulley system. An advantage of gears is that the teeth of a gear prevent slippage.

When two gears mesh, if one gear is bigger than the other, a mechanical advantage is produced, with the rotational speeds, and the torques, of the two gears differing in proportion to their diameters.

In transmissions with multiple gear ratios—such as bicycles, motorcycles, and cars—the term "gear" as in "first gear" refers to a gear ratio rather than an actual physical gear. The term describes similar devices, even when the gear ratio is continuous rather than discrete, or when the device does not actually contain gears, as in a continuously variable transmission.[2]

History

Early examples of gears date from the 4th century BC in China[3] (Zhan Guo times – Late East Zhou dynasty), which have been preserved at the Luoyang Museum of Henan Province, China. The earliest preserved gears in Europe were found in the Antikythera mechanism, an example of a very early and intricate geared device, designed to calculate astronomical positions. Its time of construction is now estimated between 150 and 100 BC.[4] Gears appear in works connected to Hero of Alexandria, in Roman Egypt circa AD 50,[5] but can be traced back to the mechanics of the Alexandrian school in 3rd-century BC Ptolemaic Egypt, and were greatly developed by the Greek polymath Archimedes (287–212 BC).[6]

The differential gear first appeared in the Chinese south-pointing chariot, dated to the first millennium BC.[7] The segmental gear, which receives/communicates reciprocating motion from/to a cogwheel, consisting of a sector of a circular gear/ring having cogs on the periphery,[8] was invented by Arab engineer Al-Jazari in 1206.[9] The worm gear was invented in the Indian subcontinent, for use in roller cotton gins, some time during the 13th–14th centuries.[10]

Examples of early gear applications include:

Comparison with drive mechanisms

The definite ratio that teeth give gears provides an advantage over other drives (such as traction drives and V-belts) in precision machines such as watches that depend upon an exact velocity ratio. In cases where driver and follower are proximal, gears also have an advantage over other drives in the reduced number of parts required; the downside is that gears are more expensive to manufacture and their lubrication requirements may impose a higher operating cost per hour.

Types

External vs internal gears

Internal gear

An external gear is one with the teeth formed on the outer surface of a cylinder or cone. Conversely, an internal gear is one with the teeth formed on the inner surface of a cylinder or cone. For bevel gears, an internal gear is one with the pitch angle exceeding 90 degrees. Internal gears do not cause output shaft direction reversal.[11]

Spur

Spur gear
Spur gears or straight-cut gears are the simplest type of gear. They consist of a cylinder or disk with teeth projecting radially. Though the teeth are not straight-sided (but usually of special form to achieve a constant drive ratio, mainly involute but less commonly cycloidal), the edge of each tooth is straight and aligned parallel to the axis of rotation. These gears mesh together correctly only if fitted to parallel shafts.[12] No axial thrust is created by the tooth loads. Spur gears are excellent at moderate speeds but tend to be noisy at high speeds.[13]

Helical

Helical gears
Top: parallel configuration
Bottom: crossed configuration

Helical or "dry fixed" gears offer a refinement over spur gears. The leading edges of the teeth are not parallel to the axis of rotation, but are set at an angle. Since the gear is curved, this angling makes the tooth shape a segment of a helix. Helical gears can be meshed in parallel or crossed orientations. The former refers to when the shafts are parallel to each other; this is the most common orientation. In the latter, the shafts are non-parallel, and in this configuration the gears are sometimes known as "skew gears".

The angled teeth engage more gradually than do spur gear teeth, causing them to run more smoothly and quietly.[14] With parallel helical gears, each pair of teeth first make contact at a single point at one side of the gear wheel; a moving curve of contact then grows gradually across the tooth face to a maximum, then recedes until the teeth break contact at a single point on the opposite side. In spur gears, teeth suddenly meet at a line contact across their entire width, causing stress and noise. Spur gears make a characteristic whine at high speeds. For this reason spur gears are used in low-speed applications and in situations where noise control is not a problem, and helical gears are used in high-speed applications, large power transmission, or where noise abatement is important.[15] The speed is considered high when the pitch line velocity exceeds 25 m/s.[16]

A disadvantage of helical gears is a resultant thrust along the axis of the gear, which must be accommodated by appropriate thrust bearings, and a greater degree of sliding friction between the meshing teeth, often addressed with additives in the lubricant.

Skew gears

For a "crossed" or "skew" configuration, the gears must have the same pressure angle and normal pitch; however, the helix angle and handedness can be different. The relationship between the two shafts is actually defined by the helix angle(s) of the two shafts and the handedness, as defined:[17]

for gears of the same handedness,
for gears of opposite handedness,

where is the helix angle for the gear. The crossed configuration is less mechanically sound because there is only a point contact between the gears, whereas in the parallel configuration there is a line contact.[17]

Quite commonly, helical gears are used with the helix angle of one having the negative of the helix angle of the other; such a pair might also be referred to as having a right-handed helix and a left-handed helix of equal angles. The two equal but opposite angles add to zero: the angle between shafts is zero—that is, the shafts are parallel. Where the sum or the difference (as described in the equations above) is not zero, the shafts are crossed. For shafts crossed at right angles, the helix angles are of the same hand because they must add to 90 degrees. (This is the case with the gears in the illustration above: they mesh correctly in the crossed configuration: for the parallel configuration, one of the helix angles should be reversed. The gears illustrated cannot mesh with the shafts parallel.)

Double helical

Herringbone gears

Double helical gears and herringbone gears are similar, but the difference is that herringbone gears do not have a groove in the middle like double helical gears do. Double helical gears overcome the problem of axial thrust presented by single helical gears by using two sets of teeth that are set in a V shape. A double helical gear can be thought of as two mirrored helical gears joined together. This arrangement cancels out the net axial thrust, since each half of the gear thrusts in the opposite direction, resulting in a net axial force of zero. This arrangement can remove the need for thrust bearings. However, double helical gears are more difficult to manufacture due to their more complicated shape.

For both possible rotational directions, there exist two possible arrangements for the oppositely-oriented helical gears or gear faces. One arrangement is stable, and the other is unstable. In a stable orientation, the helical gear faces are oriented so that each axial force is directed toward the center of the gear. In an unstable orientation, both axial forces are directed away from the center of the gear. In both arrangements, the total (or net) axial force on each gear is zero when the gears are aligned correctly. If the gears become misaligned in the axial direction, the unstable arrangement generates a net force that may lead to disassembly of the gear train, while the stable arrangement generates a net corrective force. If the direction of rotation is reversed, the direction of the axial thrusts is also reversed, so a stable configuration becomes unstable, and conversely.

Stable double helical gears can be directly interchanged with spur gears without any need for different bearings.

Bevel

Bevel gear

A bevel gear is shaped like a right circular cone with most of its tip cut off. When two bevel gears mesh, their imaginary vertices must occupy the same point. Their shaft axes also intersect at this point, forming an arbitrary non-straight angle between the shafts. The angle between the shafts can be anything except zero or 180 degrees. Bevel gears with equal numbers of teeth and shaft axes at 90 degrees are called miter gears.

Spiral bevels

Spiral bevel gears

Spiral bevel gears can be manufactured as Gleason types (circular arc with non-constant tooth depth), Oerlikon and Curvex types (circular arc with constant tooth depth), Klingelnberg Cyclo-Palloid (Epicycloide with constant tooth depth) or Klingelnberg Palloid. Spiral bevel gears have the same advantages and disadvantages relative to their straight-cut cousins as helical gears do to spur gears. Straight bevel gears are generally used only at speeds below 5 m/s (1000 ft/min), or, for small gears, 1000 r.p.m.[18]

Note: The cylindrical gear tooth profile corresponds to an involute, but the bevel gear tooth profile to an octoid. All traditional bevel gear generators (like Gleason, Klingelnberg, Heidenreich & Harbeck, WMW Modul) manufacture bevel gears with an octoidal tooth profile. IMPORTANT: For 5-axis milled bevel gear sets it is important to choose the same calculation / layout like the conventional manufacturing method. Simplified calculated bevel gears on the basis of an equivalent cylindrical gear in normal section with an involute tooth form show a deviant tooth form with reduced tooth strength by 10-28% without offset and 45% with offset [Diss. Hünecke, TU Dresden]. Furthermore, the "involute bevel gear sets" cause more noise.

Hypoid

Hypoid gear

Hypoid gears resemble spiral bevel gears except the shaft axes do not intersect. The pitch surfaces appear conical but, to compensate for the offset shaft, are in fact hyperboloids of revolution.[19][20] Hypoid gears are almost always designed to operate with shafts at 90 degrees. Depending on which side the shaft is offset to, relative to the angling of the teeth, contact between hypoid gear teeth may be even smoother and more gradual than with spiral bevel gear teeth, but also have a sliding action along the meshing teeth as it rotates and therefore usually require some of the most viscous types of gear oil to avoid it being extruded from the mating tooth faces, the oil is normally designated HP (for hypoid) followed by a number denoting the viscosity. Also, the pinion can be designed with fewer teeth than a spiral bevel pinion, with the result that gear ratios of 60:1 and higher are feasible using a single set of hypoid gears.[21] This style of gear is most common in motor vehicle drive trains, in concert with a differential. Whereas a regular (nonhypoid) ring-and-pinion gear set is suitable for many applications, it is not ideal for vehicle drive trains because it generates more noise and vibration than a hypoid does. Bringing hypoid gears to market for mass-production applications was an engineering improvement of the 1920s.

Crown

Crown gear

Crown gears or contrate gears are a particular form of bevel gear whose teeth project at right angles to the plane of the wheel; in their orientation the teeth resemble the points on a crown. A crown gear can only mesh accurately with another bevel gear, although crown gears are sometimes seen meshing with spur gears. A crown gear is also sometimes meshed with an escapement such as found in mechanical clocks.

Worm

Worm gear
4-start worm and wheel

Worms resemble screws. A worm is meshed with a worm wheel, which looks similar to a spur gear.

Worm-and-gear sets are a simple and compact way to achieve a high torque, low speed gear ratio. For example, helical gears are normally limited to gear ratios of less than 10:1 while worm-and-gear sets vary from 10:1 to 500:1.[22] A disadvantage is the potential for considerable sliding action, leading to low efficiency.[23]

A worm gear is a species of helical gear, but its helix angle is usually somewhat large (close to 90 degrees) and its body is usually fairly long in the axial direction. These attributes give it screw like qualities. The distinction between a worm and a helical gear is that at least one tooth persists for a full rotation around the helix. If this occurs, it is a 'worm'; if not, it is a 'helical gear'. A worm may have as few as one tooth. If that tooth persists for several turns around the helix, the worm appears, superficially, to have more than one tooth, but what one in fact sees is the same tooth reappearing at intervals along the length of the worm. The usual screw nomenclature applies: a one-toothed worm is called single thread or single start; a worm with more than one tooth is called multiple thread or multiple start. The helix angle of a worm is not usually specified. Instead, the lead angle, which is equal to 90 degrees minus the helix angle, is given.

In a worm-and-gear set, the worm can always drive the gear. However, if the gear attempts to drive the worm, it may or may not succeed. Particularly if the lead angle is small, the gear's teeth may simply lock against the worm's teeth, because the force component circumferential to the worm is not sufficient to overcome friction.

Worm-and-gear sets that do lock are called self locking, which can be used to advantage, as for instance when it is desired to set the position of a mechanism by turning the worm and then have the mechanism hold that position. An example is the machine head found on some types of stringed instruments.

If the gear in a worm-and-gear set is an ordinary helical gear only a single point of contact is achieved.[21][24] If medium to high power transmission is desired, the tooth shape of the gear is modified to achieve more intimate contact by making both gears partially envelop each other. This is done by making both concave and joining them at a saddle point; this is called a cone-drive[25] or "Double enveloping".

Worm gears can be right or left-handed, following the long-established practice for screw threads.[11]

Non-circular

Non-circular gears

Non-circular gears are designed for special purposes. While a regular gear is optimized to transmit torque to another engaged member with minimum noise and wear and maximum efficiency, a non-circular gear's main objective might be ratio variations, axle displacement oscillations and more. Common applications include textile machines, potentiometers and continuously variable transmissions.

Rack and pinion

Rack and pinion gearing

A rack is a toothed bar or rod that can be thought of as a sector gear with an infinitely large radius of curvature. Torque can be converted to linear force by meshing a rack with a pinion: the pinion turns; the rack moves in a straight line. Such a mechanism is used in automobiles to convert the rotation of the steering wheel into the left-to-right motion of the tie rod(s). Racks also feature in the theory of gear geometry, where, for instance, the tooth shape of an interchangeable set of gears may be specified for the rack, (infinite radius), and the tooth shapes for gears of particular actual radii are then derived from that. The rack and pinion gear type is employed in a rack railway.

Epicyclic

Epicyclic gearing

In epicyclic gearing one or more of the gear axes moves. Examples are sun and planet gearing (see below), cycloidal drive, and mechanical differentials.

Sun and planet

Sun (yellow) and planet (red) gearing

Sun and planet gearing is a method of converting reciprocating motion into rotary motion that was used in steam engines. James Watt used it on his early steam engines to get around the patent on the crank, but it also provided the advantage of increasing the flywheel speed so Watt could use a lighter flywheel.

In the illustration, the sun is yellow, the planet red, the reciprocating arm is blue, the flywheel is green and the driveshaft is gray.

Harmonic gear

Harmonic gearing

A harmonic gear is a specialized gearing mechanism often used in industrial motion control, robotics and aerospace for its advantages over traditional gearing systems, including lack of backlash, compactness and high gear ratios.

Cage gear

Cage gear in Pantigo Windmill, Long Island (with the driving gearwheel disengaged)

A cage gear, also called a lantern gear or lantern pinion has cylindrical rods for teeth, parallel to the axle and arranged in a circle around it, much as the bars on a round bird cage or lantern. The assembly is held together by disks at each end, into which the tooth rods and axle are set. Cage gears are more efficient than solid pinions,[citation needed] and dirt can fall through the rods rather than becoming trapped and increasing wear. They can be constructed with very simple tools as the teeth are not formed by cutting or milling, but rather by drilling holes and inserting rods.

Sometimes used in clocks, the cage gear should always be driven by a gearwheel, not used as the driver. The cage gear was not initially favoured by conservative clock makers. It became popular in turret clocks where dirty working conditions were most commonplace. Domestic American clock movements often used them.

Magnetic gear

All cogs of each gear component of magnetic gears act as a constant magnet with periodic alternation of opposite magnetic poles on mating surfaces. Gear components are mounted with a backlash capability similar to other mechanical gearings. Although they cannot exert as much force as a traditional gear, such gears work without touching and so are immune to wear, have very low noise and can slip without damage making them very reliable.[26] They can be used in configurations that are not possible for gears that must be physically touching and can operate with a non-metallic barrier completely separating the driving force from the load. The magnetic coupling can transmit force into a hermetically sealed enclosure without using a radial shaft seal, which may leak.

Nomenclature

General nomenclature

Rotational frequency, n 
Measured in rotation over time, such as revolutions per minute (RPM or rpm).
Angular frequency, ω 
Measured in radians/second. 1 RPM = 2π rad/minute = π/30 rad/second.
Number of teeth, N 
How many teeth a gear has, an integer. In the case of worms, it is the number of thread starts that the worm has.
Gear, wheel 
The larger of two interacting gears or a gear on its own.
Pinion 
The smaller of two interacting gears.
Path of contact 
Path followed by the point of contact between two meshing gear teeth.
Line of action, pressure line 
Line along which the force between two meshing gear teeth is directed. It has the same direction as the force vector. In general, the line of action changes from moment to moment during the period of engagement of a pair of teeth. For involute gears, however, the tooth-to-tooth force is always directed along the same line—that is, the line of action is constant. This implies that for involute gears the path of contact is also a straight line, coincident with the line of action—as is indeed the case.
Axis 
Axis of revolution of the gear; center line of the shaft.
Pitch point 
Point where the line of action crosses a line joining the two gear axes.
Pitch circle, pitch line 
Circle centered on and perpendicular to the axis, and passing through the pitch point. A predefined diametral position on the gear where the circular tooth thickness, pressure angle and helix angles are defined.
Pitch diameter, d 
A predefined diametral position on the gear where the circular tooth thickness, pressure angle and helix angles are defined. The standard pitch diameter is a basic dimension and cannot be measured, but is a location where other measurements are made. Its value is based on the number of teeth, the normal module (or normal diametral pitch), and the helix angle. It is calculated as:
in metric units or in imperial units.[27]
Module or modulus, m 
Since it is impractical to calculate circular pitch with irrational numbers, mechanical engineers usually use a scaling factor that replaces it with a regular value instead. This is known as the module or modulus of the wheel and is simply defined as
where m is the module and p the circular pitch. The units of module are customarily millimeters; an English Module is sometimes used with the units of inches. When the diametral pitch, DP, is in English units,
in conventional metric units.
The distance between the two axis becomes
where a is the axis distance, z1 and z2 are the number of cogs (teeth) for each of the two wheels (gears). These numbers (or at least one of them) is often chosen among primes to create an even contact between every cog of both wheels, and thereby avoid unnecessary wear and damage. An even uniform gear wear is achieved by ensuring the tooth counts of the two gears meshing together are relatively prime to each other; this occurs when the greatest common divisor (GCD) of each gear tooth count equals 1, e.g. GCD(16,25)=1; if a 1:1 gear ratio is desired a relatively prime gear may be inserted in between the two gears; this maintains the 1:1 ratio but reverses the gear direction; a second relatively prime gear could also be inserted to restore the original rotational direction while maintaining uniform wear with all 4 gears in this case. Mechanical engineers, at least in continental Europe, usually use the module instead of circular pitch. The module, just like the circular pitch, can be used for all types of cogs, not just evolvent based straight cogs.[28]
Operating pitch diameters 
Diameters determined from the number of teeth and the center distance at which gears operate.[11] Example for pinion:
Pitch surface 
In cylindrical gears, cylinder formed by projecting a pitch circle in the axial direction. More generally, the surface formed by the sum of all the pitch circles as one moves along the axis. For bevel gears it is a cone.
Angle of action 
Angle with vertex at the gear center, one leg on the point where mating teeth first make contact, the other leg on the point where they disengage.
Arc of action 
Segment of a pitch circle subtended by the angle of action.
Pressure angle,  
The complement of the angle between the direction that the teeth exert force on each other, and the line joining the centers of the two gears. For involute gears, the teeth always exert force along the line of action, which, for involute gears, is a straight line; and thus, for involute gears, the pressure angle is constant.
Outside diameter,  
Diameter of the gear, measured from the tops of the teeth.
Root diameter 
Diameter of the gear, measured at the base of the tooth.
Addendum, a 
Radial distance from the pitch surface to the outermost point of the tooth.
Dedendum, b 
Radial distance from the depth of the tooth trough to the pitch surface.
Whole depth,  
The distance from the top of the tooth to the root; it is equal to addendum plus dedendum or to working depth plus clearance.
Clearance 
Distance between the root circle of a gear and the addendum circle of its mate.
Working depth 
Depth of engagement of two gears, that is, the sum of their operating addendums.
Circular pitch, p 
Distance from one face of a tooth to the corresponding face of an adjacent tooth on the same gear, measured along the pitch circle.
Diametral pitch, DP 
Ratio of the number of teeth to the pitch diameter. Could be measured in teeth per inch or teeth per centimeter, but conventionally has units of per inch of diameter. Where the module, m, is in metric units
in English units
Base circle 
In involute gears, the tooth profile is generated by the involute of the base circle. The radius of the base circle is somewhat smaller than that of the pitch circle
Base pitch, normal pitch,  
In involute gears, distance from one face of a tooth to the corresponding face of an adjacent tooth on the same gear, measured along the base circle
Interference 
Contact between teeth other than at the intended parts of their surfaces
Interchangeable set 
A set of gears, any of which mates properly with any other

Helical gear nomenclature

Helix angle,  
Angle between a tangent to the helix and the gear axis. It is zero in the limiting case of a spur gear, albeit it can considered as the hypotenuse angle as well.
Normal circular pitch,  
Circular pitch in the plane normal to the teeth.
Transverse circular pitch, p 
Circular pitch in the plane of rotation of the gear. Sometimes just called "circular pitch".

Several other helix parameters can be viewed either in the normal or transverse planes. The subscript n usually indicates the normal.

Worm gear nomenclature

Lead 
Distance from any point on a thread to the corresponding point on the next turn of the same thread, measured parallel to the axis.
Linear pitch, p 
Distance from any point on a thread to the corresponding point on the adjacent thread, measured parallel to the axis. For a single-thread worm, lead and linear pitch are the same.
Lead angle,  
Angle between a tangent to the helix and a plane perpendicular to the axis. Note that the complement of the helix angle is usually given for helical gears.
Pitch diameter,  
Same as described earlier in this list. Note that for a worm it is still measured in a plane perpendicular to the gear axis, not a tilted plane.

Subscript w denotes the worm, subscript g denotes the gear.

Tooth contact nomenclature

Point of contact 
Any point at which two tooth profiles touch each other.
Line of contact
A line or curve along which two tooth surfaces are tangent to each other.
Path of action 
The locus of successive contact points between a pair of gear teeth, during the phase of engagement. For conjugate gear teeth, the path of action passes through the pitch point. It is the trace of the surface of action in the plane of rotation.
Line of action 
The path of action for involute gears. It is the straight line passing through the pitch point and tangent to both base circles.
Surface of action 
The imaginary surface in which contact occurs between two engaging tooth surfaces. It is the summation of the paths of action in all sections of the engaging teeth.
Plane of action
The surface of action for involute, parallel axis gears with either spur or helical teeth. It is tangent to the base cylinders.
Zone of action (contact zone) 
For involute, parallel-axis gears with either spur or helical teeth, is the rectangular area in the plane of action bounded by the length of action and the effective face width.
Path of contact
The curve on either tooth surface along which theoretical single point contact occurs during the engagement of gears with crowned tooth surfaces or gears that normally engage with only single point contact.
Length of action
The distance on the line of action through which the point of contact moves during the action of the tooth profile.
Arc of action, Qt 
The arc of the pitch circle through which a tooth profile moves from the beginning to the end of contact with a mating profile.
Arc of approach, Qa 
The arc of the pitch circle through which a tooth profile moves from its beginning of contact until the point of contact arrives at the pitch point.
Arc of recess, Qr 
The arc of the pitch circle through which a tooth profile moves from contact at the pitch point until contact ends.
Contact ratio, mc, ε 
The number of angular pitches through which a tooth surface rotates from the beginning to the end of contact. In a simple way, it can be defined as a measure of the average number of teeth in contact during the period during which a tooth comes and goes out of contact with the mating gear.
Transverse contact ratio, mp, εα 
The contact ratio in a transverse plane. It is the ratio of the angle of action to the angular pitch. For involute gears it is most directly obtained as the ratio of the length of action to the base pitch.
Face contact ratio, mF, εβ 
The contact ratio in an axial plane, or the ratio of the face width to the axial pitch. For bevel and hypoid gears it is the ratio of face advance to circular pitch.
Total contact ratio, mt, εγ 
The sum of the transverse contact ratio and the face contact ratio.
Modified contact ratio, mo 
For bevel gears, the square root of the sum of the squares of the transverse and face contact ratios.
Limit diameter 
Diameter on a gear at which the line of action intersects the maximum (or minimum for internal pinion) addendum circle of the mating gear. This is also referred to as the start of active profile, the start of contact, the end of contact, or the end of active profile.
Start of active profile (SAP) 
Intersection of the limit diameter and the involute profile.
Face advance 
Distance on a pitch circle through which a helical or spiral tooth moves from the position at which contact begins at one end of the tooth trace on the pitch surface to the position where contact ceases at the other end.

Tooth thickness nomenclature

Circular thickness 
Length of arc between the two sides of a gear tooth, on the specified datum circle.
Transverse circular thickness 
Circular thickness in the transverse plane.
Normal circular thickness 
Circular thickness in the normal plane. In a helical gear it may be considered as the length of arc along a normal helix.
Axial thickness
In helical gears and worms, tooth thickness in an axial cross section at the standard pitch diameter.
Base circular thickness
In involute teeth, length of arc on the base circle between the two involute curves forming the profile of a tooth.
Normal chordal thickness
Length of the chord that subtends a circular thickness arc in the plane normal to the pitch helix. Any convenient measuring diameter may be selected, not necessarily the standard pitch diameter.
Chordal addendum (chordal height) 
Height from the top of the tooth to the chord subtending the circular thickness arc. Any convenient measuring diameter may be selected, not necessarily the standard pitch diameter.
Profile shift 
Displacement of the basic rack datum line from the reference cylinder, made non-dimensional by dividing by the normal module. It is used to specify the tooth thickness, often for zero backlash.
Rack shift 
Displacement of the tool datum line from the reference cylinder, made non-dimensional by dividing by the normal module. It is used to specify the tooth thickness.
Measurement over pins 
Measurement of the distance taken over a pin positioned in a tooth space and a reference surface. The reference surface may be the reference axis of the gear, a datum surface or either one or two pins positioned in the tooth space or spaces opposite the first. This measurement is used to determine tooth thickness.
Span measurement 
Measurement of the distance across several teeth in a normal plane. As long as the measuring device has parallel measuring surfaces that contact on an unmodified portion of the involute, the measurement wis along a line tangent to the base cylinder. It is used to determine tooth thickness.
Modified addendum teeth 
Teeth of engaging gears, one or both of which have non-standard addendum.
Full-depth teeth 
Teeth in which the working depth equals 2.000 divided by the normal diametral pitch.
Stub teeth 
Teeth in which the working depth is less than 2.000 divided by the normal diametral pitch.
Equal addendum teeth 
Teeth in which two engaging gears have equal addendums.
Long and short-addendum teeth 
Teeth in which the addendums of two engaging gears are unequal.

Pitch nomenclature

Pitch is the distance between a point on one tooth and the corresponding point on an adjacent tooth.[11] It is a dimension measured along a line or curve in the transverse, normal, or axial directions. The use of the single word pitch without qualification may be ambiguous, and for this reason it is preferable to use specific designations such as transverse circular pitch, normal base pitch, axial pitch.

Circular pitch, p 
Arc distance along a specified pitch circle or pitch line between corresponding profiles of adjacent teeth.
Transverse circular pitch, pt 
Circular pitch in the transverse plane.
Normal circular pitch, pn, pe 
Circular pitch in the normal plane, and also the length of the arc along the normal pitch helix between helical teeth or threads.
Axial pitch, px 
Linear pitch in an axial plane and in a pitch surface. In helical gears and worms, axial pitch has the same value at all diameters. In gearing of other types, axial pitch may be confined to the pitch surface and may be a circular measurement. The term axial pitch is preferred to the term linear pitch. The axial pitch of a helical worm and the circular pitch of its worm gear are the same.
Normal base pitch, pN, pbn 
An involute helical gear is the base pitch in the normal plane. It is the normal distance between parallel helical involute surfaces on the plane of action in the normal plane, or is the length of arc on the normal base helix. It is a constant distance in any helical involute gear.
Transverse base pitch, pb, pbt 
In an involute gear, the pitch is on the base circle or along the line of action. Corresponding sides of involute gear teeth are parallel curves, and the base pitch is the constant and fundamental distance between them along a common normal in a transverse plane.
Diametral pitch (transverse), Pd 
Ratio of the number of teeth to the standard pitch diameter in inches.
Normal diametral pitch, Pnd 
Value of diametral pitch in a normal plane of a helical gear or worm.
Angular pitch, θN, τ 
Angle subtended by the circular pitch, usually expressed in radians.
degrees or radians

Backlash

Backlash is the error in motion that occurs when gears change direction. It exists because there is always some gap between the trailing face of the driving tooth and the leading face of the tooth behind it on the driven gear, and that gap must be closed before force can be transferred in the new direction. The term "backlash" can also be used to refer to the size of the gap, not just the phenomenon it causes; thus, one could speak of a pair of gears as having, for example, "0.1 mm of backlash." A pair of gears could be designed to have zero backlash, but this would presuppose perfection in manufacturing, uniform thermal expansion characteristics throughout the system, and no lubricant. Therefore, gear pairs are designed to have some backlash. It is usually provided by reducing the tooth thickness of each gear by half the desired gap distance. In the case of a large gear and a small pinion, however, the backlash is usually taken entirely off the gear and the pinion is given full sized teeth. Backlash can also be provided by moving the gears further apart. The backlash of a gear train equals the sum of the backlash of each pair of gears, so in long trains backlash can become a problem.

For situations that require precision, such as instrumentation and control, backlash can be minimised through one of several techniques. For instance, the gear can be split along a plane perpendicular to the axis, one half fixed to the shaft in the usual manner, the other half placed alongside it, free to rotate about the shaft, but with springs between the two halves providing relative torque between them, so that one achieves, in effect, a single gear with expanding teeth. Another method involves tapering the teeth in the axial direction and letting the gear slide in the axial direction to take up slack.

Shifting of gears

In some machines (e.g., automobiles) it is necessary to alter the gear ratio to suit the task, a process known as gear shifting or changing gear. There are several ways of shifting gears, for example:

There are several outcomes of gear shifting in motor vehicles. In the case of vehicle noise emissions, there are higher sound levels emitted when the vehicle is engaged in lower gears. The design life of the lower ratio gears is shorter, so cheaper gears may be used, which tend to generate more noise due to smaller overlap ratio and a lower mesh stiffness etc. than the helical gears used for the high ratios. This fact has been used to analyze vehicle-generated sound since the late 1960s, and has been incorporated into the simulation of urban roadway noise and corresponding design of urban noise barriers along roadways.[29]

Tooth profile

A profile is one side of a tooth in a cross section between the outside circle and the root circle. Usually a profile is the curve of intersection of a tooth surface and a plane or surface normal to the pitch surface, such as the transverse, normal, or axial plane.

The fillet curve (root fillet) is the concave portion of the tooth profile where it joins the bottom of the tooth space.2

As mentioned near the beginning of the article, the attainment of a nonfluctuating velocity ratio is dependent on the profile of the teeth. Friction and wear between two gears is also dependent on the tooth profile. There are a great many tooth profiles that provides a constant velocity ratio. In many cases, given an arbitrary tooth shape, it is possible to develop a tooth profile for the mating gear that provides a constant velocity ratio. However, two constant velocity tooth profiles are the most commonly used in modern times: the cycloid and the involute. The cycloid was more common until the late 1800s. Since then, the involute has largely superseded it, particularly in drive train applications. The cycloid is in some ways the more interesting and flexible shape; however the involute has two advantages: it is easier to manufacture, and it permits the center-to-center spacing of the gears to vary over some range without ruining the constancy of the velocity ratio. Cycloidal gears only work properly if the center spacing is exactly right. Cycloidal gears are still used in mechanical clocks.

An undercut is a condition in generated gear teeth when any part of the fillet curve lies inside of a line drawn tangent to the working profile at its point of juncture with the fillet. Undercut may be deliberately introduced to facilitate finishing operations. With undercut the fillet curve intersects the working profile. Without undercut the fillet curve and the working profile have a common tangent.

Gear materials

Numerous nonferrous alloys, cast irons, powder-metallurgy and plastics are used in the manufacture of gears. However, steels are most commonly used because of their high strength-to-weight ratio and low cost. Plastic is commonly used where cost or weight is a concern. A properly designed plastic gear can replace steel in many cases because it has many desirable properties, including dirt tolerance, low speed meshing, the ability to "skip" quite well[30] and the ability to be made with materials that don't need additional lubrication. Manufacturers have used plastic gears to reduce costs in consumer items including copy machines, optical storage devices, cheap dynamos, consumer audio equipment, servo motors, and printers. Another advantage of the use of plastics, formerly (such as in the 1980s), was the reduction of repair costs for certain expensive machines. In cases of severe jamming (as of the paper in a printer), the plastic gear teeth would be torn free of their substrate, allowing the drive mechanism to then spin freely (instead of damaging itself by straining against the jam). This use of "sacrificial" gear teeth avoided destroying the much more expensive motor and related parts. This method has been superseded, in more recent designs, by the use of clutches and torque- or current-limited motors.

Standard pitches and the module system

Although gears can be made with any pitch, for convenience and interchangeability standard pitches are frequently used. Pitch is a property associated with linear dimensions and so differs whether the standard values are in the Imperial (inch) or Metric systems. Using inch measurements, standard diametral pitch values with units of "per inch" are chosen; the diametral pitch is the number of teeth on a gear of one inch pitch diameter. Common standard values for spur gears are 3, 4, 5, 6, 8, 10, 12, 16, 20, 24, 32, 48, 64, 72, 80, 96, 100, 120, and 200.[31] Certain standard pitches such as 1/10 and 1/20 in inch measurements, which mesh with linear rack, are actually (linear) circular pitch values with units of "inches"[31]

When gear dimensions are in the metric system the pitch specification is generally in terms of module or modulus, which is effectively a length measurement across the pitch diameter. The term module is understood to mean the pitch diameter in millimeters divided by the number of teeth. When the module is based upon inch measurements, it is known as the English module to avoid confusion with the metric module. Module is a direct dimension, unlike diametral pitch, which is an inverse dimension ("threads per inch"). Thus, if the pitch diameter of a gear is 40 mm and the number of teeth 20, the module is 2, which means that there are 2 mm of pitch diameter for each tooth.[32] The preferred standard module values are 0.1, 0.2, 0.3, 0.4, 0.5, 0.6, 0.8, 1.0, 1.25, 1.5, 2.0, 2.5, 3, 4, 5, 6, 8, 10, 12, 16, 20, 25, 32, 40 and 50.[33]

Manufacture

As of 2014, an estimated 80% of all gearing produced worldwide is produced by net shape molding. Molded gearing is usually either powder metallurgy or plastic.[34] Many gears are done when they leave the mold (including injection molded plastic and die cast metal gears), but powdered metal gears require sintering and sand castings or investment castings require gear cutting or other machining to finish them. The most common form of gear cutting is hobbing, but gear shaping, milling, and broaching also exist. 3D printing as a production method is expanding rapidly. For metal gears in the transmissions of cars and trucks, the teeth are heat treated to make them hard and more wear resistant while leaving the core soft and tough. For large gears that are prone to warp, a quench press is used.

Gear box designing

The essential information required for designing a Gear box are as follows.

  1. The lowest output rpm, n min
  2. The highest output rpm, n max
  3. The number of steps z into which the range between n max and n min is divided and
  4. The number of stages in which the required number of speed steps are to be achieved.

Procedure for a stepwise solution

Let n1, n2, n3… n z be the rpm values available on machine tool be in geometric progression.

Rn= nz/( n1)= Ø z-1

Where Rn= Range ratio, Ø= Progression Ratio

Ø= Rn (1/z-1)

Z= log Rn. Ø/ log Ø

Suppose a speed on one shaft yields two speed values on next shaft i.e. No. of speed steps of particular transmission group is p=2. The transmission ratio that provide two speed values must lie in following range:

I max= 2 & I min= ¼

Maximum reduction of speed is limited to four times to keep the radial dimensions of Gear box within reasonable limits, Maximum increase of speed is limited to two times due to limitations of the pitch line velocity.

I max/I min= 8

Structural formula: z= p1(x1) p2(x2) p3(x3)

Here x1= 1, x2= characteristics of x1= p1 & x3=characteristics of x1x2= p1p2

Let us understand this by an e.g. n min = 16 rpm n max =770 rpm Ø= 1.41 Rn= 770/( 16)= 1.4112-1 Z= log (770/16). 1.41/ log 1.41 Z=12 Z= 2X2X3 Z= 2(1) X 2(2) X 3(4)

This is called structural formula.

The possible structural formula for above Z are: 2(1) X 2(2) X 3(4), 2(1) X 2(2) X 3(4), 2(2) X 2(1) X 3(4), 2(6) X 2(1) X 3(2), 2(6) X 2(3) X 3(1), 2(3) X 2(6) X 3(1), 3(1) X 2(3) X 2(6), 3(1) X 2(6) X 2(3), 3(2) X 2(1) X 2(6), 3(4) X 2(1) X 2(2), 3(4) X 2(2) X 2(1), 3(2) X 2(6) X 2(1) 2(1) X 3(2) X 2(6), 2(1) X 3(4) X 2(2), 2(3) X 3(1) X 2(6), 2(6) X 3(1) X 2(3), 2(6) X 3(2) X 2(1), 2(2) X 3(4) X 2(1), In z= p1(x1) p2(x2) p3(x3)

The best version which ensures that it will be one in which the n min values of the intermediate shafts are maximum and n max values of the intermediate shafts re minimum P1>p2>p3 & x1<x2<x3

Of the above 18 structural formula3(1) X 2(3) X 2(6) is the most appropriate structural diagram. Let us draw structural diagram for the generated structural formula.

u = No. of stages

Here in this case u=3 transmission group

  1. Draw u+1(Here 4) vertical line at convenient distance where first vertical line represents the transmission from motor shaft and the rest represent the transmission groups of speed box.
  2. Draw array of horizontal lines (Here 12) is equal to the number of speed steps z of speed intersecting the vertical lines distance of log Ø from each other.
  3. Select the best structure diagram from the above structure diagrams. The number of gears on the last shaft (spindle) should be minimum possible. The transmission ratio between spindle and the shaft preceding it should be the maximum possible i.e. speed reduction should be the maximum possible. The structure diagram shod be narrow towards the starting point (on input shaft) i.e. parabolic in nature.

Speed chart

Structural diagram only depicts the range ratio of transmission groups but gives no information about transmission ratios. In order to determine the transmission ratios of all transmissions and the rpm values of gearbox shafts, need to draw speed chart.

  • The line is horizontal, it corresponds to transmission ratio I =1, i.e. no speed change.
  • The line is inclined upward, it depicts I >1, i.e., speed increase.
  • The line is inclined downward, it depicts I <1, i.e., speed reduction.

Draw z+1 No. of vertical lines and u+1 horizontal lines intersecting the vertical lines at convenient distance. (here 13 horizontal lines and 4 vertical lines.)

Draw the rays depicting transmission between shaft and the shaft preceding it. The rays are drawn from the lowest rpm of last shaft keeping in mind the transmission ratio restriction condition I max≤ 2 and I min>=1/4.

Here. I max= 2 = ф 2 [(1.41) 2 = 1.9881

I min = 1/4 = 1/ ф 4 [(1.41) 4 = 3.9525],

Mark speeds of shaft in front of each horizontal line, starting with n min* ф on first line, n min* ф2 on second line, n min* ф3 on third line and so on.

Select the best speed chart i.e. It should have concave shape.

Gear box diagram

No. of teeth on the smallest gear should be such that there is no undercutting of gear teeth Z min≥17. If gears are on parallel shafts sum of no. of teeth of mating gear pair should be same. Spacing between two adjacent gears should be such that one should be such that one should disengage before other mate. Center distance between two shafts, A=m (Z1+Z2)/2. In machine tools with large inertia of driven member, friction clutch and brake should be provided on input shaft. Reversing devices should be provided so that tool can be returned to its initial position after completion of the cutting process. Reversal speed = 1.3-1.5 times greater than the cutting speed. If spindle head traverse, electric motor should be mounted on the speed box and the transmission from motor shaft to input shaft of the speed box obtained through a clutch or gear pair. Spindle is kinematic ally linked to feed mechanism, from the spindle to feed train must be shown on gearing diagram. The largest of gears on the spindle should be mounted closest to front spindle bearing.

Z min=2 k (1+√(1±i(2±i) sin⁡〖 ^2 α〗 ))/((2±i)sin⁡〖 ^2 α〗 )

K=tooth addendum

i= transmission ratio

α= pressure angle

Z min=17

Let's return to our question:

n min = 16 rpm, n max =770 rpm, Ø= 1.41, n motor =1440 rpm, input shaft=630 rpm.

from gearbox diagram z7 is a link gear

z7/z14= 250/250

z10/z11= 63/250 z10 +z11= 86, z10=23, z11=63

z12/z13= 63/250 z12+ z13= 86, z12=17, z13=69

z15/z16= 125/63 z15=60, z18=30

z17/z18= 16/63 z17=18, z18= 72

[35]

Inspection

Overall gear geometry can be inspected and verified using various methods such as industrial CT scanning, coordinate-measuring machines, white light scanner or laser scanning. Particularly useful for plastic gears, industrial CT scanning can inspect internal geometry and imperfections such as porosity.

Important dimensional variations of gears result from variations in the combinations of the dimensions of the tools used to manufacture them. An important parameter for meshing qualities such as backlash and noise generation is the variation of the actual contact point as the gear rotates, or the instantaneous pitch radius. Precision gears were frequently inspected by a method that produced a paper "gear tape" record showing variations with a resolution of .0001 inches as the gear was rotated.[31]

The American Gear Manufacturers Association was organized in 1916 to formulate quality standards for gear inspection to reduce noise from automotive timing gears;[36] in 1993 AGMA assumed leadership of the ISO committee governing international standards for gearing. The ANSI/AGMA 2000 A88 Gear Classification and Inspection Handbook specifies quality numbers from Q3 to Q15 to represent the accuracy of tooth geometry; the higher the number the better the tolerance.[37] Some dimensions can be measured to millionths of an inch in controlled-environment rooms.[37]

Gear model in modern physics

Modern physics adopted the gear model in different ways. In the nineteenth century, James Clerk Maxwell developed a model of electromagnetism in which magnetic field lines were rotating tubes of incompressible fluid. Maxwell used a gear wheel and called it an "idle wheel" to explain the electric current as a rotation of particles in opposite directions to that of the rotating field lines.[38]

More recently, quantum physics uses "quantum gears" in their model. A group of gears can serve as a model for several different systems, such as an artificially constructed nanomechanical device or a group of ring molecules.[39]

The Three Wave Hypothesis compares the wave–particle duality to a bevel gear.[40]

Gear mechanism in natural world

Issus coleoptratus

The gear mechanism was previously considered exclusively artificial, but in 2013, scientists from the University of Cambridge announced their discovery that the juvenile form of a common insect Issus (species Issus coleoptratus), found in many European gardens, has a gear-like mechanism in its hind legs. Each leg has joints that form two 180° helix-shaped strips with 12 fully interlocking spur-type gear teeth, including filleted curves at the base of each tooth to reduce the risk of shearing. The joint rotates like mechanical gears and synchronizes Issus's legs when it jumps.[41][42]

See also



This article uses material from the Wikipedia article "Gear", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD