powered by CADENAS

Social Share

Amazon

Continent (145 views - Countries & Continents)

A continent is one of several very large landmasses of the world. Generally identified by convention rather than any strict criteria, up to seven regions are commonly regarded as continents. Ordered from largest in area to smallest, they are: Asia, Africa, North America, South America, Antarctica, Europe, and Australia.Geologically, the continents largely correspond to areas of continental crust that are found on the continental plates. However, some areas of continental crust are regions covered with water not usually included in the list of continents. Zealandia is one such area (see submerged continents below). Islands are frequently grouped with a neighbouring continent to divide all the world's land into geopolitical regions. Under this scheme, most of the island countries and territories in the Pacific Ocean are grouped together with the continent of Australia to form a geopolitical region called Oceania.
Go to Article

Explanation by Hotspot Model

Youtube


    

Continent

Continent

Continent

A continent is one of several very large landmasses of the world. Generally identified by convention rather than any strict criteria, up to seven regions are commonly regarded as continents. Ordered from largest in area to smallest, they are: Asia, Africa, North America, South America, Antarctica, Europe, and Australia.[1]

Geologically, the continents largely correspond to areas of continental crust that are found on the continental plates. However, some areas of continental crust are regions covered with water not usually included in the list of continents. Zealandia is one such area (see submerged continents below).

Islands are frequently grouped with a neighbouring continent to divide all the world's land into geopolitical regions. Under this scheme, most of the island countries and territories in the Pacific Ocean are grouped together with the continent of Australia to form a geopolitical region called Oceania.

Definitions and application

By convention, "continents are understood to be large, continuous, discrete masses of land, ideally separated by expanses of water."[2] Several of the seven conventionally recognized continents are not discrete landmasses separated completely by water. The criterion "large" leads to arbitrary classification: Greenland, with a surface area of 2,166,086 square kilometres (836,330 sq mi) is considered the world's largest island, while Australia, at 7,617,930 square kilometres (2,941,300 sq mi) is deemed the smallest continent.

Earth's major landmasses all have coasts on a single, continuous World Ocean, which is divided into a number of principal oceanic components by the continents and various geographic criteria.[3][4]

Extent

The most restricted meaning of continent is that of a continuous[5] area of land or mainland, with the coastline and any land boundaries forming the edge of the continent. In this sense the term continental Europe (sometimes referred to in Britain as "the Continent") is used to refer to mainland Europe, excluding islands such as Great Britain, Ireland, Malta and Iceland, and the term continent of Australia may refer to the mainland of Australia, excluding Tasmania and New Guinea. Similarly, the continental United States refers to the 48 contiguous states and the District of Columbia in central North America and may include Alaska in the northwest of the continent (the two being separated by Canada), while excluding Hawaii, Puerto Rico, and Guam in the oceans.

From the perspective of geology or physical geography, continent may be extended beyond the confines of continuous dry land to include the shallow, submerged adjacent area (the continental shelf)[6] and the islands on the shelf (continental islands), as they are structurally part of the continent.[7]

From this perspective, the edge of the continental shelf is the true edge of the continent, as shorelines vary with changes in sea level.[8] In this sense the islands of Great Britain and Ireland are part of Europe, while Australia and the island of New Guinea together form a continent.

As a cultural construct, the concept of a continent may go beyond the continental shelf to include oceanic islands and continental fragments. In this way, Iceland is considered part of Europe and Madagascar part of Africa. Extrapolating the concept to its extreme, some geographers group the Australian continental plate with other islands in the Pacific into one continent called Oceania. This divides the entire land surface of Earth into continents or quasi-continents.[9]

Separation

The ideal criterion that each continent is a discrete landmass is commonly relaxed due to historical conventions. Of the seven most globally recognized continents, only Antarctica and Australia are completely separated from other continents by the ocean. Several continents are defined not as absolutely distinct bodies but as "more or less discrete masses of land".[10] Asia and Africa are joined by the Isthmus of Suez, and North and South America by the Isthmus of Panama. In both cases, there is no complete separation of these landmasses by water (disregarding the Suez Canal and Panama Canal, which are both narrow and shallow, as well as being artificial). Both these isthmuses are very narrow compared to the bulk of the landmasses they unite.

North America and South America are treated as separate continents in the seven-continent model. However, they may also be viewed as a single continent known as America or the Americas. This viewpoint was common in the United States until World War II, and remains prevalent in some Asian six-continent models.[11] This remains the more common vision in Latin American countries, Spain, Portugal, France, Italy, Greece and Hungary where they are taught as a single continent.

The criterion of a discrete landmass is completely disregarded if the continuous landmass of Eurasia is classified as two separate continents: Europe and Asia. Physiographically, Europe and South Asia are peninsulas of the Eurasian landmass. However, Europe is widely considered a continent with its comparatively large land area of 10,180,000 square kilometres (3,930,000 sq mi), while South Asia, with less than half that area, is considered a subcontinent. The alternative view—in geology and geography—that Eurasia is a single continent results in a six-continent view of the world. Some view separation of Eurasia into Asia and Europe as a residue of Eurocentrism: "In physical, cultural and historical diversity, China and India are comparable to the entire European landmass, not to a single European country. [...]."[12] However, for historical and cultural reasons,[which?] the view of Europe as a separate continent continues in several categorizations.[citation needed]

If continents are defined strictly as discrete landmasses, embracing all the contiguous land of a body, then Africa, Asia, and Europe form a single continent which may be referred to as Afro-Eurasia. This produces a four-continent model consisting of Afro-Eurasia, America, Antarctica and Australia.

When sea levels were lower during the Pleistocene ice ages, greater areas of continental shelf were exposed as dry land, forming land bridges. At those times Australia–New Guinea was a single, continuous continent. Likewise, the Americas and Afro-Eurasia were joined by the Bering land bridge. Other islands such as Great Britain were joined to the mainlands of their continents. At that time there were just three discrete continents: Afro-Eurasia-America, Antarctica, and Australia-New Guinea.

Number

There are several ways of distinguishing the continents:

Models
Color-coded map showing the various continents. Similar shades exhibit areas that may be consolidated or subdivided.
Four continents     Afro-Eurasia    America   Antarctica   Australia [13]
Five continents   Africa    Eurasia    America   Antarctica   Australia
Six continents   Africa   Asia   Europe    America   Antarctica   Australia/Oceania [14]
Six continents   Africa    Eurasia   North America   South America   Antarctica   Australia/Oceania [15][16]
Seven continents   Africa   Asia   Europe   North America   South America   Antarctica   Australia/Oceania [16][17][18][19][20][21]

The term Oceania refers to a group of island countries and territories in the Pacific Ocean, together with the continent of Australia.[14][18] Pacific islands with ties to other continents (such as Japan, Hawaii or Easter Island) are usually grouped with those continents rather than Oceania. This term is used in several different continental models instead of Australia.

Area and population

The following table summarizes the area and population of the continental regions used by the United Nations.[27] These regions differ from the physical continents in various ways that are explained in the notes.

Continent Area (km²)
[not in citation given]
Area (mi²)
[not in citation given]
Percent
total
landmass
[not in citation given]
Population Percent
total pop.
Most populous
city (proper)
Africa [note 1] 30,370,000 11,730,000 20.4% 1,287,920,000 16.9% Lagos, Nigeria
Antarctica [note 2] 14,000,000 5,400,000 9.2% 4,490[28] 0.0% McMurdo Station
Asia [note 3] 44,579,000 17,212,000 29.5% 4,545,133,000 59.5% Shanghai, China
Europe [note 4] 10,180,000 3,930,000 6.8% 742,648,000 9.7% Moscow, Russia[29]
North America [note 5] 24,709,000 9,540,000 16.5% 587,615,000 7.7% Mexico City, Mexico
Australia [note 6] 8,600,000 3,300,000 5.9% 41,261,000 0.5% Sydney, Australia
South America 17,840,000 6,890,000 12.0% 428,240,000 5.6% São Paulo, Brazil
  1. ^ Includes the Sinai Peninsula in Egypt.
  2. ^ Population is non-permanent and varies.
  3. ^ Includes East Thrace (Turkey) and Western New Guinea (Indonesia), excludes European Russia and Egypt.
  4. ^ Includes Asiatic Russia, excludes Turkey.
  5. ^ Includes Central America and the Caribbean.
  6. ^ Excludes Indonesia.

The total land area of all continents is 148,647,000 square kilometres (57,393,000 sq mi), or 29.1% of earth's surface (510,065,600 km2 or 196,937,400 sq mi).

Other divisions

Supercontinents

Aside from the conventionally known continents, the scope and meaning of the term continent varies. Supercontinents, largely in evidence earlier in the geological record, are landmasses that comprise more than one craton or continental core. These have included Laurasia, Gondwana, Vaalbara, Kenorland, Columbia, Rodinia, and Pangaea.

Subcontinents

Certain parts of continents are recognized as subcontinents, especially the large peninsulas separated from the main continental landmass by geographical features. The most notable examples are the Indian subcontinent and the Arabian Peninsula.[30] The Southern Cone of South America and Alaskan peninsula of North America are other examples.[30]

In many of these cases, the "subcontinents" concerned are on different tectonic plates from the rest of the continent, providing a geological justification for the terminology.[31] Greenland, generally reckoned as the world's largest island on the northeastern periphery of the North American Plate, is sometimes referred to as a subcontinent.[32][33] This is a significant departure from the more conventional view of a subcontinent as comprising a very large peninsula on the fringe of a continent.

Where the Americas are viewed as a single continent (America), it is divided into two subcontinents (North America and South America)[34][35][36] or three (with Central America being the third).[37][38] When Eurasia is regarded as a single continent, Europe is treated as a subcontinent.[30]

Submerged continents

Some areas of continental crust are largely covered by the sea and may be considered submerged continents. Notable examples are Zealandia, emerging from the sea primarily in New Zealand and New Caledonia, and the almost completely submerged Kerguelen Plateau in the southern Indian Ocean.

Microcontinents

Some islands lie on sections of continental crust that have rifted and drifted apart from a main continental landmass. While not considered continents because of their relatively small size, they may be considered microcontinents. Madagascar, the largest example, is usually considered an island of Africa but has been referred to as "the eighth continent" from a biological perspective[clarification needed].[39]

Botanical continents

"Continents" may be defined differently for specific purposes. The Biodiversity Information Standards organization has developed the World Geographical Scheme for Recording Plant Distributions, used in many international plant databases. This scheme divides the world into nine "botanical continents". Some match the traditional geographical continents, but some differ significantly. Thus the Americas are divided between Northern America (Mexico northwards) and Southern America (Central America and the Caribbean southwards) rather than between North America and South America.[40]

History of continental configurations

History of the concept

The Ancient Greek geographer Strabo holding a globe showing Europa and Asia

Early concepts of the Old World continents

The term "continent" translates Greek ἤπειρος, properly "landmass, terra firma", the proper name of Epirus and later especially used of Asia (i.e. Asia Minor),[41] The first distinction between continents was made by ancient Greek mariners who gave the names Europe and Asia to the lands on either side of the waterways of the Aegean Sea, the Dardanelles strait, the Sea of Marmara, the Bosporus strait and the Black Sea.[42] The names were first applied just to lands near the coast and only later extended to include the hinterlands.[43] But the division was only carried through to the end of navigable waterways and "... beyond that point the Hellenic geographers never succeeded in laying their finger on any inland feature in the physical landscape that could offer any convincing line for partitioning an indivisible Eurasia ..."[42]

Ancient Greek thinkers subsequently debated whether Africa (then called Libya) should be considered part of Asia or a third part of the world. Division into three parts eventually came to predominate.[44] From the Greek viewpoint, the Aegean Sea was the center of the world; Asia lay to the east, Europe to the north and west, and Africa to the south.[45] The boundaries between the continents were not fixed. Early on, Europe–Asia boundary was taken to run from the Black Sea along the Rioni River (known then as the Phasis) in Georgia. Later it was viewed as running from the Black Sea through Kerch Strait, the Sea of Azov and along the Don River (known then as the Tanais) in Russia.[46] The boundary between Asia and Africa was generally taken to be the Nile River. Herodotus[47] in the 5th century BC, however, objected to the unity of Egypt being split into Asia and Africa ("Libya") and took the boundary to lie along the western border of Egypt, regarding Egypt as part of Asia. He also questioned the division into three of what is really a single landmass,[48] a debate that continues nearly two and a half millennia later.

Eratosthenes, in the 3rd century BC, noted that some geographers divided the continents by rivers (the Nile and the Don), thus considering them "islands". Others divided the continents by isthmuses, calling the continents "peninsulas". These latter geographers set the border between Europe and Asia at the isthmus between the Black Sea and the Caspian Sea, and the border between Asia and Africa at the isthmus between the Red Sea and the mouth of Lake Bardawil on the Mediterranean Sea.[49]

Through the Roman period and the Middle Ages, a few writers took the Isthmus of Suez as the boundary between Asia and Africa, but most writers continued to consider it the Nile or the western border of Egypt (Gibbon)[citation needed]. In the Middle Ages, the world was usually portrayed on T and O maps, with the T representing the waters dividing the three continents. By the middle of the 18th century, "the fashion of dividing Asia and Africa at the Nile, or at the Great Catabathmus [the boundary between Egypt and Libya] farther west, had even then scarcely passed away".[50]

European arrival in the Americas

Christopher Columbus sailed across the Atlantic Ocean to the West Indies in 1492, sparking a period of European exploration of the Americas. But despite four voyages to the Americas, Columbus never believed he had reached a new continent—he always thought it was part of Asia.

In 1501, Amerigo Vespucci and Gonçalo Coelho attempted to sail around what they considered the southern end of the Asian mainland into the Indian Ocean, passing through Fernando de Noronha. After reaching the coast of Brazil, they sailed a long way further south along the coast of South America, confirming that this was a land of continental proportions and that it also extended much further south than Asia was known to.[51] On return to Europe, an account of the voyage, called Mundus Novus ("New World"), was published under Vespucci's name in 1502 or 1503,[52] although it seems that it had additions or alterations by another writer.[53] Regardless of who penned the words, Mundus Novus credited Vespucci with saying, "I have discovered a continent in those southern regions that is inhabited by more numerous people and animals than our Europe, or Asia or Africa",[54] the first known explicit identification of part of the Americas as a continent like the other three.

Within a few years, the name "New World" began appearing as a name for South America on world maps, such as the Oliveriana (Pesaro) map of around 1504–1505. Maps of this time though, still showed North America connected to Asia and showed South America as a separate land.[53]

Universalis Cosmographia, Waldseemüller's 1507 world map—the first to show the Americas separate from Asia

In 1507 Martin Waldseemüller published a world map, Universalis Cosmographia, which was the first to show North and South America as separate from Asia and surrounded by water. A small inset map above the main map explicitly showed for the first time the Americas being east of Asia and separated from Asia by an ocean, as opposed to just placing the Americas on the left end of the map and Asia on the right end. In the accompanying book Cosmographiae Introductio, Waldseemüller noted that the earth is divided into four parts, Europe, Asia, Africa and the fourth part, which he named "America" after Amerigo Vespucci's first name.[55] On the map, the word "America" was placed on part of South America.

The word continent

From the 16th century the English noun continent was derived from the term continent land, meaning continuous or connected land[56] and translated from the Latin terra continens.[57] The noun was used to mean "a connected or continuous tract of land" or mainland.[56] It was not applied only to very large areas of land—in the 17th century, references were made to the continents (or mainlands) of Isle of Man, Ireland and Wales and in 1745 to Sumatra.[56] The word continent was used in translating Greek and Latin writings about the three "parts" of the world, although in the original languages no word of exactly the same meaning as continent was used.[58]

While continent was used on the one hand for relatively small areas of continuous land, on the other hand geographers again raised Herodotus's query about why a single large landmass should be divided into separate continents. In the mid-17th century, Peter Heylin wrote in his Cosmographie that "A Continent is a great quantity of Land, not separated by any Sea from the rest of the World, as the whole Continent of Europe, Asia, Africa." In 1727, Ephraim Chambers wrote in his Cyclopædia, "The world is ordinarily divided into two grand continents: the old and the new." And in his 1752 atlas, Emanuel Bowen defined a continent as "a large space of dry land comprehending many countries all joined together, without any separation by water. Thus Europe, Asia, and Africa is one great continent, as America is another."[59] However, the old idea of Europe, Asia and Africa as "parts" of the world ultimately persisted with these being regarded as separate continents.

Beyond four continents

From the late 18th century, some geographers started to regard North America and South America as two parts of the world, making five parts in total. Overall though, the fourfold division prevailed well into the 19th century.[60]

Europeans discovered Australia in 1606, but for some time it was taken as part of Asia. By the late 18th century, some geographers considered it a continent in its own right, making it the sixth (or fifth for those still taking America as a single continent).[60] In 1813, Samuel Butler wrote of Australia as "New Holland, an immense island, which some geographers dignify with the appellation of another continent" and the Oxford English Dictionary was just as equivocal some decades later.[61]

Antarctica was sighted in 1820 during the First Russian Antarctic Expedition and described as a continent by Charles Wilkes on the United States Exploring Expedition in 1838, the last continent identified, although a great "Antarctic" (antipodean) landmass had been anticipated for millennia. An 1849 atlas labelled Antarctica as a continent but few atlases did so until after World War II.[62]

From the mid-19th century, atlases published in the United States more commonly treated North and South America as separate continents, while atlases published in Europe usually considered them one continent. However, it was still not uncommon for American atlases to treat them as one continent up until World War II.[63]

From the 1950s, most U.S. geographers divided the Americas into two continents.[63] With the addition of Antarctica, this made the seven-continent model. However, this division of the Americas never appealed to Latin Americans, who saw their region spanning an América as a single landmass, and there the conception of six continents remains dominant, as it does in scattered other countries.[citation needed]

Some geographers regard Europe and Asia together as a single continent, dubbed Eurasia.[64] In this model, the world is divided into six continents, with North America and South America considered separate continents.

Geology

Geologists use the term continent in a different manner from geographers. In geology a continent is defined by continental crust: a platform of metamorphic and igneous rock, largely of granitic composition. Some geologists restrict the term 'continent' to portions of the crust built around stable Precambrian "shield", typically 1.5 to 3.8 billion years old, called a craton. The craton itself is an accretionary complex of ancient mobile belts (mountain belts) from earlier cycles of subduction, continental collision and break-up from plate tectonic activity. An outward-thickening veneer of younger minimally deformed sedimentary rock covers much of the craton. The margins of geologic continents are characterized by currently active or relatively recently active mobile belts and deep troughs of accumulated marine or deltaic sediments. Beyond the margin, there is either a continental shelf and drop off to the basaltic ocean basin or the margin of another continent, depending on the current plate-tectonic setting of the continent. A continental boundary does not have to be a body of water. Over geologic time, continents are periodically submerged under large epicontinental seas, and continental collisions result in a continent becoming attached to another continent. The current geologic era is relatively anomalous in that so much of the continental areas are "high and dry"; that is, many parts of the continents that were once below sea level are now elevated well above it due to changes in sea levels and the subsequent uplifting of those continental areas from tectonic activity.[65]

The tectonic plates underlying the continents and oceans

Some argue that continents are accretionary crustal "rafts" that, unlike the denser basaltic crust of the ocean basins, are not subjected to destruction through the plate tectonic process of subduction. This accounts for the great age of the rocks comprising the continental cratons. By this definition, Eastern Europe, India and some other regions could be regarded as continental masses distinct from the rest of Eurasia because they have separate ancient shield areas (i.e. East European craton and Indian craton). Younger mobile belts (such as the Ural Mountains and Himalayas) mark the boundaries between these regions and the rest of Eurasia.

There are many microcontinents, or continental fragments, that are built of continental crust but do not contain a craton. Some of these are fragments of Gondwana or other ancient cratonic continents: Zealandia, which includes New Zealand and New Caledonia; Madagascar; the northern Mascarene Plateau, which includes the Seychelles. Other islands, such as several in the Caribbean Sea, are composed largely of granitic rock as well, but all continents contain both granitic and basaltic crust, and there is no clear boundary as to which islands would be considered microcontinents under such a definition. The Kerguelen Plateau, for example, is largely volcanic, but is associated with the breakup of Gondwanaland and is considered a microcontinent,[66][67] whereas volcanic Iceland and Hawaii are not. The British Isles, Sri Lanka, Borneo, and Newfoundland are margins of the Laurasian continent—only separated by inland seas flooding its margins.

Plate tectonics offers yet another way of defining continents. Today, Europe and most of Asia constitute the unified Eurasian Plate, which is approximately coincident with the geographic Eurasian continent excluding India, Arabia, and far eastern Russia. India contains a central shield, and the geologically recent Himalaya mobile belt forms its northern margin. North America and South America are separate continents, the connecting isthmus being largely the result of volcanism from relatively recent subduction tectonics. North American continental rocks extend to Greenland (a portion of the Canadian Shield), and in terms of plate boundaries, the North American plate includes the easternmost portion of the Asian landmass. Geologists do not use these facts to suggest that eastern Asia is part of the North American continent, even though the plate boundary extends there; the word continent is usually used in its geographic sense and additional definitions ("continental rocks," "plate boundaries") are used as appropriate.

The movement of plates has caused the formation and break-up of continents over time, including occasional formation of a supercontinent that contains most or all of the continents. The supercontinent Columbia or Nuna formed during a period of 2.0–1.8 billion years ago and broke up about 1.5–1.3 billion years ago.[68][69] The supercontinent Rodinia is thought to have formed about 1 billion years ago and to have embodied most or all of Earth's continents, and broken up into eight continents around 600 million years ago. The eight continents later re-assembled into another supercontinent called Pangaea; Pangaea broke up into Laurasia (which became North America and Eurasia) and Gondwana (which became the remaining continents).

Highest and lowest points

The following table lists the seven continents with their highest and lowest points on land, sorted in decreasing highest points.

Continent Highest point Elevation (m) Elevation (ft) Country or territory containing highest point Lowest point Elevation (m) Elevation (ft) Country or territory containing lowest point
Asia Mount Everest 8,848 29,029 China and Nepal Dead Sea −427 −1,401 Israel, Jordan and Palestine
South America Aconcagua 6,960 22,830 Argentina Laguna del Carbón −105 −344 Argentina
North America Denali 6,198 20,335 United States Death Valley −86 −282 United States
Africa Mount Kilimanjaro 5,895 19,341 Tanzania Lake Assal −155 −509 Djibouti
Europe Mount Elbrus 5,642 18,510 Russia Caspian Sea −28 −92 Russia
Antarctica Vinson Massif 4,892 16,050 (none) Deep Lake, Vestfold Hills −50 −160 (none)
Australia Puncak Jaya 4,884 16,024 Indonesia (Papua) Lake Eyre −15 −49 Australia

† The lowest exposed points are given for North America and Antarctica. The lowest non-submarine bedrock elevations in these continents are the trough beneath Jakobshavn Glacier (−1,512 metres (−4,961 ft)[70]) and Bentley Subglacial Trench (−2,540 metres (−8,330 ft)), but these are covered by kilometers of ice.

Some sources list the Kuma–Manych Depression (a remnant of the Paratethys) as the geological border between Europe and Asia. This would place the Caucasus outside of Europe, thus making Mont Blanc (elevation 4810 m) in the Graian Alps the highest point in Europe – the lowest point would still be the shore of the Caspian Sea.

See also



This article uses material from the Wikipedia article "Continent", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Countries & Continents

3D,cad,europe,americas,apac,emea,asia,australia,africa,