powered by CADENAS

Social Share

Recyclebot (2433 views - 3D Printing Dictionary)

A recyclebot (or RecycleBot) is an open-source hardware device for converting waste plastic into filament for open-source 3D printers like the RepRap. Making DIY 3D printer filament at home is both less costly and better for the environment than purchasing conventional 3D printer filament.
Go to Article

Recyclebot

Recyclebot

A recyclebot (or RecycleBot) is an open-source hardware device for converting waste plastic into filament for open-source 3D printers like the RepRap.[1] Making DIY 3D printer filament at home is both less costly and better for the environment than purchasing conventional 3D printer filament.[2][3][4]

Recyclebot technology

RepRap 3D printers have been shown to reduce costs for consumers by offsetting purchases that can be printed.[5][6][7][8] The RepRap's plastic feedstock is one area where cost can still be reduced. In 2014 professor Joshua Pearce pointed out that "Filament is retailing for between $36 and $50 a kilogram and you can produce your own filament for 10 cents a kilogram if you use recycled plastic"[9] The device can thus further enhance RepRap affordability by reducing operating costs.[10] In addition, to assisting prosumers to reduce their reliance on purchased products, following an open source model, the RepRap and the recyclebot, have made it feasible for 3D printing to be used for small-scale manufacturing to aid sustainable development.[11][12]

The RecycleBot is an open-source hardware project – thus its plans are freely available on the Internet.

It has been postulated that recycled filament production could also offer an alternative income source by the Ethical Filament Foundation[15][16] or as a form of "fair trade filament".[17] It has also been shown to improve the energy payback time of even known green energy technologies like solar photovoltaics.[18]

History

The history of the RecycleBot was largely derived from the work on the RepRap Wiki under GNU Free Documentation License1.2.[19]

The first recyclebot was developed by students at Victoria University of Wellington, New Zealand.[20][21][22] This design was a proof of concept and was a hand-powered design, which thus had a good environmental or ecological footprint, but did not create filament of high enough quality to be useful for 3D printers. The design for the waste plastic extruder (Recyclebot v2.0 and v2.1) developed at Queen's University Canada and Michigan Tech was heavily influenced by the Web4Deb extruder, which extrudes HDPE for use as a growth medium in aquaponics.[23] This design for the recyclebot was developed, tested and published in the peer-reviewed rapid prototyping literature.[24] This device proved viable for producing 3D printing filament. The Recyclebot v2.2 is now being carried out by the Michigan Tech in Open Sustainability Technology Research Group.[25] Many makers or DIY enthusiasts have made various versions of RecycleBots, with the most notable being the Lyman Filament Extruder as Lyman, a retired engineer won a design contest to make a low-cost 3D filament fabrication system.[26] There are now many types of recyclebots, many of which are at the early stages of commercialization (in 2014).

Commercialization

Several versions of open-source RecycleBots have been commercialized via crowd funding such as a with Kickstarter that include:

Futurist speculation

Jeremy Rifkin has hypothesized that such recycling with recyclebots and distributed production with 3D printing will lead to a zero marginal cost society.[31] The science-fiction author, Bruce Sterling wondered in Wired if recyclebots and 3D printers might be used to turn waste into guns.[32] Recyclebots can provide a new method of recycling.[33]

  1. ^ Baechler, Christian; DeVuono, Matthew; Pearce, Joshua M. (2013). "Distributed Recycling of Waste Polymer into RepRap Feedstock". Rapid Prototyping Journal. 19 (2): 118–125. doi:10.1108/13552541311302978. 
  2. ^ Kreiger, M.A.; Mulder, M.L.; Glover, A.G.; Pearce, J. M. "Life Cycle Analysis of Distributed Recycling of Post-consumer High Density Polyethylene for 3-D Printing Filament". Journal of Cleaner Production. 70: 90–96. doi:10.1016/j.jclepro.2014.02.009. 
  3. ^ The importance of the Lyman Extruder, Filamaker, Recyclebot and Filabot to 3D printing – VoxelFab, 2013.
  4. ^ Kreiger, M.; Anzalone, G. C.; Mulder, M. L.; Glover, A.; Pearce, J. M (2013). "Distributed Recycling of Post-Consumer Plastic Waste in Rural Areas". MRS Online Proceedings Library. 1492. doi:10.1557/opl.2013.258. 
  5. ^ B.T. Wittbrodt, A.G. Glover, J. Laureto, G.C. Anzalone, D. Oppliger, J.L. Irwin, J.M. Pearce (2013), Life-cycle economic analysis of distributed manufacturing with open-source 3-D printers, Mechatronics, 23 (2013), pp. 713–726. open access
  6. ^ Study: At-home 3-D printing could save consumers 'thousands' – CNN, 2013
  7. ^ Printing Keychains and Shower Heads: 3-D Printing Goes Beyond the Lab – ABC News
  8. ^ A 3-D Printer Can Pay For Itself In Less Than A Year – Popular Science, 2013
  9. ^ Turning old plastic into 3D printer filament is greener than conventional recycling – 3Ders, 2014
  10. ^ Study: At-home 3-D printing could save consumers 'thousands' – CNN, 2013
  11. ^ 3-D Printing of Open Source Appropriate Technologies for Self-Directed Sustainable Development
  12. ^ DJ Pangburn. 2014.How 3D Printers Are Boosting Off-The-Grid, Underdeveloped Communities - MotherBoard
  13. ^ http://www.thingiverse.com/thing:12948
  14. ^ http://www.thingiverse.com/thing:54180
  15. ^ http://techfortrade.org/our-initiatives/3d4d-challenge/the-ethical-filament-foundation/ Tech for Trade – Ethical Filament Foundation
  16. ^ Charity Targets 3D Printing’s Plastic Waste Problem With Standards For An Ethical Alternative 7 November 2013 by Natasha Lomas, Tech Crunch, http://techcrunch.com/2013/11/07/ethical-additive-manufacturing/
  17. ^ Feeley, S. R.; Wijnen, B.; Pearce, J. M. (2014). "Evaluation of Potential Fair Trade Standards for an Ethical 3-D Printing Filament". Journal of Sustainable Development. 7 (5): 1–12. doi:10.5539/jsd.v7n5p1. 
  18. ^ Shan Zhong, S. et al. Energy Payback Time of a Solar Photovoltaic Powered Waste Plastic Recyclebot System. Recycling 2017, 2(2), 10; doi: 10.3390/recycling2020010
  19. ^ http://reprap.org/wiki/Recyclebot
  20. ^ Burgess, Phil (5 August 2010). "Recyclebot digests milk jugs to feed MakerBot". hackaday.com/. hackaday. 
  21. ^ Duann (3 August 2010). "RecycleBot: Greening the MakerBot". The Shapeways Blog. shapeways. 
  22. ^ Pettis, Bre (3 August 2010). "Recyclebot makes HDPE for your MakerBot from Milk Jugs!". makerbot.com blog. makerbot. 
  23. ^ Web4Deb's blog.
  24. ^ Baechler, Christian; DeVuono, Matthew; Pearce, Joshua M. "Distributed Recycling of Waste Polymer into RepRap Feedstock". Rapid Prototyping Journal. 19 (2): 118–125. doi:10.1108/13552541311302978. 
  25. ^ [1]
  26. ^ Harry McCracken (4 March 2013). "How an 83-Year-Old Inventor Beat the High Cost of 3D Printing". Time. 
  27. ^ Filastruder
  28. ^ Filafab
  29. ^ Filabot
  30. ^ Felfil Evo
  31. ^ Jeremy Rifkin, Zero Marginal Cost Society, Palgrave Macmillan, 2014.
  32. ^ 3D Printed gun moving from sinister joke to sinister business model By Bruce Sterling – Wired – Beyond the Beyond
  33. ^ Baltodano, S. (2013). RISE. http://www.mme.fiu.edu/wp-content/uploads/2013/12/F13-OR-T-4.pdf


This article uses material from the Wikipedia article "Recyclebot", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

3D Printing Dictionary

OpenLAB, Fablab, OpenSCAD, FreeCAD, BRL-CAD, RhinocerosCAD, LibreCAD, Vectary, 123D, TinkerCAD, Wings 3D, MOI3D, leapfrog 3D, Geomagic, Paint3D, STLfinder, Yeggi, Yobi3D, 3D Shape Search, PARTcloud, Thingiverse, GrabCAD, AMF, Additive Manufacturing, STL, Stereolitography, Mesh, MeshMixer, Free Download, lowpoly, 3D voxel,things, digital design, physical objects, rapid prototyping, 3D objects, 3D printing, reprap, fabrication, laser cutter,abs