powered by CADENAS

Social Share

Amazon

Diagram (179 views - Basics)

A diagram is a symbolic representation of information according to visualization technique. Diagrams have been used since ancient times, but became more prevalent during the Enlightenment. Sometimes, the technique uses a three-dimensional visualization which is then projected onto a two-dimensional surface. The word graph is sometimes used as a synonym for diagram.
Go to Article

Explanation by Hotspot Model

Diagram

Diagram

Diagram

A diagram is a symbolic representation of information according to visualization technique. Diagrams have been used since ancient times, but became more prevalent during the Enlightenment.[1] Sometimes, the technique uses a three-dimensional visualization which is then projected onto a two-dimensional surface. The word graph is sometimes used as a synonym for diagram.

Overview

The term "diagram" in its commonly used sense can have a general or specific meaning:

  • visual information device : Like the term "illustration", "diagram" is used as a collective term standing for the whole class of technical genres, including graphs, technical drawings and tables.[2]
  • specific kind of visual display : This is the genre that shows qualitative data with shapes that are connected by lines, arrows, or other visual links.

In science the term is used in both ways. For example, Anderson (1997) stated more generally: "diagrams are pictorial, yet abstract, representations of information, and maps, line graphs, bar charts, engineering blueprints, and architects' sketches are all examples of diagrams, whereas photographs and video are not".[3] On the other hand, Lowe (1993) defined diagrams as specifically "abstract graphic portrayals of the subject matter they represent".[4]

In the specific sense diagrams and charts contrast with computer graphics, technical illustrations, infographics, maps, and technical drawings, by showing "abstract rather than literal representations of information".[2] The essence of a diagram can be seen as:[2]

  • a form of visual formatting devices
  • a display that does not show quantitative data (numerical data), but rather relationships and abstract information
  • with building blocks such as geometrical shapes connected by lines, arrows, or other visual links.

Or in Hall's (1996) words "diagrams are simplified figures, caricatures in a way, intended to convey essential meaning".[5] These simplified figures are often based on a set of rules. The basic shape according to White (1984) can be characterized in terms of "elegance, clarity, ease, pattern, simplicity, and validity".[2] Elegance is basically determined by whether or not the diagram is "the simplest and most fitting solution to a problem".[6]

Main diagram types

There are at least the following types of diagrams:

  • Chart-like diagrams, which take a collection of items and relationships between them, and express them by giving each item a 2D position, while the relationships are expressed as connections between the items or overlaps between the items; examples of such techniques:
  • Graph-based diagrams; these display a relationship between two variables that take either discrete or a continuous ranges of values; examples:

Schematics and other types of diagrams, e.g.,

Many of these types of diagrams are commonly generated using diagramming software such as Visio and Gliffy. Thousands of diagram techniques exist. Some more examples follow.

Diagrams may also be classified according to use or purpose, for example, explanatory and/or how to diagrams.

Specific diagram types

See also



This article uses material from the Wikipedia article "Diagram", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Basics

3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted