powered by CADENAS

Social Share

Amazon

Specular reflection (231 views - Basics)

Specular reflection, also known as regular reflection, is the mirror-like reflection of waves, such as light, from a surface. In this process, each incident ray is reflected at the same angle to the surface normal as the incident ray, but on the opposing side of the surface normal in the plane formed by incident and reflected rays. The result is that an image reflected by the surface is reproduced in mirror-like (specular) fashion. The law of reflection states that for each incident ray the angle of incidence equals the angle of reflection, and the incident, normal, and reflected directions are coplanar. This behavior was first described by Hero of Alexandria (AD c. 10–70). It may be contrasted with diffuse reflection, in which light is scattered away from the surface in a range of directions rather than just one.
Go to Article

Explanation by Hotspot Model

Youtube


    

Specular reflection

Specular reflection

Specular reflection

Licensed under Creative Commons Attribution-Share Alike 3.0 (No machine-readable author provided. Arvelius assumed (based on copyright claims).).

Specular reflection, also known as regular reflection, is the mirror-like reflection of waves, such as light, from a surface. In this process, each incident ray is reflected at the same angle to the surface normal as the incident ray, but on the opposing side of the surface normal in the plane formed by incident and reflected rays. The result is that an image reflected by the surface is reproduced in mirror-like (specular) fashion.

The law of reflection states that for each incident ray the angle of incidence equals the angle of reflection, and the incident, normal, and reflected directions are coplanar. This behavior was first described by Hero of Alexandria (AD c. 10–70).[1] It may be contrasted with diffuse reflection, in which light is scattered away from the surface in a range of directions rather than just one.

Background

When light hits a surface, there are three possible outcomes.[2] Light may be absorbed by the material, light may be transmitted through the surface, or light may be reflected. Materials often show some mix of these behaviors, with the proportion of light that goes to each depending on the properties of the material, the wavelength of the light, and the angle of incidence. For most interfaces between materials, the fraction of the light that is reflected increases with increasing angle of incidence .

Reflected light can be divided into two sub-types, specular reflection and diffuse reflection. Specular reflection reflects all light which arrives from a given direction at the same angle, whereas diffuse reflection reflects that light in a broad range of directions. An example of the distinction between specular and diffuse reflection would be glossy and matte paints. Matte paints have almost exclusively diffuse reflection, while glossy paints have both specular and diffuse reflection. A surface built from a non-absorbing powder, such as plaster, can be a nearly perfect diffuser, whereas polished metallic objects can specularly reflect light very efficiently. The reflecting material of mirrors is usually aluminum or silver.

Law of reflection

The law of reflection describes the angle of reflected light: the angle of incident light is the same as the angle of the reflected light.

The law of reflection arises from diffraction of a plane wave with small wavelength on a flat boundary: when the boundary size is much larger than the wavelength, then electrons of the boundary are seen oscillating exactly in phase only from one direction – the specular direction. If a mirror becomes very small compared to the wavelength, the law of reflection no longer holds, and the behavior of light is more complicated.

Vector formulation

The law of reflection can also be equivalently expressed using linear algebra. The direction of a reflected ray is determined by the vector of incidence and the surface normal vector. Given an incident direction from the surface to the light source and the surface normal direction the specularly reflected direction (all unit vectors) is:[3][4]

where is a scalar obtained with the dot product. Different authors may define the incident and reflection directions with different signs. Assuming these Euclidean vectors are represented in column form, the equation can be equivalently expressed as a matrix-vector multiplication:

where is the so-called Householder transformation matrix, defined as:

in terms of the identity matrix and twice the outer product of .

Reflectivity

Reflectivity is the ratio of the power of the reflected wave to that of the incident wave. It is a function of the wavelength of radiation, and is related to the refractive index of the material as expressed by Fresnel's equations.[5] In regions of the electromagnetic spectrum in which absorption by the material is significant, it is related to the electronic absorption spectrum through the imaginary component of the complex refractive index. The electronic absorption spectrum of an opaque material, which is difficult or impossible to measure directly, may therefore be indirectly determined from the reflection spectrum by a Kramers-Kronig transform. The polarization of the reflected light depends on the symmetry of the arrangement of the incident probing light with respect to the absorbing transitions dipole moments in the material.

Measurement of specular reflection is performed with normal or varying incidence reflection spectrophotometers (reflectometer) using a scanning variable-wavelength light source. Lower quality measurements using a glossmeter quantify the glossy appearance of a surface in gloss units.

Consequences

Internal reflection

When light is propagating in a material and strikes an interface with a material of lower index of refraction, some of the light is reflected. If the angle of incidence is greater than the critical angle, total internal reflection occurs: all of the light is reflected. The critical angle can be shown to be given by

Polarization

When light strikes an interface between two materials, the reflected light is generally partially polarized. However, if the light strikes the interface at Brewster's angle, the reflected light is completely linearly polarized parallel to the interface. Brewster's angle is given by

Reflected images

The image in a flat mirror has these features:

  • It is the same distance behind the mirror as the object is in front.
  • It is the same size as the object.
  • It is the right way up (erect).
  • It is reversed.
  • It is virtual, meaning that the image appears to be behind the mirror, and cannot be projected onto a screen.

The reversal of images by a plane mirror is perceived differently depending on the circumstances. In many cases, the image in a mirror appears to be reversed from left to right. If a flat mirror is mounted on the ceiling it can appear to reverse up and down if a person stands under it and looks up at it. Similarly a car turning left will still appear to be turning left in the rear view mirror for the driver of a car in front of it. The reversal of directions, or lack thereof, depends on how the directions are defined. More specifically a mirror changes the handedness of the coordinate system, one axis of the coordinate system appears to be reversed, and the chirality of the image may change. For example, the image of a right shoe will look like a left shoe.

Examples

A classic example of specular reflection is a mirror, which is specifically designed for specular reflection.

In addition to visible light, specular reflection can be observed in the ionospheric reflection of radiowaves and the reflection of radio- or microwave radar signals by flying objects. The measurement technique of x-ray reflectivity exploits specular reflectivity to study thin films and interfaces with sub-nanometer resolution, using either modern laboratory sources or synchrotron x-rays.

Non-electromagnetic waves can also exhibit specular reflection, as in acoustic mirrors which reflect sound, and atomic mirrors, which reflect neutral atoms. For the efficient reflection of atoms from a solid-state mirror, very cold atoms and/or grazing incidence are used in order to provide significant quantum reflection; ridged mirrors are used to enhance the specular reflection of atoms. Neutron reflectometry uses specular reflection to study material surfaces and thin film interfaces in an analogous fashion to x-ray reflectivity.

See also



This article uses material from the Wikipedia article "Specular reflection", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Basics

3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted