powered by CADENAS

Social Share

Wrench (14043 views - Tooling)

A wrench (or spanner outside of North America) is a tool used to provide grip and mechanical advantage in applying torque to turn objects—usually rotary fasteners, such as nuts and bolts—or keep them from turning. In Commonwealth English (excluding Canada), spanner is the standard term. The most common shapes are called open-ended spanner and ring spanner. The term wrench is generally used for tools that turn non-fastening devices (e.g. tap wrench and pipe wrench), or may be used for a monkey wrench - an adjustable spanner. In North American English, wrench is the standard term. The most common shapes are called open-end wrench and box-end wrench. In American English, spanner refers to a specialised wrench with a series of pins or tabs around the circumference. (These pins or tabs fit into the holes or notches cut into the object to be turned.) In American commerce, such a wrench may be called a spanner wrench to distinguish it from the British sense of spanner. Higher quality wrenches are typically made from chromium-vanadium alloy tool steels and are often drop-forged. They are frequently chrome-plated to resist corrosion and for ease of cleaning. Hinged tools, such as pliers or tongs, are not generally considered wrenches in English, but exceptions are the plumber wrench (pipe wrench in British English) and Mole wrench (sometimes Mole grips in British English). The word can also be used in slang to describe an unexpected obstacle, for example, "He threw a spanner into our plans" (in U.S. English, "monkey wrench").
Go to Article

Explanation by Hotspot Model

Wrench

Wrench

A wrench (or spanner outside of North America) is a tool used to provide grip and mechanical advantage in applying torque to turn objects—usually rotary fasteners, such as nuts and bolts—or keep them from turning.

In Commonwealth English (excluding Canada), spanner is the standard term. The most common shapes are called open-ended spanner and ring spanner. The term wrench is generally used for tools that turn non-fastening devices (e.g. tap wrench and pipe wrench), or may be used for a monkey wrench - an adjustable spanner.[1]

In North American English, wrench is the standard term. The most common shapes are called open-end wrench and box-end wrench. In American English, spanner refers to a specialised wrench with a series of pins or tabs around the circumference. (These pins or tabs fit into the holes or notches cut into the object to be turned.) In American commerce, such a wrench may be called a spanner wrench to distinguish it from the British sense of spanner.

Higher quality wrenches are typically made from chromium-vanadium alloy tool steels and are often drop-forged. They are frequently chrome-plated to resist corrosion and for ease of cleaning.

Hinged tools, such as pliers or tongs, are not generally considered wrenches in English, but exceptions are the plumber wrench (pipe wrench in British English) and Mole wrench (sometimes Mole grips in British English).

The word can also be used in slang to describe an unexpected obstacle, for example, "He threw a spanner into our plans" (in U.S. English, "monkey wrench").

History

Wrenches and applications using wrenches or devices that needed wrenches, such as pipe clamps and suits of armor, have been noted by historians as far back as the 15th century.[2] Adjustable coach wrenches for the odd-sized nuts of wagon wheels were manufactured in England and exported to North America in the late eighteenth and early nineteenth centuries. The mid 19th century began to see patented wrenches which used a screw to narrowing or widening the jaws, including patented monkey wrenches.

Types

American name British/Commonwealth name Description Group
open-end wrench open-ended spanner A one-piece wrench with a U-shaped opening that grips two opposite faces of the bolt or nut. This wrench is often double-ended, with a different-sized opening at each end. The ends are generally oriented at an angle of around 15 degrees to the longitudinal axis of the handle. This allows a greater range of movement in enclosed spaces by flipping the wrench over. common
box-end wrench ring spanner A one-piece wrench with an enclosed opening that grips the faces of the bolt or nut. The recess is generally a six-point or twelve-point opening for use with nuts or bolt heads with a hexagonal shape. The twelve-point fits onto the fastening at twice as many angles, an advantage where swing is limited. Eight-point wrenches are also made for square-shaped nuts and bolt heads. Ring spanners are often double-ended and usually with offset handles to improve access to the nut or bolt. common
combination wrench combination spanner
open-ring spanner
A double-ended tool with one end being like an open-end wrench or open-ended spanner, and the other end being like a box-end wrench or ring spanner. Both ends generally fit the same size of bolt. common
flare-nut wrench
tube wrench
line wrench
flare spanner
flare nut spanner
brake spanner
crow's-foot spanner
A wrench that is used for gripping the nuts on the ends of tubes. It is similar to a box-end wrench but, instead of encircling the nut completely, it has a narrow opening just wide enough to allow the wrench to fit over the tube, and thick jaws to increase the contact area with the nut. This allows for maximum contact on plumbing nuts, which are typically softer metals and therefore more prone to damage from open-ended wrenches. common
ratcheting box wrench ratcheting ring spanner A type of ring spanner, or box wrench, whose end section ratchets. Ratcheting can be reversed by flipping over the wrench, or by activating a reversing lever on the wrench. This type of wrench combines compact design of a box wrench, with the utility and quickness of use of a ratchet wrench. A variety of ratcheting mechanisms are used, from simple pawls to more complex captured rollers, with the latter being more compact, smoother, but also more expensive to manufacture. The one pictured also features a drift pin on the tail. common
flex-head socket wrench
Saltus wrench
scaffolders spanner Similar in concept to a socket wrench. A Saltus wrench features a socket permanently affixed to a handle. Sockets are not interchangeable as with a socket wrench. The socket often rotates around the handle to allow the user to access a fastener from a variety of angles. Commonly a Saltus wrench is part of a double-ended wrench, with an open-end type head on the opposite side from the socket head. common
spanner wrench or simply spanner [referring to any of these]; [when specifying pin vs hook vs C, the same terms are used as in British English] pin spanner
hook spanner
C spanner
pin face spanner
A wrench with one or several pins or hooks, designed to drive spanner head screws, threaded collars and retainer rings, shafts, and so on. Note the difference in the American and British senses of the word "spanner". In American English, "spanners" are a subset of the class of tools called "wrenches". common
striking face box wrench
slammer wrench
slugger wrench
hammer wrench
slogging spanner
flogging spanner
This is a specialized thick, short, stocky wrench with a block end to the handle specifically designed for use with a hammer, enabling one to impart great force. Used commonly with large fasteners, especially a nut and stud which both have index marks: the nut is screwed hand-tight, then further tightened with the striking wrench a known number of index marks calculated from the elasticity of the bolt or stud, thus giving precise torque (preload). Striking wrenches also provide shock and high force used to release large and/or stuck nuts and bolts; and when space does not allow room for a large wrench. common
adjustable wrench
adjustable end wrench
Crescent wrench
adjustable spanner
shifting spanner
shifter
wrench
The most common type of adjustable wrench in use today. The adjustable end wrench differs from the monkey wrench in that the gripping faces of the jaws are displaced to a (typically) 15 degree angle relative to the tool's handle, a design feature that facilitates the wrench's use in close quarters. The modern adjustable end wrench was invented by Johan Petter Johansson [3]of Bahco. The common use of "Crescent wrench" to describe this design is derived from the Crescent brand, owned by Apex Brands, Inc. Apex Tool Group, LLC. adjustable
self-adjusting wrench self-adjusting spanner
With a serrated jaw which is self-tightening. adjustable
monkey wrench gas grips
King Dick
An old type of adjustable wrench with a straight handle and smooth jaws whose gripping faces are perpendicular to the handle. historical
pipe wrench Stillson wrench
Stillsons
Pipe wrench
A tool that is similar in design and appearance to a monkey wrench, but with self-tightening properties and hardened, serrated jaws that securely grip soft iron pipe and pipe fittings. Sometimes known by the original patent holder's brand name as a "Stillson wrench". adjustable
socket wrench socket wrench
socket spanner
A hollow cylinder that fits over one end of a nut or bolt head. It may include a handle, if it does not then it is often just referred to as a socket and is usually used with various drive tools to make it a wrench or spanner such as a ratchet handle, a tee bar (sliding tommy bar) bar or a knuckle bar (single axis pivot). It generally has a six-point, eight-point or twelve-point recess, may be shallow or deep, and may have a built-in universal joint. (The photo shows both ratchet and sockets.) socket
breaker bar
break-over handle
knuckle bar
jointed nut spinner
flex head nut spinner
Power Bar
This tool is a long non-ratcheting bar that allows the user to impart considerable torque to fasteners, especially in cases where corrosion has resulted in a difficult-to-loosen part. socket
crowfoot wrench
crow's-foot wrench
crow's foot A type of wrench designed to use the same drive sizes as socket wrenches, but non-cylindrical in shape. The ends are the same as those found on the open-end, box-end, or the flare-nut wrenches. These wrenches are used when torque must be measured, or when the application precludes the use of a regular socket or wrench. Also used in place of conventional open/box wrenches where the wrenches are large, usually at a lower cost, or for when space and weight restrictions are critical. socket
ratchet wrench ratchet handle It contains a one-way mechanism which allows the socket to be turned without removing it from the nut or bolt simply by cycling the handle backward and forward. (The photo shows both ratchet and sockets.) socket
speed handle
speed wrench
speed handle
crank handle
speed brace
A crank-shaped handle that drives a socket. The socket-driving analog of the brace used to drive a drill bit. Used instead of a ratchet in a few contexts when it can save substantial time and effort—that is, when there is a lot of turning to be done (many fasteners), ample room to swing the handle, ample access to the fastener heads, etc. Has less leverage than a conventional ratchet wrench. Used occasionally in automotive repair or job shop work. socket
torque wrench torque wrench A socket wrench drive tool that is employed to impart a precise amount of torque to a fastener, essential in many cases during the assembly of precision mechanisms. socket
Allen wrench
Allen key
hex key
L wrench
Allen key A wrench used to turn screw or bolt heads designed with a hexagonal socket (recess) to receive the wrench. The wrenches come in two common forms: L-shaped and T-handles. The L-shaped wrenches are formed from hexagonal wire stock, while the T-handles are the same hex wire stock with a metal or plastic handle attached to the end. There are also indexable-driver-bits that can be used in indexable screwdrivers. keys
Bristol wrench
Bristol spline wrench
 ? Another wrench designed for internal socket-head screws and bolts. The cross-section resembles a square-toothed gear. Not a common design, it is chiefly used on small set screws. keys
Torx wrench Torx key An internal socket-head screw design. The cross-section resembles a star. Commonly used in automobiles, automated equipment, and computer components as it is resistant to wrench cam-out and so suitable for use in the types of powered tools used in production-line assembly. keys
alligator wrench  ? A formerly common type of wrench that was popular with mechanics, factory workers, and farmers for maintenance, repair and operations tasks in the days when fasteners often had square rather than hex heads. The wrench's shape suggests the open mouth of an alligator. historical
cone wrench cone spanner A thin open-end wrench used to fit narrow wrench flats of adjustable bearing bicycle hubs. Called a "cone" wrench because it fits wrench flats of the cone section of a "cup and cone" hub, this tool is also used with some other adjustable hub bearings. The wrench is very thin so has little strength; to compensate, cone wrenches typically have a large head. Most bicycle front hubs use a 13 mm; most rears use 15 mm. specialty
die-stock
die wrench[4]
die stock
die holder
A double-handled wrench for turning the dies used in threading operations (cutting the male threads such as on a bolt). specialty
drum key
lug wrench
drum wrench
drum key A small, square-head socket wrench used on drum (percussion musical instrument) tuning lugs and fasteners. This key is often interchangeable with radiator bleed keys. specialty
spark plug wrench box spanner
tube spanner
spark plug spanner
A tube with six-sided sockets on both ends. It is turned with a short length of rod (tommy bar or T bar) inserted through two holes in the middle of the tube. common
drum wrench
bung wrench
 ? A tool commonly used to open bungs on large 55-gallon drums (cylindrical containers). specialty
fire hydrant wrench (hose connection)  ? The hose connection has a threaded collar with a protruding pin. From the handle of the wrench an arc has at its end a loop to engage the pin. specialty
fire hydrant wrench (valve operator)  ? This is a pentagonal (five-sided) box wrench. The unusual shape of the lug makes the valve tamper-resistant: with the opposite faces nonparallel, unauthorized opening of the hydrant is more difficult without a suitable tool. specialty
curb key Toby key This is a wrench for opening and closing valves on municipal water pipes (often at the curb, hence the name). The valve usually has a rectangular lug and is set deep into the ground, requiring the key. specialty
golf shoe spike wrench  ? A T-handle wrench with two pins and clearance for the spike—allows removal and insertion of spikes in shoes. specialty
head nut wrench  ? A flat wrench with a circular hole and two inward protruding pins to engage slots in the nut. This type of nut is used on bicycles to secure the front fork pivot bearing to the headpiece of the frame. specialty
4-way lug wrench
wheel lug cross wrench
cross rim wrench
spider wrench
wheel brace
tyre spanner
A socket wrench used to turn lug nuts on automobile wheels. specialty

oil-filter wrench oil filter wrench
chain wrench
A type of wrench for removing cylindrical oil filters. It may be either a strap-type wrench or a socket. specialty
plumber wrench multigrips
multigrip pliers
A tool to screw (rotate with force) various pipes during plumbing. specialty
 ? rigger-jigger A spanner can be used in attaching riggers to rowing boats with offset to allow users fingers to keep grip when flush with boat. 10 mm at one end, 13 mm at the other. specialty
basin wrench
sink wrench
basin wrench A self-tightening wrench mounted at the end of a shaft with a transverse handle at the opposite end. Used to tighten or loosen fasteners located in recesses. specialty
dogbone wrench dumbbell spanner A compact spanner for multiple sizes, usually used for bicycles specialty
spoke wrench nipple wrench
spoke key
A wrench with a clearance slot for a wire wheel spoke such as a bicycle wheel and a drive head for the adjustment nipple nut. The handle is offset to make the wrench more convenient to grip, and the handle is short to fit between spokes, allowing the wrench to turn 360 degrees without being removed. specialty
spud wrench podging spanner
podger
A steel erecting tool which consists of a normal wrench at one end and a spike (drift pin) at the other, used for lining up bolt holes (typically when mating two pipe flanges). specialty
chain whip A self-tightening wrench that engages the teeth of a chain drive sprocket, and used typically to remove bicycle cogsets. Similar to a strap wrench, but uses positive engagement rather than friction, and so needs to grab only one end of the chain. specialty

strap wrench
chain wrench
strap wrench
chain wrench
A self-tightening wrench with either a chain or strap of metal, leather, or rubber attached to a handle, used to grip and turn smooth cylindrical objects (such as automotive oil filters). It relies entirely on friction between the strap or chain and the object to be manipulated. Similar to a pipe wrench, but uses a chain similar to a drive chain or strap, instead of an adjustable jaw. The links of the chain have extended pegs which fit into grooves in the front of the handle, with one end of the chain attached permanently to the handle. This is used in situations where pipe wrenches cannot maintain a proper grip on an object such as a wet or oily pipe. Larger versions of chain wrenches are sometimes known as "bull tongs" and are used with large diameter pipe such as is used deep wells. specialty
tap wrench
tap handle
T-handle
tap wrench A double-handled wrench for turning the square drive on taps used in threading operations (cutting the female threads such as within a nut) or a precision reamer. specialty
tappet wrench  ? A spanner of small to moderate size constructed similarly to an open ended wrench, but with a thinner cross section. Its purpose is to apply torque to the fasteners found on the valve trains of older engines, especially automobile engines, where the valve train required adjustment of the tappets (also known as lifters). Tappets, push rods, rocker arms and similar adjustable pieces are often equipped with locknuts which are thinner than standard nuts, due to space limitations. Frequently, the hex section of the adjustment is contiguous to the lock nut, thus requiring a thinner "tappet wrench" to be used. specialty
tuning wrench tuning "T" hammer
piano tuning lever
A socket wrench used to tune some stringed musical instruments. Similar, and in some cases identical to drum tuning keys, but often provide greater torque due to the higher tension of strings. specialty
wing nut wrench A tool specifically for use with wing nuts, allowing the application of greater torque than is possible by hand. It is generally advised[by whom?] not to use such spanners for tightening the wing nut, but rather only for loosening. It is a "hand saver" more than anything else. specialty
graduated wrench[citation needed]  ? An adjustable wrench with a small number (usually 2–4) of discrete sizes. This is sometimes used as an inexpensive substitute for a monkey wrench.
power wrench  ? A broad type of wrenches that use electricity or compressed air to power the wrench. power
impact wrench
impact driver
pneumatic spanner
windy spanner
rattle gun
impact driver

Windy gun

A powered wrench which delivers quick, repeated impulses of torque. Typically powered by air, but can also be electric. Most people have heard its familiar rap-rap-rap noise while being used in an auto repair shop. Although many professionals use them to tighten lug nuts on vehicle wheels, do-it-yourselfers should use a torque wrench since an impact wrench can often over-torque and damage the threads on lug nuts and wheel studs. Impact wrenches are great for loosening stubborn, difficult-to-remove nuts and bolts. power

Other types of keys

These types of keys are not emically classified as wrenches by English speakers, but they are etically similar in function to wrenches.

American name British/Commonwealth name Description Group
chuck key chuck key A key used to tighten or loosen a chuck.[5] household/industrial
church key, bottle opener church key, bottle opener A key used to remove bottle caps or to pierce can lids.[6] household
paint can key  ? A key used to open the lids of paint cans. Its upturned edge helps to apply a levering motion to the crimped lip of the can lid. household
sillcock key sillcock key, loose key, tap key A key used to open or close sillcock valves. Many are designed the same way as a spider-type lug wrench, with four common sizes (one on each end) built into one portable tool. household
window crank window crank A socket-like key slipped over the splined shaft that operates the opening and closing of some types of window. household
sardine can key sardine tin key A key used in opening the lids of canned fish or canned meat. A tab on the metal lid fits into the slot in the shaft of the key and the lid is wound onto the key, tearing it away from the can. household
dental key dental key A key formerly used in dentistry for leverage in pulling teeth historical

Size designations

Size is usually designated by dimensions such as across-flats distance (inscribed-hexagon size). In the 19th and early 20th centuries, it had been common to define the nominal size of the wrench according to the nominal size of the screw thread that it was meant to be used with. Modern practice uses a size designation based on across-flats distance, whether measured in metric or in inch units.

  1. ^ "AskOxford". Retrieved 2010-04-20. 
  2. ^ Henry C. Mercer, Ancient Carpenters' Tools: Illustrated and Explained, Together with the Implements of the Lumberman, Joiner and Cabinet-Maker, 1928, reprint Courier Corporation - 2013, pages 271-272
  3. ^ http://www.bahco.com/en/about/
  4. ^ "McMaster-Carr Catalog". www.mcmaster.com. McMaster-Carr. Retrieved October 10, 2016. 
  5. ^ "Drill Chuck Keys & Keyleashes". Retrieved 13 April 2016. 
  6. ^ "World Wide Words: Church key". World Wide Words. Retrieved 13 April 2016. 


This article uses material from the Wikipedia article "Wrench", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Tooling

tooling,tool,drill,cam,manufacturing