powered by CADENAS

Social Share

Amazon

Electrohydrodynamics (321 views - Electrical Engineering)

Electrohydrodynamics (EHD), also known as electro-fluid-dynamics (EFD) or electrokinetics, is the study of the dynamics of electrically charged fluids. It is the study of the motions of ionized particles or molecules and their interactions with electric fields and the surrounding fluid. The term may be considered to be synonymous with the rather elaborate electrostrictive hydrodynamics. ESHD covers the following types of particle and fluid transport mechanisms: electrophoresis, electrokinesis, dielectrophoresis, electro-osmosis, and electrorotation. In general, the phenomena relate to the direct conversion of electrical energy into kinetic energy, and vice versa. In the first instance, shaped electrostatic fields (ESF's) create hydrostatic pressure (HSP, or motion) in dielectric media. When such media are fluids, a flow is produced. If the dielectric is a vacuum or a solid, no flow is produced. Such flow can be directed against the electrodes, generally to move the electrodes. In such case, the moving structure acts as an electric motor. Practical fields of interest of EHD are the common air ioniser, electrohydrodynamic thrusters and EHD cooling systems. In the second instance, the converse takes place. A powered flow of medium within a shaped electrostatic field adds energy to the system which is picked up as a potential difference by electrodes. In such case, the structure acts as an electrical generator.
Go to Article

Explanation by Hotspot Model

Youtube


    

Electrohydrodynamics

Electrohydrodynamics

Electrohydrodynamics (EHD), also known as electro-fluid-dynamics (EFD) or electrokinetics, is the study of the dynamics of electrically charged fluids.[1] It is the study of the motions of ionized particles or molecules and their interactions with electric fields and the surrounding fluid. The term may be considered to be synonymous with the rather elaborate electrostrictive hydrodynamics. ESHD covers the following types of particle and fluid transport mechanisms: electrophoresis, electrokinesis, dielectrophoresis, electro-osmosis, and electrorotation. In general, the phenomena relate to the direct conversion of electrical energy into kinetic energy, and vice versa.

In the first instance, shaped electrostatic fields (ESF's) create hydrostatic pressure (HSP, or motion) in dielectric media. When such media are fluids, a flow is produced. If the dielectric is a vacuum or a solid, no flow is produced. Such flow can be directed against the electrodes, generally to move the electrodes. In such case, the moving structure acts as an electric motor. Practical fields of interest of EHD are the common air ioniser, electrohydrodynamic thrusters and EHD cooling systems.

In the second instance, the converse takes place. A powered flow of medium within a shaped electrostatic field adds energy to the system which is picked up as a potential difference by electrodes. In such case, the structure acts as an electrical generator.

Electrokinesis

Electrokinesis is the particle or fluid transport produced by an electric field acting on a fluid having a net mobile charge. (See -kinesis for explanation and further uses of the -kinesis suffix.) Electrokinesis was first observed by Ferdinand Frederic Reuss during 1808, in the electrophoresis of clay particles [2] The effect was also noticed and publicized in the 1920s by Thomas Townsend Brown which he called the Biefeld–Brown effect, although he seems to have miss-identified it as an electric field acting on gravity.[3] The flow rate in such a mechanism is linear in the electric field. Electrokinesis is of considerable practical importance in microfluidics,[4][5][6] because it offers a way to manipulate and convey fluids in microsystems using only electric fields, with no moving parts.

The force acting on the fluid, is given by the equation

where, is the resulting force, measured in newtons, is the current, measured in amperes, is the distance between electrodes, measured in metres, and is the ion mobility coefficient of the dielectric fluid, measured in m2/(V·s).

If the electrodes are free to move within the fluid, while keeping their distance fixed from each other, then such a force will actually propel the electrodes with respect to the fluid.

Electrokinesis has also been observed in biology, where it was found to cause physical damage to neurons by inciting movement in their membranes.[7][8] It is discussed in R.J.Elul's "Fixed charge in the cell membrane" (1967).

Water electrokinetics

In October 2003, Dr. Daniel Kwok, Dr. Larry Kostiuk and two graduate students from the University of Alberta discussed a method of hydrodynamic to electrical energy conversion by exploiting the natural electrokinetic properties of a liquid such as ordinary tap water, by pumping fluids through tiny micro-channels with a pressure difference.[9] This technology could some day provide a practical and clean energy storage device, replacing today's batteries, for devices such as mobile phones or calculators which would be charged up by simply pumping water to high pressure. Pressure would then be released on demand, for fluid flow to take place over the micro-channels. When water travels, or streams over a surface, the ions of which water is made "rub" against the solid, leaving the surface slightly charged. Kinetic energy from the moving ions would thus be converted to electrical energy. Although the power generated from a single channel is extremely small, millions of parallel micro-channels can be used to increase the power output. This streaming potential, water-flow phenomenon was discovered in 1859 by German physicist Georg Hermann Quincke.[citation needed][5][6][10]

Electrokinetic instabilities

The fluid flows in microfluidic and nanofluidic devices are often stable and strongly damped by viscous forces (with Reynolds numbers of order unity or smaller). However, heterogeneous ionic conductivity fields in the presence of applied electric fields can, under certain conditions, generate an unstable flow field owing to electrokinetic instabilities (EKI). Conductivity gradients are prevalent in on-chip electrokinetic processes such as preconcentration methods (e.g. field amplified sample stacking and isoelectric focusing), multidimensional assays, and systems with poorly specified sample chemistry. The dynamics and periodic morphology of electrokinetic instabilities are similar to other systems with Rayleigh–Taylor instabilities. The particular case of a plat plane geometry with homogeneous ions injection in the bottom side leads to a mathematical frame identical to the Rayleigh–Bénard convection.

EKI's can be leveraged for rapid mixing or can cause undesirable dispersion in sample injection, separation and stacking. These instabilities are caused by a coupling of electric fields and ionic conductivity gradients that results in an electric body force. This coupling results in an electric body force in the bulk liquid, outside the electric double layer, that can generate temporal, convective, and absolute flow instabilities. Electrokinetic flows with conductivity gradients become unstable when the electroviscous stretching and folding of conductivity interfaces grows faster than the dissipative effect of molecular diffusion.

Since these flows are characterized by low velocities and small length scales, the Reynolds number is below 0.01 and the flow is laminar. The onset of instability in these flows is best described as an electric "Rayleigh number".

Misc

Liquids can be printed at nanoscale by pyro-EHD.[11]

See also



This article uses material from the Wikipedia article "Electrohydrodynamics", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electrical Engineering

EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced