powered by CADENAS

Social Share

Amazon

Photography (1351 views - Consumer products)

Photography is the art, application and practice of creating durable images by recording light or other electromagnetic radiation, either electronically by means of an image sensor, or chemically by means of a light-sensitive material such as photographic film. It is employed in many fields of science, manufacturing (e.g., photolithography), and business, as well as its more direct uses for art, film and video production, recreational purposes, hobby, and mass communication.Typically, a lens is used to focus the light reflected or emitted from objects into a real image on the light-sensitive surface inside a camera during a timed exposure. With an electronic image sensor, this produces an electrical charge at each pixel, which is electronically processed and stored in a digital image file for subsequent display or processing. The result with photographic emulsion is an invisible latent image, which is later chemically "developed" into a visible image, either negative or positive depending on the purpose of the photographic material and the method of processing. A negative image on film is traditionally used to photographically create a positive image on a paper base, known as a print, either by using an enlarger or by contact printing.
Go to Article

Explanation by Hotspot Model

Youtube


    

Photography

Photography

Photography

Photography
Lens and mounting of a large-format camera
Other namesScience or art of creating durable images
TypesRecording light or other electromagnetic radiation
InventorThomas Wedgwood (1800)
RelatedStereoscopic, Full-spectrum, Light field, Electrophotography, Photograms, Scanner

Photography is the art, application and practice of creating durable images by recording light or other electromagnetic radiation, either electronically by means of an image sensor, or chemically by means of a light-sensitive material such as photographic film. It is employed in many fields of science, manufacturing (e.g., photolithography), and business, as well as its more direct uses for art, film and video production, recreational purposes, hobby, and mass communication.[1]

Typically, a lens is used to focus the light reflected or emitted from objects into a real image on the light-sensitive surface inside a camera during a timed exposure. With an electronic image sensor, this produces an electrical charge at each pixel, which is electronically processed and stored in a digital image file for subsequent display or processing. The result with photographic emulsion is an invisible latent image, which is later chemically "developed" into a visible image, either negative or positive depending on the purpose of the photographic material and the method of processing. A negative image on film is traditionally used to photographically create a positive image on a paper base, known as a print, either by using an enlarger or by contact printing.

Etymology

The word "photography" was created from the Greek roots φωτός (phōtos), genitive of φῶς (phōs), "light"[2] and γραφή (graphé) "representation by means of lines" or "drawing",[3] together meaning "drawing with light".[4]

Several people may have coined the same new term from these roots independently. Hercules Florence, a French painter and inventor living in Campinas, Brazil, used the French form of the word, photographie, in private notes which a Brazilian historian believes were written in 1834.[5] This claim is widely reported but apparently has never been independently confirmed as beyond reasonable doubt.[citation needed]

The German newspaper Vossische Zeitung of 25 February 1839 contained an article entitled Photographie, discussing several priority claims – especially Henry Fox Talbot's – regarding Daguerre's claim of invention.[6][dead link] The article is the earliest known occurrence of the word in public print. It was signed "J.M.", believed to have been Berlin astronomer Johann von Maedler.[7]

The inventors Nicéphore Niépce, Henry Fox Talbot and Louis Daguerre seem not to have known or used the word "photography", but referred to their processes as "Heliography" (Niépce), "Photogenic Drawing"/"Talbotype"/"Calotype" (Talbot) and "Daguerreotype" (Daguerre).[7]

History

Precursor technologies

Photography is the result of combining several technical discoveries, relating to seeing an image and capturing the image. The discovery of the camera obscura ("dark chamber" in Latin) that provides an image of a scene dates back to ancient China. Greek mathematicians Aristotle and Euclid independently described a pinhole camera in the 5th and 4th centuries BCE.[8][9] In the 6th century CE, Byzantine mathematician Anthemius of Tralles used a type of camera obscura in his experiments.[10] The Arab physicist Ibn al-Haytham (Alhazen) (965–1040) also invented a camera obscura and pinhole camera.[9][11]

Leonardo da Vinci mentions natural camera obscura that are formed by dark caves on the edge of a sunlit valley. A hole in the cave wall will act as a pinhole camera and project a laterally reversed, upside down image on a piece of paper. Renaissance painters used the camera obscura which, in fact, gives the optical rendering in color that dominates Western Art. It is a box with a hole in it which allows light to go through and create an image onto the piece of paper.

The birth of photography was then concerned with inventing means to capture and keep the image produced by the camera obscura. Albertus Magnus (1193–1280) discovered silver nitrate,[12] and Georg Fabricius (1516–1571) discovered silver chloride,[13] and the techniques described in Ibn al-Haytham's Book of Optics are capable of producing primitive photographs using medieval materials.[14][15]

Daniele Barbaro described a diaphragm in 1566.[16] Wilhelm Homberg described how light darkened some chemicals (photochemical effect) in 1694.[17] The fiction book Giphantie, published in 1760, by French author Tiphaigne de la Roche, described what can be interpreted as photography.[16]

Around the year 1800, British inventor Thomas Wedgwood made the first known attempt to capture the image in a camera obscura by means of a light-sensitive substance. He used paper or white leather treated with silver nitrate. Although he succeeded in capturing the shadows of objects placed on the surface in direct sunlight, and even made shadow copies of paintings on glass, it was reported in 1802 that "the images formed by means of a camera obscura have been found too faint to produce, in any moderate time, an effect upon the nitrate of silver." The shadow images eventually darkened all over.[18]

Invention

Earliest known surviving heliographic engraving, 1825, printed from a metal plate made by Nicéphore Niépce.[19] The plate was exposed under an ordinary engraving and copied it by photographic means. This was a step towards the first permanent photograph taken with a camera.

The first permanent photoetching was an image produced in 1822 by the French inventor Nicéphore Niépce, but it was destroyed in a later attempt to make prints from it.[19] Niépce was successful again in 1825. In 1826 or 1827, he made the View from the Window at Le Gras, the earliest surviving photograph from nature (i.e., of the image of a real-world scene, as formed in a camera obscura by a lens).[20]

Because Niépce's camera photographs required an extremely long exposure (at least eight hours and probably several days), he sought to greatly improve his bitumen process or replace it with one that was more practical. In partnership with Louis Daguerre, he worked out post-exposure processing methods that produced visually superior results and replaced the bitumen with a more light-sensitive resin, but hours of exposure in the camera were still required. With an eye to eventual commercial exploitation, the partners opted for total secrecy.

Niépce died in 1833 and Daguerre then redirected the experiments toward the light-sensitive silver halides, which Niépce had abandoned many years earlier because of his inability to make the images he captured with them light-fast and permanent. Daguerre's efforts culminated in what would later be named the daguerreotype process. The essential elements—a silver-plated surface sensitized by iodine vapor, developed by mercury vapor, and "fixed" with hot saturated salt water—were in place in 1837. The required exposure time was measured in minutes instead of hours. Daguerre took the earliest confirmed photograph of a person in 1838 while capturing a view of a Paris street: unlike the other pedestrian and horse-drawn traffic on the busy boulevard, which appears deserted, one man having his boots polished stood sufficiently still throughout the several-minutes-long exposure to be visible. The existence of Daguerre's process was publicly announced, without details, on 7 January 1839. The news created an international sensation. France soon agreed to pay Daguerre a pension in exchange for the right to present his invention to the world as the gift of France, which occurred when complete working instructions were unveiled on 19 August 1839. In that same year, American photographer Robert Cornelius is credited with taking the earliest surviving photographic self-portrait.

A latticed window in Lacock Abbey, England, photographed by William Fox Talbot in 1835. Shown here in positive form, this may be the oldest extant photographic negative made in a camera.

In Brazil, Hercules Florence had apparently started working out a silver-salt-based paper process in 1832, later naming it Photographie.

Meanwhile, a British inventor, William Fox Talbot, had succeeded in making crude but reasonably light-fast silver images on paper as early as 1834 but had kept his work secret. After reading about Daguerre's invention in January 1839, Talbot published his hitherto secret method and set about improving on it. At first, like other pre-daguerreotype processes, Talbot's paper-based photography typically required hours-long exposures in the camera, but in 1840 he created the calotype process, which used the chemical development of a latent image to greatly reduce the exposure needed and compete with the daguerreotype. In both its original and calotype forms, Talbot's process, unlike Daguerre's, created a translucent negative which could be used to print multiple positive copies; this is the basis of most modern chemical photography up to the present day, as Daguerreotypes could only be replicated by rephotographing them with a camera.[21] Talbot's famous tiny paper negative of the Oriel window in Lacock Abbey, one of a number of camera photographs he made in the summer of 1835, may be the oldest camera negative in existence.[22][23]

British chemist John Herschel made many contributions to the new field. He invented the cyanotype process, later familiar as the "blueprint". He was the first to use the terms "photography", "negative" and "positive". He had discovered in 1819 that sodium thiosulphate was a solvent of silver halides, and in 1839 he informed Talbot (and, indirectly, Daguerre) that it could be used to "fix" silver-halide-based photographs and make them completely light-fast. He made the first glass negative in late 1839.

In the March 1851 issue of The Chemist, Frederick Scott Archer published his wet plate collodion process. It became the most widely used photographic medium until the gelatin dry plate, introduced in the 1870s, eventually replaced it. There are three subsets to the collodion process; the Ambrotype (a positive image on glass), the Ferrotype or Tintype (a positive image on metal) and the glass negative, which was used to make positive prints on albumen or salted paper.

Many advances in photographic glass plates and printing were made during the rest of the 19th century. In 1891, Gabriel Lippmann introduced a process for making natural-color photographs based on the optical phenomenon of the interference of light waves. His scientifically elegant and important but ultimately impractical invention earned him the Nobel Prize in Physics in 1908.

Glass plates were the medium for most original camera photography from the late 1850s until the general introduction of flexible plastic films during the 1890s. Although the convenience of the film greatly popularized amateur photography, early films were somewhat more expensive and of markedly lower optical quality than their glass plate equivalents, and until the late 1910s they were not available in the large formats preferred by most professional photographers, so the new medium did not immediately or completely replace the old. Because of the superior dimensional stability of glass, the use of plates for some scientific applications, such as astrophotography, continued into the 1990s, and in the niche field of laser holography, it has persisted into the 2010s.

Film

Hurter and Driffield began pioneering work on the light sensitivity of photographic emulsions in 1876. Their work enabled the first quantitative measure of film speed to be devised.

The first flexible photographic roll film was marketed by George Eastman in 1885, but this original "film" was actually a coating on a paper base. As part of the processing, the image-bearing layer was stripped from the paper and transferred to a hardened gelatin support. The first transparent plastic roll film followed in 1889. It was made from highly flammable nitrocellulose ("celluloid"), now usually called "nitrate film".

Although cellulose acetate or "safety film" had been introduced by Kodak in 1908,[24] at first it found only a few special applications as an alternative to the hazardous nitrate film, which had the advantages of being considerably tougher, slightly more transparent, and cheaper. The changeover was not completed for X-ray films until 1933, and although safety film was always used for 16 mm and 8 mm home movies, nitrate film remained standard for theatrical 35 mm motion pictures until it was finally discontinued in 1951.

Films remained the dominant form of photography until the early 21st century when advances in digital photography drew consumers to digital formats.[25] Although modern photography is dominated by digital users, film continues to be used by enthusiasts and professional photographers. The distinctive "look" of film based photographs compared to digital images is likely due to a combination of factors, including: (1) differences in spectral and tonal sensitivity (S-shaped density-to-exposure (H&D curve) with film vs. linear response curve for digital CCD sensors) [26] (2) resolution and (3) continuity of tone.[27]

Black-and-white

Originally, all photography was monochrome, or black-and-white. Even after color film was readily available, black-and-white photography continued to dominate for decades, due to its lower cost and its "classic" photographic look. The tones and contrast between light and dark areas define black-and-white photography.[28] It is important to note that monochromatic pictures are not necessarily composed of pure blacks, whites, and intermediate shades of gray but can involve shades of one particular hue depending on the process. The cyanotype process, for example, produces an image composed of blue tones. The albumen print process first used more than 170 years ago, produces brownish tones.

Many photographers continue to produce some monochrome images, sometimes because of the established archival permanence of well-processed silver-halide-based materials. Some full-color digital images are processed using a variety of techniques to create black-and-white results, and some manufacturers produce digital cameras that exclusively shoot monochrome. Monochrome printing or electronic display can be used to salvage certain photographs taken in color which are unsatisfactory in their original form; sometimes when presented as black-and-white or single-color-toned images they are found to be more effective. Although color photography has long predominated, monochrome images are still produced, mostly for artistic reasons. Almost all digital cameras have an option to shoot in monochrome, and almost all image editing software can combine or selectively discard RGB color channels to produce a monochrome image from one shot in color.

Color

Color photography was explored beginning in the 1840s. Early experiments in color required extremely long exposures (hours or days for camera images) and could not "fix" the photograph to prevent the color from quickly fading when exposed to white light.

The first permanent color photograph was taken in 1861 using the three-color-separation principle first published by Scottish physicist James Clerk Maxwell in 1855.[29][30] The foundation of virtually all practical color processes, Maxwell's idea was to take three separate black-and-white photographs through red, green and blue filters.[29][30] This provides the photographer with the three basic channels required to recreate a color image. Transparent prints of the images could be projected through similar color filters and superimposed on the projection screen, an additive method of color reproduction. A color print on paper could be produced by superimposing carbon prints of the three images made in their complementary colors, a subtractive method of color reproduction pioneered by Louis Ducos du Hauron in the late 1860s.

Color photography was possible long before Kodachrome, as this 1903 portrait by Sarah Angelina Acland demonstrates, but in its earliest years, the need for special equipment, long exposures, and complicated printing processes made it extremely rare.

Russian photographer Sergei Mikhailovich Prokudin-Gorskii made extensive use of this color separation technique, employing a special camera which successively exposed the three color-filtered images on different parts of an oblong plate. Because his exposures were not simultaneous, unsteady subjects exhibited color "fringes" or, if rapidly moving through the scene, appeared as brightly colored ghosts in the resulting projected or printed images.

Implementation of color photography was hindered by the limited sensitivity of early photographic materials, which were mostly sensitive to blue, only slightly sensitive to green, and virtually insensitive to red. The discovery of dye sensitization by photochemist Hermann Vogel in 1873 suddenly made it possible to add sensitivity to green, yellow and even red. Improved color sensitizers and ongoing improvements in the overall sensitivity of emulsions steadily reduced the once-prohibitive long exposure times required for color, bringing it ever closer to commercial viability.

Autochrome, the first commercially successful color process, was introduced by the Lumière brothers in 1907. Autochrome plates incorporated a mosaic color filter layer made of dyed grains of potato starch, which allowed the three color components to be recorded as adjacent microscopic image fragments. After an Autochrome plate was reversal processed to produce a positive transparency, the starch grains served to illuminate each fragment with the correct color and the tiny colored points blended together in the eye, synthesizing the color of the subject by the additive method. Autochrome plates were one of several varieties of additive color screen plates and films marketed between the 1890s and the 1950s.

Kodachrome, the first modern "integral tripack" (or "monopack") color film, was introduced by Kodak in 1935. It captured the three color components in a multi-layer emulsion. One layer was sensitized to record the red-dominated part of the spectrum, another layer recorded only the green part and a third recorded only the blue. Without special film processing, the result would simply be three superimposed black-and-white images, but complementary cyan, magenta, and yellow dye images were created in those layers by adding color couplers during a complex processing procedure.

Agfa's similarly structured Agfacolor Neu was introduced in 1936. Unlike Kodachrome, the color couplers in Agfacolor Neu were incorporated into the emulsion layers during manufacture, which greatly simplified the processing. Currently, available color films still employ a multi-layer emulsion and the same principles, most closely resembling Agfa's product.

Instant color film, used in a special camera which yielded a unique finished color print only a minute or two after the exposure, was introduced by Polaroid in 1963.

Color photography may form images as positive transparencies, which can be used in a slide projector, or as color negatives intended for use in creating positive color enlargements on specially coated paper. The latter is now the most common form of film (non-digital) color photography owing to the introduction of automated photo printing equipment. After a transition period centered around 1995–2005, color film was relegated to a niche market by inexpensive multi-megapixel digital cameras. Film continues to be the preference of some photographers because of its distinctive "look".

Digital

In 1981, Sony unveiled the first consumer camera to use a charge-coupled device for imaging, eliminating the need for film: the Sony Mavica. While the Mavica saved images to disk, the images were displayed on television, and the camera was not fully digital. In 1991, Kodak unveiled the DCS 100, the first commercially available digital single lens reflex camera. Although its high cost precluded uses other than photojournalism and professional photography, commercial digital photography was born.

Digital imaging uses an electronic image sensor to record the image as a set of electronic data rather than as chemical changes on film.[31] An important difference between digital and chemical photography is that chemical photography resists photo manipulation because it involves film and photographic paper, while digital imaging is a highly manipulative medium. This difference allows for a degree of image post-processing that is comparatively difficult in film-based photography and permits different communicative potentials and applications.

Digital photography dominates the 21st century. More than 99% of photographs taken around the world are through digital cameras, increasingly through smartphones.

Synthesis

Synthesis photography is part of computer-generated imagery (CGI) where the shooting process is modeled on real photography. The CGI, creating digital copies of real universe, requires a visual representation process of these universes. Synthesis photography is the application of analog and digital photography in digital space. With the characteristics of the real photography but not being constrained by the physical limits of real world, synthesis photography allows artists to move into areas beyond the grasp of real photography.[32]

Techniques

A large variety of photographic techniques and media are used in the process of capturing images for photography. These include the camera; stereoscopy; dualphotography; full-spectrum, ultraviolet and infrared media; light field photography; and other imaging techniques.

Cameras

The camera is the image-forming device, and a photographic plate, photographic film or a silicon electronic image sensor is the capture medium. The respective recording medium can be the plate or film itself, or a digital magnetic or electronic memory.[33]

Photographers control the camera and lens to "expose" the light recording material to the required amount of light to form a "latent image" (on plate or film) or RAW file (in digital cameras) which, after appropriate processing, is converted to a usable image. Digital cameras use an electronic image sensor based on light-sensitive electronics such as charge-coupled device (CCD) or complementary metal-oxide-semiconductor (CMOS) technology. The resulting digital image is stored electronically, but can be reproduced on a paper.

The camera (or 'camera obscura') is a dark room or chamber from which, as far as possible, all light is excluded except the light that forms the image. It was discovered and used in the 16th century by painters. The subject being photographed, however, must be illuminated. Cameras can range from small to very large, a whole room that is kept dark while the object to be photographed is in another room where it is properly illuminated. This was common for reproduction photography of flat copy when large film negatives were used (see Process camera).

As soon as photographic materials became "fast" (sensitive) enough for taking candid or surreptitious pictures, small "detective" cameras were made, some actually disguised as a book or handbag or pocket watch (the Ticka camera) or even worn hidden behind an Ascot necktie with a tie pin that was really the lens.

The movie camera is a type of photographic camera which takes a rapid sequence of photographs on recording medium. In contrast to a still camera, which captures a single snapshot at a time, the movie camera takes a series of images, each called a "frame". This is accomplished through an intermittent mechanism. The frames are later played back in a movie projector at a specific speed, called the "frame rate" (number of frames per second). While viewing, a person's eyes and brain merge the separate pictures to create the illusion of motion.[34]

Stereoscopic

Photographs, both monochrome and color, can be captured and displayed through two side-by-side images that emulate human stereoscopic vision. Stereoscopic photography was the first that captured figures in motion.[35] While known colloquially as "3-D" photography, the more accurate term is stereoscopy. Such cameras have long been realized by using film and more recently in digital electronic methods (including cell phone cameras).

Dualphotography

Dualphotography consists of photographing a scene from both sides of a photographic device at once (e.g. camera for back-to-back dualphotography, or two networked cameras for portal-plane dualphotography). The dualphoto apparatus can be used to simultaneously capture both the subject and the photographer, or both sides of a geographical place at once, thus adding a supplementary narrative layer to that of a single image.[36]

Full-spectrum, ultraviolet and infrared

Ultraviolet and infrared films have been available for many decades and employed in a variety of photographic avenues since the 1960s. New technological trends in digital photography have opened a new direction in full spectrum photography, where careful filtering choices across the ultraviolet, visible and infrared lead to new artistic visions.

Modified digital cameras can detect some ultraviolet, all of the visible and much of the near infrared spectrum, as most digital imaging sensors are sensitive from about 350 nm to 1000 nm. An off-the-shelf digital camera contains an infrared hot mirror filter that blocks most of the infrared and a bit of the ultraviolet that would otherwise be detected by the sensor, narrowing the accepted range from about 400 nm to 700 nm.[37]

Replacing a hot mirror or infrared blocking filter with an infrared pass or a wide spectrally transmitting filter allows the camera to detect the wider spectrum light at greater sensitivity. Without the hot-mirror, the red, green and blue (or cyan, yellow and magenta) colored micro-filters placed over the sensor elements pass varying amounts of ultraviolet (blue window) and infrared (primarily red and somewhat lesser the green and blue micro-filters).

Uses of full spectrum photography are for fine art photography, geology, forensics and law enforcement.

Light field

Digital methods of image capture and display processing have enabled the new technology of "light field photography" (also known as synthetic aperture photography). This process allows focusing at various depths of field to be selected after the photograph has been captured.[38] As explained by Michael Faraday in 1846, the "light field" is understood as 5-dimensional, with each point in 3-D space having attributes of two more angles that define the direction of each ray passing through that point.

These additional vector attributes can be captured optically through the use of microlenses at each pixel point within the 2-dimensional image sensor. Every pixel of the final image is actually a selection from each sub-array located under each microlens, as identified by a post-image capture focus algorithm.

Other

Besides the camera, other methods of forming images with light are available. For instance, a photocopy or xerography machine forms permanent images but uses the transfer of static electrical charges rather than photographic medium, hence the term electrophotography. Photograms are images produced by the shadows of objects cast on the photographic paper, without the use of a camera. Objects can also be placed directly on the glass of an image scanner to produce digital pictures.

Modes of production

Amateur

An amateur photographer is one who practices photography as a hobby/passion and not necessarily for profit. The quality of some amateur work is comparable to that of many professionals and may be highly specialized or eclectic in choice of subjects. Amateur photography is often pre-eminent in photographic subjects which have little prospect of commercial use or reward. Amateur photography grew during the late 19th century due to the popularization of the hand-held camera.[39] Nowadays it has spread widely through social media and is carried out throughout different platforms and equipment, switching to the use of cell phone. Good pictures can now be taken with a cell phone which is a key tool for making photography more accessible to everyone.[40]

Commercial

Commercial photography is probably best defined as any photography for which the photographer is paid for images rather than works of art. In this light, money could be paid for the subject of the photograph or the photograph itself. Wholesale, retail, and professional uses of photography would fall under this definition. The commercial photographic world could include:

  • Advertising photography: photographs made to illustrate and usually sell a service or product. These images, such as packshots, are generally done with an advertising agency, design firm or with an in-house corporate design team.
  • Fashion and glamour photography usually incorporates models and is a form of advertising photography. Fashion photography, like the work featured in Harper's Bazaar, emphasizes clothes and other products; glamour emphasizes the model and body form. Glamour photography is popular in advertising and men's magazines. Models in glamour photography sometimes work nude.
  • Concert photography focuses on capturing candid images of both the artist or band as well as the atmosphere (including the crowd). Many of these photographers work freelance and are contracted through an artist or their management to cover a specific show. Concert photographs are often used to promote the artist or band in addition to the venue.
  • Crime scene photography consists of photographing scenes of crime such as robberies and murders. A black and white camera or an infrared camera may be used to capture specific details.
  • Still life photography usually depicts inanimate subject matter, typically commonplace objects which may be either natural or man-made. Still life is a broader category for food and some natural photography and can be used for advertising purposes.
  • Food photography can be used for editorial, packaging or advertising use. Food photography is similar to still life photography but requires some special skills.
  • Editorial photography illustrates a story or idea within the context of a magazine. These are usually assigned by the magazine and encompass fashion and glamour photography features.
    • Photojournalism can be considered a subset of editorial photography. Photographs made in this context are accepted as a documentation of a news story.
  • Portrait and wedding photography: photographs made and sold directly to the end user of the images.
  • Landscape photography depicts locations.
  • Wildlife photography demonstrates the life of animals.
  • Paparazzi is a form of photojournalism in which the photographer captures candid images of athletes, celebrities, politicians, and other prominent people.
  • Pet photography involves several aspects that are similar to traditional studio portraits. It can also be done in natural lighting, outside of a studio, such as in a client's home.

The market for photographic services demonstrates the aphorism "A picture is worth a thousand words", which has an interesting basis in the history of photography. Magazines and newspapers, companies putting up Web sites, advertising agencies and other groups pay for photography.

Many people take photographs for commercial purposes. Organizations with a budget and a need for photography have several options: they can employ a photographer directly, organize a public competition, or obtain rights to stock photographs. Photo stock can be procured through traditional stock giants, such as Getty Images or Corbis; smaller microstock agencies, such as Fotolia; or web marketplaces, such as Cutcaster.

Art

During the 20th century, both fine art photography and documentary photography became accepted by the English-speaking art world and the gallery system. In the United States, a handful of photographers, including Alfred Stieglitz, Edward Steichen, John Szarkowski, F. Holland Day, and Edward Weston, spent their lives advocating for photography as a fine art. At first, fine art photographers tried to imitate painting styles. This movement is called Pictorialism, often using soft focus for a dreamy, 'romantic' look. In reaction to that, Weston, Ansel Adams, and others formed the Group f/64 to advocate 'straight photography', the photograph as a (sharply focused) thing in itself and not an imitation of something else.

The aesthetics of photography is a matter that continues to be discussed regularly, especially in artistic circles. Many artists argued that photography was the mechanical reproduction of an image. If photography is authentically art, then photography in the context of art would need redefinition, such as determining what component of a photograph makes it beautiful to the viewer. The controversy began with the earliest images "written with light"; Nicéphore Niépce, Louis Daguerre, and others among the very earliest photographers were met with acclaim, but some questioned if their work met the definitions and purposes of art.

Clive Bell in his classic essay Art states that only "significant form" can distinguish art from what is not art.

There must be some one quality without which a work of art cannot exist; possessing which, in the least degree, no work is altogether worthless. What is this quality? What quality is shared by all objects that provoke our aesthetic emotions? What quality is common to Sta. Sophia and the windows at Chartres, Mexican sculpture, a Persian bowl, Chinese carpets, Giotto's frescoes at Padua, and the masterpieces of Poussin, Piero della Francesca, and Cezanne? Only one answer seems possible – significant form. In each, lines and colors combined in a particular way, certain forms and relations of forms, stir our aesthetic emotions.[41]

On 7 February 2007, Sotheby's London sold the 2001 photograph 99 Cent II Diptychon for an unprecedented $3,346,456 to an anonymous bidder, making it the most expensive at the time.[42]

Conceptual photography turns a concept or idea into a photograph. Even though what is depicted in the photographs are real objects, the subject is strictly abstract.

Photojournalism

Photojournalism is a particular form of photography (the collecting, editing, and presenting of news material for publication or broadcast) that employs images in order to tell a news story. It is now usually understood to refer only to still images, but in some cases the term also refers to video used in broadcast journalism. Photojournalism is distinguished from other close branches of photography (e.g., documentary photography, social documentary photography, street photography or celebrity photography) by complying with a rigid ethical framework which demands that the work be both honest and impartial whilst telling the story in strictly journalistic terms. Photojournalists create pictures that contribute to the news media, and help communities connect with one other. Photojournalists must be well informed and knowledgeable about events happening right outside their door. They deliver news in a creative format that is not only informative, but also entertaining.

Science and forensics

The camera has a long and distinguished history as a means of recording scientific phenomena from the first use by Daguerre and Fox-Talbot, such as astronomical events (eclipses for example), small creatures and plants when the camera was attached to the eyepiece of microscopes (in photomicroscopy) and for macro photography of larger specimens. The camera also proved useful in recording crime scenes and the scenes of accidents, such as the Wootton bridge collapse in 1861. The methods used in analysing photographs for use in legal cases are collectively known as forensic photography. Crime scene photos are taken from three vantage point. The vantage points are overview, mid-range, and close-up.[43]

In 1845 Francis Ronalds, the Honorary Director of the Kew Observatory, invented the first successful camera to make continuous recordings of meteorological and geomagnetic parameters. Different machines produced 12- or 24- hour photographic traces of the minute-by-minute variations of atmospheric pressure, temperature, humidity, atmospheric electricity, and the three components of geomagnetic forces. The cameras were supplied to numerous observatories around the world and some remained in use until well into the 20th century.[44][45] Charles Brooke a little later developed similar instruments for the Greenwich Observatory.[46]

Science uses image technology that has derived from the design of the Pin Hole camera. X-Ray machines are similar in design to Pin Hole cameras with high-grade filters and laser radiation.[47] Photography has become universal in recording events and data in science and engineering, and at crime scenes or accident scenes. The method has been much extended by using other wavelengths, such as infrared photography and ultraviolet photography, as well as spectroscopy. Those methods were first used in the Victorian era and improved much further since that time.[48]

The first photographed atom was discovered in 2012 by physicists at Griffith University, Australia. They used an electric field to trap an "Ion" of the element, Ytterbium. The image was recorded on a CCD, an electronic photographic film.[49]

Social and cultural implications

There are many ongoing questions about different aspects of photography. In her writing "On Photography" (1977), Susan Sontag discusses concerns about the objectivity of photography. This is a highly debated subject within the photographic community.[50] Sontag argues, "To photograph is to appropriate the thing photographed. It means putting one's self into a certain relation to the world that feels like knowledge, and therefore like power."[51] Photographers decide what to take a photo of, what elements to exclude and what angle to frame the photo, and these factors may reflect a particular socio-historical context. Along these lines, it can be argued that photography is a subjective form of representation.

Modern photography has raised a number of concerns on its effect on society. In Alfred Hitchcock's Rear Window (1954), the camera is presented as promoting voyeurism. 'Although the camera is an observation station, the act of photographing is more than passive observing'.[51]

The camera doesn't rape or even possess, though it may presume, intrude, trespass, distort, exploit, and, at the farthest reach of metaphor, assassinate – all activities that, unlike the sexual push and shove, can be conducted from a distance, and with some detachment.[51]

Digital imaging has raised ethical concerns because of the ease of manipulating digital photographs in post-processing. Many photojournalists have declared they will not crop their pictures or are forbidden from combining elements of multiple photos to make "photomontages", passing them as "real" photographs. Today's technology has made image editing relatively simple for even the novice photographer. However, recent changes of in-camera processing allow digital fingerprinting of photos to detect tampering for purposes of forensic photography.

Photography is one of the new media forms that changes perception and changes the structure of society.[52] Further unease has been caused around cameras in regards to desensitization. Fears that disturbing or explicit images are widely accessible to children and society at large have been raised. Particularly, photos of war and pornography are causing a stir. Sontag is concerned that "to photograph is to turn people into objects that can be symbolically possessed." Desensitization discussion goes hand in hand with debates about censored images. Sontag writes of her concern that the ability to censor pictures means the photographer has the ability to construct reality.[51]

One of the practices through which photography constitutes society is tourism. Tourism and photography combine to create a "tourist gaze"[53] in which local inhabitants are positioned and defined by the camera lens. However, it has also been argued that there exists a "reverse gaze"[54] through which indigenous photographees can position the tourist photographer as a shallow consumer of images.

Additionally, photography has been the topic of many songs in popular culture.

Law

Photography is both restricted as well as protected by the law in many jurisdictions. Protection of photographs is typically achieved through the granting of copyright or moral rights to the photographer. In the United States, photography is protected as a First Amendment right and anyone is free to photograph anything seen in public spaces as long as it is in plain view.[55] In the UK a recent law (Counter-Terrorism Act 2008) increases the power of the police to prevent people, even press photographers, from taking pictures in public places.[56]

See also



This article uses material from the Wikipedia article "Photography", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Consumer products

.max, Maya, Challenge, Competition, Rendering, 3D, Blender, Autodesk Maya, 3D Studio MAX (.3DS, .MAX), Maxwell, Animation, 3D Model, Autodesk Softimage, Cinema 4D, Rendering, Animation, 3Dartist, c4d, maxon, lowpoly, 3Dart, blender3D, 3D library