powered by CADENAS

Social Share

Amazon

Wind power (1303 views - Environmental Protection)

Wind power is the use of air flow through wind turbines to provide the mechanical power to turn electric generators. Wind power, as an alternative to burning fossil fuels, is plentiful, renewable, widely distributed, clean, produces no greenhouse gas emissions during operation, consumes no water, and uses little land. The net effects on the environment are far less problematic than those of nonrenewable power sources. Wind farms consist of many individual wind turbines, which are connected to the electric power transmission network. Onshore wind is an inexpensive source of electric power, competitive with or in many places cheaper than coal or gas plants. Offshore wind is steadier and stronger than on land and offshore farms have less visual impact, but construction and maintenance costs are considerably higher. Small onshore wind farms can feed some energy into the grid or provide electric power to isolated off-grid locations.Wind power gives variable power, which is very consistent from year to year but has significant variation over shorter time scales. It is therefore used in conjunction with other electric power sources to give a reliable supply. As the proportion of wind power in a region increases, a need to upgrade the grid and a lowered ability to supplant conventional production can occur. Power-management techniques such as having excess capacity, geographically distributed turbines, dispatchable sources, sufficient hydroelectric power, exporting and importing power to neighboring areas, energy storage, or reducing demand when wind production is low, can in many cases overcome these problems.Weather forecasting permits the electric-power network to be readied for the predictable variations in production that occur.In 2017, global wind power capacity expanded 10% to 539 GW.. Yearly wind energy production grew 17% reaching 4.4% of worldwide electric power usage, and providing 11.6% of the electricity in the European Union.Denmark is the country with the highest penetration of wind power, with 43.4% of its consumed electricity from wind in 2017. At least 83 other countries around the world are using wind power to supply their electric power grids.
Go to Article

Explanation by Hotspot Model

Youtube


    

Wind power

Wind power

Wind power

Licensed under Creative Commons Attribution-Share Alike 2.0 (林 慕尧 / Chris Lim from East Coast (东海岸), Singapore (新加坡)).

2016 World [civil] power generation by source [IEA, 2018] (Percentages of 24.973 TWh)[2]

  Coal (38.4%)
  Natural Gas (23.2%)
  Hydro (16.3%)
  Nuclear fission (10.4%)
  Oil (3.7%)
  Non hydro renew. (8%)

Wind power is the use of air flow through wind turbines to provide the mechanical power to turn electric generators. Wind power, as an alternative to burning fossil fuels, is plentiful, renewable, widely distributed, clean, produces no greenhouse gas emissions during operation, consumes no water, and uses little land.[3] The net effects on the environment are far less problematic than those of nonrenewable power sources.

Wind farms consist of many individual wind turbines, which are connected to the electric power transmission network. Onshore wind is an inexpensive source of electric power, competitive with or in many places cheaper than coal or gas plants.[4][5][6] Offshore wind is steadier and stronger than on land and offshore farms have less visual impact, but construction and maintenance costs are considerably higher. Small onshore wind farms can feed some energy into the grid or provide electric power to isolated off-grid locations.[7]

Wind power gives variable power, which is very consistent from year to year but has significant variation over shorter time scales. It is therefore used in conjunction with other electric power sources to give a reliable supply. As the proportion of wind power in a region increases, a need to upgrade the grid and a lowered ability to supplant conventional production can occur.[8][9] Power-management techniques such as having excess capacity, geographically distributed turbines, dispatchable sources, sufficient hydroelectric power, exporting and importing power to neighboring areas, energy storage, or reducing demand when wind production is low, can in many cases overcome these problems.[10][11] Weather forecasting permits the electric-power network to be readied for the predictable variations in production that occur.[12][13][14]

In 2017, global wind power capacity expanded 10% to 539 GW.[15]. Yearly wind energy production grew 17% reaching 4.4% of worldwide electric power usage,[16] and providing 11.6% of the electricity in the European Union.[17] Denmark is the country with the highest penetration of wind power, with 43.4% of its consumed electricity from wind in 2017.[18][19] At least 83 other countries around the world are using wind power to supply their electric power grids.[20]

History

Wind power has been used as long as humans have put sails into the wind. For more than two millennia wind-powered machines have ground grain and pumped water. Wind power was widely available and not confined to the banks of fast-flowing streams, or later, requiring sources of fuel. Wind-powered pumps drained the polders of the Netherlands, and in arid regions such as the American mid-west or the Australian outback, wind pumps provided water for livestock and steam engines.

The first windmill used for the production of electric power was built in Scotland in July 1887 by Prof James Blyth of Anderson's College, Glasgow (the precursor of Strathclyde University).[21] Blyth's 10 metres (33 ft) high, cloth-sailed wind turbine was installed in the garden of his holiday cottage at Marykirk in Kincardineshire and was used to charge accumulators developed by the Frenchman Camille Alphonse Faure, to power the lighting in the cottage,[21] thus making it the first house in the world to have its electric power supplied by wind power.[22] Blyth offered the surplus electric power to the people of Marykirk for lighting the main street, however, they turned down the offer as they thought electric power was "the work of the devil."[21] Although he later built a wind turbine to supply emergency power to the local Lunatic Asylum, Infirmary and Dispensary of Montrose the invention never really caught on as the technology was not considered to be economically viable.[21]

Across the Atlantic, in Cleveland, Ohio a larger and heavily engineered machine was designed and constructed in the winter of 1887–1888 by Charles F. Brush,[23] this was built by his engineering company at his home and operated from 1886 until 1900.[24] The Brush wind turbine had a rotor 17 metres (56 ft) in diameter and was mounted on an 18 metres (59 ft) tower. Although large by today's standards, the machine was only rated at 12 kW. The connected dynamo was used either to charge a bank of batteries or to operate up to 100 incandescent light bulbs, three arc lamps, and various motors in Brush's laboratory.[25]

With the development of electric power, wind power found new applications in lighting buildings remote from centrally-generated power. Throughout the 20th century parallel paths developed small wind stations suitable for farms or residences, and larger utility-scale wind generators that could be connected to electric power grids for remote use of power. Today wind powered generators operate in every size range between tiny stations for battery charging at isolated residences, up to near-gigawatt sized offshore wind farms that provide electric power to national electrical networks.

Wind energy

Wind energy is the kinetic energy of air in motion, also called wind. Total wind energy flowing through an imaginary surface with area A during the time t is:

[27]

where ρ is the density of air; v is the wind speed; Avt is the volume of air passing through A (which is considered perpendicular to the direction of the wind); Avtρ is therefore the mass m passing through "A". Note that ½ ρv2 is the kinetic energy of the moving air per unit volume.

Power is energy per unit time, so the wind power incident on A (e.g. equal to the rotor area of a wind turbine) is:

[27]

Wind power in an open air stream is thus proportional to the third power of the wind speed; the available power increases eightfold when the wind speed doubles. Wind turbines for grid electric power therefore need to be especially efficient at greater wind speeds.

Wind is the movement of air across the surface of the Earth, affected by areas of high pressure and of low pressure.[28] The global wind kinetic energy averaged approximately 1.50 MJ/m2 over the period from 1979 to 2010, 1.31 MJ/m2 in the Northern Hemisphere with 1.70 MJ/m2 in the Southern Hemisphere. The atmosphere acts as a thermal engine, absorbing heat at higher temperatures, releasing heat at lower temperatures. The process is responsible for production of wind kinetic energy at a rate of 2.46 W/m2 sustaining thus the circulation of the atmosphere against frictional dissipation.[29]

Through wind resource assessment it is possible to provide estimates of wind power potential globally, by country or region, or for a specific site. A global assessment of wind power potential is available via the Global Wind Atlas provided by the Technical University of Denmark in partnership with the World Bank.[26] [30][31] Unlike 'static' wind resource atlases which average estimates of wind speed and power density across multiple years, tools such as Renewables.ninja provide time-varying simulations of wind speed and power output from different wind turbine models at an hourly resolution.[32]. More detailed, site specific assessments of wind resource potential can be obtained from specialist commercial providers, and many of the larger wind developers will maintain in-house modeling capabilities.

The total amount of economically extractable power available from the wind is considerably more than present human power use from all sources.[33] Axel Kleidon of the Max Planck Institute in Germany, carried out a "top down" calculation on how much wind energy there is, starting with the incoming solar radiation that drives the winds by creating temperature differences in the atmosphere. He concluded that somewhere between 18 TW and 68 TW could be extracted.[34]

Cristina Archer and Mark Z. Jacobson presented a "bottom-up" estimate, which unlike Kleidon's are based on actual measurements of wind speeds, and found that there is 1700 TW of wind power at an altitude of 100 metres over land and sea. Of this, "between 72 and 170 TW could be extracted in a practical and cost-competitive manner".[34] They later estimated 80 TW.[35] However research at Harvard University estimates 1 Watt/m2 on average and 2–10 MW/km2 capacity for large scale wind farms, suggesting that these estimates of total global wind resources are too high by a factor of about 4.[36]

The strength of wind varies, and an average value for a given location does not alone indicate the amount of energy a wind turbine could produce there.

To assess prospective wind power sites a probability distribution function is often fit to the observed wind speed data.[37] Different locations will have different wind speed distributions. The Weibull model closely mirrors the actual distribution of hourly/ten-minute wind speeds at many locations. The Weibull factor is often close to 2 and therefore a Rayleigh distribution can be used as a less accurate, but simpler model.[38]

Wind farms

Large onshore wind farms
Wind farm Capacity
(MW)
Country Refs
Gansu Wind Farm 6,800  China [39][40]
Muppandal wind farm 1,500  India [41]
Alta (Oak Creek-Mojave) 1,320  United States [42]
Jaisalmer Wind Park 1,064  India [43]
Shepherds Flat Wind Farm 845  United States [44]
Roscoe Wind Farm 782  United States
Horse Hollow Wind Energy Center 736  United States [45][46]
Capricorn Ridge Wind Farm 662  United States [45][46]
Fântânele-Cogealac Wind Farm 600  Romania [47]
Fowler Ridge Wind Farm 600  United States [48]
Whitelee Wind Farm 539  United Kingdom [49]

A wind farm is a group of wind turbines in the same location used for production of electric power. A large wind farm may consist of several hundred individual wind turbines distributed over an extended area, but the land between the turbines may be used for agricultural or other purposes. For example, Gansu Wind Farm, the largest wind farm in the world, has several thousand turbines. A wind farm may also be located offshore.

Almost all large wind turbines have the same design — a horizontal axis wind turbine having an upwind rotor with three blades, attached to a nacelle on top of a tall tubular tower.

In a wind farm, individual turbines are interconnected with a medium voltage (often 34.5 kV), power collection system and communications network. In general, a distance of 7D (7 × Rotor Diameter of the Wind Turbine) is set between each turbine in a fully developed wind farm.[50] At a substation, this medium-voltage electric current is increased in voltage with a transformer for connection to the high voltage electric power transmission system.[citation needed]

Generator characteristics and stability

Induction generators, which were often used for wind power projects in the 1980s and 1990s, require reactive power for excitation so substations used in wind-power collection systems include substantial capacitor banks for power factor correction. Different types of wind turbine generators behave differently during transmission grid disturbances, so extensive modelling of the dynamic electromechanical characteristics of a new wind farm is required by transmission system operators to ensure predictable stable behaviour during system faults. In particular, induction generators cannot support the system voltage during faults, unlike steam or hydro turbine-driven synchronous generators.

Today these generators aren't used any more in modern turbines. Instead today most turbines use variable speed generators combined with partial- or full-scale power converter between the turbine generator and the collector system, which generally have more desirable properties for grid interconnection and have Low voltage ride through-capabilities.[51] Modern concepts use either doubly fed machines with partial-scale converters or squirrel-cage induction generators or synchronous generators (both permanently and electrically excited) with full scale converters.[52]

Transmission systems operators will supply a wind farm developer with a grid code to specify the requirements for interconnection to the transmission grid. This will include power factor, constancy of frequency and dynamic behaviour of the wind farm turbines during a system fault.[53][54]

Offshore wind power

Offshore wind power refers to the construction of wind farms in large bodies of water to generate electric power. These installations can utilize the more frequent and powerful winds that are available in these locations and have less aesthetic impact on the landscape than land based projects. However, the construction and the maintenance costs are considerably higher.[55][56]

Siemens and Vestas are the leading turbine suppliers for offshore wind power. Ørsted, Vattenfall and E.ON are the leading offshore operators.[57] As of October 2010, 3.16 GW of offshore wind power capacity was operational, mainly in Northern Europe. According to BTM Consult, more than 16 GW of additional capacity will be installed before the end of 2014 and the UK and Germany will become the two leading markets. Offshore wind power capacity is expected to reach a total of 75 GW worldwide by 2020, with significant contributions from China and the US.[57] The UK's investments in offshore wind power have resulted in a rapid decrease of the usage of coal as an energy source between 2012 and 2017, as well as a drop in the usage of natural gas as an energy source in 2017.[58]

In 2012, 1,662 turbines at 55 offshore wind farms in 10 European countries produced 18 TWh, enough to power almost five million households.[59] As of September 2018 the Walney Extension in the United Kingdom is the largest offshore wind farm in the world at 659 MW.[60]

World's largest offshore wind farms
Wind farm Capacity (MW) Country Turbines and model Commissioned Refs
Walney Extension 659  United Kingdom 47 x Vestas 8MW
40 x Siemens Gamesa 7MW
2018 [60]
London Array 630  United Kingdom 175 × Siemens SWT-3.6 2012 [61][62][63]
Gemini Wind Farm 600  The Netherlands 150 × Siemens SWT-4.0 2017 [64]
Gwynt y Môr 576  United Kingdom 160 × Siemens SWT-3.6 107 2015 [65]
Greater Gabbard 504  United Kingdom 140 × Siemens SWT-3.6 2012 [66]
Anholt 400  Denmark 111 × Siemens SWT-3.6–120 2013 [67]
BARD Offshore 1 400  Germany 80 BARD 5.0 turbines 2013 [68]

Collection and transmission network

In a wind farm, individual turbines are interconnected with a medium voltage (usually 34.5 kV) power collection system and communications network. At a substation, this medium-voltage electric current is increased in voltage with a transformer for connection to the high voltage electric power transmission system.

A transmission line is required to bring the generated power to (often remote) markets. For an off-shore station this may require a submarine cable. Construction of a new high-voltage line may be too costly for the wind resource alone, but wind sites may take advantage of lines installed for conventionally fueled generation.

One of the biggest current challenges to wind power grid integration in the United States is the necessity of developing new transmission lines to carry power from wind farms, usually in remote lowly populated states in the middle of the country due to availability of wind, to high load locations, usually on the coasts where population density is higher. The current transmission lines in remote locations were not designed for the transport of large amounts of energy.[69] As transmission lines become longer the losses associated with power transmission increase, as modes of losses at lower lengths are exacerbated and new modes of losses are no longer negligible as the length is increased, making it harder to transport large loads over large distances.[70] However, resistance from state and local governments makes it difficult to construct new transmission lines. Multi state power transmission projects are discouraged by states with cheap electric power rates for fear that exporting their cheap power will lead to increased rates. A 2005 energy law gave the Energy Department authority to approve transmission projects states refused to act on, but after an attempt to use this authority, the Senate declared the department was being overly aggressive in doing so.[69] Another problem is that wind companies find out after the fact that the transmission capacity of a new farm is below the generation capacity, largely because federal utility rules to encourage renewable energy installation allow feeder lines to meet only minimum standards. These are important issues that need to be solved, as when the transmission capacity does not meet the generation capacity, wind farms are forced to produce below their full potential or stop running all together, in a process known as curtailment. While this leads to potential renewable generation left untapped, it prevents possible grid overload or risk to reliable service.[71]

Wind power capacity and production

As of 2015, there are over 200,000 wind turbines operating, with a total nameplate capacity of 432 GW worldwide.[74] The European Union passed 100 GW nameplate capacity in September 2012,[75] while the United States surpassed 75 GW in 2015 and China's grid connected capacity passed 145 GW in 2015.[74] In 2015 wind power constituted 15.6% of all installed power generation capacity in the European Union and it generated around 11.4% of its power.[17]

World wind generation capacity more than quadrupled between 2000 and 2006, doubling about every 3 years. The United States pioneered wind farms and led the world in installed capacity in the 1980s and into the 1990s. In 1997 installed capacity in Germany surpassed the United States and led until once again overtaken by the United States in 2008. China has been rapidly expanding its wind installations in the late 2000s and passed the United States in 2010 to become the world leader. As of 2011, 83 countries around the world were using wind power on a commercial basis.[20]

The actual amount of electric power that wind is able to generate is calculated by multiplying the nameplate capacity by the capacity factor, which varies according to equipment and location. Estimates of the capacity factors for wind installations are in the range of 35% to 44%.[76]

Top wind power producing countries in 2015[77]
Country Wind-power
Production (TWh)
United States 190.7
China 185.8
Germany 78.9
Spain 48.1
India 42.8
United Kingdom 40.3
Canada 26.2
Brazil 21.6
France 21.2
Sweden 16.3
(rest of world) 161.7
World Total 833.6

Growth trends

The wind power industry set new records in 2014 – more than 50 GW of new capacity was installed. Another record breaking year occurred in 2015, with 22% annual market growth resulting in the 60 GW mark being passed.[79] In 2015, close to half of all new wind power was added outside of the traditional markets in Europe and North America. This was largely from new construction in China and India. Global Wind Energy Council (GWEC) figures show that 2015 recorded an increase of installed capacity of more than 63 GW, taking the total installed wind energy capacity to 432.9 GW, up from 74 GW in 2006. In terms of economic value, the wind energy sector has become one of the important players in the energy markets, with the total investments reaching US$329bn (296.6bn), an increase of 4% over 2014.[80][81]

Although the wind power industry was affected by the global financial crisis in 2009 and 2010, GWEC predicts that the installed capacity of wind power will be 792.1 GW by the end of 2020[79] and 4,042 GW by end of 2050.[82] The increased commissioning of wind power is being accompanied by record low prices for forthcoming renewable electric power. In some cases, wind onshore is already the cheapest electric power generation option and costs are continuing to decline. The contracted prices for wind onshore for the next few years are now as low as 30 USD/MWh.

In the EU in 2015, 44% of all new generating capacity was wind power; while in the same period net fossil fuel power capacity decreased.[17]

Capacity factor

Since wind speed is not constant, a wind farm's annual energy production is never as much as the sum of the generator nameplate ratings multiplied by the total hours in a year. The ratio of actual productivity in a year to this theoretical maximum is called the capacity factor. Typical capacity factors are 15–50%; values at the upper end of the range are achieved in favourable sites and are due to wind turbine design improvements.[83][84][nb 1]

Online data is available for some locations, and the capacity factor can be calculated from the yearly output.[85][86] For example, the German nationwide average wind power capacity factor over all of 2012 was just under 17.5% (45,867 GW·h/yr / (29.9 GW × 24 × 366) = 0.1746),[87] and the capacity factor for Scottish wind farms averaged 24% between 2008 and 2010.[88]

Unlike fueled generating plants, the capacity factor is affected by several parameters, including the variability of the wind at the site and the size of the generator relative to the turbine's swept area. A small generator would be cheaper and achieve a higher capacity factor but would produce less electric power (and thus less profit) in high winds. Conversely, a large generator would cost more but generate little extra power and, depending on the type, may stall out at low wind speed. Thus an optimum capacity factor of around 40–50% would be aimed for.[84][89]

A 2008 study released by the U.S. Department of Energy noted that the capacity factor of new wind installations was increasing as the technology improves, and projected further improvements for future capacity factors.[90] In 2010, the department estimated the capacity factor of new wind turbines in 2010 to be 45%.[91] The annual average capacity factor for wind generation in the US has varied between 29.8% and 34% during the period 2010–2015.[92]

Penetration

Country Penetration
Denmark (2015)[93][19] 42%
Portugal (2013)[94][95] 23%
Spain (2011)[96] 16%
Ireland (2012)[97] 16%
United Kingdom (2015)[98] 11%
Germany (2011)[99] 8%
United States (2016)[100] 6%

Wind energy penetration is the fraction of energy produced by wind compared with the total generation. The wind power penetration in world electric power generation in 2015 was 3.5%.[101][102]

There is no generally accepted maximum level of wind penetration. The limit for a particular grid will depend on the existing generating plants, pricing mechanisms, capacity for energy storage, demand management and other factors. An interconnected electric power grid will already include reserve generating and transmission capacity to allow for equipment failures. This reserve capacity can also serve to compensate for the varying power generation produced by wind stations. Studies have indicated that 20% of the total annual electrical energy consumption may be incorporated with minimal difficulty.[103] These studies have been for locations with geographically dispersed wind farms, some degree of dispatchable energy or hydropower with storage capacity, demand management, and interconnected to a large grid area enabling the export of electric power when needed. Beyond the 20% level, there are few technical limits, but the economic implications become more significant. Electrical utilities continue to study the effects of large scale penetration of wind generation on system stability and economics.[104][105][106][107]

A wind energy penetration figure can be specified for different duration of time, but is often quoted annually. To obtain 100% from wind annually requires substantial long term storage or substantial interconnection to other systems which may already have substantial storage. On a monthly, weekly, daily, or hourly basis—or less—wind might supply as much as or more than 100% of current use, with the rest stored or exported. Seasonal industry might then take advantage of high wind and low usage times such as at night when wind output can exceed normal demand. Such industry might include production of silicon, aluminum,[108] steel, or of natural gas, and hydrogen, and using future long term storage to facilitate 100% energy from variable renewable energy.[109][110] Homes can also be programmed to accept extra electric power on demand, for example by remotely turning up water heater thermostats.[111]

In Australia, the state of South Australia generates around half of the nation's wind power capacity. By the end of 2011 wind power in South Australia, championed by Premier (and Climate Change Minister) Mike Rann, reached 26% of the State's electric power generation, edging out coal for the first time.[112] At this stage South Australia, with only 7.2% of Australia's population, had 54% of Australia's installed capacity.[96][112]

Variability

Electric power generated from wind power can be highly variable at several different timescales: hourly, daily, or seasonally. Annual variation also exists, but is not as significant. Because instantaneous electrical generation and consumption must remain in balance to maintain grid stability, this variability can present substantial challenges to incorporating large amounts of wind power into a grid system. Intermittency and the non-dispatchable nature of wind energy production can raise costs for regulation, incremental operating reserve, and (at high penetration levels) could require an increase in the already existing energy demand management, load shedding, storage solutions or system interconnection with HVDC cables.

Fluctuations in load and allowance for failure of large fossil-fuel generating units requires operating reserve capacity, which can be increased to compensate for variability of wind generation.

Wind power is variable, and during low wind periods it must be replaced by other power sources. Transmission networks presently cope with outages of other generation plants and daily changes in electrical demand, but the variability of intermittent power sources such as wind power, is more frequent than those of conventional power generation plants which, when scheduled to be operating, may be able to deliver their nameplate capacity around 95% of the time.

Presently, grid systems with large wind penetration require a small increase in the frequency of usage of natural gas spinning reserve power plants to prevent a loss of electric power in the event that there is no wind. At low wind power penetration, this is less of an issue.[113][114][115]

GE has installed a prototype wind turbine with onboard battery similar to that of an electric car, equivalent of 1 minute of production. Despite the small capacity, it is enough to guarantee that power output complies with forecast for 15 minutes, as the battery is used to eliminate the difference rather than provide full output. In certain cases the increased predictability can be used to take wind power penetration from 20 to 30 or 40 per cent. The battery cost can be retrieved by selling burst power on demand and reducing backup needs from gas plants.[116]

In the UK there were 124 separate occasions from 2008 to 2010 when the nation's wind output fell to less than 2% of installed capacity.[117] A report on Denmark's wind power noted that their wind power network provided less than 1% of average demand on 54 days during the year 2002.[118] Wind power advocates argue that these periods of low wind can be dealt with by simply restarting existing power stations that have been held in readiness, or interlinking with HVDC.[119] Electrical grids with slow-responding thermal power plants and without ties to networks with hydroelectric generation may have to limit the use of wind power.[118] According to a 2007 Stanford University study published in the Journal of Applied Meteorology and Climatology, interconnecting ten or more wind farms can allow an average of 33% of the total energy produced (i.e. about 8% of total nameplate capacity) to be used as reliable, baseload electric power which can be relied on to handle peak loads, as long as minimum criteria are met for wind speed and turbine height.[120][121]

Conversely, on particularly windy days, even with penetration levels of 16%, wind power generation can surpass all other electric power sources in a country. In Spain, in the early hours of 16 April 2012 wind power production reached the highest percentage of electric power production till then, at 60.46% of the total demand.[122] In Denmark, which had power market penetration of 30% in 2013, over 90 hours, wind power generated 100% of the country's power, peaking at 122% of the country's demand at 2 am on 28 October.[123]

Increase in system operation costs, Euros per MWh, for 10% & 20% wind share[8]
Country 10% 20%
Germany 2.5 3.2
Denmark 0.4 0.8
Finland 0.3 1.5
Norway 0.1 0.3
Sweden 0.3 0.7

A 2006 International Energy Agency forum presented costs for managing intermittency as a function of wind-energy's share of total capacity for several countries, as shown in the table on the right. Three reports on the wind variability in the UK issued in 2009, generally agree that variability of wind needs to be taken into account by adding 20% to the operating reserve, but it does not make the grid unmanageable. The additional costs, which are modest, can be quantified.[9]

The combination of diversifying variable renewables by type and location, forecasting their variation, and integrating them with dispatchable renewables, flexible fueled generators, and demand response can create a power system that has the potential to meet power supply needs reliably. Integrating ever-higher levels of renewables is being successfully demonstrated in the real world:

In 2009, eight American and three European authorities, writing in the leading electrical engineers' professional journal, didn't find "a credible and firm technical limit to the amount of wind energy that can be accommodated by electric power grids". In fact, not one of more than 200 international studies, nor official studies for the eastern and western U.S. regions, nor the International Energy Agency, has found major costs or technical barriers to reliably integrating up to 30% variable renewable supplies into the grid, and in some studies much more.

— [124]

Solar power tends to be complementary to wind.[125][126] On daily to weekly timescales, high pressure areas tend to bring clear skies and low surface winds, whereas low pressure areas tend to be windier and cloudier. On seasonal timescales, solar energy peaks in summer, whereas in many areas wind energy is lower in summer and higher in winter.[nb 2][127] Thus the seasonal variation of wind and solar power tend to cancel each other somewhat. In 2007 the Institute for Solar Energy Supply Technology of the University of Kassel pilot-tested a combined power plant linking solar, wind, biogas and hydrostorage to provide load-following power around the clock and throughout the year, entirely from renewable sources.[128]

Predictability

Wind power forecasting methods are used, but predictability of any particular wind farm is low for short-term operation. For any particular generator there is an 80% chance that wind output will change less than 10% in an hour and a 40% chance that it will change 10% or more in 5 hours.[129]

However, studies by Graham Sinden (2009) suggest that, in practice, the variations in thousands of wind turbines, spread out over several different sites and wind regimes, are smoothed. As the distance between sites increases, the correlation between wind speeds measured at those sites, decreases.[130]

Thus, while the output from a single turbine can vary greatly and rapidly as local wind speeds vary, as more turbines are connected over larger and larger areas the average power output becomes less variable and more predictable.[14][131]

Wind power hardly ever suffers major technical failures, since failures of individual wind turbines have hardly any effect on overall power, so that the distributed wind power is reliable and predictable,[132][unreliable source?] whereas conventional generators, while far less variable, can suffer major unpredictable outages.

Energy storage

Typically, conventional hydroelectricity complements wind power very well. When the wind is blowing strongly, nearby hydroelectric stations can temporarily hold back their water. When the wind drops they can, provided they have the generation capacity, rapidly increase production to compensate. This gives a very even overall power supply and virtually no loss of energy and uses no more water.

Alternatively, where a suitable head of water is not available, pumped-storage hydroelectricity or other forms of grid energy storage such as compressed air energy storage and thermal energy storage can store energy developed by high-wind periods and release it when needed. The type of storage needed depends on the wind penetration level – low penetration requires daily storage, and high penetration requires both short and long term storage – as long as a month or more. Stored energy increases the economic value of wind energy since it can be shifted to displace higher cost generation during peak demand periods. The potential revenue from this arbitrage can offset the cost and losses of storage. For example, in the UK, the 1.7 GW Dinorwig pumped-storage plant evens out electrical demand peaks, and allows base-load suppliers to run their plants more efficiently. Although pumped-storage power systems are only about 75% efficient, and have high installation costs, their low running costs and ability to reduce the required electrical base-load can save both fuel and total electrical generation costs.[133][134]

In particular geographic regions, peak wind speeds may not coincide with peak demand for electrical power. In the U.S. states of California and Texas, for example, hot days in summer may have low wind speed and high electrical demand due to the use of air conditioning. Some utilities subsidize the purchase of geothermal heat pumps by their customers, to reduce electric power demand during the summer months by making air conditioning up to 70% more efficient;[135] widespread adoption of this technology would better match electric power demand to wind availability in areas with hot summers and low summer winds. A possible future option may be to interconnect widely dispersed geographic areas with an HVDC "super grid". In the U.S. it is estimated that to upgrade the transmission system to take in planned or potential renewables would cost at least USD 60 bn,[136] while the society value of added windpower would be more than that cost.[137]

Germany has an installed capacity of wind and solar that can exceed daily demand, and has been exporting peak power to neighboring countries, with exports which amounted to some 14.7 billion kWh in 2012.[138] A more practical solution is the installation of thirty days storage capacity able to supply 80% of demand, which will become necessary when most of Europe's energy is obtained from wind power and solar power. Just as the EU requires member countries to maintain 90 days strategic reserves of oil it can be expected that countries will provide electric power storage, instead of expecting to use their neighbors for net metering.[139]

Capacity credit, fuel savings and energy payback

The capacity credit of wind is estimated by determining the capacity of conventional plants displaced by wind power, whilst maintaining the same degree of system security.[140][141] According to the American Wind Energy Association, production of wind power in the United States in 2015 avoided consumption of 73 billion gallons of water and reduced CO2 emissions by 132 million metric tons, while providing USD 7.3 bn in public health savings.[142][143]

The energy needed to build a wind farm divided into the total output over its life, Energy Return on Energy Invested, of wind power varies but averages about 20–25.[144][145] Thus, the energy payback time is typically around a year.

Economics

Wind turbines reached grid parity (the point at which the cost of wind power matches traditional sources) in some areas of Europe in the mid-2000s, and in the US around the same time. Falling prices continue to drive the levelized cost down and it has been suggested that it has reached general grid parity in Europe in 2010, and will reach the same point in the US around 2016 due to an expected reduction in capital costs of about 12%.[146]

Electric power cost and trends

Wind power is capital intensive, but has no fuel costs.[148] The price of wind power is therefore much more stable than the volatile prices of fossil fuel sources.[149] The marginal cost of wind energy once a station is constructed is usually less than 1-cent per kW·h.[150]

However, the estimated average cost per unit of electric power must incorporate the cost of construction of the turbine and transmission facilities, borrowed funds, return to investors (including cost of risk), estimated annual production, and other components, averaged over the projected useful life of the equipment, which may be in excess of twenty years. Energy cost estimates are highly dependent on these assumptions so published cost figures can differ substantially. In 2004, wind energy cost a fifth of what it did in the 1980s, and some expected that downward trend to continue as larger multi-megawatt turbines were mass-produced.[151] In 2012 capital costs for wind turbines were substantially lower than 2008–2010 but still above 2002 levels.[152] A 2011 report from the American Wind Energy Association stated, "Wind's costs have dropped over the past two years, in the range of 5 to 6 cents per kilowatt-hour recently.... about 2 cents cheaper than coal-fired electric power, and more projects were financed through debt arrangements than tax equity structures last year.... winning more mainstream acceptance from Wall Street's banks.... Equipment makers can also deliver products in the same year that they are ordered instead of waiting up to three years as was the case in previous cycles.... 5,600 MW of new installed capacity is under construction in the United States, more than double the number at this point in 2010. Thirty-five percent of all new power generation built in the United States since 2005 has come from wind, more than new gas and coal plants combined, as power providers are increasingly enticed to wind as a convenient hedge against unpredictable commodity price moves."[153]

A British Wind Energy Association report gives an average generation cost of onshore wind power of around 3.2 pence (between US 5 and 6 cents) per kW·h (2005).[154] Cost per unit of energy produced was estimated in 2006 to be 5 to 6 percent above the cost of new generating capacity in the US for coal and natural gas: wind cost was estimated at $55.80 per MW·h, coal at $53.10/MW·h and natural gas at $52.50.[155] Similar comparative results with natural gas were obtained in a governmental study in the UK in 2011.[156] In 2011 power from wind turbines could be already cheaper than fossil or nuclear plants; it is also expected that wind power will be the cheapest form of energy generation in the future.[11] The presence of wind energy, even when subsidised, can reduce costs for consumers (€5 billion/yr in Germany) by reducing the marginal price, by minimising the use of expensive peaking power plants.[157]

A 2012 EU study shows base cost of onshore wind power similar to coal, when subsidies and externalities are disregarded. Wind power has some of the lowest external costs.[158]

In February 2013 Bloomberg New Energy Finance (BNEF) reported that the cost of generating electric power from new wind farms is cheaper than new coal or new baseload gas plants. When including the current Australian federal government carbon pricing scheme their modeling gives costs (in Australian dollars) of $80/MWh for new wind farms, $143/MWh for new coal plants and $116/MWh for new baseload gas plants. The modeling also shows that "even without a carbon price (the most efficient way to reduce economy-wide emissions) wind energy is 14% cheaper than new coal and 18% cheaper than new gas."[159] Part of the higher costs for new coal plants is due to high financial lending costs because of "the reputational damage of emissions-intensive investments". The expense of gas fired plants is partly due to "export market" effects on local prices. Costs of production from coal fired plants built in "the 1970s and 1980s" are cheaper than renewable energy sources because of depreciation.[159] In 2015 BNEF calculated LCOE prices per MWh energy in new powerplants (excluding carbon costs) : $85 for onshore wind ($175 for offshore), $66–75 for coal in the Americas ($82–105 in Europe), gas $80–100.[160][161][162] A 2014 study showed unsubsidized LCOE costs between $37–81, depending on region.[163] A 2014 US DOE report showed that in some cases power purchase agreement prices for wind power had dropped to record lows of $23.5/MWh.[164]

The cost has reduced as wind turbine technology has improved. There are now longer and lighter wind turbine blades, improvements in turbine performance and increased power generation efficiency. Also, wind project capital and maintenance costs have continued to decline.[165] For example, the wind industry in the US in early 2014 were able to produce more power at lower cost by using taller wind turbines with longer blades, capturing the faster winds at higher elevations. This has opened up new opportunities and in Indiana, Michigan, and Ohio, the price of power from wind turbines built 300 feet to 400 feet above the ground can now compete with conventional fossil fuels like coal. Prices have fallen to about 4 cents per kilowatt-hour in some cases and utilities have been increasing the amount of wind energy in their portfolio, saying it is their cheapest option.[166]

A number of initiatives are working to reduce costs of electric power from offshore wind. One example is the Carbon Trust Offshore Wind Accelerator, a joint industry project, involving nine offshore wind developers, which aims to reduce the cost of offshore wind by 10% by 2015. It has been suggested that innovation at scale could deliver 25% cost reduction in offshore wind by 2020.[167] Henrik Stiesdal, former Chief Technical Officer at Siemens Wind Power, has stated that by 2025 energy from offshore wind will be one of the cheapest, scalable solutions in the UK, compared to other renewables and fossil fuel energy sources, if the true cost to society is factored into the cost of energy equation.[168] He calculates the cost at that time to be 43 EUR/MWh for onshore, and 72 EUR/MWh for offshore wind.[169]

In August 2017, the Department of Energy's National Renewable Energy Laboratory (NREL) published a new report on a 50% reduction in wind power cost by 2030. The NREL is expected to achieve advances in wind turbine design, materials and controls to unlock performance improvements and reduce costs. According to international surveyors, this study shows that cost cutting is projected to fluctuate between 24% and 30% by 2030. In more aggressive cases, experts estimate cost reduction Up to 40 percent if the research and development and technology programs result in additional efficiency.[170]

Incentives and community benefits

U.S. landowners typically receive $3,000–$5,000 annual rental income per wind turbine, while farmers continue to grow crops or graze cattle up to the foot of the turbines.[171] Shown: the Brazos Wind Farm, Texas.
Some of the 6,000 turbines in California's Altamont Pass Wind Farm aided by tax incentives during the 1980s.[172]

The wind industry in the United States generates tens of thousands of jobs and billions of dollars of economic activity.[173] Wind projects provide local taxes, or payments in lieu of taxes and strengthen the economy of rural communities by providing income to farmers with wind turbines on their land.[171][174] Wind energy in many jurisdictions receives financial or other support to encourage its development. Wind energy benefits from subsidies in many jurisdictions, either to increase its attractiveness, or to compensate for subsidies received by other forms of production which have significant negative externalities.

In the US, wind power receives a production tax credit (PTC) of 1.5¢/kWh in 1993 dollars for each kW·h produced, for the first ten years; at 2.2 cents per kW·h in 2012, the credit was renewed on 2 January 2012, to include construction begun in 2013.[175] A 30% tax credit can be applied instead of receiving the PTC.[176][177] Another tax benefit is accelerated depreciation. Many American states also provide incentives, such as exemption from property tax, mandated purchases, and additional markets for "green credits".[178] The Energy Improvement and Extension Act of 2008 contains extensions of credits for wind, including microturbines. Countries such as Canada and Germany also provide incentives for wind turbine construction, such as tax credits or minimum purchase prices for wind generation, with assured grid access (sometimes referred to as feed-in tariffs). These feed-in tariffs are typically set well above average electric power prices.[179][180] In December 2013 U.S. Senator Lamar Alexander and other Republican senators argued that the "wind energy production tax credit should be allowed to expire at the end of 2013"[181] and it expired 1 January 2014 for new installations.

Secondary market forces also provide incentives for businesses to use wind-generated power, even if there is a premium price for the electricity. For example, socially responsible manufacturers pay utility companies a premium that goes to subsidize and build new wind power infrastructure. Companies use wind-generated power, and in return they can claim that they are undertaking strong "green" efforts. In the US the organization Green-e monitors business compliance with these renewable energy credits.[182] Turbine prices have fallen significantly in recent years due to tougher competitive conditions such as the increased use of energy auctions, and the elimination of subsidies in many markets. For example, Vestas, a wind turbine manufacturer, whose largest onshore turbine can pump out 4.2 megawatts of power, enough to provide electricity to roughly 5,000 homes, has seen prices for its turbines fall from €950,000 per megawatt in late 2016, to around €800,000 per megawatt in the third quarter of 2017.[183]

Small-scale wind power

Small-scale wind power is the name given to wind generation systems with the capacity to produce up to 50 kW of electrical power.[184] Isolated communities, that may otherwise rely on diesel generators, may use wind turbines as an alternative. Individuals may purchase these systems to reduce or eliminate their dependence on grid electric power for economic reasons, or to reduce their carbon footprint. Wind turbines have been used for household electric power generation in conjunction with battery storage over many decades in remote areas.[185]

Recent examples of small-scale wind power projects in an urban setting can be found in New York City, where, since 2009, a number of building projects have capped their roofs with Gorlov-type helical wind turbines. Although the energy they generate is small compared to the buildings' overall consumption, they help to reinforce the building's 'green' credentials in ways that "showing people your high-tech boiler" cannot, with some of the projects also receiving the direct support of the New York State Energy Research and Development Authority.[186]

Grid-connected domestic wind turbines may use grid energy storage, thus replacing purchased electric power with locally produced power when available. The surplus power produced by domestic microgenerators can, in some jurisdictions, be fed into the network and sold to the utility company, producing a retail credit for the microgenerators' owners to offset their energy costs.[187]

Off-grid system users can either adapt to intermittent power or use batteries, photovoltaic or diesel systems to supplement the wind turbine. Equipment such as parking meters, traffic warning signs, street lighting, or wireless Internet gateways may be powered by a small wind turbine, possibly combined with a photovoltaic system, that charges a small battery replacing the need for a connection to the power grid.[188]

A Carbon Trust study into the potential of small-scale wind energy in the UK, published in 2010, found that small wind turbines could provide up to 1.5 terawatt hours (TW·h) per year of electric power (0.4% of total UK electric power consumption), saving 0.6 million tonnes of carbon dioxide (Mt CO2) emission savings. This is based on the assumption that 10% of households would install turbines at costs competitive with grid electric power, around 12 pence (US 19 cents) a kW·h.[189] A report prepared for the UK's government-sponsored Energy Saving Trust in 2006, found that home power generators of various kinds could provide 30 to 40% of the country's electric power needs by 2050.[190]

Distributed generation from renewable resources is increasing as a consequence of the increased awareness of climate change. The electronic interfaces required to connect renewable generation units with the utility system can include additional functions, such as the active filtering to enhance the power quality.[191]

Environmental effects

The environmental impact of wind power when compared to the environmental impacts of fossil fuels, is relatively minor. According to the IPCC, in assessments of the life-cycle global warming potential of energy sources, wind turbines have a median value of between 12 and 11 (gCO2eq/kWh) depending on whether off- or onshore turbines are being assessed.[193][194] Compared with other low carbon power sources, wind turbines have some of the lowest global warming potential per unit of electrical energy generated.[195]

While a wind farm may cover a large area of land, many land uses such as agriculture are compatible with it, as only small areas of turbine foundations and infrastructure are made unavailable for use.[196][197]

There are reports of bird and bat mortality at wind turbines as there are around other artificial structures. The scale of the ecological impact may[198] or may not[199] be significant, depending on specific circumstances. Prevention and mitigation of wildlife fatalities, and protection of peat bogs,[200] affect the siting and operation of wind turbines.

Wind turbines generate some noise. At a residential distance of 300 metres (980 ft) this may be around 45 dB, which is slightly louder than a refrigerator. At 1.5 km (1 mi) distance they become inaudible.[201][202] There are anecdotal reports of negative health effects from noise on people who live very close to wind turbines.[203] Peer-reviewed research has generally not supported these claims.[204][205][206]

The United States Air Force and Navy have expressed concern that siting large wind turbines near bases "will negatively impact radar to the point that air traffic controllers will lose the location of aircraft."[207]

Aesthetic aspects of wind turbines and resulting changes of the visual landscape are significant.[208] Conflicts arise especially in scenic and heritage protected landscapes.

Politics

Central government

Nuclear power and fossil fuels are subsidized by many governments, and wind power and other forms of renewable energy are also often subsidized. For example, a 2009 study by the Environmental Law Institute[209] assessed the size and structure of U.S. energy subsidies over the 2002–2008 period. The study estimated that subsidies to fossil-fuel based sources amounted to approximately $72 billion over this period and subsidies to renewable fuel sources totalled $29 billion. In the United States, the federal government has paid US$74 billion for energy subsidies to support R&D for nuclear power ($50 billion) and fossil fuels ($24 billion) from 1973 to 2003. During this same time frame, renewable energy technologies and energy efficiency received a total of US$26 billion. It has been suggested that a subsidy shift would help to level the playing field and support growing energy sectors, namely solar power, wind power, and biofuels.[210] History shows that no energy sector was developed without subsidies.[210]

According to the International Energy Agency (IEA) (2011), energy subsidies artificially lower the price of energy paid by consumers, raise the price received by producers or lower the cost of production. "Fossil fuels subsidies costs generally outweigh the benefits. Subsidies to renewables and low-carbon energy technologies can bring long-term economic and environmental benefits".[211] In November 2011, an IEA report entitled Deploying Renewables 2011 said "subsidies in green energy technologies that were not yet competitive are justified in order to give an incentive to investing into technologies with clear environmental and energy security benefits". The IEA's report disagreed with claims that renewable energy technologies are only viable through costly subsidies and not able to produce energy reliably to meet demand.

However, IEA's views are not universally accepted. Between 2010 and 2016, subsidies for wind were between 1.3¢ and 5.7¢ per kWh. Subsidies for coal, natural gas and nuclear are all between 0.05¢ and 0.2¢ per kWh over all years. On a per-kWh basis, wind is subsidized 50 times as much as traditional sources.[212]

In the United States, the wind power industry has recently increased its lobbying efforts considerably, spending about $5 million in 2009 after years of relative obscurity in Washington.[213] By comparison, the U.S. nuclear industry alone spent over $650 million on its lobbying efforts and campaign contributions during a ten-year period ending in 2008.[214][215][216]

Following the 2011 Japanese nuclear accidents, Germany's federal government is working on a new plan for increasing energy efficiency and renewable energy commercialization, with a particular focus on offshore wind farms. Under the plan, large wind turbines will be erected far away from the coastlines, where the wind blows more consistently than it does on land, and where the enormous turbines won't bother the inhabitants. The plan aims to decrease Germany's dependence on energy derived from coal and nuclear power plants.[217]

Public opinion

Surveys of public attitudes across Europe and in many other countries show strong public support for wind power.[218][219][220] About 80% of EU citizens support wind power.[221] In Germany, where wind power has gained very high social acceptance, hundreds of thousands of people have invested in citizens' wind farms across the country and thousands of small and medium-sized enterprises are running successful businesses in a new sector that in 2008 employed 90,000 people and generated 8% of Germany's electric power.[222][223]

Bakker et al. (2012) discovered in their study that when residents did not want the turbines located by them their annoyance was significantly higher than those "that benefited economically from wind turbines the proportion of people who were rather or very annoyed was significantly lower".[224]

Although wind power is a popular form of energy generation, the construction of wind farms is not universally welcomed, often for aesthetic reasons.[196][218][219][220][221][225][226]

In Spain, with some exceptions, there has been little opposition to the installation of inland wind parks. However, the projects to build offshore parks have been more controversial.[227] In particular, the proposal of building the biggest offshore wind power production facility in the world in southwestern Spain in the coast of Cádiz, on the spot of the 1805 Battle of Trafalgar[228] has been met with strong opposition who fear for tourism and fisheries in the area,[229] and because the area is a war grave.[228]

Which should be increased in Scotland?[230]

In a survey conducted by Angus Reid Strategies in October 2007, 89 per cent of respondents said that using renewable energy sources like wind or solar power was positive for Canada, because these sources were better for the environment. Only 4 per cent considered using renewable sources as negative since they can be unreliable and expensive.[231] According to a Saint Consulting survey in April 2007, wind power was the alternative energy source most likely to gain public support for future development in Canada, with only 16% opposed to this type of energy. By contrast, 3 out of 4 Canadians opposed nuclear power developments.[232]

A 2003 survey of residents living around Scotland's 10 existing wind farms found high levels of community acceptance and strong support for wind power, with much support from those who lived closest to the wind farms. The results of this survey support those of an earlier Scottish Executive survey 'Public attitudes to the Environment in Scotland 2002', which found that the Scottish public would prefer the majority of their electric power to come from renewables, and which rated wind power as the cleanest source of renewable energy.[233] A survey conducted in 2005 showed that 74% of people in Scotland agree that wind farms are necessary to meet current and future energy needs. When people were asked the same question in a Scottish renewables study conducted in 2010, 78% agreed. The increase is significant as there were twice as many wind farms in 2010 as there were in 2005. The 2010 survey also showed that 52% disagreed with the statement that wind farms are "ugly and a blot on the landscape". 59% agreed that wind farms were necessary and that how they looked was unimportant.[234] Regarding tourism, query responders consider power pylons, cell phone towers, quarries and plantations more negatively than wind farms.[235] Scotland is planning to obtain 100% of electric power from renewable sources by 2020.[236]

In other cases there is direct community ownership of wind farm projects. The hundreds of thousands of people who have become involved in Germany's small and medium-sized wind farms demonstrate such support there.[237]

A 2010 Harris Poll reflects the strong support for wind power in Germany, other European countries, and the United States.[218][219][238]

Opinion on increase in number of wind farms, 2010 Harris Poll[239]
U.S. Great
Britain
France Italy Spain Germany
% % % % % %
Strongly oppose 3 6 6 2 2 4
Oppose more than favour 9 12 16 11 9 14
Favour more than oppose 37 44 44 38 37 42
Strongly favour 50 38 33 49 53 40

Community

Many wind power companies work with local communities to reduce environmental and other concerns associated with particular wind farms.[242][243][244] In other cases there is direct community ownership of wind farm projects. Appropriate government consultation, planning and approval procedures also help to minimize environmental risks.[218][245][246] Some may still object to wind farms[247] but, according to The Australia Institute, their concerns should be weighed against the need to address the threats posed by climate change and the opinions of the broader community.[248]

In America, wind projects are reported to boost local tax bases, helping to pay for schools, roads and hospitals. Wind projects also revitalize the economy of rural communities by providing steady income to farmers and other landowners.[171]

In the UK, both the National Trust and the Campaign to Protect Rural England have expressed concerns about the effects on the rural landscape caused by inappropriately sited wind turbines and wind farms.[249][250]

Some wind farms have become tourist attractions. The Whitelee Wind Farm Visitor Centre has an exhibition room, a learning hub, a café with a viewing deck and also a shop. It is run by the Glasgow Science Centre.[251]

In Denmark, a loss-of-value scheme gives people the right to claim compensation for loss of value of their property if it is caused by proximity to a wind turbine. The loss must be at least 1% of the property's value.[252]

Despite this general support for the concept of wind power in the public at large, local opposition often exists and has delayed or aborted a number of projects.[253][254][255] For example, there are concerns that some installations can negatively affect TV and radio reception and Doppler weather radar, as well as produce excessive sound and vibration levels leading to a decrease in property values.[256] Potential broadcast-reception solutions include predictive interference modeling as a component of site selection.[257][258] A study of 50,000 home sales near wind turbines found no statistical evidence that prices were affected.[259]

While aesthetic issues are subjective and some find wind farms pleasant and optimistic, or symbols of energy independence and local prosperity, protest groups are often formed to attempt to block new wind power sites for various reasons.[247][260][261]

This type of opposition is often described as NIMBYism,[262] but research carried out in 2009 found that there is little evidence to support the belief that residents only object to renewable power facilities such as wind turbines as a result of a "Not in my Back Yard" attitude.[263]

Turbine design

Wind turbines are devices that convert the wind's kinetic energy into electrical power. The result of over a millennium of windmill development and modern engineering, today's wind turbines are manufactured in a wide range of horizontal axis and vertical axis types. The smallest turbines are used for applications such as battery charging for auxiliary power. Slightly larger turbines can be used for making small contributions to a domestic power supply while selling unused power back to the utility supplier via the electrical grid. Arrays of large turbines, known as wind farms, have become an increasingly important source of renewable energy and are used in many countries as part of a strategy to reduce their reliance on fossil fuels.

Wind turbine design is the process of defining the form and specifications of a wind turbine to extract energy from the wind.[264] A wind turbine installation consists of the necessary systems needed to capture the wind's energy, point the turbine into the wind, convert mechanical rotation into electrical power, and other systems to start, stop, and control the turbine.

In 1919 the German physicist Albert Betz showed that for a hypothetical ideal wind-energy extraction machine, the fundamental laws of conservation of mass and energy allowed no more than 16/27 (59%) of the kinetic energy of the wind to be captured. This Betz limit can be approached in modern turbine designs, which may reach 70 to 80% of the theoretical Betz limit.[265][266]

The aerodynamics of a wind turbine are not straightforward. The air flow at the blades is not the same as the airflow far away from the turbine. The very nature of the way in which energy is extracted from the air also causes air to be deflected by the turbine. In addition the aerodynamics of a wind turbine at the rotor surface exhibit phenomena that are rarely seen in other aerodynamic fields. The shape and dimensions of the blades of the wind turbine are determined by the aerodynamic performance required to efficiently extract energy from the wind, and by the strength required to resist the forces on the blade.[267]

In addition to the aerodynamic design of the blades, the design of a complete wind power system must also address the design of the installation's rotor hub, nacelle, tower structure, generator, controls, and foundation.[268] Turbine design makes extensive use of computer modelling and simulation tools. These are becoming increasingly sophisticated as highlighted by a recent state-of-the-art review by Hewitt et al.[269] Further design factors must also be considered when integrating wind turbines into electrical power grids.

See also



This article uses material from the Wikipedia article "Wind power", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Environmental Protection

Environment Ecology