powered by CADENAS

Social Share

Glasses (7892 views - Consumer products)

Glasses, also known as eyeglasses or spectacles, are devices consisting of glass or hard plastic lenses mounted in a frame that holds them in front of a person's eyes, typically using a bridge over the nose and arms which rest over the ears. Glasses are typically used for vision correction, such as with reading glasses and glasses used for nearsightedness. Safety glasses provide eye protection against flying debris for construction workers or lab technicians; these glasses may have protection for the sides of the eyes as well as in the lenses. Some types of safety glasses are used to protect against visible and near-visible light or radiation. Glasses are worn for eye protection in some sports, such as squash. Glasses wearers may use a strap to prevent the glasses from falling off during movement or sports. Wearers of glasses that are used only part of the time may have the glasses attached to a cord that goes around their neck, to prevent the loss of the glasses. Sunglasses allow better vision in bright daylight, and may protect one's eyes against damage from high levels of ultraviolet light. Typical sunglasses are darkened for protection against bright light or glare; some specialized glasses are clear in dark or indoor conditions, but turn into sunglasses when in bright light. Most sunglasses do not have corrective power in the lenses; however, special prescription sunglasses can be ordered. Specialized glasses may be used for viewing specific visual information (such as stereoscopy) or 3D glasses for viewing three-dimensional movies. Sometimes glasses with no corrective power in the lenses are worn simply for aesthetic or fashion purposes. Even with glasses used for vision correction, a wide range of designs are available for fashion purposes, using plastic, wire, and other materials. People are more likely to need glasses the older they get with 93% of people between the age of 65-75 wearing corrective lenses.
Go to Article

Explanation by Hotspot Model

Glasses

Glasses

Glasses
A modern pair of prescription reading glasses

Glasses, also known as eyeglasses or spectacles, are devices consisting of glass or hard plastic lenses mounted in a frame that holds them in front of a person's eyes, typically using a bridge over the nose and arms which rest over the ears. Glasses are typically used for vision correction, such as with reading glasses and glasses used for nearsightedness. Safety glasses provide eye protection against flying debris for construction workers or lab technicians; these glasses may have protection for the sides of the eyes as well as in the lenses. Some types of safety glasses are used to protect against visible and near-visible light or radiation. Glasses are worn for eye protection in some sports, such as squash. Glasses wearers may use a strap to prevent the glasses from falling off during movement or sports. Wearers of glasses that are used only part of the time may have the glasses attached to a cord that goes around their neck, to prevent the loss of the glasses.

Sunglasses allow better vision in bright daylight, and may protect one's eyes against damage from high levels of ultraviolet light. Typical sunglasses are darkened for protection against bright light or glare; some specialized glasses are clear in dark or indoor conditions, but turn into sunglasses when in bright light. Most sunglasses do not have corrective power in the lenses; however, special prescription sunglasses can be ordered. Specialized glasses may be used for viewing specific visual information (such as stereoscopy) or 3D glasses for viewing three-dimensional movies. Sometimes glasses with no corrective power in the lenses are worn simply for aesthetic or fashion purposes. Even with glasses used for vision correction, a wide range of designs are available for fashion purposes, using plastic, wire, and other materials.

People are more likely to need glasses the older they get with 93% of people between the age of 65-75 wearing corrective lenses.[1][2]

Types

Glasses come in many types. They can be classified by their primary function, but also appear in combinations such as prescription sunglasses or safety glasses with enhanced magnification.

Corrective

Corrective lenses are used to correct refractive errors by bending the light entering the eye in order to alleviate the effects of conditions such as nearsightedness (myopia), farsightedness (Hypermetropia) or astigmatism. The ability of one's eyes to accommodate their focus to near and distant focus alters over time. Also, few people have eyes that show exactly equal refractive characteristics; one may need a "stronger", (i.e. more refracting), lens than the other. A common condition in people over forty years old is presbyopia, which is caused by the eye's crystalline lens losing elasticity, progressively reducing the ability of the lens to accommodate (i.e. to focus on objects close to the eye). Corrective lenses, to bring the image back into focus on the retina, are made to conform to the prescription of an ophthalmologist or optometrist. A lensmeter can be used to verify the specifications of an existing pair of glasses. Corrective eyeglasses can significantly improve the life quality of the wearer. Not only do they enhance the wearer's visual experience, but can also reduce problems that result from eye strain, such as headaches or squinting.

Pinhole glasses are a type of corrective glasses that do not use a lens. Pinhole glasses do not actually refract the light or change focal length. Instead, they create a diffraction limited system, which has an increased depth of field, similar to using a small aperture in photography. This form of correction has many limitations that prevent it from gaining popularity in everyday use. Pinhole glasses can be made in a DIY fashion by making small holes in a piece of card which is then held in front of the eyes with a strap or cardboard arms.

The most common type of corrective lens is "single vision", which has a uniform refractive index. For people with presbyopia and hyperopia, bifocal and trifocal glasses provide two or three different refractive indices, respectively, and progressive lenses have a continuous gradient. Reading glasses provide a separate set of glasses for focusing on close-by objects. Reading glasses are available without prescription from drugstores, and offer a cheap, practical solution, though these have two simple lenses of equal power, so will not correct refraction problems like astigmatism or refractive or prismatic variations between the left and right eye. For total correction of the individual's sight, glasses complying to a recent ophthalmic prescription are required. Adjustable-focus eyeglasses might be used to replace bifocals or trifocals, or might be used to produce cheaper single-vision glasses (since they don't have to be custom-manufactured for every person).

Safety

Safety glasses are worn to protect the eyes during a variety of tasks. They are made with shatter-resistant plastic lenses to protect the eye from flying debris or other matter. Construction workers, factory workers, machinists and lab technicians are often required to wear safety glasses to shield the eyes from flying debris or hazardous splatters such as blood or chemicals. As of 2017, dentists and surgeons in Canada and other countries are required to wear safety glasses to protect against infection from patients' blood or other body fluids. There are also safety glasses for welding, which are styled like wraparound sunglasses, but with much darker lenses, for use in welding where a full sized welding helmet is inconvenient or uncomfortable. These are often called "flash goggles", because they provide protection from welding flash. Nylon frames are usually used for protection eyewear for sports because of their lightweight and flexible properties. Unlike most regular glasses, safety glasses often include protection beside the eyes as well as in front of the eyes.

Sunglasses

Sunglasses provide improved comfort and protection against bright light and often against ultraviolet (UV) light. Photochromic lenses, which are photosensitive, darken when struck by UV light. The dark tint of the lenses in a pair of sunglasses blocks the transmission of light through the lens.

Light polarization is an added feature that can be applied to sunglass lenses. Polarization filters are positioned to remove horizontally polarized rays of light, which eliminates glare from horizontal surfaces (allowing wearers to see into water when reflected light would otherwise overwhelm the scene). Polarized sunglasses may present some difficulties for pilots since reflections from water and other structures often used to gauge altitude may be removed. Liquid crystal displays often emit polarized light making them sometimes difficult to view with polarized sunglasses. Sunglasses may be worn just for aesthetic purposes, or simply to hide the eyes. Examples of sunglasses that were popular for these reasons include teashades and mirrorshades. Many blind people wear nearly opaque glasses to hide their eyes for cosmetic reasons.

Sunglasses may also have corrective lenses, which requires a prescription. Clip-on sunglasses or sunglass clips can be attached to another pair of glasses. Some wrap-around sunglasses are large enough to be worn over top of another pair of glasses. Otherwise, many people opt to wear contact lenses to correct their vision so that standard sunglasses can be used.

3D glasses

The illusion of three dimensions on a two dimensional surface can be created by providing each eye with different visual information. 3D glasses create the illusion of three dimensions by filtering a signal containing information for both eyes. The signal, often light reflected off a movie screen or emitted from an electronic display, is filtered so that each eye receives a slightly different image. The filters only work for the type of signal they were designed for.

Anaglyph 3D glasses have a different colored filter for each eye, typically red and blue or red and green. A polarized 3D system on the other hand uses polarized filters. Polarized 3D glasses allow for color 3D, while the red-blue lenses produce an image with distorted coloration. An active shutter 3D system uses electronic shutters. Head-mounted displays can filter the signal electronically and then transmit light directly into the viewers eyes.

Anaglyph and polarized glasses are distributed to audiences at 3D movies. Polarized and active shutter glasses are used with many home theaters. Head-mounted displays are used by a single person, but the input signal can be shared between multiple units.

Magnification (bioptics)

Glasses can also provide magnification that is useful for people with vision impairments or specific occupational demands. An example would be bioptics or bioptic telescopes which have small telescopes mounted on, in, or behind their regular lenses. Newer designs use smaller lightweight telescopes, which can be embedded into the corrective glass and improve aesthetic appearance (mini telescopic spectacles). They may take the form of self-contained glasses that resemble goggles or binoculars, or may be attached to existing glasses.

Yellow-tinted computer/gaming glasses

Yellow tinted glasses are type of glasses, with a minor yellow tint. Basically performs minor color correction, on top of reducing headaches due to lack of blinking. May also be considered minor, corrective, unprescribed glasses[citation needed]. Depending on the company, these computer or gaming glasses can also filter out high energy blue and ultra-violet light from LCD screens, fluorescent lighting, and other sources of light. This allows for reduced eye-strain[citation needed]. These glasses can be ordered as standard or prescription lenses that fit into standard optical frames.[3] Due to the blue energy blocking nature of these lenses, they also help users sleep at night along with reducing age-related macular degeneration.[4][citation needed]

Frames

The ophthalmic frame is the part of a pair of glasses which is designed to hold the lenses in proper position. Ophthalmic frames come in a variety of styles, sizes, materials, shapes, and colors.[5]

Parts

  • two eye wires or rims surrounding and holding the lenses in place
  • bridge which connects the two eye wires,
  • chassis, the combination of the eye wires and the bridge
  • top bar or brow bar, a bar just above the bridge providing structural support and/or style enhancement. The addition of a top bar makes a pair of glasses aviator eyeglasses
  • brows or caps – plastic or metal caps which fit over the top of the eye wire for style enhancement and to provide additional support for the lenses. The addition of brows makes a pair of glasses Brow line glasses
  • two nose pads that allow a comfortable resting of the eye wires on the nose
  • two pad arms which connect the eye wire to the nose pads
  • two end pieces which connect the eye wire via the "hinges" to the temples
  • two hinges connecting the end pieces to the frames and allowing a swivel movement
  • pair of frame-front end pieces
  • two temples (earpieces) on either side of the skull
  • two temple tips at the end of each temple

Temple types

  • Spring-loaded flex hinge temples: These flex hinges are equipped with a small spring that affords the arms a greater range of movement and does not limit them to the traditional, 90 degree angle. Repairs can be made by using Self Aligning Spring Hinge Screws. Use screw insertion pliers to push the tip beyond the first barrel of a spring hinge at a 45 degree angle and use a standard screwdriver to tighten. As the screw moves down the barrel, it will move to a 90 degree angle. When finished, use a plier to break off the excess.[6]
  • Skull temples: bend down behind the ears, follow the contour of the skull and rest evenly against the skull
  • Library temples: generally straight and do not bend down behind the ears. Hold the glasses primarily through light pressure against the side of the skull
  • Convertible temples: used either as library or skull temples depending on the bent
  • Riding bow temples: curve around the ear and extend down to the level of the ear lobe. Used mostly on athletic, children’s, and industrial safety frames;
  • Comfort cable temples: similar to the Riding bow but constructed from coiled, metal, flexible cable

Materials

Plastic

Metal

Natural materials

  • Wood
  • Bone
  • Ivory
  • Leather
  • Semi-precious or precious stone

Corrective lens shape

Corrective lenses can be produced in many different shapes from a circular lens called a lens blank. Lens blanks are cut to fit the shape of the frame that will hold them. Frame styles vary and fashion trends change over time, resulting in a multitude of lens shapes. For lower power lenses, there are few restrictions which allows for many trendy and fashionable shapes. Higher power lenses can cause distortion of peripheral vision and may become thick and heavy if a large lens shape is used. However, if the lens becomes too small, the field of view can be drastically reduced.

Bifocal, trifocal, and progressive lenses generally require a taller lens shape to leave room for the different segments while preserving an adequate field of view through each segment. Frames with rounded edges are the most efficient for correcting myopic prescriptions, with perfectly round frames being the most efficient. Before the advent of eyeglasses as a fashion item, when frames were constructed with only functionality in mind, virtually all eyeglasses were either round, oval, or curved octagons. It was not until glasses began to be seen as an accessory that different shapes were introduced to be more aesthetically pleasing than functional.

History

Precursors

The use of a convex lens to form an enlarged/magnified image is discussed in Alhazen's Book of Optics (1021). Its translation into Latin from Arabic in the 12th century was instrumental to the invention of eyeglasses in 13th century Italy.[8] Englishman Robert Grosseteste's treatise De iride ("On the Rainbow"), written between 1220 and 1235, mentions using optics to "read the smallest letters at incredible distances". A few years later in 1262, Roger Bacon is also known to have written on the magnifying properties of lenses.[9]

Sunglasses, in the form of flat panes of smoky quartz, were used in China during the 12th century.[a] Similarly, the Inuit have used snow goggles for eye protection. While they did not offer any corrective benefits[11] they did improve visual acuity via the pinhole effect.

Invention

The Glasses Apostle by Conrad von Soest (1403)

The first eyeglasses were made in Italy in about 1286, but it is not clear who the inventor was. In a sermon delivered on February 23, 1306, the Dominican friar Giordano da Pisa (ca. 1255–1311) wrote "It is not yet twenty years since there was found the art of making eyeglasses, which make for good vision... And it is so short a time that this new art, never before extant, was discovered. ... I saw the one who first discovered and practiced it, and I talked to him."[12] Giordano's colleague Friar Alessandro della Spina of Pisa (d. 1313) was soon making eyeglasses. The Ancient Chronicle of the Dominican Monastery of St. Catherine in Pisa records: "Eyeglasses, having first been made by someone else, who was unwilling to share them, he [Spina] made them and shared them with everyone with a cheerful and willing heart."[13] By 1301, there were guild regulations in Venice governing the sale of eyeglasses.[14]

Seated apostle holding lenses in position for reading. Detail from Death of the Virgin, by the Master of Heiligenkreuz, ca. 1400–30 (Getty Center).

The earliest pictorial evidence for the use of eyeglasses is Tommaso da Modena's 1352 portrait of the cardinal Hugh de Provence reading in a scriptorium. Another early example would be a depiction of eyeglasses found north of the Alps in an altarpiece of the church of Bad Wildungen, Germany, in 1403. These early glasses had convex lenses that could correct both hyperopia (farsightedness), and the presbyopia that commonly develops as a symptom of aging. It was not until 1604 that Johannes Kepler published the first correct explanation as to why convex and concave lenses could correct presbyopia and myopia.[b]

Early frames for glasses consisted of two magnifying glasses riveted together by the handles so that they could grip the nose. These are referred to as "rivet spectacles". The earliest surviving examples were found under the floorboards at Kloster Wienhausen, a convent near Celle in Germany; they have been dated to circa 1400.[17]

Other claims

Claims that Salvino degli Armati of Florence invented eyeglasses have been exposed as hoaxes.[18][19]

Marco Polo is sometimes claimed to have encountered eyeglasses during his travels in China in the 13th century, no such statement appears in his accounts.[20][21] Indeed, the earliest mentions of eyeglasses in China occur in the 15th century and those Chinese sources state that eyeglasses were imported.[22]

It is also sometimes claimed that glasses were first invented in India. In 1907 Professor Berthold Laufer stated in his history of glasses that "the opinion that spectacles originated in India is of the greatest probability and that spectacles must have been known in India earlier than in Europe".[23] However, Joseph Needham showed that the mention of glasses in the manuscript Laufer used to justify the prior invention of them in Asia did not exist in older versions of that manuscript, and the reference to them in later versions was added during the Ming dynasty.[24] In an 1971 article in the British Journal of Ophthalmology it was argued that it: "...is therefore most likely that the use of lenses reached Europe via the Arabs, as did Hindu mathematics and the ophthalmological works of the ancient Hindu surgeon Susruta",[25] but all dates given are well after the existence of eyeglasses in Italy was established, and there had been significant shipments of eye glasses from Italy to the Middle East, with one shipment as large as 24,000 glasses.[26]

Later developments

A portrait of Francisco de Quevedo y Villegas, 1580–1645

The American scientist Benjamin Franklin, who suffered from both myopia and presbyopia, invented bifocals. Serious historians have from time to time produced evidence to suggest that others may have preceded him in the invention; however, a correspondence between George Whatley and John Fenno, editor of The Gazette of the United States, suggested that Franklin had indeed invented bifocals, and perhaps 50 years earlier than had been originally thought.[27] The first lenses for correcting astigmatism were designed by the British astronomer George Airy in 1825.[28]

Over time, the construction of frames for glasses also evolved. Early eyepieces were designed to be either held in place by hand or by exerting pressure on the nose (pince-nez). Girolamo Savonarola suggested that eyepieces could be held in place by a ribbon passed over the wearer's head, this in turn secured by the weight of a hat. The modern style of glasses, held by temples passing over the ears, was developed some time before 1727, possibly by the British optician Edward Scarlett. These designs were not immediately successful, however, and various styles with attached handles such as "scissors-glasses" and lorgnettes were also fashionable from the second half of the 18th century and into the early 19th century.

In the early 20th century, Moritz von Rohr and Zeiss (with the assistance of H. Boegehold and A. Sonnefeld[29]), developed the Zeiss Punktal spherical point-focus lenses that dominated the eyeglass lens field for many years. In 2008, Joshua Silver designed eyewear with adjustable corrective glasses. They work by silicone liquid, a syringe, and a pressure mechanism.[30]

Despite the increasing popularity of contact lenses and laser corrective eye surgery, glasses remain very common, as their technology has improved. For instance, it is now possible to purchase frames made of special memory metal alloys that return to their correct shape after being bent. Other frames have spring-loaded hinges. Either of these designs offers dramatically better ability to withstand the stresses of daily wear and the occasional accident. Modern frames are also often made from strong, light-weight materials such as titanium alloys, which were not available in earlier times.

In fashion

In the 1930s, "spectacles" were described as "medical appliances."[31] Wearing spectacles was sometimes considered socially humiliating. In the 1970s, fashionable glasses started to become available through manufacturers, and the government also recognized the demand for stylized eyewear.[31]

Graham Pullin describes how devices for disability, like glasses, have traditionally been designed to camouflage against the skin and restore ability without being visible.[31] In the past, design for disability has "been less about projecting a positive image as about trying not to project an image at all."[31] Pullin uses the example of spectacles, traditionally categorized as a medical device for "patients", and outlines how they are now described as eyewear: a fashionable accessory.[31] Much like other fashion designs and accessories, eyewear is created by designers, has reputable labels, and comes in collections, by season and designer.[31] It is becoming more common for consumers purchase eyewear with clear, non-prescription lenses, illustrating that glasses are no longer a social stigma, but a fashionable accessory that "frames your face."[31]

Society and culture

Redistribution

Some organizations like Lions Clubs International,[32] Unite For Sight,[33], ReSpectacle,[34] and New Eyes for the Needy provide a way to donate glasses and sunglasses. Unite For Sight has redistributed more than 200,000 pairs.[35]

Fashion

Many people require glasses for the reasons listed above. There are many shapes, colors, and materials that can be used when designing frames and lenses that can be utilized in various combinations. Oftentimes, the selection of a frame is made based on how it will affect the appearance of the wearer. Some people with good natural eyesight like to wear eyeglasses as a style accessory.

Personal image

For most of their history, eyeglasses were seen as unfashionable, and carried several potentially negative connotations: wearing glasses caused individuals to be stigmatized and stereotyped as pious clergymen (as those in religious vocation were the most likely to be literate and therefore the most likely to need reading glasses), elderly, or physically weak and passive.[36][37] The stigma began to fall away in the early 1900s when the popular Theodore Roosevelt was regularly photographed wearing eyeglasses, and in the 1910s when popular comedian Harold Lloyd began wearing a pair of horn-rimmed glasses as the "Glasses" character in his films.[36][37]

Former United States senator Barry Goldwater in horn-rimmed glasses

Since, eyeglasses have become an acceptable fashion item and often act as a key component in individuals' personal image. Musicians Buddy Holly and John Lennon became synonymous with the styles of eye-glasses they wore to the point that thick, black horn-rimmed glasses are often called "Buddy Holly glasses" and perfectly round metal eyeglass frames called "John Lennon (or Harry Potter) Glasses." British comedic actor Eric Sykes was known in the United Kingdom for wearing thick, square, horn-rimmed glasses, which were in fact a sophisticated hearing aid that alleviated his deafness by allowing him to "hear" vibrations.[38] Some celebrities have become so associated with their eyeglasses that they continued to wear them even after taking alternate measures against vision problems: United States Senator Barry Goldwater and comedian Drew Carey continued to wear non-prescription glasses after being fitted for contacts and getting laser eye surgery, respectively.

Other celebrities have used glasses to differentiate themselves from the characters they play, such as Anne Kirkbride, who wore oversized, 1980s-style round horn-rimmed glasses as Deirdre Barlow in the soap opera Coronation Street, and Masaharu Morimoto, who wears glasses to separate his professional persona as a chef from his stage persona as Iron Chef Japanese. In 2012 some NBA players wear lensless glasses with thick plastic frames like horn-rimmed glasses during post-game interviews, geek chic that draws comparisons to Steve Urkel.[39][40]

In superhero fiction, eyeglasses have become a standard component of various heroes' disguises (as masks), allowing them to adopt a nondescript demeanor when they are not in their superhero persona: Superman is well known for wearing 1950s style horn-rimmed glasses as Clark Kent, while Wonder Woman wears either round, Harold Lloyd style glasses or 1970s style bug-eye glasses as Diana Prince. An example of the halo effect is seen in the stereotype that those who wear glasses are intelligent.

Styles

In the 20th century, eyeglasses came to be considered a component of fashion; as such, various different styles have come in and out of popularity. Most are still in regular use, albeit with varying degrees of frequency.

See also



This article uses material from the Wikipedia article "Glasses", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Consumer products

.max, Maya, Challenge, Competition, Rendering, 3D, Blender, Autodesk Maya, 3D Studio MAX (.3DS, .MAX), Maxwell, Animation, 3D Model, Autodesk Softimage, Cinema 4D, Rendering, Animation, 3Dartist, c4d, maxon, lowpoly, 3Dart, blender3D, 3D library