powered by CADENAS

Social Share

Amazon

Ballpoint pen (1174 views - Business & Office)

A ballpoint pen, also known as a biro or ball pen, is a pen that dispenses ink (usually in paste form) over a metal ball at its point, i.e. over a "ball point". The metal commonly used is steel, brass, or tungsten carbide. It was conceived and developed as a cleaner and more reliable alternative to dip pens and fountain pens, and it is now the world's most-used writing instrument: millions are manufactured and sold daily. As a result, it has influenced art and graphic design and spawned an artwork genre. Pen manufacturers produce designer ballpoint pens for the high-end and collectors' markets. The Bic Cristal is a popular disposable type of ballpoint pen whose design is recognised by its place in the permanent collection of the Museum of Modern Art, New York.
Go to Article

Explanation by Hotspot Model

Youtube


    

Ballpoint pen

Ballpoint pen

Ballpoint pen

Licensed under Creative Commons Attribution-Share Alike 2.5 (No machine-readable author provided. Pavel Krok~commonswiki assumed (based on copyright claims).).

Ballpoint pen
A retractable ballpoint pen assemblage (Schneider K15)
Inventor
Inception1888

A ballpoint pen, also known as a biro[1] or ball pen, is a pen that dispenses ink (usually in paste form) over a metal ball at its point, i.e. over a "ball point". The metal commonly used is steel, brass, or tungsten carbide.[2] It was conceived and developed as a cleaner and more reliable alternative to dip pens and fountain pens, and it is now the world's most-used writing instrument:[3] millions are manufactured and sold daily.[4] As a result, it has influenced art and graphic design and spawned an artwork genre.

Pen manufacturers produce designer ballpoint pens for the high-end and collectors' markets.

The Bic Cristal is a popular disposable type of ballpoint pen whose design is recognised by its place in the permanent collection of the Museum of Modern Art, New York.[5]

History

Origins

At left, an authentic Birome made in Argentina by Bíró & Meyne. At right, Birome advertisement in Argentine magazine Leoplán, 1945.

The concept of using a ball point within a writing instrument as a method of applying ink to paper has existed since the late 19th century. In these inventions, the ink was placed in a thin tube whose end was blocked by a tiny ball, held so that it could not slip into the tube or fall out of the pen.

The first patent for a ballpoint pen[6][7] was issued on 30 October 1888 to John J. Loud,[8] who was attempting to make a writing instrument that would be able to write "on rough surfaces-such as wood, coarse wrapping-paper, and other articles"[9] which then-common fountain pens could not. Loud's pen had a small rotating steel ball, held in place by a socket. Although it could be used to mark rough surfaces such as leather, as Loud intended, it proved to be too coarse for letter-writing. With no commercial viability, its potential went unexploited[1] and the patent eventually lapsed.[10]

The manufacture of economical, reliable ballpoint pens as we know them arose from experimentation, modern chemistry, and precision manufacturing capabilities of the early 20th century.[3] Patents filed worldwide during early development are testaments to failed attempts at making the pens commercially viable and widely available.[11] Early ballpoints did not deliver the ink evenly; overflow and clogging were among the obstacles inventors faced toward developing reliable ballpoint pens.[4] If the ball socket was too tight, or the ink too thick, it would not reach the paper. If the socket was too loose, or the ink too thin, the pen would leak or the ink would smear.[4] Ink reservoirs pressurized by piston, spring, capillary action, and gravity would all serve as solutions to ink-delivery and flow problems.[12][13]

László Bíró, a Hungarian newspaper editor frustrated by the amount of time that he wasted filling up fountain pens and cleaning up smudged pages, noticed that inks used in newspaper printing dried quickly, leaving the paper dry and smudge free. He decided to create a pen using the same type of ink.[4] Bíró enlisted the help of his brother György, a chemist,[4] to develop viscous ink formulae for new ballpoint designs.[3]

Bíró's innovation successfully coupled ink-viscosity with a ball-socket mechanism which acted compatibly to prevent ink from drying inside the reservoir while allowing controlled flow.[4] Bíró filed a British patent on 15 June 1938.[1][14]

In 1941, the Bíró brothers and a friend, Juan Jorge Meyne, fled Germany and moved to Argentina, where they formed Bíró Pens of Argentina and filed a new patent in 1943.[1] Their pen was sold in Argentina as the Birome (portmanteau of the names Bíró and Meyne), which is how ballpoint pens are still known in that country.[1] This new design was licensed by the British, who produced ballpoint pens for RAF aircrew as the Biro. Ballpoint pens were found to be more versatile than fountain pens, especially at high altitudes, where fountain pens were prone to ink-leakage.[4]

Bíró's patent, and other early patents on ballpoint pens often used the term "ball-point fountain pen".[15][16][17][18][19][20]

Postwar proliferation

Following World War II, many companies vied to commercially produce their own ballpoint pen design. In post-war Argentina, success of the Birome ballpoint was limited, but in mid-1945, the Eversharp Co., a maker of mechanical pencils, teamed up with Eberhard Faber Co. to license the rights from Birome for sales in the United States.[1][10]

During the same period, American entrepreneur Milton Reynolds came across a Birome ballpoint pen during a business trip to Buenos Aires, Argentina.[1][10] Recognizing commercial potential, he purchased several ballpoint samples, returned to the United States, and founded Reynolds International Pen Company. Reynolds bypassed the Birome patent with sufficient design alterations to obtain an American patent, beating Eversharp and other competitors to introduce the pen to the U.S. market.[1][10] Debuting at Gimbels department store in New York City on 29 October 1945,[10] for US$12.50 each (1945 US dollar value, about $170 in 2017 dollars),[10] Reynolds Rocket became the first commercially successful ballpoint pen.[1][4][21] Reynolds went to great extremes to market the pen, with great success; Gimbel's sold many thousands of pens within one week. In Britain, the Miles Martin pen company was producing the first commercially successful ballpoint pens there by the end of 1945.[1]

Neither Reynolds' nor Eversharp's ballpoint lived up to consumer expectations in America. Ballpoint pen sales peaked in 1946, and consumer interest subsequently plunged due to market-saturation.[10] By the early 1950s the ballpoint boom had subsided and Reynolds' company folded.[1]

Paper Mate pens, among the emerging ballpoint brands of the 1950s, bought the rights to distribute their own ballpoint pens in Canada.[22] Facing concerns about ink-reliability, Paper Mate pioneered new ink formulas and advertised them as "banker-approved".[10] In 1954, Parker Pens released The Jotter—the company's first ballpoint—boasting additional features and technological advances which also included the use of tungsten-carbide textured ball-bearings in their pens.[1] In less than a year, Parker sold several million pens at prices between three and nine dollars.[1] In the 1960s, the failing Eversharp Co. sold its pen division to Parker and ultimately folded.[1]

Marcel Bich also introduced a ballpoint pen to the American marketplace in the 1950s, licensed from Bíró and based on the Argentine designs.[3][23] Bich shortened his name to Bic in 1953, becoming the ballpoint brand now recognised globally.[4] Bic pens struggled until the company launched its "Writes The First Time, Every Time!" advertising campaign in the 1960s.[4] Competition during this era forced unit prices to drop considerably.[4]

Inks

Ballpoint pen ink is normally a paste containing around 25 to 40 percent dye. The dyes are suspended in a solvent of "oil". The most common of the oils are benzyl alcohol or phenoxyethanol, which mix with the dyes to create a smooth paste that dries quickly. The dyes used in blue and black ballpoint pens are basic dyes based on triarylmethane and acid dyes derived from diazo compounds or phthalocyanine. Common dyes in blue (and black) ink are Prussian blue, Victoria blue, methyl violet, crystal violet and phthalocyanine blue. The dye eosin is commonly used for red ink.

The inks are resistant to water after drying but can be defaced by certain solvents.

Types of ballpoint pens

Ballpoint pens are produced in both disposable and refillable models. Refills allow for the entire internal ink reservoir, including a ballpoint and socket, to be replaced. Such characteristics are usually associated with designer-type pens or those constructed of finer materials. The simplest types of ballpoint pens are disposable and have a cap to cover the tip when the pen is not in use, or a mechanism for retracting the tip,[3] which varies between manufacturers but is usually a spring- or screw-mechanism.

Rollerball pens employ the same ballpoint mechanics, but with the use of water-based inks instead of oil-based inks. Compared to oil-based ballpoints, rollerball pens are said to provide more fluid ink-flow, but the water-based inks will blot if held stationary against the writing surface. Water-based inks also remain wet longer when freshly applied and are thus prone to smearing—posing problems to left-handed people (or right handed people writing right-to-left script)—and running, should the writing surface become wet.

Some ballpoint pens use a hybrid ink formulation whose viscosity is lower than that of standard ballpoint ink, but greater than rollerball ink. The ink dries faster than a standard ballpoint to prevent smearing when writing. These pens are better suited for left handed persons. Examples are the Uni Jetstream and Pilot Acroball ranges. These pens are also labelled "extra smooth", as they offer a smoother writing experience compared to normal ballpoint pens.

Because of a ballpoint pen's reliance on gravity to coat the ball with ink, most cannot be used to write upside-down. However, technology developed by Fisher pens in the United States resulted in the production of what came to be known as the "Fisher Space Pen". Space Pens combine a more viscous ink with a pressurised ink reservoir[4] that forces the ink toward the point. Unlike standard ballpoints, the rear end of a Space Pen's pressurized reservoir is sealed, eliminating evaporation and leakage,[4] thus allowing the pen to write upside-down, in zero-gravity environments, and reportedly underwater.[24] Astronauts have made use of these pens in outer space.[4]

Ballpoint pens with erasable ink were pioneered by the Paper Mate pen company.[25] The ink formulas of erasable ballpoints have properties similar to rubber cement, allowing the ink to be literally rubbed clean from the writing surface before drying and eventually becoming permanent.[25] Erasable ink is much thicker than standard ballpoint inks, requiring pressurised cartridges to facilitate inkflow—meaning they can also write upside-down. Though these pens are equipped with erasers, any eraser will suffice.[25]

The inexpensive, disposable Bic Cristal (also simply Bic pen or Biro) is reportedly the most widely sold pen in the world.[23][26] It was the Bic company's first product and is still synonymous with the company name.[27][28] The Bic Cristal is part of the permanent collection at the Museum of Modern Art in New York City, acknowledged for its industrial design.[5][26] Its hexagonal barrel mimics that of a wooden pencil and is transparent, showing the ink level in the reservoir. Originally a sealed streamlined cap, the modern pen cap has a small hole at the top to meet safety standards, helping to prevent suffocation if children suck it into the throat.[29]

Multipens are pens that feature multiple varying colored ballpoint refills. Sometimes ballpoint refills are combined with another non-ballpoint refill.

Sometimes ballpoint pens combine a ballpoint tip on one end and touchscreen stylus on the other.

Ballpoint pens are sometimes provided free by businesses, such as hotels, as a form of advertising—printed with a company's name; a ballpoint pen is a relatively low cost advertisement that is highly effective (customers will use, and therefore see, a pen daily). Businesses and charities include ballpoint pens in direct mail campaigns to increase a customer's interest in the mailing. Ballpoints have also been produced to commemorate events, such as a pen commemorating the 1963 assassination of President John F. Kennedy.[3]

As art medium

Ballpoint pens have proven to be a versatile art medium for professional artists as well as amateur doodlers.[30] Low cost, availability, and portability are cited by practitioners as qualities which make this common writing tool a convenient, alternative art supply.[31] Some artists use them within mixed-media works, while others use them solely as their medium-of-choice.[32]

Effects not generally associated with ballpoint pens can be achieved.[33] Traditional pen-and-ink techniques such as stippling and cross-hatching can be used to create half-tones[34] or the illusion of form and volume.[35] For artists whose interests necessitate precision line-work, ballpoints are an obvious attraction; ballpoint pens allow for sharp lines not as effectively executed using a brush.[36] Finely applied, the resulting imagery has been mistaken for airbrushed artwork[37] and photography,[38] causing reactions of disbelief which ballpoint artist Lennie Mace refers to as the Wow Factor.[36][37]

Famous 20th-century artists such as Andy Warhol, among others, have utilised ballpoint pens to some extent during their careers.[39] Ballpoint pen artwork continues to attract interest in the 21st century, with contemporary artists gaining recognition for their specific use of ballpoint pens; for their technical proficiency, imagination, and innovation. Korean-American artist Il Lee has been creating large-scale, ballpoint-only abstract artwork since the late 1970s.[30] Since the 1980s, Lennie Mace creates imaginative, ballpoint-only artwork of varying content and complexity, applied to unconventional surfaces including wood and denim.[40] The artist coined terms such as PENtings and Media Graffiti to describe his varied output.[36] More recently, British artist James Mylne has been creating photo-realistic artwork using mostly black ballpoints, sometimes with minimal mixed-media color.[38] In the mid-2000s (decade), Juan Francisco Casas generated Internet attention for a series of large-scale, photo-realistic ballpoint duplications of his own snapshots of friends, utilising only blue pens.[41]

Using ballpoint pens to create artwork is not without limitations. Color availability and sensitivity of ink to light are among concerns of ballpoint pen artists.[42] Mistakes pose greater risks to ballpoint artists; once a line is drawn, it generally cannot be erased.[36] Additionally, "blobbing" of ink on the drawing surface and "skipping" of ink-flow require consideration when using ballpoint pens for artistic purposes.[32] Although the mechanics of ballpoint pens remain relatively unchanged, ink composition has evolved to solve certain problems over the years, resulting in unpredictable sensitivity to light and some extent of fading.[42]

Manufacturing

Although designs and construction vary between brands, basic components of all ballpoint pens are universal.[3] Standard components of a ballpoint tip include the freely rotating ball itself (distributing the ink on the writing surface), a socket holding the ball in place, small ink channels that provide ink to the ball through the socket, and a self-contained ink reservoir supplying ink to the ball.[4] In modern disposable pens, narrow plastic tubes contain the ink, which is compelled downward to the ball by gravity.[4] Brass, steel, or tungsten carbide are used to manufacture the ball bearing-like points,[4] then housed in a brass socket.[43]

The function of these components can be compared with the ball-applicator of roll-on antiperspirant; the same technology at a larger scale. The ballpoint tip delivers the ink to the writing surface while acting as a buffer between the ink in the reservoir and the air outside, preventing the quick-drying ink from drying inside the reservoir. Modern ballpoints are said to have a two-year shelf life, on average.[4]

A ballpoint tip that can write comfortably for a long period of time is not easy to produce as it requires high-precision machinery and thin high grade steel alloy plates. China, which currently (2017) produces about 80 percent of the world's ballpoint pens, relied up to 2017 on imported ballpoint tips and metal alloys.[44]

The common ballpoint pen is a product of mass production, with components produced separately on assembly lines.[43] Basic steps in the manufacturing process include the production of ink formulas, moulding of metal and plastic components, and assembly.[3] Marcel Bich was involved in developing the production of inexpensive ballpoint pens.[4]

Standards

The International Organization for Standardization has published standards for ball point and roller ball pens:

ISO 12756
1998: Drawing and writing instruments – Ball point pens – Vocabulary[45]
ISO 12757-1
1998: Ball point pens and refills – Part 1: General use[46]
ISO 12757-2
1998: Ball point pens and refills – Part 2: Documentary use (DOC)[47]
ISO 14145-1
1998: Roller ball pens and refills – Part 1: General use[48]
ISO 14145-2
1998: Roller ball pens and refills – Part 2: Documentary use (DOC)[49]

Guinness World Records

  • The world's largest functioning ballpoint pen was made by Acharya Makunuri Srinivasa in India. The pen measures 5.5 m (18 ft 0.53 in) long and weighs 37.23 kg (82.08 lb 1.24 oz).[50]
  • The world's most popular pen is Bic's disposable ball-point pen (the 100 billionth of which was sold in September 2006). Bic Launched the Bic Cristal pen in 1950 and has gone on to sell 57 per second, that is enough pens to fill the Arc de Triomphe 23 times over![51]

See also



This article uses material from the Wikipedia article "Ballpoint pen", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Business & Office

3D