powered by CADENAS

Social Share

Arch (6039 views - Architecure & BIM & MEP)

An arch is a curved structure that spans an elevated space and may or may not support the weight above it. Arches may be synonymous with vaults, but a vault may be distinguished as a continuous arch forming a roof. Arches appeared as early as the 2nd millennium BC in Mesopotamian brick architecture, and their systematic use started with the Ancient Romans who were the first to apply the technique to a wide range of structures.
Go to Article

Arch

Arch

An arch is a curved structure that spans an elevated space and may or may not support the weight above it.[1]

Arches may be synonymous with vaults, but a vault may be distinguished as a continuous arch[2] forming a roof. Arches appeared as early as the 2nd millennium BC in Mesopotamian brick architecture,[3] and their systematic use started with the Ancient Romans who were the first to apply the technique to a wide range of structures.

Basic concepts

An arch is a pure compression form. It can span a large area by resolving forces into compressive stresses and, in turn eliminating tensile stresses. This is sometimes referred to as arch action.[4] As the forces in the arch are carried to the ground, the arch will push outward at the base, called thrust. As the rise, or height of the arch decreases, the outward thrust increases.[5] In order to maintain arch action and prevent the arch from collapsing, the thrust needs to be restrained, either with internal ties or external bracing, such as abutments.[6]

Fixed vs hinged arch

The most common true arch configurations are the fixed arch, the two-hinged arch, and the three-hinged arch.[7]

The fixed arch is most often used in reinforced concrete bridge and tunnel construction, where the spans are short. Because it is subject to additional internal stress caused by thermal expansion and contraction, this type of arch is considered to be statically indeterminate.[6]

The two-hinged arch is most often used to bridge long spans.[6] This type of arch has pinned connections at the base. Unlike the fixed arch, the pinned base is able to rotate,[8] allowing the structure to move freely and compensate for the thermal expansion and contraction caused by changes in outdoor temperature. However, this can result in additional stresses, so the two-hinged arch is also statically indeterminate, although not to the degree of the fixed arch.[6]

The three-hinged arch is not only hinged at its base, like the two-hinged arch, but at the mid-span as well. The additional connection at the mid-span allows the three-hinged arch to move in two opposite directions and compensate for any expansion and contraction. This type of arch is thus not subject to additional stress caused by thermal change. The three-hinged arch is therefore said to be statically determinate.[7] It is most often used for medium-span structures, such as large building roofs.

Another advantage of the three-hinged arch is that the pinned bases are more easily developed than fixed ones, allowing for shallow, bearing-type foundations in medium-span structures. In the three-hinged arch, "thermal expansion and contraction of the arch will cause vertical movements at the peak pin joint but will have no appreciable effect on the bases," further simplifying the foundation design.[6]

Types of arches

Arches have many forms, but all fall into three basic categories: circular, pointed, and parabolic. Arches can also be configured to produce vaults and arcades.[6]

Arches with a circular form, also referred to as rounded arches, were commonly employed by the builders of ancient, heavy masonry arches.[9] Ancient Roman builders relied heavily on the rounded arch to span large, open areas. Several rounded arches placed in-line, end-to-end, form an arcade, such as the Roman aqueduct.[10]

Pointed arches were most often used by builders of Gothic-style architecture.[11] The advantage to using a pointed arch, rather than a circular one, is that the arch action produces less thrust at the base. This innovation allowed for taller and more closely spaced openings, typical of Gothic architecture.[12][13]

Vaults are essentially "adjacent arches [that] are assembled side by side." If vaults intersect, complex forms are produced with the intersections. The forms, along with the "strongly expressed ribs at the vault intersections, were dominant architectural features of Gothic cathedrals."[9]

The parabolic arch employs the principle that when weight is uniformly applied to an arch, the internal compression resulting from that weight will follow a parabolic profile. Of all arch types, the parabolic arch produces the most thrust at the base, but can span the largest areas. It is commonly used in bridge design, where long spans are needed.[9]

The catenary arch has a shape different from the parabolic curve. The shape of the curve traced by a loose span of chain or rope, the catenary is the structurally ideal shape for a freestanding arch of constant thickness.

Types of arches displayed chronologically, roughly in the order in which they were developed:

History

True arches, as opposed to corbel arches, were known by a number of civilizations in the Ancient Near East and the Levant, but their use was infrequent and mostly confined to underground structures, such as drains where the problem of lateral thrust is greatly diminished.[14] A rare exception is the Bronze Age arched city gate of Ashkelon (modern day Israel), dating to ca. 1850 B.C.[15] An early example of a voussoir arch appears in the Greek Rhodes Footbridge.[16] Corbel arches were found in other parts of ancient Asia, Africa, Europe and the Americas. In 2010, a robot discovered a long arch-roofed passageway underneath the Pyramid of Quetzalcoatl, which stands in the ancient city of Teotihuacan north of Mexico City, dated to around 200 AD.[17] In ancient Persia, the Achaemenid Empire built small barrel vaults (essentially a series of arches built together to form a hall) known as iwan, which became massive, monumental structures during the later Parthian Empire.[18][19][20] This architectural tradition was continued by the Sasanian Empire, which built the Taq Kasra at Ctesiphon in the 6th century, the largest free-standing vault until modern times.[21]

The ancient Greeks introduced the arch to Italy visible today in the south of the peninsula and in Sicily.

The ancient Romans learned the arch from the Etruscans, refined it and were the first builders to tap its full potential for above ground buildings:

The Romans were the first builders in Europe, perhaps the first in the world, fully to appreciate the advantages of the arch, the vault and the dome.[22]
Throughout the Roman empire, their engineers erected arch structures such as bridges, aqueducts, and gates. They also introduced the triumphal arch as a military monument. Vaults began to be used for roofing large interior spaces such as halls and temples, a function that was also assumed by domed structures from the 1st century BC onwards.

The segmental arch was first built by the Romans who realized that an arch in a bridge did not have to be a semicircle,[23][24] such as in Alconétar Bridge or Ponte San Lorenzo. They were also routinely used in house construction, as in Ostia Antica (see picture).

In ancient China, most architecture was wooden, including the few known arch bridges from literature and one artistic depiction in stone-carved relief.[25][26][27] Therefore, the only surviving examples of architecture from the Han Dynasty (202 BC - 220 AD) are rammed earth defensive walls and towers, ceramic roof tiles from no longer existent wooden buildings,[28][29][30] stone gate towers,[31][32] and underground brick tombs that, although featuring vaults, domes, and archways, were built with the support of the earth and weren't free-standing.[33][34] China's oldest surviving stone arch bridge is the Anji Bridge, built between 595-605 during the Sui Dynasty, and is the oldest open-spandrel segmental arch bridge in stone.[35][36] However, the ancient Romans had virtually all of these components beforehand, such as Trajan's Bridge that had open-spandrels built in wood on stone pillars.[37]

The first example of an early Gothic arch in Europe is in Sicily in the Greek fortifications of Gela. The semicircular arch was followed in Europe by the pointed Gothic arch or ogive, whose centreline more closely follows the forces of compression and which is therefore stronger. The semicircular arch can be flattened to make an elliptical arch, as in the Ponte Santa Trinita. Both the parabolic and catenary arches are now known to be the theoretically strongest forms. Parabolic arches were introduced in construction by the Spanish architect Antoni Gaudí, who admired the structural system of the Gothic style, but for the buttresses, which he termed "architectural crutches". The catenary and parabolic arches carry all horizontal thrust to the foundation and so do not need additional elements. The first examples of the pointed arch in the European architecture are in Sicily and date back to the Arab-Norman period.

The horseshoe arch is based on the semicircular arch, but its lower ends are extended further round the circle until they start to converge. The first known built horseshoe arches are from Aksum (modern day Ethiopia and Eritrea) from around the 3rd–4th century, around the same time as the earliest contemporary examples in Roman Syria, suggesting either an Aksumite or Syrian origin for the type.[38][page needed]

Construction

Since it is a pure compression form, the arch is useful because many building materials, including stone and unreinforced concrete can resist compression, but are weak when tensile stress is applied to them.[39]

An arch is held in place by the weight of all of its members, making construction problematic. One answer is to build a frame (historically, of wood) which exactly follows the form of the underside of the arch. This is known as a centre or centring. Voussoirs are laid on it until the arch is complete and self-supporting. For an arch higher than head height, scaffolding would be required, so it could be combined with the arch support. Occasionally, arches would fall down when the frame was removed if construction or planning had been incorrect. (The A85 bridge at Dalmally, Scotland suffered this fate on its first attempt, in the 1940s[citation needed]). The interior and lower line or curve of an arch is known as the intrados.

Old arches sometimes need reinforcement due to decay of the keystones, forming what is known as bald arch.

In reinforced concrete construction, the principle of the arch is used so as to benefit from the concrete's strength in resisting compressive stress. Where any other form of stress is raised, such as tensile or torsional stress, it has to be resisted by carefully placed reinforcement rods or fibres.[40]

Other types

A blind arch is an arch infilled with solid construction so it cannot function as a window, door, or passageway.

A special form of the arch is the triumphal arch, usually built to celebrate a victory in war. A famous example is the Arc de Triomphe in Paris, France.

Rock formations may form natural arches through erosion, rather than being carved or constructed. Structures such as this can be found in Arches National Park.

Some rock balance sculptures are in the form of an arch.

Gallery

See also



This article uses material from the Wikipedia article "Arch", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Example Part

Architecure & BIM & MEP

Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, BIM Object, BIM component, BIM library, BIM family, BIM catalog, GIS, Advanced Steel, AutoCAD MEP, linear, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, BIM family creation, 3D, Download, MEP BIM product library