powered by CADENAS

Social Share

Amazon

Reflex camera (860 views - Basics)

A reflex camera is a camera that permits the photographer to view the image that will be seen through the lens, and therefore to see exactly what will be captured, contrary to viewfinder cameras where the image could be significantly different from what will be captured. A single-lens reflex camera typically uses a mirror and prism system (hence "reflex", from the mirror's reflection) to accomplish this. The mirrorless interchangeable-lens camera achieves the same result by providing the photographer with a digitally captured image. The twin-lens reflex camera provides both a viewfinder image and the reflected image from the actual camera lens.
Go to Article

Explanation by Hotspot Model

Youtube


    

Reflex camera

Reflex camera

A reflex camera is a camera that permits the photographer to view the image that will be seen through the lens, and therefore to see exactly what will be captured, contrary to viewfinder cameras where the image could be significantly different from what will be captured. A single-lens reflex camera typically uses a mirror and prism system (hence "reflex", from the mirror's reflection) to accomplish this. The mirrorless interchangeable-lens camera achieves the same result by providing the photographer with a digitally captured image. The twin-lens reflex camera provides both a viewfinder image and the reflected image from the actual camera lens.



This article uses material from the Wikipedia article "Reflex camera", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Basics

3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted