powered by CADENAS

Social Share

Amazon

Halogen lamp (2960 views - Electronics & PCB)

A halogen lamp, also known as a tungsten halogen, quartz-halogen or quartz iodine lamp, is an incandescent lamp consisting of a tungsten filament sealed into a compact transparent envelope that is filled with a mixture of an inert gas and a small amount of a halogen such as iodine or bromine. The combination of the halogen gas and the tungsten filament produces a halogen cycle chemical reaction which redeposits evaporated tungsten to the filament, increasing its life and maintaining the clarity of the envelope. Because of this, a halogen lamp can be operated at a higher temperature than a standard gas-filled lamp of similar power and operating life, producing light of a higher luminous efficacy and color temperature. The small size of halogen lamps permits their use in compact optical systems for projectors and illumination.
Go to Article

Explanation by Hotspot Model

Halogen lamp

Halogen lamp

Halogen lamp

A halogen lamp, also known as a tungsten halogen, quartz-halogen or quartz iodine lamp, is an incandescent lamp consisting of a tungsten filament sealed into a compact transparent envelope that is filled with a mixture of an inert gas and a small amount of a halogen such as iodine or bromine. The combination of the halogen gas and the tungsten filament produces a halogen cycle chemical reaction which redeposits evaporated tungsten to the filament, increasing its life and maintaining the clarity of the envelope. Because of this, a halogen lamp can be operated at a higher temperature than a standard gas-filled lamp of similar power and operating life, producing light of a higher luminous efficacy and color temperature. The small size of halogen lamps permits their use in compact optical systems for projectors and illumination.

History

A carbon filament lamp using chlorine to prevent darkening of the envelope was patented[1] in 1882, and chlorine-filled "NoVak" lamps were marketed in 1892.[2] The use of iodine was proposed in a 1933 patent,[3] which also described the cyclic redeposition of tungsten back onto the filament. In 1959, General Electric patented[3] a practical lamp using iodine.[4]

In 2009, the EU began its phase-out of inefficient bulbs. The production and importation of directional mains-voltage halogen bulbs was banned on 1 September 2016. Non-directional halogen bulbs are set to follow on 1 September 2018.[5]

Halogen cycle

In ordinary incandescent lamps, evaporated tungsten mostly deposits onto the inner surface of the bulb, causing the bulb to blacken and the filament to grow increasingly weak until it eventually breaks. The presence of the halogen, however, sets up a reversible chemical reaction cycle with this evaporated tungsten. The halogen cycle keeps the bulb clean and causes the light output to remain almost constant throughout the bulb's life. At moderate temperatures the halogen reacts with the evaporating tungsten, the halide formed being moved around in the inert gas filling. At some point, however, it will reach higher temperature regions within the bulb where it then dissociates, releasing tungsten back onto the filament and freeing the halogen to repeat the process. The overall bulb envelope temperature must be significantly higher than in conventional incandescent lamps for this reaction to succeed, however: it is only at temperatures of above 250 °C (482 °F) on the inside of the glass envelope that the halogen vapor can combine with the tungsten and return it to the filament rather than the tungsten becoming deposited on the glass.[6] A 300 watt tubular halogen bulb operated at full power quickly reaches a temperature of about 540 °C (1,004 °F), while a 500 watt regular incandescent bulb operates at only 180 °C (356 °F) and a 75 watt regular incandescent at only 130 °C (266 °F).[7]

The bulb must be made of fused silica (quartz) or a high-melting-point glass (such as aluminosilicate glass). Since quartz is very strong, the gas pressure can be higher,[8] which reduces the rate of evaporation of the filament, permitting it to run a higher temperature (and so luminous efficacy) for the same average life. The tungsten released in hotter regions does not generally redeposit where it came from, so the hotter parts of the filament eventually thin out and fail.

Quartz iodine lamps, using elemental iodine, were the first commercial halogen lamps launched by GE in 1959.[9][10] Quite soon, bromine was found to have advantages, but was not used in elemental form. Certain hydrocarbon bromine compounds gave good results.[11][12] Regeneration of the filament is also possible with fluorine, but its chemical reactivity is so great that other parts of the lamp are attacked.[11][13] The halogen is normally mixed with a noble gas, often krypton or xenon.[14] The first lamps used only tungsten for filament supports, but some designs use molybdenum – an example being the molybdenum shield in the H4 twin filament headlight for the European Asymmetric Passing Beam.

For a fixed power and life, the luminous efficacy of all incandescent lamps is greatest at a particular design voltage. Halogen lamps made for 12 to 24 volt operation have good light outputs, and the very compact filaments are particularly beneficial for optical control (see picture). The ranges of multifaceted reflector "MR" lamps of 20–50 watts were originally conceived for the projection of 8 mm film, but are now widely used for display lighting and in the home. More recently, wider beam versions have become available designed for direct use on supply voltages of 120 or 230 V.

Effect of voltage on performance

Tungsten halogen lamps behave in a similar manner to other incandescent lamps when run on a different voltage. However the light output is reported as proportional to , and the luminous efficacy proportional to .[15] The normal relationship regarding the lifetime is that it is proportional to . For example, a bulb operated at 5% higher than its design voltage would produce about 15% more light, and the luminous efficacy would be about 6.5% higher, but would be expected to have only half the rated life.

Halogen lamps are manufactured with enough halogen to match the rate of tungsten evaporation at their design voltage. Increasing the applied voltage increases the rate of evaporation, so at some point there may be insufficient halogen and the lamp goes black. Over-voltage operation is not generally recommended. With a reduced voltage the evaporation is lower and there may be too much halogen, which can lead to abnormal failure. At much lower voltages, the bulb temperature may be too low to support the halogen cycle, but by this time the evaporation rate is too low for the bulb to blacken significantly. There are many situations where halogen lamps are dimmed successfully. However, lamp life may not be extended as much as predicted. The life span on dimming depends on lamp construction, the halogen additive used and whether dimming is normally expected for this type.

Spectrum

Like all incandescent light bulbs, a halogen lamp produces a continuous spectrum of light, from near ultraviolet to deep into the infrared.[16] Since the lamp filament can operate at a higher temperature than a non-halogen lamp, the spectrum is shifted toward blue, producing light with a higher effective color temperature and higher power efficiency. This makes halogen lamps the only option for consumer light source with black-body radiation spectrum similar to that of the Sun and most suitable for the eyes.[citation needed] Alternatively, multi-component glasses can be used, which have a natural UV-block. These glasses belong to the family of the aluminosilicate-glasses.

High temperature filaments emit some energy in the UV region. Small amounts of other elements can be mixed into the quartz, so that the doped quartz (or selective optical coating) blocks harmful UV radiation. Hard glass blocks UV and has been used extensively for the bulbs of car headlights.[17] Alternatively, the halogen lamp can be mounted inside an outer bulb, similar to an ordinary incandescent lamp, which also reduces the risks from the high bulb temperature. Undoped quartz halogen lamps are used in some scientific, medical and dental instruments as a UV-B source.

Safety

Halogen lamps get hotter than regular incandescent lamps because the heat is concentrated on a smaller envelope surface, and because the surface is closer to the filament. This high temperature is essential to their operation. Because the halogen lamp operates at very high temperatures, it can pose fire and burn hazards. In Australia, numerous house fires each year are attributed to ceiling-mounted halogen downlights.[18][19] The Western Australia Department of Fire and Emergency Services recommends that home owners consider instead using compact fluorescent lamps or light emitting diode lamps because they produce less heat.[20] Some safety codes now require halogen bulbs to be protected by a grid or grille, especially for high-power (1–2 kW) bulbs used in theatre, or by the glass and metal housing of the fixture to prevent ignition of draperies or flammable objects in contact with the lamp.

To reduce unintentional ultraviolet (UV) exposure, and to contain hot bulb fragments in the event of explosive bulb failure, general-purpose lamps usually have a UV-absorbing glass filter over or around the bulb. Alternatively, lamp bulbs may be doped or coated to filter out the UV radiation. With adequate filtering, a halogen lamp exposes users to less UV than a standard incandescent lamp producing the same effective level of illumination without filtering.[citation needed]

Any surface contamination, notably the oil from human fingertips, can damage the quartz envelope when it is heated. Contaminants will create a hot spot on the bulb surface when the lamp is turned on. This extreme, localized heat causes the quartz to change from its vitreous form into a weaker, crystalline form that leaks gas. This weakening may also cause the bulb to form a bubble, weakening it and leading to its explosion.[21]

Form factors

Halogen lamps are available in a series of different shapes and sizes, and are designated according to a coding system that specifies the diameter of the bulb as well as whether or not the bulb has a built-in dichroic reflector. Many such lamps have designations that begin with the letter "T" to indicate that they are "tubular" followed by a number indicating the diameter of the tube in eighths of an inch: a T3 bulb, then is a tubular halogen bulb that is 3/8ths of an inch in diameter[Note 1] The designation MR means "metal reflector", with the number following this still corresponding to eighths of an inch in diameter of the overall bulb.[Note 2] If a lamp has a "G" code,[Note 3] this will mean the lamp is a bipin shape and the number following the G will indicate the distance in millimeters between the pins, usually either 4,6.35 or 10; if the G is followed by a letter "Y", then the lamp's pins are thicker than normal— thus, a G6.35 has pins that are 1 mm in diameter but a GY6.35 has pins that are 1.3 mm in diameter. If there is a "C" code, this represents the number of coils in the filament.[22] The length of any two-ended cylindrical bulb must be specified separately from its form factor code, usually in millimeters, as must the lamp's voltage and wattage— hence, T3 120 v 150 W 118 mm means a double-ended tube-shaped bulb with a diameter of 3/8ths of an inch that operates at 120v and is 150 watts and that is also 118 millimeters long.

An R7S is a double ended, recessed single contact (RSC) linear halogen lamp measuring either 118mm or 78mm. Some less common lengths are 189mm, 254mm and 331mm. These lamps have a T3 shape on an RSC/R7S base. These can also be known as J type and T type lamps.

Applications

Medical halogen penlight to observe pupillary light reflex

Halogen headlamps are used in many automobiles. Halogen floodlights for outdoor lighting systems as well as for watercraft are also manufactured for commercial and recreational use. They are now also used in desktop lamps.

Tungsten-halogen lamps are frequently used as a near-infrared light source in Infrared spectroscopy.

Halogen lamps were used on the Times Square Ball from 1999 to 2006. However, from 2007 onwards, the halogen lamps were replaced with LEDs, due to the much longer potential lifespan (about ten times longer for LED over incandescent).[23] The 'New Year' numerals that light up when the Times Square Ball reaches the base used halogen lighting for the last time for the 2009 ball drop. It was announced on the Times Square website that the year numerals for the 2010 ball drop would use LEDs.[24]

Heating

Halogen lamps are the heating-elements in halogen ovens. Banks of powerful tubular halogen lamps were used to simulate the heat of re-entry of space vehicles [25].

General lighting

Fixed-mount lamps are used in indoor and outdoor flood lighting, although improvements in LED systems are displacing halogen lamps. Round lamps with built-in multifaceted reflectors are widely used in residential and commercial lighting. Tubular halogen lamps provide a large quantity of light from a small source and so can be used to produce powerful flood lamps for architectural lighting effects, or for lighting large areas outdoors.

Low voltage lamps use the GU5.3 and similar bi-pin bases, whereas mains voltage lamps use the same caps as normal mains tungsten filament lamps, or a special GU10/GZ10 base. The GU10/GZ10 bases are shaped to prevent dichroic reflector lamps being used in luminaires intended for aluminised reflector lamps, which could cause overheating of the fitting. Higher efficiency LED versions of all of these lamps are now available, but these have widely varying light output and quality.

Tubular lamps with electrical contacts at each end are now being used in standalone lamps and household fixtures. These come in various lengths and wattages (50–300 W). More powerful lamps are used as portable work lights, with bulbs rated 250 or 500 watts.

Stage lighting

Tungsten halogen lamps are used in the majority of theatrical and studio (film and television) fixtures, including Ellipsoidal reflector spotlights, Source Four, and Fresnels. PAR Cans are also predominately tungsten halogen.

Specialized

Projection lamps are used in motion-picture and slide projectors for homes and small office or school use. The compact size of the halogen lamp permits a reasonable size for portable projectors, although heat-absorbing filters must be placed between the lamp and the film to prevent melting. Halogen lamps are sometimes used for inspection lights and microscope stage illuminators. Halogen lamps were used for early flat-screen LCD backlighting, but other types of lamps are now used.

Disposal

Halogen lamps do not contain any mercury. General Electric claims that none of the materials making up their halogen lamps would cause the lamps to be classified as hazardous waste.[26]

See also



This article uses material from the Wikipedia article "Halogen lamp", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electronics & PCB

Cadence, Mentor Graphics, Eagle CAD, Altium Designer, AUTODESK EAGLE, Cadence Allegro, DesignSpark PCB , Mentor PADS, Mentor Xpedition, Novarm DipTrace, Pulsonix, TARGET 3001!, Xpedition xDX Designer, Zuken CADSTAR, Altium P-CAD, Agnisys, Altera Quartus, OrCAD, kiCAD, Solido Design Automation, ELectronics, PCB, Curcuit Board, 3D drawings, 3D library, 3D content, PCB Design, 2D symbols, 2D drawings, 2D icons, 2D schematics