powered by CADENAS

Social Share

Bidet (3794 views - Interior Design)

A bidet (US: or UK: ) is a plumbing fixture or type of sink intended for washing the genitalia, perineum, inner buttocks, and anus of the human body, and is typically installed in a bathroom. Lower-cost add-ons combining a toilet seat and "electronic bidet" are becoming increasingly popular as well. "Bidet" is a French loanword.
Go to Article

Bidet

Bidet

Bidet

A bidet (US: /bˈd/ or UK: /ˈbd/) is a plumbing fixture or type of sink intended for washing the genitalia, perineum, inner buttocks, and anus of the human body, and is typically installed in a bathroom. Lower-cost add-ons combining a toilet seat and "electronic bidet" are becoming increasingly popular as well. "Bidet" is a French loanword.

Applications

Bidets are primarily used to wash and clean the genitalia, perineum, inner buttocks, and anus. Traditional designs may also be used to clean any other part of the human body, such as the feet. Despite appearing similar to a toilet, a traditional bidet may be more accurately compared to a sink. There are also bidets that are attachable to ordinary toilet bowls. They have the advantage of being inexpensive and saving space.

They are usually not meant to replace the use of toilet paper as they are used after some paper to achieve full cleanliness without immediately having to take a shower. Bidets with a vertical jet are intended to replace the use of toilet paper, as they can achieve a high level of cleanliness of the anal area.

Types

Bidet shower

A bidet shower (also known as "bidet spray", "bidet sprayer", or "health faucet") is a hand-held triggered nozzle, similar to that on a kitchen sink sprayer, that delivers a spray of water to assist in anal cleansing and cleaning the genitals after defecation and urination. In contrast to a bidet that is integrated with the toilet, a bidet shower has to be held by the hands, and cleaning does not take place automatically. Bidet showers are common in countries where water is considered essential for anal cleansing.

Drawbacks include the possibility of wetting a user's clothing if used carelessly. In addition, a user must be reasonably mobile and flexible to use a hand-held bidet shower.

Conventional or standalone bidet

A bidet is a plumbing fixture that is installed as a separate unit in the bathroom besides toilet, shower and sink, which users have to straddle. Some bidets resemble a large hand basin, with taps and a stopper so they can be filled up; other designs have a nozzle that squirts a jet of water to aid in cleansing.

Add-on bidets

How they are divided.

  1. Those Producing oblique (more or less) water jet, from back to forward. mechanically or electronically controlled, some offering warm water, some having, fixed either on back rim, either on toilet seat, double nozzle.
  2. Those producing vertical jet, always mechaniclly controlled, with nozzle under side rim.

In the past, getting a bidet meant installing a completely new plumbing unit into the bathroom. Newer bidets are often no longer standalone units: A bidet may be a movable or fixed nozzle attached to an existing toilet on back or side toilet rim, or a part of the toilet itself. In these cases, their use is restricted to cleaning the anus and genitals. Some bidets of this type produce a vertical water jet and others a more or less oblique one. Others have one nozzle on the side rim for both anal and genital areas, and other designs have two nozzles on the back rim, the shorter one, called the "family nozzle", is used for washing the area around the anus, and the longer one ("bidet nozzle") is designed for women to wash their vulvas.

Such attachable bidets (also called "electronic bidets", "electric bidets", "combined toilets", "bidet attachments", or "add-on bidets") are controlled either mechanically or electronically. Mechanically controlled bidets tend to be simple mechanisms manually controlled by a valve. There are add on bidets, mechanically controlled, that produce oblique water jet and others vertical jets.The first ones have their flash tubes fixed at the back toilet rim, while the second ones at the side rim. From the last ones some have the apparatus fixed on bowl rim and others on bowl lid. The attachable bidets may be manufactured of plastic, chrome-plated metal, or stainless steel to accommodate many tastes and budgets.

Electronic bidets are controlled with waterproof electrical switches rather than with a traditional manual valve. There are models that have a heating element which blows warm air to dry the user after washing, that offer heated seats, wireless remote controls, illumination through built in night lights, or built in deodorizers and activated carbon filters to remove odors. Further refinements include adjustable water pressure, temperature compensation, and directional spray control. Where bathroom appearance is of concern, under-the-seat mounting types have become more popular.

An add-on bidet typically connects to the existing water supply of a toilet via the addition of a threaded tee pipe adapter, and requires no soldering or other plumbing work.[1] Electronic add-on bidets also require a GFCI protected grounded electrical outlet.

Health aspects

Bidet attachments are sometimes included on hospital toilets because of their utility in maintaining hygiene. In such cases and also in public toilets, disinfection after each use must be easy, and preferably automatic. Warm-water bidets may harbor dangerous microbes if not properly disinfected.[2]

Environmental aspects

From an environmental standpoint, some argue that bidets can reduce the need for toilet paper, saving households money on paper products and allowing users to reduce their carbon footprint by reducing their paper waste over time.[1][3] On the other hand, they increase the amount of heated water used in the bathroom, and, when combined with a toilet, the added complexity increases their total cost of ownership, perhaps causing them to be replaced or upgraded more frequently than simpler toilets.[3] Until further experimentation is done on internal and external losses, the environmental advantages of bidets remain unclear.

Costs

In countries where bidet are common, their prices are much lower than in countries where they are not common. In Italy, for example, the price for a bidet starts from €30 and seldom exceeds €150 (about US$167). Now all over the world bidets may cost as low as €40 (about US$46). In Middle Eastern countries, bidet attachments are much cheaper, being priced at around the equivalent of US$10–20, which is attributed to their popularity and availability.[citation needed]

Attachable or add-on bidets, mechanically controlled, are cheaper than stand-alone and electronic units. The expense of remodeling a typical North American bathroom to accommodate a traditional bidet fixture is large, in the thousands of dollars, while a mechanical add-on bidet can be purchased for around US$46, and an add-on electronic bidet costs around US$300. Additional features like warm air dryers, heated seats, or wireless remote controls may be more expensive.

Society and culture

Prevalence

Bidets are becoming increasingly popular with the ageing community, or for use among people with physical disabilities. These combined units make independent toileting possible for many people, affording greater independence. These are often special units with higher toilet seats allowing easier wheelchair transfer, and with some form of electronic remote control that benefits an individual with limited mobility or requiring assistance.

Bidets are common bathroom fixtures in many southern European countries, especially Italy, where they are found in 97% of households (the installation of a bidet in a bathroom has been mandatory since 1975),[4] Spain, and Portugal (installation is mandatory also since 1975).[5] Additionally, they are rather widespread, although not standard, in France, and are often found in Albania, Bosnia and Herzegovina, Croatia, Germany, Hungary, Slovenia, Malta, and Greece. Outside of Europe, they are very popular in some South American countries, notably in Argentina and Uruguay. Electronic bidet-integrated toilets, along with functions like toilet seat warmers, are commonly found in Japan.

In northern Europe, bidets are rare, although in Finland bidet showers are common.[6] Bidet showers are also common in South-East Asia, South Asia and parts of the Middle East.

In 1980, the first "paperless toilet" was launched in Japan by manufacturer Toto,[7] a combination of toilet and bidet which also dries the user after washing. These combination toilet-bidets (washlet) with seat warmers, or attachable bidets are particularly popular in Japan and South Korea, and are found in approximately 76% of Japanese households as of 2015.[1] They are commonly found in hotels and even some public facilities. These bidet-toilets, along with toilet seat and bidet units (to convert an existing toilet) are sold in many countries, including the United States.

Bidet seat conversions are much easier and lower cost to install than traditional bidets, and have disrupted the market for the older fixtures.[1] Acceptance worldwide is facilitated by cultural preferences for washing, as well as poor quality and availability of toilet paper in many parts of the world.[1] After a slow start in the 1990s, electronic bidets are gaining increasing popularity in the United States.[1]

In the UK, toilet-integrated bidets with drying facility are becoming more widespread for use among people with physical disabilities.

Etymology

Bidet is a French word for "pony", and in Old French, bider meant "to trot". This etymology comes from the notion that one "rides" or straddles a bidet much like a pony is ridden. The word "bidet" was used in 15th century France to refer to the pet ponies that French royalty kept.[8]

History

The bidet appears to have been an invention of French furniture makers in the late 17th century, although no exact date or inventor is known.[9][10] The earliest written reference to the bidet is in 1710 in Italy.[citation needed] The bidet is possibly associated with the chamber pot and the bourdaloue, the latter being a small chamber pot like object specifically for the use of ladies on long trips.

Historical antecedents and early functions of the bidet are believed to include devices used for contraception.[11] Bidets are considered ineffective by today's standards of contraception, and their use for this function was quickly abandoned and forgotten with the advent of modern contraceptives such as the pill.[12]

By 1900, due to plumbing improvements, the bidet (and chamber pot) moved from the bedroom to the bathroom. This was common in French palaces.

In the United States in 1928 John Harvey Kellogg applied for a patent on an "anal douche".[13] In his application, he uses the term to describe a system comparable to what today might be called a bidet nozzle which can be attached to a toilet to perform anal cleansing with water.[original research?]

In 1965 the American Bidet Company featured an adjustable spray nozzle and warm water option seeking to make the bidet a household item.[1]

The early 1980s saw the introduction of the electronic bidet from Japan, with names such as Clean Sense, Galaxy, Infinity, Novita and non electric chrome plated brass attachments such as Gobidet. These devices have attachments that connect to existing toilet arrangements, and can be used for bathrooms lacking the space for both a separate bidet and toilet having advantages such as instant heating warm water, night lights and a heated seat.

See also



This article uses material from the Wikipedia article "Bidet", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Example Part

Interior Design

3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art