powered by CADENAS

Social Share

Amazon

Shuriken (1639 views - Entertainment)

A shuriken (Japanese 手裏剣; literally: "hidden hand blade") is a Japanese concealed weapon that was used as a hidden dagger or metsubushi to distract or misdirect. Shuriken came in a variety of forms; some were manufactured, while others were improvised from tools. The edges of shuriken were often sharpened, so they could be used to penetrate skin or open arteries. They are also known as throwing stars or ninja stars, although they were originally designed in many different shapes. The major varieties of shuriken are the bō shuriken (棒手裏剣, stick shuriken) and the hira shuriken (平手裏剣, flat shuriken) or shaken (車剣, also read as kurumaken, wheel shuriken). Shuriken were supplementary weapons to the sword or various other weapons in a samurai's arsenal, although they often had an important tactical effect in battle. The art of wielding the shuriken is known as shurikenjutsu and was taught as a minor part of the martial arts curriculum of many famous schools, such as Yagyū Shinkage-ryū, Tenshin Shōden Katori Shintō-ryū, Ittō-ryū, Kukishin-ryū, and Togakure-ryū.
Go to Article

Explanation by Hotspot Model

Youtube


    

Shuriken

Shuriken

Shuriken

A shuriken (Japanese 手裏剣; literally: "hidden hand blade") is a Japanese concealed weapon that was used as a hidden dagger or metsubushi to distract or misdirect.

Shuriken came in a variety of forms; some were manufactured, while others were improvised from tools. The edges of shuriken were often sharpened, so they could be used to penetrate skin or open arteries.

They are also known as throwing stars or ninja stars, although they were originally designed in many different shapes. The major varieties of shuriken are the bō shuriken (棒手裏剣, stick shuriken) and the hira shuriken (平手裏剣, flat shuriken) or shaken (車剣, also read as kurumaken, wheel shuriken).

Shuriken were supplementary weapons to the sword or various other weapons in a samurai's arsenal, although they often had an important tactical effect in battle.[1] The art of wielding the shuriken is known as shurikenjutsu and was taught as a minor part of the martial arts curriculum of many famous schools, such as Yagyū Shinkage-ryū, Tenshin Shōden Katori Shintō-ryū, Ittō-ryū, Kukishin-ryū, and Togakure-ryū.

Bo shuriken

Bo-shuriken are throwing weapons consisting of a straight iron or steel spike, usually four-sided but sometimes round or octagonal in section. Some examples have points on both ends. The length ranges from 12 to 21 cm (5–8​12 in) and the average weight from 35 to 150 grams (1.2–5.4 ounces).[2] They should not be confused with the kunai, which is a thrusting and stabbing implement that is sometimes thrown.

Bo-shuriken were constructed from a wide variety of everyday items, hence there were many shapes and sizes. Some derived their names from the materials of which they were made, such as kugi-gata (nail form), hari-gata (needle form) and tantō-gata (knife form); some were named after an object of similar appearance, such as hoko-gata (spear form), matsuba-gata (pine-needle form); others have names that are a simple description of the object being thrown, such as kankyuto (piercing tool form), kunai-gata (utility tool form), or teppan (plate metal) and biao (pin).[2]

The bo-shuriken is thrown in a number of ways, such as overhead, underarm, sideways and rearwards, but in each case the throw involves the blade sliding out of the hand through the fingers in a smooth, controlled flight. The major throwing methods are the jiki da-ho (direct-hit method), and the han-ten da-ho (turning-hit method). These two are technically different, in that the former does not allow the blade to spin before it hits the target, while the latter requires that the blade should spin.

Other items such as hairpins, kogata (utility knife), and chopsticks were thrown in the same way as bo-shuriken although they are not associated with any particular school of shurikenjutsu.

The origins of the bo-shuriken in Japan are still unclear despite continuing research. This is partly because shurikenjutsu was a secret art and also due to the fact that throughout early Japanese history there were many independent exponents of the skill of throwing long, thin objects. The earliest-known reference to a school teaching shurikenjutsu is to Ganritsu Ryu, active during the 17th century. This school utilized a long, thin implement with a bulbous head, thought to be derived from the arrow. Surviving examples of blades used by this school appear to combine an arrow's shape with that of a needle traditionally used in Japanese leatherwork and armor manufacture.[2]

There are earlier mentions in written records,[clarification needed] such as the Osaka Gunki (大阪軍記, the military records of Osaka), of the standard knife and short sword being thrown in battle. Miyamoto Musashi is said to have won a duel by throwing his short sword at his opponent, killing him.

Hira shuriken/shaken

Hira-shuriken generally resemble the popular conception of shuriken. They are constructed from thin, flat plates of metal derived from a variety of sources including hishi-gane (coins), kugi-nuki (carpentry tools), spools and senban (nail removers).

They often have a hole in the center and possess a fairly thin blade sharpened mainly at the tip. The holes derive from their source in items that had holes – old coins, washers, and nail-removing tools. This proved convenient for the shuriken user as the weapons could be strung on a string or dowel in the belt for transport, and the hole also had aerodynamic and weighting effects that aided the flight of the blade.[2]

There are a wide variety of forms of hira-shuriken and they are now usually identified by the number of points the blades possess. As with bo-shuriken, the various shapes of hira-shuriken were usually representative of a particular school (ryū) or region that preferred the use of such shapes and it is therefore possible to identify the school by the type of blade used.[2]

Usage

Contrary to popular belief, shuriken were not primarily intended as killing weapons, but rather in a secondary role[3] as a nuisance or distraction. Targets were primarily the more exposed parts of the body: the eyes, face, hands, or feet. The shuriken would sometimes be thrown in a way that slashed the opponent in a glancing blow and travelled on, becoming lost, leaving him confused about the cause of the wound.[1]

Shuriken, especially hira-shuriken, were also used in novel ways—they could be embedded in the ground, injuring those who stepped on them (similar to a caltrop), wrapped in fuse to be lit and thrown to cause fire, or wrapped in a cloth soaked in poison and lit to cover an area with a cloud of poisonous smoke.[4] They could also be used as a handheld weapon in close combat.[5]

There are reports of shuriken being coated with poison, intended either as a throwing weapon or to be left in a conspicuous place for a victim to pick up.[6] Other reports indicate that shuriken may have been buried in dirt or animal feces and allowed to harbor the bacterium Clostridium tetani—if the point penetrated a victim deeply enough, the bacteria transferred into the wound could cause a then-incurable tetanus infection.

Shuriken are simple weapons, but their historical value has increased. Unlike the treasured katana and other bladed weapons, antique shuriken are not often well preserved, largely due to their expendable nature.[7]

Today

Modern shuriken are most often made of stainless steel and are commercially available in many knife shops in Europe and North America, or via the Internet. They are illegal to possess or carry in some countries, such as Belgium, the Netherlands, Canada,[8] Germany,[9] and the United Kingdom (manufacture, sale, distribution and import).[10] In the United States, some states prohibit them (e.g., California,[11] Indiana,[12] New York)[13] while others allow them. In some cases they may be allowed but are still subject to specific local legislation. Owners may be required to possess a certificate for the possession of knives.

See also



This article uses material from the Wikipedia article "Shuriken", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Entertainment

Entertainment