powered by CADENAS

Social Share

Dot matrix printing (1680 views - Basics)

Dot matrix printing is the process of computer printing from a collection of dot matrix data to a device, which can be one of: Impact dot matrix printers, what The New York Times calls "dot-matrix impact printers." non-impact dot matrix printers, such as inkjet, thermal, or laser printers. Dot matrix (impact) printing is a type of computer printing which uses a print head that moves back-and-forth, or in an up-and-down motion, on the page and prints by impact, striking an ink-soaked cloth ribbon against the paper, much like the print mechanism on a typewriter. However, unlike a typewriter or daisy wheel printer, letters are drawn out of a dot matrix, and thus, varied fonts and arbitrary graphics can be produced. These printers can print on multi-part (carbon paper) forms since they print using mechanical pressure.
Go to Article

Explanation by Hotspot Model

Dot matrix printing

Dot matrix printing

Dot matrix printing

Dot matrix printing is the process of computer printing from a collection of dot matrix data to a device, which can be one of:

  • Impact dot matrix printers, what The New York Times calls "dot-matrix impact printers."[1]
  • non-impact dot matrix printers, such as inkjet, thermal, or laser printers.

Dot matrix (impact) printing is a type of computer printing which uses a print head that moves back-and-forth, or in an up-and-down motion, on the page and prints by impact, striking an ink-soaked cloth ribbon against the paper, much like the print mechanism on a typewriter. However, unlike a typewriter or daisy wheel printer, letters are drawn out of a dot matrix, and thus, varied fonts and arbitrary graphics can be produced.

These printers can print on multi-part (carbon paper) forms since they print using mechanical pressure.

Dot-matrix impact printing

Sometimes called impact matrix printing or dot matrix printing, this is a type of computer printing which uses a print head that moves back-and-forth, or in an up-and-down motion, on the page and prints by impact, striking an ink-soaked cloth ribbon against the paper, much like the print mechanism on a typewriter. However, unlike a typewriter or daisy wheel printer, letters are drawn out of a dot matrix, and thus, varied fonts and arbitrary graphics can be produced.

Although nearly all inkjet, thermal, and laser printers also print closely spaced dots rather than continuous lines or characters, it is not customary to call them dot matrix printers.

Design

Each dot is produced by a tiny metal rod, also called a "wire" or "pin", which is driven forward by the power of a tiny electromagnet or solenoid, either directly or through small levers (pawls). Facing the ribbon and the paper is a small guide plate named ribbon mask holder or protector, sometimes also called butterfly for its typical shape. It is pierced with holes to serve as guides for the pins. This plate may be made of hard plastic or an artificial jewel such as sapphire or ruby.

The portion of the printer containing the pins is called the print head. When running the printer, it generally prints one line of text at a time. There are two approaches to achieve this:

The common serial dot matrix printers use a horizontally moving print head. The print head can be thought of featuring a single vertical column of seven or more pins approximately the height of a character box. In reality, the pins are arranged in up to four vertically or/and horizontally slightly displaced columns in order to increase the dot density and print speed through interleaving without causing the pins to jam. Thereby, up to 48 pins can be used to form the characters of a line while the print head moves horizontally.

In a considerably different configuration, so called line dot matrix printers use a fixed print head almost as wide as the paper path utilizing a horizontal line of thousands of pins for printing. Sometimes two horizontally slightly displaced rows are used to improve the effective dot density through interleaving. While still line-oriented, these printers for the professional heavy-duty market effectively print a whole line at once while the paper moves forward below the print head.

The printing speed of serial dot matrix printers with moving heads varies from 30[2] to 1550 cps.[3] In contrast to this, line matrix printers are capable of printing much more than 1000 cps, resulting in a throughput of up to 800 pages/hour.

Because the printing involves mechanical pressure, both of these types of printers can create carbon copies and carbonless copies.

These machines can be highly durable. When they do wear out, it is generally due to ink invading the guide plate of the print head, causing grit to adhere to it; this grit slowly causes the channels in the guide plate to wear from circles into ovals or slots, providing less and less accurate guidance to the printing wires. Eventually, even with tungsten blocks and titanium pawls, the printing becomes too unclear to read, a common problem when users failed to maintain the printer with regular cleaning as outlined in most user manuals.

A variation on the dot matrix printer was the cross hammer dot printer, patented by Seikosha in 1982.[4] The smooth cylindrical roller of a conventional printer was replaced by a spinning, fluted cylinder. The print head was a simple hammer, with a vertical projecting edge, operated by an electromagnet. Where the vertical edge of the hammer intersected the horizontal flute of the cylinder, compressing the paper and ribbon between them, a single dot was marked on the paper. Characters were built up of multiple dots.

Early history

In 1925, Rudolf Hell invented the Hellschreiber, an early facsimile-like dot matrix-based teletypewriter device,[5] patented in 1929.

Between 1952 and 1954 Fritz Karl Preikschat filed five patent applications[6][7][8] for his teletype writer 7 stylus 35 dot matrix aka PKT printer,[5] a dot matrix teletypewriter built between 1954 and 1956 in Germany.[8] Like the earlier Hellschreiber, it still used electromechanical means of coding and decoding, but it used a start-stop method (asynchronous transmission) rather than synchronous transmission for communication.[5] In 1956, while he was employed at Telefonbau und Normalzeit GmbH (TuN, later called Tenovis), the device was introduced to the Deutsche Bundespost (German Post Office), which did not show interest. When Preikschat emigrated into the USA in 1957 he sold the rights to utilize the applications in any countries (except for the USA) to TuN.[8] The prototype was also shown to General Mills in 1957.[9] An improved transistorized design[5] became the basis for a portable dot matrix facsimile machine, which was prototyped and evaluated for military use by Boeing around 1966–1967.[10][11]

The first non-impact dot matrix printer was marketed by IBM in 1957.[12][13]

In 1968, the Japanese manufacturer OKI introduced its first serial impact dot matrix printer (SIDM), the OKI Wiredot. The printer supported a character generator for 128 characters with a print matrix of 7×5. It was aimed at governmental, financial, scientific and educational markets. For this achievement, OKI received an award from the Information Processing Society of Japan (IPSJ) in 2013.[14][15][16]

In 1970 Digital Equipment Corporation (DEC) introduced an impact dot matrix printer, the LA30, as did Centronics (then of Hudson, New Hampshire): the Centronics 101.[17] The search for a reliable printer mechanism led it to develop a relationship with Brother Industries, Ltd of Japan, and the sale of Centronics-badged Brother printer mechanisms equipped with a Centronics print head and Centronics electronics. Unlike Digital, Centronics concentrated on the low-end line printer marketplace with their distinctive units. In the process, they designed the parallel electrical interface that was to become standard on most printers until it began to be replaced by the Universal Serial Bus (USB) in the late 1990s.

Printer head positioning

The printer head is attached to a metal bar that ensures correct alignment, but horizontal positioning is controlled by a band that attaches to sprockets on two wheels at each side which is then driven with an electric motor. This band may be made of stainless steel, phosphor bronze or beryllium copper alloys, nylon or various synthetic materials with a twisted nylon core to prevent stretching. Actual position can be found out either by dead count using a stepper motor, rotary encoder attached to one wheel or a transparent plastic band with markings that is read by an optical sensor on the printer head (common on inkjets).

Uses

The hardware known as dot matrix printers, in the 1970s and 1980s, were generally considered the best combination of expense and versatility, and until the 1990s they were by far the most common form of printer used with personal and home computers.

Advantages and disadvantages

Dot matrix printers, like any impact printer, can print on multi-part stationery or make carbon-copies. Impact printers have one of the lowest printing costs per page. As the ink is running out, the printout gradually fades rather than suddenly stopping partway through a job. They are able to use continuous paper rather than requiring individual sheets, making them useful for data logging. They are good, reliable workhorses ideal for use in situations where low printing cost is more important than quality. The ink ribbon also does not easily dry out, including both the ribbon stored in the casing as well as the portion that is stretched in front of the print head; this unique property allows the dot-matrix printer to be used in environments where printer duty can be rare, for instance, as with a Fire Alarm Control Panel's output.

Impact printers create noise when the pins or typeface strike the ribbon to the paper,[18] and sound-damping enclosures may have to be used in quiet environments. They can only print lower-resolution graphics, with limited color performance, limited quality, and lower speeds compared to non-impact printers. While they support fanfold paper with tractor holes well, single-sheet paper may have to be wound in and aligned by hand, which is relatively time-consuming, or a sheet feeder may be utilized which can have a lower paper feed reliability. When printing labels on release paper, they are prone to paper jams when a print wire snags the leading edge of the label while printing at its very edge. For text-only labels (e.g. mailing labels), a daisy wheel printer or band printer may offer better print quality and a lower risk of damaging the paper.

The advantages are: low purchase cost, can handle multipart forms, cheap to operate, only needs fresh ribbons, rugged, low repair cost and the ability to print on continuous paper. This makes it possible to print long banners that span across several sheets of paper.

The disadvantages are: noisy, low resolution (dots making up each character are visible), not all can do color, color looks faded and streaky, slowness and more prone to jamming - with jams that are more difficult to clear. This is because paper is fed in using two sprockets engaging with holes in the paper. A small tear on the side of a sheet can cause a jam, with paper debris that is tedious to remove.

See also



This article uses material from the Wikipedia article "Dot matrix printing", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Basics

3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted