powered by CADENAS

Social Share

Pipe (2007 views - Plant Design)

Pipe usually refers to: Pipe (fluid conveyance), a hollow cylinder following certain dimension rules Piping, the use of pipes in industry Smoking pipe Pipe may also refer to:
Go to Article

Explanation by Hotspot Model

Pipe

Pipe

Pipe usually refers to:

Pipe may also refer to:

Music

  • Pipe (instrument), a traditional perforated wind instrument
  • Bagpipe, a class of musical instrument, aerophones using enclosed reeds
    • Uilleann pipes, a unique form of bagpipes originating in Ireland
    • Pipes and drums or pipe bands, composed of musicians who play the Scottish and Irish bagpipes
  • Pan pipes, see Pan flute, an ancient musical instrument based on the principle of the stopped pipe
  • Organ pipe, one of the tuned resonators that produces the main sound of a pipe organ
  • Boatswain's pipe, an instrument used for signalling or to issue commands on a warship

Computing

Proper noun

Other uses

See also



This article uses material from the Wikipedia article "Pipe", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Plant Design

Aveva Tribon, Aveva PDMS, Intergraph Smartplant, Intergraph Smartmarine, Offshore, Onshore, Marine, Shipyard, Plantdesign