powered by CADENAS

Social Share

Clothing (3214 views - Consumer products)

Clothing (also known as clothes and attire) is fibre and textile material worn on the body. The wearing of clothing is mostly restricted to human beings and is a feature of nearly all human societies. The amount and type of clothing worn depends on body type, social, and geographic considerations. Some clothing can be gender-specific. Physically, clothing serves many purposes: it can serve as protection from the elements, and can enhance safety during hazardous activities such as hiking and cooking. It protects the wearer from rough surfaces, rash-causing plants, insect bites, splinters, thorns and prickles by providing a barrier between the skin and the environment. Clothes can insulate against cold or hot conditions. Further, they can provide a hygienic barrier, keeping infectious and toxic materials away from the body. Clothing also provides protection from ultraviolet radiation. Wearing clothes is also a social norm, as being deprived of clothing in front of others may be embarrassing, or not wearing clothes in public to the extent that genitals, breasts or buttocks are visible could be seen as indecent exposure.
Go to Article

Explanation by Hotspot Model

Clothing

Clothing

Clothing

Clothing (also known as clothes and attire) is fibre and textile material worn on the body. The wearing of clothing is mostly restricted to human beings and is a feature of nearly all human societies. The amount and type of clothing worn depends on body type, social, and geographic considerations. Some clothing can be gender-specific.

Physically, clothing serves many purposes: it can serve as protection from the elements, and can enhance safety during hazardous activities such as hiking and cooking. It protects the wearer from rough surfaces, rash-causing plants, insect bites, splinters, thorns and prickles by providing a barrier between the skin and the environment. Clothes can insulate against cold or hot conditions. Further, they can provide a hygienic barrier, keeping infectious and toxic materials away from the body. Clothing also provides protection from ultraviolet radiation. Wearing clothes is also a social norm, as being deprived of clothing in front of others may be embarrassing, or not wearing clothes in public to the extent that genitals, breasts or buttocks are visible could be seen as indecent exposure.

Origin of clothing

There is no easy way to determine when clothing was first developed, but some information has been inferred by studying lice which estimates put the introduction of clothing at roughly 42,000–72,000 years ago.[1][2][3][4][5]

Functions

The most obvious function of clothing is to improve the comfort of the wearer, by protecting the wearer from the elements. In hot climates, clothing provides protection from sunburn or wind damage, while in cold climates its thermal insulation properties are generally more important. Shelter usually reduces the functional need for clothing. For example, coats, hats, gloves, and other superficial layers are normally removed when entering a warm home, particularly if one is residing or sleeping there. Similarly, clothing has seasonal and regional aspects, so that thinner materials and fewer layers of clothing are generally worn in warmer seasons and regions than in colder ones.

Clothing performs a range of social and cultural functions, such as individual, occupational and gender differentiation, and social status.[6] In many societies, norms about clothing reflect standards of modesty, religion, gender, and social status. Clothing may also function as a form of adornment and an expression of personal taste or style.

Clothing can and has in history been made from a very wide variety of materials. Materials have ranged from leather and furs, to woven materials, to elaborate and exotic natural and synthetic fabrics. Not all body coverings are regarded as clothing. Articles carried rather than worn (such as purses), worn on a single part of the body and easily removed (scarves), worn purely for adornment (jewelry), or those that serve a function other than protection (eyeglasses), are normally considered accessories rather than clothing, as are footwear and hats.

Clothing protects against many things that might injure the uncovered human body. Clothes protect people from the elements, including rain, snow, wind, and other weather, as well as from the sun. However, clothing that is too sheer, thin, small, tight, etc., offers less protection. Clothes also reduce risk during activities such as work or sport. Some clothing protects from specific environmental hazards, such as insects, noxious chemicals, weather, weapons, and contact with abrasive substances. Conversely, clothing may protect the environment from the clothing wearer, as with doctors wearing medical scrubs.

Humans have shown extreme invention in devising clothing solutions to environmental hazards. Examples include: space suits, air conditioned clothing, armor, diving suits, swimsuits, bee-keeper gear, motorcycle leathers, high-visibility clothing, and other pieces of protective clothing. Meanwhile, the distinction between clothing and protective equipment is not always clear-cut—since clothes designed to be fashionable often have protective value and clothes designed for function often consider fashion in their design. Wearing clothes also has social implications. They cover parts of the body that social norms require to be covered, act as a form of adornment, and serve other social purposes. Someone who lacks the means to procure reasonable clothing due to poverty or affordability is sometimes said to be scruffy ragged or shabby.[7]

Scholarship

Although dissertations on clothing and its function appear from the 19th century as colonising countries dealt with new environments,[8] concerted scientific research into psycho-social, physiological and other functions of clothing (e.g. protective, cartage) occurred in the first half of the 20th century, with publications such as J. C. Flügel's Psychology of Clothes in 1930,[6] and Newburgh's seminal Physiology of Heat Regulation and The Science of Clothing in 1949.[9] By 1968, the field of environmental physiology had advanced and expanded significantly, but the science of clothing in relation to environmental physiology had changed little.[10] While considerable research has since occurred and the knowledge-base has grown significantly, the main concepts remain unchanged, and indeed Newburgh's book is still cited by contemporary authors, including those attempting to develop thermoregulatory models of clothing development.[11]

Cultural aspects

Gender differentiation

Former 3rd Duke of Fife wearing a traditional Scottish kilt. (1984)

In most cultures, gender differentiation of clothing is considered appropriate. The differences are in styles, colors and fabrics.

In Western societies, skirts, dresses and high-heeled shoes are usually seen as women's clothing, while neckties are usually seen as men's clothing. Trousers were once seen as exclusively male clothing, but can nowadays be worn by both genders. Male clothes are often more practical (that is, they can function well under a wide variety of situations), but a wider range of clothing styles are available for females. Males are typically allowed to bare their chests in a greater variety of public places. It is generally more or less acceptable for a woman to wear clothing perceived as masculine, while the opposite is seen as unusual.

In some cultures, sumptuary laws regulate what men and women are required to wear. Islam requires women to wear more modest forms of attire, usually hijab. What qualifies as "modest" varies in different Muslim societies. However, women are usually required to cover more of their bodies than men are. Articles of clothing Muslim women wear for modesty range from the head-scarf to the burqa.

Men may sometimes choose to wear men's skirts such as togas or kilts, especially on ceremonial occasions. Such garments were (in previous times) often worn as normal daily clothing by men.

Clothing designed to be worn by either sex is called unisex clothing. Unisex clothes, such as T-shirts, tends to be cut straighter to fit a wider variety of bodies. The majority of unisex clothing styles have started out as menswear, but some articles, like the fedora, were originally worn by women.

Social status

Alim Khan's bemedaled robe sends a social message about his wealth, status, power, and ego.

In some societies, clothing may be used to indicate rank or status. In ancient Rome, for example, only senators could wear garments dyed with Tyrian purple. In traditional Hawaiian society, only high-ranking chiefs could wear feather cloaks and palaoa, or carved whale teeth. In China, before establishment of the republic, only the emperor could wear yellow. History provides many examples of elaborate sumptuary laws that regulated what people could wear. In societies without such laws, which includes most modern societies, social status is instead signaled by the purchase of rare or luxury items that are limited by cost to those with wealth or status. In addition, peer pressure influences clothing choice.

Religion

Muslim men traditionally wear white robes and a cap during prayers

Religious clothing might be considered a special case of occupational clothing. Sometimes it is worn only during the performance of religious ceremonies. However, it may also be worn everyday as a marker for special religious status.

For example, Jains and Muslim men wear unstitched cloth pieces when performing religious ceremonies. The unstitched cloth signifies unified and complete devotion to the task at hand, with no digression.[citation needed] Sikhs wear a turban as it is a part of their religion.

The cleanliness of religious dresses in Eastern religions like Hinduism, Sikhism, Buddhism, Islam and Jainism is of paramount importance, since it indicates purity.

Clothing figures prominently in the Bible where it appears in numerous contexts, the more prominent ones being: the story of Adam and Eve who made coverings for themselves out of fig leaves, Joseph's cloak, Judah and Tamar, Mordecai and Esther. Furthermore, the priests officiating in the Temple had very specific garments, the lack of which made one liable to death.

The Quran says about husbands and wives, regarding clothing: "...They are clothing/covering (Libaas) for you; and you for them" (chapter 2:187).

Jewish ritual also requires rending of one's upper garment as a sign of mourning. This practice is found in the Bible when Jacob hears of the apparent death of his son Joseph.[12]

Origin and history

First recorded use

According to archaeologists and anthropologists, the earliest clothing likely consisted of fur, leather, leaves, or grass that were draped, wrapped, or tied around the body. Knowledge of such clothing remains inferential, since clothing materials deteriorate quickly compared to stone, bone, shell and metal artifacts. Archeologists have identified very early sewing needles of bone and ivory from about 30,000 BC, found near Kostenki, Russia in 1988.[13] Dyed flax fibers that could have been used in clothing have been found in a prehistoric cave in the Republic of Georgia that date back to 36,000 BP.[14][15]

Scientists are still debating when people started wearing clothes. Ralf Kittler, Manfred Kayser and Mark Stoneking, anthropologists at the Max Planck Institute for Evolutionary Anthropology, have conducted a genetic analysis of human body lice that suggests clothing originated quite recently, around 170,000 years ago. Body lice is an indicator of clothes-wearing, since most humans have sparse body hair, and lice thus require human clothing to survive. Their research suggests the invention of clothing may have coincided with the northward migration of modern Homo sapiens away from the warm climate of Africa, thought to have begun between 50,000 and 100,000 years ago. However, a second group of researchers using similar genetic methods estimate that clothing originated around 540,000 years ago [16] For now, the date of the origin of clothing remains unresolved.

Making clothing

Some human cultures, such as the various people of the Arctic Circle, traditionally make their clothing entirely of prepared and decorated furs and skins. Other cultures supplemented or replaced leather and skins with cloth: woven, knitted, or twined from various animal and vegetable fibers including wool, linen, cotton, silk, hemp, and ramie.

Although modern consumers may take the production of clothing for granted, making fabric by hand is a tedious and labor-intensive process involving fiber making, spinning, and weaving. The textile industry was the first to be mechanized – with the powered loom – during the Industrial Revolution.

Different cultures have evolved various ways of creating clothes out of cloth. One approach simply involves draping the cloth. Many people wore, and still wear, garments consisting of rectangles of cloth wrapped to fit – for example, the dhoti for men and the sari for women in the Indian subcontinent, the Scottish kilt or the Javanese sarong. The clothes may simply be tied up, as is the case of the first two garments; or pins or belts hold the garments in place, as in the case of the latter two. The precious cloth remains uncut, and people of various sizes or the same person at different sizes can wear the garment.

Another approach involves measuring, cutting, and sewing the cloth by hand or with a sewing machine. Clothing can be cut from a sewing pattern and adjusted by a tailor to a persons measurements. An adjustable sewing mannequin or dress form is used to create form fitting clothing. Fabrics are expensive and efforts are made to use every bit of the cloth rectangle in constructing the clothing. The tailor may cut triangular pieces from one corner of the cloth, and then add them elsewhere as gussets. Traditional European patterns for men's shirts and women's chemises take this approach. These remnant can also be rused to make patchwork hats, vests, and skirts.

Modern European fashion treats cloth much less conservatively, typically cutting in such a way as to leave various odd-shaped cloth remnants. Industrial sewing operations sell these as waste; home sewers may turn them into quilts.

In the thousands of years that humans have spent constructing clothing, they have created an astonishing array of styles, many of which have been reconstructed from surviving garments, photos, paintings, mosaics, etc., as well as from written descriptions. Costume history serves as a source of inspiration to current fashion designers, as well as a topic of professional interest to costumers constructing for plays, films, television, and historical reenactment.

Contemporary clothing

Western dress codes

Western dress code

The Western dress code has changed over the past 500+ years. The mechanization of the textile industry made many varieties of cloth widely available at affordable prices. Styles have changed, and the availability of synthetic fabrics has changed the definition of "stylish". In the latter half of the 20th century, blue jeans became very popular, and are now worn to events that normally demand formal attire. Activewear has also become a large and growing market.

The licensing of designer names was pioneered by designers like Pierre Cardin in the 1960s and has been a common practice within the fashion industry from about the 1970s. Among the more popular include Marc Jacobs and Gucci, named for Marc Jacobs and Guccio Gucci respectively.

Spread of western styles

By the early years of the 21st century, western clothing styles had, to some extent, become international styles. This process began hundreds of years earlier, during the periods of European colonialism. The process of cultural dissemination has perpetuated over the centuries as Western media corporations have penetrated markets throughout the world, spreading Western culture and styles. Fast fashion clothing has also become a global phenomenon. These garments are less expensive, mass-produced Western clothing. Donated used clothing from Western countries are also delivered to people in poor countries by charity organizations.

Ethnic and cultural heritage

People may wear ethnic or national dress on special occasions or in certain roles or occupations. For example, most Korean men and women have adopted Western-style dress for daily wear, but still wear traditional hanboks on special occasions, like weddings and cultural holidays. Items of Western dress may also appear worn or accessorized in distinctive, non-Western ways. A Tongan man may combine a used T-shirt with a Tongan wrapped skirt, or tupenu.

Sport and activity

Most sports and physical activities are practiced wearing special clothing, for practical, comfort or safety reasons. Common sportswear garments include shorts, T-shirts, tennis shirts, leotards, tracksuits, and trainers. Specialized garments include wet suits (for swimming, diving or surfing), salopettes (for skiing) and leotards (for gymnastics). Also, spandex materials are often used as base layers to soak up sweat. Spandex is also preferable for active sports that require form fitting garments, such as volleyball, wrestling, track & field, dance, gymnastics and swimming.

Fashion

A diverse range of styles exist in fashion, varying by geography, exposure to modern media, economic conditions, and ranging from expensive haute couture to traditional garb, to thrift store grunge. Fashion shows are events for designers to show off new and often extravagant designs.

Future trends

The world of clothing is always changing, as new cultural influences meet technological innovations. Researchers in scientific labs have been developing prototypes for fabrics that can serve functional purposes well beyond their traditional roles, for example, clothes that can automatically adjust their temperature, repel bullets, project images, and generate electricity. Some practical advances already available to consumers are bullet-resistant garments made with kevlar and stain-resistant fabrics that are coated with chemical mixtures that reduce the absorption of liquids. New blends of Spandex cotton blends allow for form fitting and stretching of closer fitting mass produced patterns. New mesh materials allow for better breathe-ability in shoes. New insulation fibers and batting make lighter rainments that keep you warm when wet and recent advances in coatings for fabrics or down also repel water.

Political issues

Working conditions in the garments industry

Though mechanization transformed most aspects of human industry by the mid-20th century, garment workers have continued to labor under challenging conditions that demand repetitive manual labor. Mass-produced clothing is often made in what are considered by some to be sweatshops, typified by long work hours, lack of benefits, and lack of worker representation. While most examples of such conditions are found in developing countries, clothes made in industrialized nations may also be manufactured similarly.[citation needed]

Coalitions of NGOs, designers (including Katharine Hamnett, American Apparel, Veja, Quiksilver, eVocal, and Edun) and campaign groups like the Clean Clothes Campaign (CCC) and the Institute for Global Labour and Human Rights as well as textile and clothing trade unions have sought to improve these conditions as much as possible by sponsoring awareness-raising events, which draw the attention of both the media and the general public to the workers.

Outsourcing production to low wage countries like Bangladesh, China, India and Sri Lanka became possible when the Multi Fibre Agreement (MFA) was abolished. The MFA, which placed quotas on textiles imports, was deemed a protectionist measure.[citation needed] Although many countries recognize treaties like the International Labour Organization, which attempt to set standards for worker safety and rights, many countries have made exceptions to certain parts of the treaties or failed to thoroughly enforce them. India for example has not ratified sections 87 and 92 of the treaty.[citation needed]

Despite the strong reactions that "sweatshops" evoked among critics of globalization, the production of textiles has functioned as a consistent industry for developing nations providing work and wages, whether construed as exploitative or not, to many thousands of people.

Fur

The use of animal fur in clothing dates to prehistoric times. It is currently associated in developed countries with expensive, designer clothing, although fur is still used by indigenous people in arctic zones and higher elevations for its warmth and protection. Once uncontroversial, it has recently been the focus of campaigns on the grounds that campaigners consider it cruel and unnecessary. PETA, along with other animal rights and animal liberation groups have called attention to fur farming and other practices they consider cruel.

Life cycle

Clothing maintenance

Clothing suffers assault both from within and without. The human body sheds skin cells and body oils, and exudes sweat, urine, and feces. From the outside, sun damage, moisture, abrasion and dirt assault garments. Fleas and lice can hide in seams. Worn clothing, if not cleaned and refurbished, itches, looks scruffy, and loses functionality (as when buttons fall off, seams come undone, fabrics thin or tear, and zippers fail).

In some cases, people wear an item of clothing until it falls apart. Cleaning leather presents difficulties, and bark cloth (tapa) cannot be washed without dissolving it. Owners may patch tears and rips, and brush off surface dirt, but old leather and bark clothing always look old.

But most clothing consists of cloth, and most cloth can be laundered and mended (patching, darning, but compare felt).

Laundry, ironing, storage

Humans have developed many specialized methods for laundering, ranging from early methods of pounding clothes against rocks in running streams, to the latest in electronic washing machines and dry cleaning (dissolving dirt in solvents other than water). Hot water washing (boiling), chemical cleaning and ironing are all traditional methods of sterilizing fabrics for hygiene purposes.

Many kinds of clothing are designed to be ironed before they are worn to remove wrinkles. Most modern formal and semi-formal clothing is in this category (for example, dress shirts and suits). Ironed clothes are believed to look clean, fresh, and neat. Much contemporary casual clothing is made of knit materials that do not readily wrinkle, and do not require ironing. Some clothing is permanent press, having been treated with a coating (such as polytetrafluoroethylene) that suppresses wrinkles and creates a smooth appearance without ironing.

Once clothes have been laundered and possibly ironed, they are usually hung on clothes hangers or folded, to keep them fresh until they are worn. Clothes are folded to allow them to be stored compactly, to prevent creasing, to preserve creases or to present them in a more pleasing manner, for instance when they are put on sale in stores.

Non-iron

A resin used for making non-wrinkle shirts releases formaldehyde, which could cause contact dermatitis for some people; no disclosure requirements exist, and in 2008 the U.S. Government Accountability Office tested formaldehyde in clothing and found that generally the highest levels were in non-wrinkle shirts and pants.[17] In 1999, a study of the effect of washing on the formaldehyde levels found that after 6 months after washing, 7 of 27 shirts had levels in excess of 75 ppm, which is a safe limit for direct skin exposure.[18]

Mending

In past times, mending was an art. A meticulous tailor or seamstress could mend rips with thread raveled from hems and seam edges so skillfully that the tear was practically invisible. When the raw material – cloth – was worth more than labor, it made sense to expend labor in saving it. Today clothing is considered a consumable item. Mass-manufactured clothing is less expensive than the labor required to repair it. Many people buy a new piece of clothing rather than spend time mending. The thrifty still replace zippers and buttons and sew up ripped hems.

Recycling

Used, unwearable clothing can be repurposed for quilts, rags, rugs, bandages, and many other household uses. It can also be recycled into paper. In Western societies, used clothing is often thrown out or donated to charity (such as through a clothing bin). It is also sold to consignment shops, dress agencies, flea markets, and in online auctions. Used clothing is also often collected on an industrial scale to be sorted and shipped for re-use in poorer countries.

There are many concerns about the life cycle of synthetics, which come primarily from petrochemicals.[weasel words] Unlike natural fibers, their source is not renewable and they are not biodegradable.[19]

See also



This article uses material from the Wikipedia article "Clothing", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Consumer products

.max, Maya, Challenge, Competition, Rendering, 3D, Blender, Autodesk Maya, 3D Studio MAX (.3DS, .MAX), Maxwell, Animation, 3D Model, Autodesk Softimage, Cinema 4D, Rendering, Animation, 3Dartist, c4d, maxon, lowpoly, 3Dart, blender3D, 3D library