powered by CADENAS

Social Share

Safari (2586 views - Nature)

A safari is an overland journey, usually a trip by tourists to Africa. In the past, the trip was often a big-game hunt, but today, safari often refers to trips to observe and photograph wildlife—or hiking and sight-seeing as well.
Go to Article

Explanation by Hotspot Model

Safari

Safari

A safari /səˈfɑːri/ is an overland journey, usually a trip by tourists to Africa. In the past, the trip was often a big-game hunt, but today, safari often refers to trips to observe and photograph wildlife—or hiking and sight-seeing as well.

Etymology

The Swahili word safari means journey, originally from the Arabic سفر (safar) meaning a journey;[1] the verb for "to travel" in Swahili is kusafiri. These words are used for any type of journey, e.g. by bus from Nairobi to Mombasa or by ferry from Dar es Salaam to Unguja. Safari entered the English language at the end of the 1850s thanks to Richard Francis Burton, the famous explorer.[2]

The Regimental March of the King's African Rifles was 'Funga Safari', literally 'tie up the March', or, in other words, pack up equipment ready to march.

Funga safari, funga safari. Funga safari, funga safari. Amri ya nani? Amri ya nani? Amri ya Bwana Kapteni, Amri ya KAR.

Which is, in English:

Prepare to March, Prepare to March. On whose orders? On whose orders? On the order of the boss captain, On the order of the KAR.

On Kenya's independence from Britain, Funga Safari was retained as the Regimental March of the Kenya Rifles, successor to the K.A.R.

History

In 1836 William Cornwallis Harris led an expedition purely to observe and record wildlife and landscapes by the expedition's members. Harris established the safari style of journey, starting with a not too strenuous rising at first light, an energetic day walking, an afternoon rest then concluding with a formal dinner and telling stories in the evening over drinks and tobacco.[3]

Literary genre

Jules Verne's first novel Five Weeks in a Balloon published in 1863 and H. Rider Haggard's first novel King Solomon's Mines published in 1885, both describe journeys of English travellers on Safari and were best sellers in their day. These two books gave rise to a genre of Safari adventure novels and films.[citation needed]

Ernest Hemingway wrote several fiction and non-fiction pieces about African safaris. His short stories "The Short Happy Life of Francis Macomber" and "The Snows of Kilimanjaro" are set on African safaris and were written after Hemingway's own experience on safari. His books Green Hills of Africa and True at First Light are both set on African safaris.

Cinematic genre

The safari provided countless hours of cinema entertainment in sound films from Trader Horn (1931) onwards. The safari was used in many adventure films such as the Tarzan, Jungle Jim, and Bomba the Jungle Boy film series up to The Naked Prey (1965) where Cornel Wilde, a white hunter, becomes game himself. The safari genre films were parodied in the Bob Hope comedies Road to Zanzibar and Call Me Bwana. A short 15-minute helicopter safari was shown in Africa Addio where clients are armed, flown from their hotel and landed in front of an unlucky and baffled elephant. Out of Africa has Karen Blixen and famous hunter Denys Finch Hatton travelling, with Denys refusing to abandon home comforts using fine china and crystal and listening to Mozart recordings over the gramophone while on safari trip.

Fashion

There is a certain theme or style associated with the word, which includes khaki clothing, belted bush jackets, pith helmets or slouch hats, and animal skin patterns. The term safari chic arose after the release of the film Out of Africa.[4] This not only included clothing but also interior design and architecture.[5]

See also



This article uses material from the Wikipedia article "Safari", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Nature

3d,model,rendering,library,tree,bush,flower,landscape,design,architecure