powered by CADENAS

Social Share

Environmental engineering (5493 views - Environmental Protection)

Environmental engineering is the branch of engineering concerned with the application of scientific and engineering principles for protection of human populations from the effects of adverse environmental factors; protection of environments, both local and global, from potentially deleterious effects of natural and human activities; and improvement of environmental quality. Environmental engineering can also be described as a branch of applied science and technology that addresses the issues of energy preservation, protection of assets and control of waste from human and animal activities. Furthermore, it is concerned with finding plausible solutions in the field of public health, such as waterborne diseases, implementing laws which promote adequate sanitation in urban, rural and recreational areas. It involves waste water management, air pollution control, recycling, waste disposal, radiation protection, industrial hygiene, animal agriculture, environmental sustainability, public health and environmental engineering law. It also includes studies on the environmental impact of proposed construction projects. Environmental engineers study the effect of technological advances on the environment. To do so, they conduct studies on hazardous-waste management to evaluate the significance of such hazards, advise on treatment and containment, and develop regulations to prevent mishaps. Environmental engineers design municipal water supply and industrial wastewater treatment systems. They address local and worldwide environmental issues such as the effects of acid rain, global warming, ozone depletion, water pollution and air pollution from automobile exhausts and industrial sources. At many universities environmental engineering programs are offered at either the department of civil engineering or the department of chemical engineering at engineering faculties. Environmental "civil" engineers focus on hydrology, water resources management, bioremediation, and water treatment plant design. Environmental "chemical" engineers, on the other hand, focus on environmental chemistry, advanced air and water treatment technologies and separation processes. Additionally, engineers are more frequently obtaining specialized training in law (J.D.) and are utilizing their technical expertise in the practices of environmental engineering law. Most jurisdictions also impose licensing and registration requirements.
Go to Article

Explanation by Hotspot Model

Environmental engineering

Environmental engineering

Environmental engineering is the branch of engineering concerned with the application of scientific and engineering principles for protection of human populations from the effects of adverse environmental factors; protection of environments, both local and global, from potentially deleterious effects of natural and human activities; and improvement of environmental quality.[1]

Environmental engineering can also be described as a branch of applied science and technology that addresses the issues of energy preservation, protection of assets and control of waste from human and animal activities. Furthermore, it is concerned with finding plausible solutions in the field of public health, such as waterborne diseases, implementing laws which promote adequate sanitation in urban, rural and recreational areas. It involves waste water management, air pollution control, recycling, waste disposal, radiation protection, industrial hygiene, animal agriculture, environmental sustainability, public health and environmental engineering law. It also includes studies on the environmental impact of proposed construction projects.

Environmental engineers study the effect of technological advances on the environment. To do so, they conduct studies on hazardous-waste management to evaluate the significance of such hazards, advise on treatment and containment, and develop regulations to prevent mishaps. Environmental engineers design municipal water supply and industrial wastewater treatment systems.[2][3] They address local and worldwide environmental issues such as the effects of acid rain, global warming, ozone depletion, water pollution and air pollution from automobile exhausts and industrial sources.[4][5][6][7]

At many universities environmental engineering programs are offered at either the department of civil engineering or the department of chemical engineering at engineering faculties. Environmental "civil" engineers focus on hydrology, water resources management, bioremediation, and water treatment plant design. Environmental "chemical" engineers, on the other hand, focus on environmental chemistry, advanced air and water treatment technologies and separation processes.[citation needed]

Additionally, engineers are more frequently obtaining specialized training in law (J.D.) and are utilizing their technical expertise in the practices of environmental engineering law.[citation needed]

Most jurisdictions also impose licensing and registration requirements.

Development

Ever since people first recognized that their health is related to the quality of their environment, they have applied principles to attempt to improve the quality of their environment. The ancient Indian Harappan civilization utilized early sewers in some cities more than 5000 years ago. The Romans constructed aqueducts to prevent drought and to create a clean, healthful water supply for the metropolis of Rome. In the 15th century, Bavaria created laws restricting the development and degradation of alpine country that constituted the region's water supply.

The field emerged as a separate environmental discipline during the middle third of the 20th century in response to widespread public concern about water and pollution and increasingly extensive environmental quality degradation. However, its roots extend back to early efforts in public health engineering.[8] Modern environmental engineering began in London in the mid-19th century when Joseph Bazalgette designed the first major sewerage system that reduced the incidence of waterborne diseases such as cholera. The introduction of drinking water treatment and sewage treatment in industrialized countries reduced waterborne diseases from leading causes of death to rarities.[9]

In many cases, as societies grew, actions that were intended to achieve benefits for those societies had longer-term impacts which reduced other environmental qualities. One example is the widespread application of the pesticide DDT to control agricultural pests in the years following World War II. While the agricultural benefits were outstanding and crop yields increased dramatically thus reducing world hunger substantially, and malaria was controlled better than it ever had been, numerous species were brought to the verge of extinction due to the impact of the DDT on their reproductive cycles. The story of DDT as vividly told in Rachel Carson's Silent Spring (1962) is considered to be the birth of the modern environmental movement and of the modern field of "environmental engineering."[10]

Conservation movements and laws restricting public actions that would harm the environment have been developed by various societies for millennia. Notable examples are the laws decreeing the construction of sewers in London and Paris in the 19th century and the creation of the U.S. national park system in the early 20th century.

Scope

Solid waste management

Environmental impact assessment and mitigation

Scientists have air pollution dispersion models to evaluate the concentration of a pollutant at a receptor or the impact on overall air quality from vehicle exhausts and industrial flue gas stack emissions. To some extent, this field overlaps the desire to decrease carbon dioxide and other greenhouse gas emissions from combustion processes. They apply scientific and engineering principles to evaluate if there are likely to be any adverse impacts to water quality, air quality, habitat quality, flora and fauna, agricultural capacity, traffic impacts, social impacts, ecological impacts, noise impacts, visual (landscape) impacts, etc. If impacts are expected, they then develop mitigation measures to limit or prevent such impacts. An example of a mitigation measure would be the creation of wetlands in a nearby location to mitigate the filling in of wetlands necessary for a road development if it is not possible to reroute the road.

In the United States, the practice of environmental assessment was formally initiated on January 1, 1970, the effective date of the National Environmental Policy Act (NEPA). Since that time, more than 100 developing and developed nations either have planned specific analogous laws or have adopted procedure used elsewhere. NEPA is applicable to all federal agencies in the United States.[11]

Water supply and treatment

They evaluate the water balance within a watershed and determine the available water supply, the water needed for various needs in that watershed, the seasonal cycles of water movement through the watershed and they develop systems to store, treat, and convey water for various uses. Water is treated to achieve water quality objectives for the end uses. In the case of a potable water supply, water is treated to minimize the risk of infectious disease transmission, the risk of non-infectious illness, and to create a palatable water flavor. Water distribution systems are designed and built to provide adequate water pressure and flow rates to meet various end-user needs such as domestic use, fire suppression, and irrigation.

Wastewater treatment

There are numerous wastewater treatment technologies. A wastewater treatment train can consist of a primary clarifier system to remove solid and floating materials, a secondary treatment system consisting of an aeration basin followed by flocculation and sedimentation or an activated sludge system and a secondary clarifier, a tertiary biological nitrogen removal system, and a final disinfection process. The aeration basin/activated sludge system removes organic material by growing bacteria (activated sludge). The secondary clarifier removes the activated sludge from the water. The tertiary system, although not always included due to costs, is becoming more prevalent to remove nitrogen and phosphorus and to disinfect the water before discharge to a surface water stream or ocean outfall.[12]

Air pollution management

Scientists have developed air pollution dispersion models to evaluate the concentration of a pollutant at a receptor or the impact on overall air quality from vehicle exhausts and industrial flue gas stack emissions. To some extent, this field overlaps the desire to decrease carbon dioxide and other greenhouse gas emissions from combustion processes.

Environmental Protection Agency

The U.S. Environmental Protection Agency (EPA) is one of the many agencies that work with environmental engineers to solve key issues. An important component of EPA's mission is to protect and improve air, water, and overall environmental quality in order to avoid or mitigate the consequences of harmful effects.

Ecological engineering for sustainable agriculture in arid and semiarid West African regions[13]

Ecological engineering offers new alternatives for the management of agricultural systems that are more tailored to the ever-changing social and environmental necessities in these regions. This requires managing the complexity of agrosystems, while striving to mimic the functioning of natural ecosystems of West African drylands and taking advantage of traditional practices and local know-how resulting from a long process of adaptation to environmental constraints.

  1. Acting on biodiversity. Biodiversity is essential to the productivity of ecosystems and their temporal stability under the impact of external disturbances. Several ecological processes related to biodiversity may be intensified for the benefit of agrosilvopastoral systems: promoting diversity and soil microorganism activity to benefit plants, associating and utilizing the mutual benefits of plants
  2. Utilizing organic matter and nutrient cycles. The productivity of agrosystems with low chemical input use in dryland regions is primarily based on efficient organic resource management, and in turn on the nutrient and energy flows they induce. It is thus possible to intervene at several levels: enhancing crop-livestock farming integration to preserve natural resources, restoring the biological activity of soils via specific organic inputs, supplying nutrients to plants locally.
  3. Enhancing available water use. Water supplies are limited and irregular in dryland areas. Current management of these supplies—which involves capturing rainwater and surface runoff—could be improved in several ways: adapting to erratic rainfall or drought risks by focusing on: (i) the organization of the farm and community (farm plot patterns in association with the random rainfall distribution, etc.), and on (ii) cropping techniques to reduce crop water needs (plant choices, weeding, etc.), preserving water in crop fields by hampering runoff, accounting for the essential role of trees regarding soil and water in drylands.
  4. Managing landscapes and associated ecological processes. Ecological crop pest regulation by their natural enemies is one ecosystem service provided by biodiversity. Better pest management could be considered in association with promoting biodiversity at different scales, e.g. from the plant to the landscape.

Education

Courses aimed at developing graduates with specific skills in environmental systems or environmental technology are becoming more common and fall into broad classes:

  • Mechanical engineering courses oriented towards designing machines and mechanical systems for environmental use such as water treatment facilities, pumping stations, garbage segregation plants and other mechanical facilities;
  • Environmental engineering or environmental systems courses oriented towards a civil engineering approach in which structures and the landscape are constructed to blend with or protect the environment;
  • Environmental chemistry, sustainable chemistry or environmental chemical engineering courses oriented towards understanding the effects (good and bad) of chemicals in the environment. Focus on mining processes, pollutants and commonly also cover biochemical processes;
  • Environmental technology courses oriented towards producing electronic or electrical graduates capable of developing devices and artifacts able to monitor, measure, model and control environmental impact, including monitoring and managing energy generation from renewable sources.

Prominent environmental engineers

See also



This article uses material from the Wikipedia article "Environmental engineering", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Environmental Protection

Environment Ecology