powered by CADENAS

Social Share

Deckchair (2629 views - Interior Design)

A deckchair (or deck chair) is a folding chair, usually with a frame of treated wood or other material. The term now usually denotes a portable folding chair, with a single strip of fabric or vinyl forming the backrest and seat. It is meant for leisure, originally on the deck of an ocean liner or cruise ship. It is easily transportable and stackable, although some styles are notoriously difficult to fold and unfold. Different versions may have an extended seat, meant to be used as a leg rest, whose height may be adjustable; and may also have arm rests.
Go to Article

Explanation by Hotspot Model

Deckchair

Deckchair

Deckchair

Licensed under Creative Commons Attribution-Share Alike 3.0 (19:44, 20. Apr 2004 by Sannse (Diskussion / Beiträge) . . 600×799 (97.605 Bytes) (Deck chairs. Photo by sannse.).

A deckchair (or deck chair) is a folding chair, usually with a frame of treated wood or other material. The term now usually denotes a portable folding chair, with a single strip of fabric or vinyl forming the backrest and seat. It is meant for leisure, originally on the deck of an ocean liner or cruise ship. It is easily transportable and stackable, although some styles are notoriously difficult to fold and unfold. Different versions may have an extended seat, meant to be used as a leg rest, whose height may be adjustable; and may also have arm rests.

History and usage

In Northern Europe, the remains of folding chairs have been found dating back to the Bronze Age. Foldable chairs were also used in Ancient Egypt, Greece and Rome. During the Middle Ages, the folding chair was widely used as a liturgical furniture piece[citation needed].

In the United States, an early patent for a folding chair was by John Cham in 1855.[1] Folding wooden chairs with woven or cane seats and backs, of the type now known in the UK as "steamer chairs", began to be used on ocean liner decks from about the 1860s, and were known at the time as "deck chairs". It is unclear whether they were first made in the US or Britain.[2] In England, John Thomas Moore (1864-1929) took out a patent for adjustable and portable folding chairs in 1886, and started manufacturing them in Macclesfield.[3] Moore made two types: the Waverley, described as "the best ship or lawn tennis chair", and the Hygienic, which was a rocking chair "valuable for those with sluggish and constipated bowels".[4]

Early versions of the deck chair were made of two rectangular wooden frames hinged together, with a third rectangle to maintain it upright. A rectangular piece of canvas, of the type used in hammocks, was attached to two of the wooden rectangles to provide a seat and support. The use of a single broad strip of canvas, originally olive green in colour but later usually of brightly coloured stripes, has been credited to a British inventor named Atkins in the late 19th century,[4] although advertisements of 1882 for a similar design refer to it as "The Yankee Hammock Chair", implying an American origin. Other sources refer to it as the "Brighton beach chair" or "chaise transatlantique" ("chaise transat"). The term 'deck' chair was used in the novels of E. Nesbit in the 1880s, and passengers on P & O liners in the 1890s were encouraged to take their own on board.[2][5] The classic deckchair can only be locked in one position. Later, the strips of wood going toward the back were lengthened and equipped with supports so that there were several possible sitting positions. A removable footrest can also add to the comfort of the user.

Folding deckchairs became widely popular in the late 19th and early 20th centuries. During the golden age of ocean liner travel, the deckchairs upon ships' decks were sometimes reserved for particular passengers for whom crew would attach a paperboard name tag to the wicker seat-back. Such a tag is visible on an empty deckchair near the center in a famous 1912 photo showing survivors of the RMS Titanic disaster after rescue while they rest on the deck of RMS Carpathia.[6][7] The same system was in use aboard Carpathia two years later; a reservation tag is visible on the empty deckchair in the lower right of a 1914 photo. The deckchairs shown on some of those photographs are of the more solid "steamer chair" type, rather than the portable canvas-seated chairs. The Titanic carried 600 such wooden chairs;[3] six were known to survive, of which one was sold in 2001 for £35,000,[3] and another was put up for sale in 2012 with an expected price of at least £62,000.[8]

The hiring out of deckchairs, on an hourly or daily basis, became established in British seaside resorts, often for use on piers and promenades, in the early 20th century. They were also often used in large public parks such as Hyde Park, and for spectators at informal sporting events such as local cricket matches. With the widespread availability of lighter and even more portable forms of seating later in the century, the use of deckchairs declined.[5] In one of the largest English resorts, Blackpool, 68,000 deckchairs were rented out in 2003, at £1.50 a day, but tourism officers suggested that they should be phased out, except on the piers themselves, because they were a reminder of the era of "cloth caps", and had "had their time in the 50s and 60s".[9]

Sunlounger

A sunlounger is somewhat like a deckchair, and bed-like in nature. The rear surface can be tilted up to allow the user to sit up and read, or it can be reclined to a flat surface to allow sleeping in the horizontal position.

Usage in metaphor

To "rearrange the deck chairs" is a popular saying meaning that things have changed only apparently. The phrase, "rearrange the deck chairs on the Titanic" amplifies on it by implying that someone is overly concerned with unimportant minutiae during a crisis.[10]

Gallery

See also



This article uses material from the Wikipedia article "Deckchair", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Interior Design

3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art