powered by CADENAS

Social Share

Table tennis (6767 views - Sports List)

Table tennis, also known as ping pong, is a sport in which two or four players hit a lightweight ball back and forth across a table using a small bat. The game takes place on a hard table divided by a net. Except for the initial serve, the rules are generally as follows: players must allow a ball played toward them to bounce one time on their side of the table, and must return it so that it bounces on the opposite side at least once. A point is scored when a player fails to return the ball within the rules. Play is fast and demands quick reactions. Spinning the ball alters its trajectory and limits an opponent's options, giving the hitter a great advantage. Table tennis is governed by the worldwide organization International Table Tennis Federation (ITTF), founded in 1926. ITTF currently includes 226 member associations. The table tennis official rules are specified in the ITTF handbook. Table tennis has been an Olympic sport since 1988, with several event categories. From 1988 until 2004, these were men's singles, women's singles, men's doubles and women's doubles. Since 2008, a team event has been played instead of the doubles.
Go to Article

Explanation by Hotspot Model

Table tennis

Table tennis

Table tennis

Licensed under Creative Commons Attribution-Share Alike 3.0 (Pierre-Yves Beaudouin / Wikimedia Commons).

Table tennis
Table tennis at the highest level
Highest governing body ITTF
First played 1880s Victorian England[1][2]
Characteristics
Contact No
Team members Single or doubles
Type Racquet sport, indoor
Equipment Poly, 40 mm (1.57 in),
2.7 g (0.095 oz)
Presence
Olympic since 1988
Paralympic since inaugural 1960 Summer Paralympics

Table tennis, also known as ping pong, is a sport in which two or four players hit a lightweight ball back and forth across a table using a small bat. The game takes place on a hard table divided by a net. Except for the initial serve, the rules are generally as follows: players must allow a ball played toward them to bounce one time on their side of the table, and must return it so that it bounces on the opposite side at least once. A point is scored when a player fails to return the ball within the rules. Play is fast and demands quick reactions. Spinning the ball alters its trajectory and limits an opponent's options, giving the hitter a great advantage.

Table tennis is governed by the worldwide organization International Table Tennis Federation (ITTF), founded in 1926. ITTF currently includes 226 member associations.[3] The table tennis official rules are specified in the ITTF handbook.[4] Table tennis has been an Olympic sport since 1988,[5] with several event categories. From 1988 until 2004, these were men's singles, women's singles, men's doubles and women's doubles. Since 2008, a team event has been played instead of the doubles.

History

The sport originated in Victorian England, where it was played among the upper-class as an after-dinner parlour game.[1][2] It has been suggested that makeshift versions of the game were developed by British military officers in India in around 1860s or 1870s, who brought it back with them.[6] A row of books stood up along the center of the table as a net, two more books served as rackets and were used to continuously hit a golf-ball.[7][8]

The name "ping-pong" was in wide use before British manufacturer J. Jaques & Son Ltd trademarked it in 1901. The name "ping-pong" then came to describe the game played using the rather expensive Jaques's equipment, with other manufacturers calling it table tennis. A similar situation arose in the United States, where Jaques sold the rights to the "ping-pong" name to Parker Brothers. Parker Brothers then enforced its trademark for the term in the 1920s making the various associations change their names to "table tennis" instead of the more common, but trademarked, term.[9]

The next major innovation was by James W. Gibb, a British enthusiast of table tennis, who discovered novelty celluloid balls on a trip to the US in 1901 and found them to be ideal for the game. This was followed by E.C. Goode who, in 1901, invented the modern version of the racket by fixing a sheet of pimpled, or stippled, rubber to the wooden blade. Table tennis was growing in popularity by 1901 to the extent that tournaments were being organized, books being written on the subject,[7] and an unofficial world championship was held in 1902.

In 1921, the Table Tennis Association was founded in Britain, and the International Table Tennis Federation (ITTF) followed in 1926.[1][10] London hosted the first official World Championships in 1926. In 1933, the United States Table Tennis Association, now called USA Table Tennis, was formed.[1][11]

In the 1930s, Edgar Snow commented in Red Star Over China that the Communist forces in the Chinese Civil War had a "passion for the English game of table tennis" which he found "bizarre".[12] On the other hand, the popularity of the sport waned in 1930s Soviet Union, partly because of the promotion of team and military sports, and partly because of a theory that the game had adverse health effects.[13]

In the 1950s, paddles that used a rubber sheet combined with an underlying sponge layer changed the game dramatically,[1] introducing greater spin and speed.[14] These were introduced to Britain by sports goods manufacturer S.W. Hancock Ltd. The use of speed glue increased the spin and speed even further, resulting in changes to the equipment to "slow the game down". Table tennis was introduced as an Olympic sport at the Olympics in 1988.[15]

Rule changes

After the 2000 Olympics in Sydney, the ITTF instituted several rule changes that were aimed at making table tennis more viable as a televised spectator sport.[16][17] First, the older 38 mm (1.50 in) balls were officially replaced by 40 mm (1.57 in) balls in October 2000.[7][18] This increased the ball's air resistance and effectively slowed down the game. By that time, players had begun increasing the thickness of the fast sponge layer on their paddles, which made the game excessively fast and difficult to watch on television. A few months later, the ITTF changed from a 21-point to an 11-point scoring system (and the serve rotation was reduced from five points to two), effective in September 2001.[7] This was intended to make games more fast-paced and exciting. The ITTF also changed the rules on service to prevent a player from hiding the ball during service, in order to increase the average length of rallies and to reduce the server's advantage, effective in 2002.[19] For the opponent to have time to realize a serve is taking place, the ball must be tossed a minimum of 16 cm in the air. The ITTF states that all events after July 2014 are played with a new poly material ball.[20] [21]

Equipment

Ball

The international rules specify that the game is played with a sphere having a mass of 2.7 grams (0.095 oz) and a diameter of 40 millimetres (1.57 in).[22] The rules say that the ball shall bounce up 24–26 cm (9.4–10.2 in) when dropped from a height of 30.5 cm (12.0 in) onto a standard steel block thereby having a coefficient of restitution of 0.89 to 0.92. The ball is made of celluloid plastic as of 2015, colored white or orange, with a matte finish. The choice of ball color is made according to the table color and its surroundings. For example, a white ball is easier to see on a green or blue table than it is on a grey table. Manufacturers often indicate the quality of the ball with a star rating system, usually from one to three, three being the highest grade. As this system is not standard across manufacturers, the only way a ball may be used in official competition is upon ITTF approval[22] (the ITTF approval can be seen printed on the ball).

The 40 mm ball was introduced after the 2000 Summer Olympics.[18] However, this created some controversy at the time as the Chinese National Team argued that this was merely to give non-Chinese players a better chance of winning since the new type of ball has a slower speed (a 40 mm table tennis ball is slower and spins less than the original 38 mm one, and at that time, most Chinese players were playing with fast attack and smashes). China won all four Olympic gold medals and three silvers in 2000, and have continued to dominate.[citation needed]

Table

The table is 2.74 m (9.0 ft) long, 1.525 m (5.0 ft) wide, and 76 cm (2.5 ft) high with any continuous material so long as the table yields a uniform bounce of about 23 cm (9.1 in) when a standard ball is dropped onto it from a height of 30 cm (11.8 in), or about 77%.[23][24] The table or playing surface is uniformly dark coloured and matte, divided into two halves by a net at 15.25 cm (6.0 in) in height. The ITTF approves only wooden tables or their derivates. Concrete tables with a steel net or a solid concrete partition are sometimes available in outside public spaces, such as parks.[25]

Paddle/racket

Players are equipped with a laminated wooden racket covered with rubber on one or two sides depending on the grip of the player. The ITTF uses the term "racket",[26] though "bat" is common in Britain, and "paddle" in the U.S. and Canada.

The wooden portion of the racket, often referred to as the "blade", commonly features anywhere between one and seven plies of wood, though cork, glass fiber, carbon fiber, aluminum fiber, and Kevlar are sometimes used. According to the ITTF regulations, at least 85% of the blade by thickness shall be of natural wood.[27] Common wood types include balsa, limba, and cypress or "hinoki", which is popular in Japan. The average size of the blade is about 17 centimetres (6.7 in) long and 15 centimetres (5.9 in) wide. Although the official restrictions only focus on the flatness and rigidness of the blade itself, these dimensions are optimal for most play styles.

Table tennis regulations allow different surfaces on each side of the racket.[28] Various types of surfaces provide various levels of spin or speed, and in some cases they nullify spin. For example, a player may have a rubber that provides much spin on one side of their racket, and one that provides no spin on the other. By flipping the racket in play, different types of returns are possible. To help a player distinguish between the rubber used by his opposing player, international rules specify that one side must be red while the other side must be black.[27] The player has the right to inspect his opponent's racket before a match to see the type of rubber used and what colour it is. Despite high speed play and rapid exchanges, a player can see clearly what side of the racket was used to hit the ball. Current rules state that, unless damaged in play, the racket cannot be exchanged for another racket at any time during a match.[29]

Gameplay

Starting a game

According to ITTF rule 2.13.1, the first service is decided by lot,[30] normally a coin toss.[31] It is also common for one player (or the umpire/scorer) to hide the ball in one or the other hand, usually hidden under the table, allowing the other player to guess which hand the ball is in. The correct or incorrect guess gives the "winner" the option to choose to serve, receive, or to choose which side of the table to use. (A common but non-sanctioned method is for the players to play the ball back and forth three times and then play out the point. This is commonly referred to as "serve to play", "rally to serve", "play for serve", or "volley for serve".)

Service and return

In game play, the player serving the ball commences a play.[32] The server first stands with the ball held on the open palm of the hand not carrying the paddle, called the freehand, and tosses the ball directly upward without spin, at least 16 cm (6.3 in) high.[33] The server strikes the ball with the racket on the ball's descent so that it touches first his court and then touches directly the receiver's court without touching the net assembly. In casual games, many players do not toss the ball upward; however, this is technically illegal and can give the serving player an unfair advantage.

The ball must remain behind the endline and above the upper surface of the table, known as the playing surface, at all times during the service. The server cannot use his/her body or clothing to obstruct sight of the ball; the opponent and the umpire must have a clear view of the ball at all times. If the umpire is doubtful of the legality of a service they may first interrupt play and give a warning to the server. If the serve is a clear failure or is doubted again by the umpire after the warning, the receiver scores a point.

If the service is "good", then the receiver must make a "good" return by hitting the ball back before it bounces a second time on receiver's side of the table so that the ball passes the net and touches the opponent's court, either directly or after touching the net assembly.[34] Thereafter, the server and receiver must alternately make a return until the rally is over. Returning the serve is one of the most difficult parts of the game, as the server's first move is often the least predictable and thus most advantageous shot due to the numerous spin and speed choices at his or her disposal.

Let

A Let is a rally of which the result is not scored, and is called in the following circumstances:[35]

  • The ball touches the net in service (service), provided the service is otherwise correct or the ball is obstructed by the player on the receiving side. Obstruction means a player touches the ball when it is above or traveling towards the playing surface, not having touched the player's court since last being struck by the player.
  • When the player on the receiving side is not ready and the service is delivered.
  • Player's failure to make a service or a return or to comply with the Laws is due to a disturbance outside the control of the player.
  • Play is interrupted by the umpire or assistant umpire.

A let is also called foul service, if the ball hits the server's side of the table, if the ball does not pass further than the edge and if the ball hits the table edge and hits the net.

Scoring

A point is scored by the player for any of several results of the rally:[36]

  • The opponent fails to make a correct service or return.
  • After making a service or a return, the ball touches anything other than the net assembly before being struck by the opponent.
  • The ball passes over the player's court or beyond his end line without touching his court, after being struck by the opponent.
  • The opponent obstructs the ball.
  • The opponent strikes the ball twice successively. Note that the hand that is holding the racket counts as part of the racket and that making a good return off one's hand or fingers is allowed. It is not a fault if the ball accidentally hits one's hand or fingers and then subsequently hits the racket.
  • The opponent strikes the ball with a side of the racket blade whose surface is not covered with rubber.
  • The opponent moves the playing surface or touches the net assembly.
  • The opponent's free hand touches the playing surface.
  • As a receiver under the expedite system, completing 13 returns in a rally.[37]
  • The opponent that has been warned by the umpire commits a second offense in the same individual match or team match. If the third offence happens, 2 points will be given to the player.[38] If the individual match or the team match has not ended, any unused penalty points can be transferred to the next game of that match.[31]

A game shall be won by the player first scoring 11 points unless both players score 10 points, when the game shall be won by the first player subsequently gaining a lead of 2 points. A match shall consist of the best of any odd number of games.[39] In competition play, matches are typically best of five or seven games.

Alternation of services and ends

Service alternates between opponents every two points (regardless of winner of the rally) until the end of the game, unless both players score ten points or the expedite system is operated, when the sequences of serving and receiving stay the same but each player serves for only one point in turn (Deuce).[40] The player serving first in a game receives first in the next game of the match.

After each game, players switch sides of the table. In the last possible game of a match, for example the seventh game in a best of seven matches, players change ends when the first player scores five points, regardless of whose turn it is to serve. Service is subject to change on game point of the match. Upon the possible last point of the match, the player with the lesser score serves. If the sequence of serving and receiving is out of turn or the ends are not changed, points scored in the wrong situation are still calculated and the game shall be resumed with the order at the score that has been reached.

Doubles game

In addition to games between individual players, pairs may also play table tennis. Singles and doubles are both played in international competition, including the Olympic Games since 1988 and the Commonwealth Games since 2002.[41] In 2005, the ITTF announced that doubles table tennis only was featured as a part of team events in the 2008 Olympics.

In doubles, all the rules of single play are applied except for the following.

Service

A line painted along the long axis of the table to create doubles courts bisects the table. This line's only purpose is to facilitate the doubles service rule, which is that service must originate from the right hand "box" in such a way that the first bounce of the serve bounces once in said right hand box and then must bounce at least once in the opponent side's right hand box (far left box for server), or the receiving pair score a point.[33]

Order of play, serving and receiving

  1. Players must hit the ball in turn. For example, if A is paired with B, X is paired with Y, A is the server and X is the receiver. The order of play shall be A→X→B→Y. The rally proceeds this way until one side fails to make a legal return and the other side scores.[42]
  2. At each change of service, the previous receiver shall become the server and the partner of the previous server shall become the receiver. For example, if the previous order of play is A→X→B→Y, the order becomes X→B→Y→A after the change of service.[40]
  3. In the second or the latter games of a match, the game begins in reverse order of play. For example, if the order of play is A→X→B→Y at beginning of the first game, the order begins with X→A→Y→B or Y→B→X→A in the second game depending on either X or Y being chosen as the first server of the game. That means the first receiver of the game is the player who served to the first server of the game in the preceding game. In each game of a doubles match, the pair having the right to serve first shall choose which of them will do so. The receiving pair, however, can only choose in the first game of the match.
  4. When a pair reaches 5 points in the final game, the pairs must switch ends of the table and change the receiver to reverse the order of play. For example, when the last order of play before a pair score 5 points in the final game is A→X→B→Y, the order after change shall be A→Y→B→X if A still has the second serve. Otherwise, X is the next server and the order becomes X→A→Y→B.

Expedite system

If a game is unfinished after 10 minutes' play and fewer than 18 points have been scored, the expedite system is initiated.[37] The umpire interrupts the game, and the game resumes with players serving for one point in turn. If the expedite system is introduced while the ball is not in play, the previous receiver shall serve first. Under the expedite system, the server must win the point before the opponent makes 13 consecutive returns or the point goes to the opponent. The system can also be initiated at any time at the request of both players or pairs. Once introduced, the expedite system remains in force until the end of the match. A rule to shorten the time of a match, it is mainly seen in defensive players' games.

Grips

Though table tennis players grip their rackets in various ways, their grips can be classified into two major families of styles, penhold and shakehand.[43] The rules of table tennis do not prescribe the manner in which one must grip the racket, and numerous grips are employed.

Penhold

The penhold grip is so-named because one grips the racket similarly to the way one holds a writing instrument.[44] The style of play among penhold players can vary greatly from player to player. The most popular style, usually referred to as the Chinese penhold style, involves curling the middle, ring, and fourth finger on the back of the blade with the three fingers always touching one another.[44] Chinese penholders favour a round racket head, for a more over-the-table style of play. In contrast, another style, sometimes referred to as the Japanese/Korean penhold grip, involves splaying those three fingers out across the back of the racket, usually with all three fingers touching the back of the racket, rather than stacked upon one another.[44] Sometimes a combination of the two styles occurs, wherein the middle, ring and fourth fingers are straight, but still stacked, or where all fingers may be touching the back of the racket, but are also in contact with one another. Japanese/Korean penholders will often use a square-headed racket for an away-from-the-table style of play. Traditionally these square-headed rackets feature a block of cork on top of the handle, as well as a thin layer of cork on the back of the racket, for increased grip and comfort. Penhold styles are popular among players originating from East Asian regions such as China, Taiwan, Japan, and South Korea.

Traditionally, penhold players use only one side of the racket to hit the ball during normal play, and the side which is in contact with the last three fingers is generally not used. This configuration is sometimes referred to as "traditional penhold" and is more commonly found in square-headed racket styles. However, the Chinese developed a technique in the 1990s in which a penholder uses both sides of the racket to hit the ball, where the player produces a backhand stroke (most often topspin) known as a reverse penhold backhand by turning the traditional side of the racket to face one's self, and striking the ball with the opposite side of the racket. This stroke has greatly improved and strengthened the penhold style both physically and psychologically, as it eliminates the strategic weakness of the traditional penhold backhand.

Shakehand grip
Forehand
Backhand

Shakehand

The shakehand grip is so-named because the racket is grasped as if one is performing a handshake.[45] Though it is sometimes referred to as the "tennis" or "Western" grip, it bears no relation to the Western tennis grip, which was popularized on the West Coast of the United States in which the racket is rotated 90°, and played with the wrist turned so that on impact the knuckles face the target. In table tennis, "Western" refers to Western nations, for this is the grip that players native to Europe and the Americas have almost exclusively employed.

The shakehand grip’s simplicity and versatility, coupled with the acceptance among top-level Chinese trainers that the European style of play should be emulated and trained against, has established it as a common grip even in China.[46] Many world class European and Asian players currently use the shakehand grip, and it is generally accepted that shakehands is easier to learn than penholder, allowing a broader range of playing styles both offensive and defensive.[47]

Seemiller

The Seemiller grip is named after the American table tennis champion Danny Seemiller, who used it. It is achieved by placing your thumb and index finger on either side of the bottom of the racquet head and holding the handle with the rest of your fingers. Since only one side of the racquet is used to hit the ball, two contrasting rubber types can be applied to the blade, offering the advantage of "twiddling" the racket to fool the opponent. Seemiller paired inverted rubber with anti-spin rubber; many players today combine inverted and long-pipped rubber. The grip is considered exceptional for blocking, especially on the backhand side, and for forehand loops of backspin balls.[48] The Seemiller grip's popularity reached its apex in 1985 when four (Danny Seemiller, Ricky Seemiller, Eric Boggan and Brian Masters) of the United States' five participants in the World Championships used it.[48]

Types of strokes

Table tennis strokes generally break down into offensive and defensive categories.

Offensive strokes

Hit

A direct hit on the ball propelling it forward back to the opponent. This stroke differs from speed drives in other racket sports like tennis because the racket is primarily perpendicular to the direction of the stroke and most of the energy applied to the ball results in speed rather than spin, creating a shot that does not arc much, but is fast enough that it can be difficult to return. A speed drive is used mostly for keeping the ball in play, applying pressure on the opponent, and potentially opening up an opportunity for a more powerful attack.

Loop

Perfected during the 1960s,[1] the loop is essentially the reverse of the speed drive. The racket is much more parallel to the direction of the stroke ("closed") and the racket thus grazes the ball, resulting in a large amount of topspin. A good loop drive will arc quite a bit, and once striking the opponent's side of the table will jump forward, much like a kick serve in tennis.

Counter-hit

The counter-hit is usually a counterattack against drives, normally high loop drives. The racket is held closed and near to the ball, which is hit with a short movement "off the bounce" (immediately after hitting the table) so that the ball travels faster to the other side. A well-timed, accurate counter-drive can be as effective as a smash.

Flip

When a player tries to attack a ball that has not bounced beyond the edge of the table, the player does not have the room to wind up in a backswing. The ball may still be attacked, however, and the resulting shot is called a flip because the backswing is compressed into a quick wrist action. A flip is not a single stroke and can resemble either a loop drive or a loop in its characteristics. What identifies the stroke is that the backswing is compressed into a short wrist flick.

Smash

The offensive trump card is the smash. A player will typically execute a smash when his or her opponent has returned a ball that bounces too high or too close to the net. Smashing consists of using a large backswing and rapid acceleration to impart as much speed on the ball as possible. The goal of a smash is to get the ball to move so quickly that the opponent simply cannot return it. Because the ball speed is the main aim of this shot, often the spin on the ball is something other than topspin. Sidespin can be used effectively with a smash to alter the ball's trajectory significantly, although most intermediate players will smash the ball with little or no spin. An offensive table tennis player will think of a rally as a build-up to a winning smash.

Defensive strokes

Push

The push (or "slice" in Asia) is usually used for keeping the point alive and creating offensive opportunities. A push resembles a tennis slice: the racket cuts underneath the ball, imparting backspin and causing the ball to float slowly to the other side of the table. While not obvious, a push can be difficult to attack because the backspin on the ball causes it to drop toward the table upon striking the opponent's racket. In order to attack a push, a player must usually loop the ball back over the net. Often, the best option for beginners is to simply push the ball back again, resulting in pushing rallies. Against good players, it may be the worst option because the opponent will counter with a loop, putting the first player in a defensive position. Another response to pushing is flipping the ball when it is close to the net. Pushing can have advantages in some circumstances, such as when the opponent makes easy mistakes.

Chop

A chop is the defensive, backspin counterpart to the offensive loop drive.[49] A chop is essentially a bigger, heavier push, taken well back from the table. The racket face points primarily horizontally, perhaps a little bit upward, and the direction of the stroke is straight down. The object of a defensive chop is to match the topspin of the opponent's shot with backspin. A good chop will float nearly horizontally back to the table, in some cases having so much backspin that the ball actually rises. Such a chop can be extremely difficult to return due to its enormous amount of backspin. Some defensive players can also impart no-spin or sidespin variations of the chop.

Block

The block is a simple shot, but nonetheless can be devastating against an attacking opponent. A block is executed by simply placing the racket in front of the ball right after the ball bounces; thus, the ball rebounds back toward the opponent with nearly as much energy as it came in with. This is not as easy as it sounds, because the ball's spin, speed, and location all influence the correct angle of a block. It is very possible for an opponent to execute a perfect loop, drive, or smash, only to have the blocked shot come back at him just as fast. Due to the power involved in offensive strokes, often an opponent simply cannot recover quickly enough, and will be unable to return the blocked shot. Blocks almost always produce the same spin as was received, many times topspin. Depending on the spin of the ball, the block may be returned to an unexpected side of the table. This may come to your advantage, as the opponent may not expect this.

Lob

The defensive lob is possibly the most impressive shot, since it propels the ball about five metres in height, only to land on the opponent's side of the table with great amounts of spin.[50] To execute, a defensive player first backs-off the table 4–6 meters; then, the stroke itself consists of lifting the ball to an enormous height before it falls back to the opponent's side of the table. A lob is inherently a creative shot, and can have nearly any kind of spin. Top-quality players use this to their advantage in order to control the spin of the ball. For instance, though the opponent may smash the ball hard and fast, a good defensive lob could be more difficult to return due to the unpredictability and heavy amounts of the spin on the ball.[50] Thus, though backed off the table by tens of feet and running to reach the ball, a good defensive player can still win the point using good lobs. However, at the professional level, lobbers will lose the point most of the time, so the lob is not used unless it is really necessary.

Effects of spin

Adding spin onto the ball causes major changes in table tennis gameplay. Although nearly every stroke or serve creates some kind of spin, understanding the individual types of spin allows players to defend against and use different spins effectively.[51]

Backspin

Backspin is where the bottom half of the ball is rotating away from the player, and is imparted by striking the base of the ball with a downward movement.[51] At the professional level, backspin is usually used defensively in order to keep the ball low.[52] Backspin is commonly employed in service because it is harder to produce an offensive return, though at the professional level most people serve sidespin with either backspin or topspin. Due to the initial lift of the ball, there is a limit on how much speed with which one can hit the ball without missing the opponent's side of the table. However, backspin also makes it harder for the opponent to return the ball with great speed because of the required angular precision of the return. Alterations are frequently made to regulations regarding equipment in an effort to maintain a balance between defensive and offensive spin choices.[citation needed] It is actually possible to smash with backspin offensively, but only on high balls that are close to the net.

Topspin

The topspin stroke has a smaller influence on the first part of the ball-curve. Like the backspin stroke, however, the axis of spin remains roughly perpendicular to the trajectory of the ball thus allowing for the Magnus effect to dictate the subsequent curvature. After the apex of the curve, the ball dips downwards as it approaches the opposing side, before bouncing. On the bounce, the topspin will accelerate the ball, much in the same way that a wheel which is already spinning would accelerate upon making contact with the ground. When the opponent attempts to return the ball, the topspin causes the ball to jump upwards and the opponent is forced to compensate for the topspin by adjusting the angle of his or her racket. This is known as "closing the racket". The speed limitation of the topspin stroke is minor compared to the backspin stroke. This stroke is the predominant technique used in professional competition because it gives the opponent less time to respond. In table tennis topspin is regarded as an offensive technique due to increased ball speed, lower bio-mechanical efficiency and the pressure that it puts on the opponent by reducing reaction time. (It is possible to play defensive topspin-lobs from far behind the table, but only highly skilled players use this stroke with any tactical efficiency.) Topspin is the least common type of spin to be found in service at the professional level, simply because it is much easier to attack a top-spin ball that is not moving at high speed.

Sidespin

This type of spin is predominantly employed during service, wherein the contact angle of the racket can be more easily varied. Unlike the two aforementioned techniques, sidespin causes the ball to spin on an axis which is vertical, rather than horizontal. The axis of rotation is still roughly perpendicular to the trajectory of the ball. In this circumstance, the Magnus effect will still dictate the curvature of the ball to some degree. Another difference is that unlike backspin and topspin, sidespin will have relatively very little effect on the bounce of the ball, much in the same way that a spinning top would not travel left or right if its axis of rotation were exactly vertical. This makes sidespin a useful weapon in service, because it is less easily recognized when bouncing, and the ball "loses" less spin on the bounce. Sidespin can also be employed in offensive rally strokes, often from a greater distance, as an adjunct to topspin or backspin. This stroke is sometimes referred to as a "hook". The hook can even be used in some extreme cases to circumvent the net when away from the table.

Corkspin

Players employ this type of spin almost exclusively when serving, but at the professional level, it is also used from time to time in the lob. Unlike any of the techniques mentioned above, corkspin (or "drill-spin") has the axis of spin relatively parallel to the ball's trajectory, so that the Magnus effect has little or no effect on the trajectory of a cork-spun ball: upon bouncing, the ball will dart right or left (according to the direction of the spin), severely complicating the return. In theory this type of spin produces the most obnoxious effects, but it is less strategically practical than sidespin or backspin, because of the limitations that it imposes upon the opponent during their return. Aside from the initial direction change when bouncing, unless it goes out of reach, the opponent can counter with either topspin or backspin. A backspin stroke is similar in the fact that the corkspin stroke has a lower maximum velocity, simply due to the contact angle of the racket when producing the stroke. To impart a spin on the ball which is parallel to its trajectory, the racket must be swung more or less perpendicular to the trajectory of the ball, greatly limiting the forward momentum that the racket transfers to the ball. Corkspin is almost always mixed with another variety of spin, since alone, it is not only less effective but also harder to produce.

Competition

Competitive table tennis is popular in East Asia and Europe, and has been[vague] gaining attention in the United States.[53] The most important international competitions are the World Table Tennis Championships, the Table Tennis World Cup, the Olympics and the ITTF World Tour]]. Continental competitions include the following:

Chinese players have won 60% of the men's World Championships since 1959;[54] in the women's competition for the Corbillin Cup, Chinese players have won all but three of the World Championships since 1971.[55] Other strong teams come from East Asia and European countries, including Austria, Belarus, Germany, Hong Kong, Portugal, Japan, South Korea, Singapore, Sweden, and Taiwan.[56]

There are also professional competitions at the clubs level; the respective leagues of Austria, Belgium, China (specifically, the China Table Tennis Super League), France, Germany and Russia are examples of the highest level. There are also some important international club teams competitions such as the European Champions League and its former competitor,[vague] the European Club Cup, where the top club teams from European countries compete.

Notable players

An official hall of fame exists at the ITTF Museum.[57] A Grand Slam is earned by a player who wins singles crowns at Olympic Games, World Championships, and World Cup.[58] Jan-Ove Waldner of Sweden first completed the grand slam at 1992 Olympic Games. Deng Yaping of China is the first female recorded at the inaugural Women's World Cup in 1996.

Name Gender Nationality Times won
Olympics World Championships World Cup
Jan-Ove Waldner Male SWE 1 (1992) 2 (1989, 1997) 1 (1990) [59]
Deng Yaping Female China 2 (1992, 1996) 3 (1991, 1995, 1997) 1 (1996) [60]
Liu Guoliang Male China 1 (1996) 1 (1999) 1 (1996) [61]
Kong Linghui Male China 1 (2000) 1 (1995) 1 (1995) [62]
Wang Nan Female China 1 (2000) 3 (1999, 2001, 2003) 4 (1997, 1998, 2003, 2007) [63]
Zhang Yining Female China 2 (2004, 2008) 2 (2005, 2009) 4 (2001, 2002, 2004, 2005) [64]
Zhang Jike Male China 1 (2012) 2 (2011, 2013) 2 (2011, 2014) [65]
Li Xiaoxia Female China 1 (2012) 1 (2013) 1 (2008) [66]
Ding Ning Female China 1 (2016) 3 (2011, 2015, 2017) 2 (2011, 2014) [67]
Ma Long Male China 1 (2016) 2 (2015, 2017) 2 (2012, 2015)

Jean-Philippe Gatien (France) and Wang Hao (China) won both the World Championships and the World Cup, but lost in the gold medal matches at the Olympics. Jörgen Persson (Sweden) also won the titles except the Olympic Games. Persson is one of the three table tennis players to have competed at seven Olympic Games. Ma Lin (China) won both the Olympic gold and the World Cup, but lost (three times, in 1999, 2005, and 2007) in the finals of the World Championships.

Governance

Founded in 1926, the International Table Tennis Federation (ITTF) is the worldwide governing body for table tennis, which maintains an international ranking system in addition to organizing events like the World Table Tennis Championships.[11] In 2007, the governance for table tennis for persons with a disability was transferred from the International Paralympic Committee to the ITTF.[68]

On many continents, there is a governing body responsible for table tennis on that continent. For example, the European Table Tennis Union (ETTU) is the governing body responsible for table tennis in Europe.[69] There are also national bodies and other local authorities responsible for the sport, such as USA Table Tennis (USATT), which is the national governing body for table tennis in the United States.[11]

See also



This article uses material from the Wikipedia article "Table tennis", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Sports List

Air sports
• Aerobatics
• Air racing
• Cluster ballooning
• Hopper ballooning

Wingsuit flying
• Gliding
• Hang gliding
• Powered hang glider
• Human powered aircraft
• Model aircraft
• Parachuting
• Banzai skydiving
• BASE jumping
• Skydiving
• Skysurfing
• Wingsuit flying
• Paragliding
• Powered paragliding
• Paramotoring
• Ultralight aviation

Archery
• Field archery
• Flight archery
• Gungdo
• Indoor archery
• Kyūdō
• Popinjay
• Target archery

Ball-over-net games
• Badminton
• Ball badminton
• Biribol
• Bossaball
• Fistball
• Footbag net
• Football tennis
• Footvolley
• Hooverball
• Jianzi
• Padel
• Peteca
• Pickleball
• Platform tennis
• Sepak takraw
• Sipa
• Throwball
• Volleyball
• Beach volleyball
• Water volleyball
• Paralympic volleyball
• Wallyball
• Ringo


Basketball family
• Basketball
• Beach basketball
• Deaf basketball
• Streetball
• Water basketball
• Wheelchair basketball
• Cestoball
• Korfball
• Netball
• Fastnet
• Indoor netball
• Ringball
• Slamball

Bat-and-ball (safe haven)
• Baseball
• Softball
• Slow pitch
• Fast-pitch softball
• 16-inch softball
• Bat and trap
• British baseball – four posts
• Brännboll – four bases
• Corkball – four bases (no base-running)
• Cricket – two creases
• Indoor cricket
• Limited overs cricket
• One Day International
• Test cricket
• Twenty20
• Danish longball
• Kickball
• Kilikiti
• Lapta – two salos (bases)
• The Massachusetts Game – four bases
• Matball
• Oina
• Old cat – variable
• Over-the-line – qv
• Palant
• Pesäpallo – four bases
• Punchball
• Rounders – four bases or posts
• Scrub baseball – four bases (not a team game per se)
• Stickball – variable
• Stool ball – two stools
• Tee-ball
• Town ball – variable
• Vigoro – two wickets
• Wireball
• Wiffleball

Baton twirling
• Baton twirling

Acro sports
• Ballet
• Dancing
• Cheerleading
• Gymnastics

Performance sports
• Drum corps
• Marching band

Board sports

• Skateboarding
• Scootering
• Casterboarding
• Freeboard (skateboard)
• Longboarding
• Streetboarding
• Skysurfing
• Streetluge
• Snowboarding
• Mountainboarding
• Sandboarding
• Snowkiting
• Surfing
• Wakesurfing
• Bodyboarding
• Riverboarding
• Skimboarding
• Windsurfing
• Wakeboarding
• Kneeboarding
• Paddleboarding

Catch games
• Dodgeball
• Ga-ga
• Keep away
• Kin-Ball
• Newcomb ball
• Quidditch
• Rundown (a.k.a. Pickle)
• Yukigassen

Climbing

• Abseiling
• Aid climbing
• Ice climbing
• Mixed climbing
• Mountaineering
• Rock climbing
• Bouldering
• Deep-water soloing
• Sport climbing
• Traditional climbing
• Other
• Canyoning (Canyoneering)
• Coasteering
• Hiking
• Rope climbing
• Pole climbing

Cycling

• Artistic cycling
• BMX
• Cyclo-cross
• Cross-country mountain biking
• Cycle polo
• Cycle speedway
• Downhill mountain biking
• Dirt jumping
• Enduro mountain biking
• Freestyle BMX
• Hardcourt Bike Polo
• Road bicycle racing
• Track cycling
• Underwater cycling

Skibob
• Skibobbing

Unicycle

• Mountain unicycling
• Unicycling
• Unicycle basketball
• Unicycle hockey
• Unicycle trials
Combat sports: wrestling and martial arts
• Aiki-jūjutsu
• Aikido
• Jujutsu
• Judo
• Brazilian jiu-jitsu
• Sambo (martial art)
• Sumo
• Wrestling
• Amateur wrestling
• Greco-Roman wrestling
• Freestyle wrestling
• Folk wrestling
• Boli Khela
• Collar-and-elbow
• Cornish wrestling
• Dumog
• Glima
• Gouren
• Kurash
• Lancashire wrestling
• Catch wrestling
• Malla-yuddha
• Mongolian wrestling
• Pehlwani
• Professional wrestling
• Schwingen
• Shuai jiao
• Ssireum
• Varzesh-e Pahlavani
• Yağlı Güreş
• Greek wrestling

Striking

• Choi Kwang-Do
• Cockfighting
• Boxing
• Bokator
• Capoeira
• Fujian White Crane
• Karate
• Kenpō
• Kickboxing
• Lethwei
• Muay Thai
• Pradal serey
• Sanshou
• Savate
• Shaolin Kung Fu
• Sikaran
• Silat
• Subak
• Taekkyeon
• Taekwondo
• Taidō
• Tang Soo Do
• Wing Chun
• Zui quan

Mixed or hybrid
• Baguazhang
• Bando
• Bartitsu
• Bujinkan
• Hapkido
• Hwa Rang Do
• Jeet Kune Do
• Kajukenbo
• Kalaripayattu
• Krav Maga
• Kuk Sool Won
• Marine Corps Martial Arts Program
• Mixed martial arts
• Northern Praying Mantis
• Ninjutsu
• Pankration
• Pencak Silat
• Sanshou
• Shidōkan Karate
• Shōrin-ryū Shidōkan
• Shoot boxing
• Shootfighting
• Shorinji Kempo
• Systema
• T'ai chi ch'uan
• Vajra-mushti
• Vale tudo
• Vovinam
• Xing Yi Quan
• Zen Bu Kan Kempo

Weapons
• Axe throwing
• Battōjutsu
• Boffer fighting
• Eskrima
• Egyptian stick fencing
• Fencing
• Gatka
• Hojōjutsu
• Iaidō
• Iaijutsu
• Jōdō
• Jogo do pau
• Jūkendō
• Jittejutsu
• Kendo
• Kenjutsu
• Krabi–krabong
• Kung fu
• Kyūdō
• Kyūjutsu
• Modern Arnis
• Naginatajutsu
• Nguni stick-fighting
• Okinawan kobudō
• Shurikenjutsu
• Silambam
• Sōjutsu
• Sword fighting
• Wushu
• Kumdo
• Wing Chun


Skirmish
• Airsoft
• Laser tag
• Paintball


Cue sports
• Carom billiards
• Three-cushion
• Five-pins
• Balkline and straight rail
• Cushion caroms
• Four-ball (yotsudama)
• Artistic billiards
• Novuss (and cued forms of carrom)
• Pocket billiards (pool)
• Eight-ball
• Blackball (a.k.a. British eight-ball pool)
• Nine-ball
• Straight pool (14.1 continuous)
• One-pocket
• Three-ball
• Seven-ball
• Ten-ball
• Rotation
• Baseball pocket billiards
• Cribbage (pool)
• Bank pool
• Artistic pool
• Trick shot competition
• Speed pool
• Bowlliards
• Chicago
• Kelly pool
• Cutthroat
• Killer
• Russian pyramid
• Snooker
• Sinuca brasileira
• Six-red snooker
• Snooker plus
• Hybrid carom–pocket games
• English billiards
• Bottle pool
• Cowboy
• Obstacle variations
• Bagatelle
• Bar billiards
• Bumper pool
• Table Sports
• Foosball


Equine sports
• Buzkashi
• Barrel racing
• Campdrafting
• Cirit
• Charreada
• Chilean rodeo
• Cross country
• Cutting
• Dressage
• Endurance riding
• English pleasure
• Equitation
• Eventing
• Equestrian vaulting
• Gymkhana
• Harness racing
• Horse racing
• Horseball
• Hunter
• Hunter-jumpers
• Jousting
• Pato
• Reining
• Rodeo
• Show jumping
• Steeplechase
• Team penning
• Tent pegging
• Western pleasure


Fishing
• Angling
• Big-game fishing
• Casting
• Noodling
• Spearfishing
• Sport fishing
• Surf fishing
• Rock fishing
• Fly fishing
• Ice fishing

Flying disc sports

• Beach ultimate
• Disc dog
• Disc golf
• Disc golf (urban)
• Dodge disc
• Double disc court
• Flutterguts
• Freestyle
• Freestyle competition
• Goaltimate
• Guts
• Hot box
• Ultimate

Football

• Ancient games
• Chinlone
• Cuju
• Episkyros
• Harpastum
• Kemari
• Ki-o-rahi
• Marn Grook
• Woggabaliri
• Yubi lakpi
• Medieval football
• Ba game
• Caid
• Calcio Fiorentino
• Camping (game)
• Chester-le-Street
• Cnapan
• Cornish hurling
• Haxey Hood
• Knattleikr
• La soule
• Lelo burti
• Mob football
• Royal Shrovetide Football
• Uppies and Downies
• Association football
• Jorkyball
• Paralympic football
• Powerchair Football
• Reduced variants
• Five-a-side football
• Beach soccer
• Futebol de Salão
• Futsal
• Papi fut
• Indoor soccer
• Masters Football
• Street football
• Freestyle football
• Keepie uppie
• Swamp football
• Three sided football
• Australian football
• Nine-a-side footy
• Rec footy
• Metro footy
• English school games
• Eton College
• Field game
• Wall game
• Harrow football
• Gaelic football
• Ladies' Gaelic football
• Gridiron football
• American football
• Eight-man football
• Flag football
• Indoor football
• Arena football
• Nine-man football
• Six-man football
• Sprint football
• Touch football
• Canadian football
• Street football (American)
• Rugby football
• Beach rugby
• Rugby league
• Masters Rugby League
• Mod league
• Rugby league nines
• Rugby league sevens
• Tag rugby
• Touch football
• Wheelchair rugby league
• Rugby union
• American flag rugby
• Mini rugby
• Rugby sevens
• Tag rugby
• Touch rugby
• Rugby tens
• Snow rugby
• Hybrid codes
• Austus
• Eton wall game
• International rules football
• Samoa rules
• Speedball
• Universal football
• Volata


Golf

• Miniature golf
• Match play
• Skins game
• Speed golf
• Stroke play
• Team play
• Shotgun start

Gymnastics

• Acrobatic gymnastics
• Aerobic gymnastics
• Artistic gymnastics
• Balance beam
• Floor
• High bar
• Parallel bars
• Pommel horse
• Still rings
• Uneven bars
• Vault
• Juggling
• Rhythmic gymnastics
• Ball
• Club
• Hoop
• Ribbon
• Rope
• Rope jumping
• Slacklining
• Trampolining
• Trapeze
• Flying trapeze
• Static trapeze
• Tumbling

Handball family
• Goalball
• Hitbal
• Tchoukball
• Team handball
• Beach handball
• Czech handball
• Field handball
• Torball
• Water polo

Hunting

• Beagling
• Big game hunting
• Deer hunting
• Fox hunting
• Hare coursing
• Wolf hunting

Ice sports
• Bandy
• Rink bandy
• Broomball
• Curling
• Ice hockey
• Ringette
• Ice yachting
• Figure skating


Kite sports
• Kite buggy
• Kite fighting
• Kite landboarding
• Kitesurfing
• Parasailing
• Snow kiting
• Sport kite (Stunt kite)

Mixed discipline
• Adventure racing
• Biathlon
• Duathlon
• Decathlon
• Heptathlon
• Icosathlon
• Modern pentathlon
• Pentathlon
• Tetrathlon
• Triathlon

Orienteering family
• Geocaching
• Orienteering
• Rogaining
• Letterboxing
• Waymarking

Pilota family
• American handball
• Australian handball
• Basque pelota
• Jai alai
• Fives
• Eton Fives
• Rugby Fives
• Frisian handball
• Four square
• Gaelic handball
• Jeu de paume
• Palla
• Patball
• Valencian pilota

Racquet (or racket) sports
• Badminton
• Ball badminton
• Basque pelota
• Frontenis
• Xare
• Beach tennis
• Fives
• Matkot
• Padel
• Paleta Frontón
• Pelota mixteca
• Pickleball
• Platform tennis
• Qianball
• Racketlon
• Racquetball
• Racquets
• Real tennis
• Soft tennis
• Speed-ball
• Speedminton
• Squash
• Hardball squash
• Squash tennis
• Stické
• Table tennis
• Tennis
Remote control
• Model aerobatics
• RC racing
• Robot combat
• Slot car racing

Rodeo-originated
• Bullriding
• Barrel Racing
• Bronc Riding
• Saddle Bronc Riding
• Roping
• Calf Roping
• Team Roping
• Steer Wrestling
• Goat Tying

Running
• Endurance
• 5K run
• 10K run
• Cross-country running
• Half marathon
• Marathon
• Road running
• Tower running
• Ultramarathon
• Sprint
• Hurdles

Sailing / Windsurfing
• Ice yachting
• Land sailing
• Land windsurfing
• Sailing
• Windsurfing
• Kiteboarding
• Dinghy sailing

Snow sports
• Alpine skiing
• Freestyle skiing
• Nordic combined
• Nordic skiing
• Cross-country skiing
• Telemark skiing
• Ski jumping
• Ski touring
• Skijoring
• Speed skiing

Sled sports

• Bobsleigh
• Luge
• Skibobbing
• Skeleton
• Toboggan

Shooting sports
• Clay pigeon shooting
• Skeet shooting
• Trap shooting
• Sporting clays
• Target shooting
• Field target
• Fullbore target rifle
• High power rifle
• Benchrest shooting
• Metallic silhouette
• Practical shooting
• Cowboy action shooting
• Metallic silhouette shooting
Stacking
• Card stacking
• Dice stacking
• Sport stacking

Stick and ball games
• Hornussen

Hockey
• Hockey
• Ball hockey
• Bando
• Bandy
• Rink bandy
• Broomball
• Moscow broomball
• Field hockey
• Indoor field hockey
• Floorball
• Ice hockey

Ice hockey 
 • Pond hockey
• Power hockey
• Ringette
• Sledge hockey
• Underwater ice hockey
• Roller hockey
• Inline hockey
• Roller hockey (Quad)
• Skater hockey
• Rossall Hockey
• Spongee
• Street hockey
• Underwater hockey
• Unicycle hockey

Hurling and shinty
• Cammag
• Hurling
• Camogie
• Shinty
• Composite rules shinty-hurling

Lacrosse
• Lacrosse
• Box lacrosse
• Field lacrosse
• Women's lacrosse
• Intercrosse


Polo
• Polo
 • Bicycle polo
• Canoe polo
• Cowboy polo
• Elephant polo
• Horse polo
• Segway polo
• Yak polo

Street sports
• Free running
• Freestyle footbag
• Freestyle football
• Powerbocking
• Parkour
• Scootering
• Street workout

Tag games

• British bulldogs (American Eagle)
• Capture the flag
• Hana Ichi Monme
• Hide and seek
• Jugger
• Kabaddi
• Kho kho
• Kick the can
• Oztag
• Red rover
• Tag

Walking
• Hiking
• Backpacking (wilderness)
• Racewalking
• Bushwhacking
• Walking

Wall-and-ball
• American handball
• Australian handball
• Basque pelota
• Butts Up
• Chinese handball
• Fives
• Gaelic handball
• International fronton
• Jorkyball
• Racquetball
• Squash
• Squash tennis
• Suicide (game)
• Valencian frontó
• Wallball
• Wallyball

Aquatic & paddle sports
• Creeking
• Flyak
• Freeboating
• Sea kayaking
• Squirt boating
• Surf kayaking
• Whitewater kayaking

Rafting
• Rafting
• White water rafting

Rowing
• Rowing (sport)
• Gig racing
• Coastal and ocean rowing
• Surfboat
• Single scull
Other paddling sports
• Dragon boat racing
• Stand up paddle boarding
• Water polo
• Canoe polo
• Waboba

Underwater
• Underwater football
• Underwater rugby
• Underwater hockey

Competitive swimming
• Backstroke
• Breaststroke
• Butterfly stroke
• Freestyle swimming
• Individual medley
• Synchronized swimming
• Medley relay

Kindred activities
• Bifins (finswimming)
• Surface finswimming

Subsurface and recreational
• Apnoea finswimming
• Aquathlon (underwater wrestling)
• Freediving
• Immersion finswimming
• Scuba diving
• Spearfishing
• Snorkelling
• Sport diving (sport)
• Underwater hockey
• Underwater orienteering
• Underwater photography (sport)
• Underwater target shooting
Diving
• Cliff diving
• Diving

Weightlifting
• Basque traditional weightlifting
• Bodybuilding
• Highland games
• Olympic weightlifting
• Powerlifting
• Strength athletics (strongman)
• Steinstossen

Motorized sports
• Autocross (a.k.a. Slalom)
• Autograss
• Banger racing
• Board track racing
• Demolition derby
• Desert racing
• Dirt track racing
• Drag racing
• Drifting
• Folkrace
• Formula racing
• Formula Libre
• Formula Student
• Hillclimbing
• Ice racing
• Kart racing
• Land speed records
• Legends car racing
• Midget car racing
• Monster truck
• Mud bogging
• Off-road racing
• Pickup truck racing
• Production car racing
• Race of Champions
• Rally raid
• Rallycross
• Rallying
• Regularity rally
• Road racing
• Short track motor racing
• Snowmobile racing
• Sports car racing
• Sprint car racing
• Street racing
• Stock car racing
• Time attack
• Tractor pulling
• Touring car racing
• Truck racing
• Vintage racing
• Wheelstand competition

Motorboat racing
• Drag boat racing
• F1 powerboat racing
• Hydroplane racing
• Jet sprint boat racing
• Offshore powerboat racing
• Personal water craft

Motorcycle racing
• Auto Race
• Board track racing
• Cross-country rally
• Endurance racing
• Enduro
• Freestyle motocross
• Grand Prix motorcycle racing
• Grasstrack
• Hillclimbing
• Ice racing
• Ice speedway
• Indoor enduro
• Motocross
• Motorcycle drag racing
• Motorcycle speedway
• Off-roading
• Rally raid
• Road racing
• Superbike racing
• Supercross
• Supermoto
• Supersport racing
• Superside
• Track racing
• Trial
• TT racing
• Free-style moto

Marker sports
• Airsoft
• Archery
• Paintball
• Darts

Musical sports
• Color guard
• Drum corps
• Indoor percussion
• Marching band

Fantasy sports
• Quidditch
• Hunger Games(Gladiating)
• Pod Racing
• Mortal Kombat(MMA)

Other
• Stihl Timbersports Series
• Woodsman

Overlapping sports
• Tennis
• Polocrosse
• Badminton
• Polo

Skating sports
• Aggressive inline skating
• Artistic roller skating
• Figure skating
• Freestyle slalom skating
• Ice dancing
• Ice skating
• Inline speed skating
• Rinkball
• Rink hockey
• Roller derby
• Roller skating
• Short track speed skating
• Skater hockey
• Speed skating
• Synchronized skating

Freestyle skiing
• Snowboarding
• Ski flying
• Skibob
• Snowshoeing
• Skiboarding