powered by CADENAS

Social Share

Torque motor (2036 views - Transportation - Air Water Earth)

A torque motor is a specialized form of electric motor which can operate indefinitely while stalled, that is, with the rotor blocked from turning, without incurring damage. In this mode of operation, the motor will apply a steady torque to the load (hence the name). A torque motor that cannot perform a complete rotation is known as a limited angle torque motor.
Go to Article

Torque motor

Torque motor

A torque motor is a specialized form of electric motor which can operate indefinitely while stalled, that is, with the rotor blocked from turning, without incurring damage. In this mode of operation, the motor will apply a steady torque to the load (hence the name). A torque motor that cannot perform a complete rotation is known as a limited angle torque motor.

Construction

Torque motors are normally induction motors of toroidal construction. Their main differences from other similar motors are their wide diameters, to allow for high levels of torque, and their thermal performance, to allow their continuous operation while drawing high current in a stalled state.

Linear versions

An analogous device, working linearly rather than by rotation, is described as a 'force motor'. These are widely used for refrigeration compressors and ultra-quiet air compressors, where the force motor produces simple harmonic motion in conjunction with a restoring spring.[1][2]

Applications

Tape recorders

A common application of a torque motor would be the supply- and take-up reel motors in a tape drive. In this application, driven from a low voltage, the characteristics of these motors allow a relatively constant light tension to be applied to the tape whether or not the capstan is feeding tape past the tape heads. Driven from a higher voltage, (and so delivering a higher torque), the torque motors can also achieve fast-forward and rewind operation without requiring any additional mechanics such as gears or clutches.

Computer games

In the computer gaming world, torque motors are used in force feedback steering wheels.

Throttle control

Another common application is the control of the throttle of an internal combustion engine in conjunction with an electronic governor. In this usage, the motor works against a return spring to move the throttle in accordance with the output of the governor. The latter monitors engine speed by counting electrical pulses from the ignition system or from a magnetic pickup and, depending on the speed, makes small adjustments to the amount of current applied to the motor. If the engine starts to slow down relative to the desired speed, the current will be increased, the motor will develop more torque, pulling against the return spring and opening the throttle. Should the engine run too fast, the governor will reduce the current being applied to the motor, causing the return spring to pull back and close the throttle.

Actuators

Torque motors can be used as actuators for direct drive mechanisms in some situations where otherwise geared electric motors would be used: for example, in motion control systems or servomechanisms.



This article uses material from the Wikipedia article "Torque motor", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Example Part

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht