powered by CADENAS

Social Share

Dieselpunk (951 views - Art Styles - Art Movements)

Dieselpunk is a genre similar to that of its more well-known cousin "steampunk" that combines the aesthetics of the diesel-based technology of the interwar period through to the 1950s with retro-futuristic technology and postmodern sensibilities. Coined in 2001 by game designer Lewis Pollak to describe his role-playing game Children of the Sun, the term has since been applied to a variety of visual art, music, motion pictures, fiction, and engineering.
Go to Article




Licensed under Creative Commons Attribution-Share Alike 3.0 (Stefan Prohaczka).

Dieselpunk is a genre similar to that of its more well-known cousin "steampunk" that combines the aesthetics of the diesel-based technology of the interwar period through to the 1950s with retro-futuristic technology[2][3] and postmodern sensibilities.[4] Coined in 2001 by game designer Lewis Pollak to describe his role-playing game Children of the Sun,[3] the term has since been applied to a variety of visual art, music, motion pictures, fiction, and engineering.[5]


The name "dieselpunk" is a derivative of the 1980s science fiction genre cyberpunk,[6] and is used to represent the time period – or "era" – from the interwar period until the 1950s, when diesel-based locomotion was the main technological focus of Western culture.[7] The "-punk" suffix attached to the name is representative of the counterculture nature of the genre with regards to its opposition to contemporary aesthetics.[4] The term also refers to the tongue-in-cheek[8] name given to a similar cyberpunk derivative, "steampunk," which focuses on science fiction based on industrial steam power and which is often set within the Victorian era.[9]

Differences from steampunk

In an interview, author Scott Westerfeld addressed the subject of where to draw the line between steampunk and dieselpunk, arguing that his own work Leviathan (2009) still qualifies as steampunk despite the technology in it including diesel engines.
I like the word dieselpunk if you are doing something like 'Weird World War II'. I think that makes perfect sense. But to me, World War I is the dividing point where modernity goes from being optimistic to being pessimistic. Because when you put the words machine and gun together, they both change. At that point, war is no longer about a sense of adventure and chivalry and a way of testing your nation's level of manhood; it's become industrial, and horrible. So playing around with that border between optimistic steampunk and a much more pessimistic dieselpunk, which is more about Nazis, was kind of interesting to me because early in the war we were definitely kind of on the steampunk side of that.[10]

Jennifer McStotts, another author, considers the two genres to be close cousins. She defines steampunk as concerned with the Victorian era, and the shift in technology and energy generation that came with industrialisation. The genre is primarily concerned with steam power, Tesla, and sustainable energy, while she defines dieselpunk as the genre combining the aesthetic and genre influences of the period of both world wars.[11]

Academic Gary K. Wolfe defines the genres by their era of setting. He defines steampunk as the genre primarily set in the Victorian era and dieselpunk as the genre primarily set in the interwar period.[12]

Dieselpunk inspiration

Dieselpunk draws its inspiration from two related sources: the diesel era and a characteristic referred to by dieselpunks as "decodence."[2] According to the web site The Gatehouse, decodence (a portmanteau of "deco" and "decadence"), "embraces the styles and technologies of the era; it rejoices in a prolonged Jazz Age ambience characterized by great enthusiasm and hopes about the future."[13]

The term "diesel era" is a period of time that begins with the start of the interbellum era, which covers the time between the end of World War I and the start of World War II. The interbellum era is central to one school of dieselpunk often labeled "Ottensian." In addition to the interbellum period, World War II also plays a major role in dieselpunk, especially in the school of the genre referred to as "Piecraftian." (See "Common themes found in dieselpunk fiction", below.) The exact ending of the diesel era is in some dispute in the dieselpunk community. Depending on the source it ends either at the conclusion of World War II or continues until the early part of the 1950s with the advent of such cultural icons as the Golden Age of Television and the replacement of Big Band and Swing music with Rock and Roll in popularity.[citation needed]

As an art movement

Although the term “dieselpunk” was not coined until 2001, a large body of art significant to the development of the genre was produced before that. Artwork (including visual arts, music, literature, and architecture) created in the dieselpunk style are heavily influenced by elements of the art movements most prevalent in Western culture during the diesel era such as:

According to Tome Wilson, owner of Dieselpunks website (www. dieselpunks.org), the term was retroactively applied to an already existing trend in literature. An alternative term was "low-brow pop surrealism". Writers of this trend blended traditional tropes and genres, such as Pulp Adventure, Film noir, and Weird Horror, with a contemporary aesthetic.[14] In his words: "They were creating a future fueled by the spirit of the Jazz Age." In their works, the reader could see Sam Spade in the era of smartphones and John Dillinger use a hovercar as his getaway vehicle. They were writing cyberpunk stories about the era of The Great Gatsby (1925).[14]

In discussing punk genres, Ted Stoltz defines dieselpunk as the quasifuture from the Art Deco era. He argues that cyberpunk, steampunk, clockpunk, atompunk, and ribopunk are all defined by their connection to their respective technological element. He found this does not apply to other related genres such as elfpunk, mythpunk, and splatterpunk where technology plays a minor role.[15]

Fiction and literature

Alternative history and World War II feature prominently in dieselpunk literature. Examples of other dieselpunk novels are Tales of the First Occult War by Kevin Cooney, Fiends of the Eastern Front by David Bishop, and Hard Magic: Book 1 of the Grimnoir Chronicles by New York Times bestselling novelist Larry Correia.

Common themes

A feature that was first identified by the online magazine The Flying Fortress is that dieselpunk can be divided into two primary themes or styles: Ottensian and Piecraftian.[16] The dividing line between the two themes is commonly acknowledged as the start of World War II.[17]

One theme, named "Piecraftian" after its proponent author "Piecraft", focuses on the aesthetics of the world wars and speculates on how human culture could theoretically cease to evolve due to constant, widespread warfare.[3][16] According to Ottens and Piecraft this theme continues the aesthetics of the diesel era into later periods of history by describing a world where survival (largely based on a reliance on diesel power) is placed above aesthetical evolution (as seen in such dystopian movies as Mad Max[18]).

A second theme, named "Ottensian" after its proponent author Nick Ottens,[13] focuses on a setting where the decadent aesthetics and utopian philosophies of the American "Roaring Twenties" continued to evolve unhindered by war or economic collapse. Ottensian dieselpunk fiction is primarily concerned with a positive vision of technology, where the utopian ideals predicted by the World’s Fairs of the times came to light.[19] As a result Ottensian dieselpunk incorporates "an enthusiasm for the predictions about the future,"[20] and often shares elements with retro-futurism.[21]


Dieselpunk features prominently in the gaming industry, in both tabletop role-playing games and computer and console video games. Dieselpunk video game titles have been extremely prominent in recent years, with the success of the popular Fallout (1997), and BioShock (2007) series of games.[22] Sven Schmalfuss feels that BioShock can be defined as both retro-futuristic biopunk and dieselpunk.[23]

World War II is also a popular theme in dieselpunk games. One of the more prominent of these was Activision's Return to Castle Wolfenstein,[22] as well as the sequel game to the 2009 game Wolfenstein, Wolfenstein: The New Order, which takes place in an alternate 1960s Europe where the Nazis had won World War II. The game features many dieselpunk style weapons and robots, as the Nazis had focussed more on scientific and military development than social development. Other games set in dieselpunk versions of the World War II era include Crimson Skies (1998 board game, 2000 videogame), Command & Conquer: Red Alert (1996),[22] and Sine Mora (2012).[24]

Cinema and television

With regard to moving pictures, dieselpunk combines the tropes, character archetypes, and settings of diesel era fiction genres such as Serial Adventure, Noir,[25] Pulp, and War with postmodern storytelling techniques and cinematography. Famous inspirations for dieselpunk cinema include Metropolis (1927) and Things To Come (1936), thanks to their period visions of utopian culture and technology.[2] Even the popular film Star Wars (1977) has been noted as having strong dieselpunk influences, as it drew heavily on pulp and World War II iconography but mixed them with futuristic settings.[26]

Some commonly referenced examples of dieselpunk cinema include:

Visual art

According to an article titled "Dieselpunk: Love Affair with a Machine", published in the online magazine Dark Roasted Blend, in dieselpunk art "takes an interest in various bizarre machines, full of esoteric levers, cracked-glass meters – all visually intense and pretty sinister-looking, when photographed."[35] The article references Japanese artist Shunya Yamashita's having created one of the definitive examples of dieselpunk art with his work I Can't Explain.[36] The article also references Kow Yokoyama as a dieselpunk artist with his figurine series titled Maschinen Krieger.[37]

Other prominent artists in the dieselpunk movement include: Alexey Lipatov,[38] Stefan Prohaczka,[1] ixlrlxi,[39][40] Keith Thompson,[41] Rob Schwager,[42] and Sam Van Olffen.[43][44][45]

As a subculture

A person defined as a dieselpunk draws inspiration and entertainment from the aesthetics of the diesel era to achieve independence from contemporary aesthetics by blending the literature, artwork, fashion, grooming styles, modes of personal transportation, music, and technology of the diesel era with contemporary sensibilities.

Part of dieselpunk's postmodern nature can be seen in the important role that the internet as a tool of international communication plays in its development. In addition to two prominent dieselpunk online communities, Dieselpunks[46] and The Gatehouse's "Smoking Lounge",[47] there are a growing number of online magazines dedicated to the genre including The Flying Fortress,[48] Dizelpanki[49] and several blogs which are simply titled "Dieselpunk".[50][51] Another active online magazine covering the dieselpunk movement is Vintage Future: Dieselpunk,[52] which describes itself as "Retro-futuristic resources from the golden era."

While there are many websites dedicated to the history of the diesel era, a growing number of sites are dedicated to topics that tie directly into dieselpunk. One such website of note is RetroTimes Production,[53] which is an independent film production company dedicated to creating documentaries about "retro living, retro design, and retro style." A few sites are springing up that have a retro pulp feel as well, including Captain Spectre and The Lightning Legion,[54] which is an online comic written and drawn in the classic serial pulp fiction style of the diesel era, and Thrilling Tales of the Downright Unusual,[55] an interactive Choose Your Own Adventure-style pulp serial.

In 2012, World Brews, a craft beer manufacturer in Novato, CA, began producing "Dieselpunk Brew", a beer line (IPA, Porter and Stout) inspired and influenced by the subculture of dieselpunk, and displaying art deco-inspired dieselpunk designs on the labels.[56]


Dieselpunk fashion blends the styles commonly found during the diesel era with contemporary styles to create a fusion of both. The "punk" nature of the subculture comes from expressing a more complete presence in public akin to the fashion styles popular during the diesel era such as waistcoats, covered arms, hosiery, styles of shoes, and head wear. Dieselpunk emphasizes the inclusion of such accoutrements to render one's look "complete," in defiance of modern custom.


Dieselpunk music,[2] which has roots in the neo-swing revival,[57] combines elements of blues, jazz, ragtime, cabaret, swing, and bluegrass commonly found during the diesel era with contemporary instrumentation, production, and composition.[58] Some commonly referenced examples of dieselpunk bands are: Big Bad Voodoo Daddy,[59] Royal Crown Revue,[60][61] Squirrel Nut Zippers,[62] The Brian Setzer Orchestra, Indigo Swing, Wolfgang Parker,[57] The End Times Spasm Band, RPM Orchestra, Big Rude Jake, and Lee Press-on and the Nails.[63]

There has been growth of a Dieselpunk music referred to as electro swing, which combines the styles of Swing music with Electronica. Prominent bands within the Electro-Swing include Caravan Palace, Good Co, and Tape Five.



Decopunk is a recent subset of Dieselpunk, inspired by the Art Deco and Streamline Moderne art styles of the period between the 1920s and 1950s. In an interview[64] at CoyoteCon, steampunk author Sara M. Harvey made the distinctions "...shinier than DieselPunk, more like DecoPunk", and "DieselPunk is a gritty version of Steampunk set in the 1920s–1950s. The big war eras, specifically. DecoPunk is the sleek, shiny very Art Deco version; same time period, but everything is chrome!"


A similar, related pop surrealist art movement, which overlaps with dieselpunk somewhat, is atompunk (sometimes called atomicpunk). Atompunk art relates to the pre-digital period of 1945–1965, including mid-century Modernism, the Atomic Age, Jet Age and Space Age, Communism and paranoia in the USA along with Soviet styling, underground cinema, Googie architecture, the Sputnik, Mercury and other early space programs, superhero fiction, the rise of the US military/industrial powers and the fall-out of Chernobyl.[65][66]

See also

This article uses material from the Wikipedia article "Dieselpunk", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Art Styles - Art Movements

3D - 3D Model - 3D CAD - 3D Library - Steampunk Bauhaus Jugendstil Klassizismus Art Nouveau Modern Art AvantGarde Cubism Kubismus