powered by CADENAS

Social Share

Inconel (6965 views - Material Database)

Inconel is a family of austenitic nickel-chromium-based superalloys. Inconel alloys are oxidation-corrosion-resistant materials well suited for service in extreme environments subjected to pressure and heat. When heated, Inconel forms a thick, stable, passivating oxide layer protecting the surface from further attack. Inconel retains strength over a wide temperature range, attractive for high temperature applications where aluminum and steel would succumb to creep as a result of thermally induced crystal vacancies. Inconel’s high temperature strength is developed by solid solution strengthening or precipitation hardening, depending on the alloy. Inconel alloys are typically used in high temperature applications. Common trade names for Inconel Alloy 625 include: Inconel 625, Chronin 625, Altemp 625, Haynes 625, Nickelvac 625 and Nicrofer 6020.
Go to Article

Inconel

Inconel

Inconel is a family of austenitic nickel-chromium-based superalloys.[1]

Inconel alloys are oxidation-corrosion-resistant materials well suited for service in extreme environments subjected to pressure and heat. When heated, Inconel forms a thick, stable, passivating oxide layer protecting the surface from further attack. Inconel retains strength over a wide temperature range, attractive for high temperature applications where aluminum and steel would succumb to creep as a result of thermally induced crystal vacancies. Inconel’s high temperature strength is developed by solid solution strengthening or precipitation hardening, depending on the alloy.[2][3]

Inconel alloys are typically used in high temperature applications. Common trade names for Inconel Alloy 625 include: Inconel 625, Chronin 625, Altemp 625, Haynes 625, Nickelvac 625 and Nicrofer 6020.[4]

History

The Inconel family of alloys was first developed in the 1940s by research teams at Wiggin Alloys (Hereford, England), which has since been acquired by SMC,[5] in support of the development of the Whittle jet engine.[6]

Composition

Different Inconels have widely varying compositions, but all are predominantly nickel, with chromium as the second element.

Inconel Element (% by mass)
Ni Cr Fe Mo Nb Co Mn Cu Al Ti Si C S P B
600[7] 72.0 14.0–17.0 6.0–10.0 1.0 0.5 0.5 0.15 0.015
617[8] 44.2–56.0 20.0–24.0 3.0 8.0–10.0 10.0–15.0 0.5 0.5 0.8–1.5 0.6 0.5 0.15 0.015 0.015 0.006
625[9] 58.0 20.0–23.0 5.0 8.0–10.0 3.15–4.15 1.0 0.5 0.4 0.4 0.5 0.1 0.015 0.015
690[10] 59.5 30 9.2 0.35 0.01 0.02 0.35 0.019 0.003
718[2] 50.0–55.0 17.0–21.0 balance 2.8–3.3 4.75–5.5 1.0 0.35 0.2–0.8 0.65–1.15 0.3 0.35 0.08 0.015 0.015 0.006
X-750[11] 70.0 14.0–17.0 5.0–9.0 0.7–1.2 1.0 1.0 0.5 0.4–1.0 2.25–2.75 0.5 0.08 0.01

Properties

Inconel alloys are oxidation- and corrosion-resistant materials well suited for service in extreme environments subjected to high pressure and kinetic energy. When heated, Inconel forms a thick and stable passivating oxide layer protecting the surface from further attack. Inconel retains strength over a wide temperature range, attractive for high-temperature applications where aluminium and steel would succumb to creep as a result of thermally induced crystal vacancies (see Arrhenius equation). Inconel's high temperature strength is developed by solid solution strengthening or precipitation strengthening, depending on the alloy. In age-hardening or precipitation-strengthening varieties, small amounts of niobium combine with nickel to form the intermetallic compound Ni3Nb or gamma prime (γ'). Gamma prime forms small cubic crystals that inhibit slip and creep effectively at elevated temperatures.[12] The formation of gamma-prime crystals increases over time, especially after three hours of a heat exposure of 850 °C, and continues to grow after 72 hours of exposure.[13]

Machining

Inconel is a difficult metal to shape and machine using traditional techniques due to rapid work hardening. After the first machining pass, work hardening tends to plastically deform either the workpiece or the tool on subsequent passes. For this reason, age-hardened Inconels such as 718 are machined using an aggressive but slow cut with a hard tool, minimizing the number of passes required. Alternatively, the majority of the machining can be performed with the workpiece in a solutionized form, with only the final steps being performed after age hardening.

External threads are machined using a lathe to "single-point" the threads or by rolling the threads in the solution treated condition (for hardenable alloys) using a screw machine. Inconel 718 can also be roll-threaded after full aging by using induction heat to 1,300 °F (704 °C) without increasing the grain size.[citation needed] Holes with internal threads are made by threadmilling. Internal threads can also be formed using a sinker EDM (electrical discharge machining).[citation needed]

Cutting of a plate is often done with a waterjet cutter. New whisker-reinforced ceramic cutters are also used to machine nickel alloys. They remove material at a rate typically eight times faster than carbide cutters. Apart from these methods, Inconel parts can also be manufactured by selective laser melting.

More often than machining, water-jet or laser, grinding is a preferred and economical method for forming Nickel alloy components to shape and finish. Due to the hardness of the abrasives used, the grinding wheels are not as affected by the material work hardening and remain sharp and durable.

Joining

Welding of some Inconel alloys (especially the gamma prime precipitation hardened family, e.g. Waspalloy and X-750) can be difficult due to cracking and microstructural segregation of alloying elements in the heat-affected zone. However, several alloys such as 625 and 718 have been designed to overcome these problems. The most common welding methods are gas tungsten arc welding and electron beam welding.[14]

Innovations in pulsed micro laser welding have also become more popular in recent years for specific applications.[citation needed]

Uses

Inconel is often encountered in extreme environments. It is common in gas turbine blades, seals, and combustors, as well as turbocharger rotors and seals, electric submersible well pump motor shafts, high temperature fasteners, chemical processing and pressure vessels, heat exchanger tubing, steam generators and core components in nuclear pressurized water reactors,[15] natural gas processing with contaminants such as H2S and CO2, firearm sound suppressor blast baffles, and Formula One, NASCAR, NHRA, and APR, LLC exhaust systems.[16][17] It is also used in the turbo system of the 3rd generation Mazda RX7, and the exhaust systems of high powered rotary engined Norton motorcycles where exhaust temperatures reach more than 1,000 degrees C.[18] Inconel is increasingly used in the boilers of waste incinerators.[19] The Joint European Torus and DIII-D (fusion reactor) tokamaks vacuum vessels are made in Inconel.[20] Inconel 718 is commonly used for cryogenic storage tanks, downhole shafts and wellhead parts.[21]

Several applications of inconel in aerospace include:

Inconel is also used in the automotive industry:

  • Tesla Motors is now using Inconel, in place of steel, to upgrade the main battery pack contactor in its Model S so that it remains springy under the heat of heavy current. Tesla claims that this allows upgraded vehicles to safely increase the maximum pack output from 1300 to 1500 amps, allowing for an increase in power output (acceleration) Tesla refers to as "Ludicrous Mode".[25][31]
  • Ford Motor Company is using Inconel to make the turbine wheel in the turbocharger of its EcoBlue diesel engines introduced in 2016.[32]
  • The exhaust valves on NHRA Top Fuel and Funny Car drag racing engines are made of Inconel.[citation needed] Inconel is also used in the manufacture of exhaust valves in high performance aftermarket turbo and Supercharged Mazda Miata engine builds (see Flying Miata INC).
  • BMW has since used Inconel in the exhaust manifold of its high performance luxury car, the BMW M5 E34 with the iconic S38 engine, withstanding higher temperatures and reducing backpressure.
  • Jaguar Cars has fit, in their Jaguar F-Type SVR high performance sports car, a new lightweight Inconel titanium exhaust system as standard which withstands higher peak temperatures, reduces backpressure and eliminates 35 lbs (16kg) of mass from the vehicle.[33]

Rolled Inconel was frequently used as the recording medium by engraving in black box recorders on aircraft.[34]

Alternatives to the use of Inconel in chemical applications such as scrubbers, columns, reactors, and pipes are Hastelloy, perfluoroalkoxy (PFA) lined carbon steel or fiber reinforced plastic.

Inconel alloys

Alloys of inconel include:

  • Inconel 600: Solid solution strengthened
  • Inconel 625: Acid resistant, good weldability. The LCF version is typically used in bellows.
  • Inconel 690: Low cobalt content for nuclear applications, and low resistivity[35]
  • Inconel 713C: Precipitation hardenable nickel-chromium base cast alloy[3]
  • Inconel 718: Gamma double prime strengthened with good weldability[36]
  • Inconel 751: Increased aluminium content for improved rupture strength in the 1600 °F range[37]
  • Inconel 792: Increased aluminium content for improved high temperature corrosion properties, used especially in gas turbines
  • Inconel 939: Gamma prime strengthened to increase weldability

In age hardening or precipitation strengthening varieties, alloying additions of aluminum and titanium combine with nickel to form the intermetallic compound Ni3(Ti,Al) or gamma prime (γ’). Gamma prime forms small cubic crystals that inhibit slip and creep effectively at elevated temperatures.

See also


41xx steelAL-6XNAlGaAlloy 20AlnicoAlumelAluminiumAluminium alloyAluminium bronzeAluminium-lithium alloyAmalgam (chemistry)Arsenical bronzeArsenical copperBell metalBerylliumBeryllium copperBillon (alloy)BirmabrightBismanolBismuthBrassBrightrayBronzeBulat steelCalamine brassCast ironCelestriumChinese silverChromelChromiumChromium hydrideCobaltColored goldConstantanCopperCopper hydrideCopper–tungstenCorinthian bronzeCrown goldCrucible steelCunifeCupronickelCymbal alloysDamascus steelDevarda's alloyDuraluminDutch metalElectrical steelElectrumElektron (alloy)ElinvarFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolGalinstanGalliumGilding metalGlassGlucydurGoldGuanín (bronze)GunmetalHaynes InternationalHepatizonHiduminiumHigh-speed steelHigh-strength low-alloy steelHydronaliumIndiumInvarIronIron–hydrogen alloyItalmaKanthal (alloy)KovarLeadMagnaliumMagnesiumMagnox (alloy)MangalloyManganinMaraging steelMarine grade stainlessMartensitic stainless steelMegalliumMelchior (alloy)MercuryMolybdochalkosMuntz metalMushet steelNichromeNickelNickel silverNordic GoldOrmoluPhosphor bronzePig ironPinchbeck (alloy)PlasticPlexiglasPlutoniumPotassiumReynolds 531RhoditeRhodiumRose's metalSamariumSanicro 28ScandiumShakudōSilverSilver steelSodiumSolderSpeculum metalSpiegeleisenSpring steelStaballoyStainless steelSteelStelliteStructural steelSurgical stainless steelTerneTinTitaniumTombacTool steelTumbagaType metalUraniumVitalliumWeathering steelWood's metalWootz steelY alloyZeron 100ZincZirconiumMonelNicrosilNisilNickel titaniumMu-metalPermalloySupermalloyNickel hydridePlutonium–gallium alloySodium-potassium alloyMischmetalLithiumTerfenol-DPseudo palladiumScandium hydrideSamarium–cobalt magnetArgentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTitanium Beta CTitanium alloyTitanium hydrideGum metalTitanium goldTitanium nitrideBabbitt (alloy)Britannia metalPewterQueen's metalWhite metalUranium hydrideZamakZirconium hydrideHydrogenHeliumBoronNitrogenOxygenFluorineMethaneMezzanineAtom

This article uses material from the Wikipedia article "Inconel", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material